Zigbee Realistic Use Case Window Covering

Revision as of 09:51, 11 December 2023 by Registered User (→‎Server side)

1. Introduction

This implementation can be seen as a simple extension of the RUC Lighting, adding another Zigbee cluster in the Home automation aspect.
Test and verify various functionality and ensure proper functioning.

2. Cluster implementation

2.1. Server side

The server is based on a STM32WB5MM-DK [1], which has a slot to put an Arduino board to expand its functionality.
It uses an Arduino Motor Shield Control (AMS) [2] based on the ST dual full-bridge driver L298P [3] to drive a DC motor, enabling the real opening and closing on a window covering.
One driver was created to enable the following functionalities:

  • Adjust the motor’s speed by modifying the duty cycle of a PWM (driven by a GPIO connected to a timer).
  • Change the rotation direction (driven by a GPIO).
  • Set a break (also driven by a GPIO)
  • Current sensing, with that possibility, this feature detects when the window covering is stuck and stops the motor.

2.2. Client side

Only three commnands are used

3. References