Product state for STM32H5

Revision as of 11:55, 4 December 2023 by Registered User (→‎Product state : Open)

1. Introduction

It is advised to start by reading the New product state article.
From the development phase until the maintenance phase a product can be configured under many product states ( also called lifecycle states).
The lifecycle controls the access to code and data.


This article lists in which product states a STM32H5 can be configured.

2. Product states

2.1. Product state : Open

STM32H573 picto.png STM32H563 picto.png

Usage

  • User develops his application in this product state.

Boot

  • According to UBE Option byte and boot pin, STM32 boots on user Flash or system Flash (Bootloader or System Flash).

STM32 resources access overview

  • User Flash: full access.
  • Option Bytes: full access.
  • OBKeys:
  • full access.
  • RSSLIB_DataProvisioning via debug port or BL: available.

STM32H5 interfaces

  • Debug port fully open.
  • Bootloader:
  • Available via bootpin set to Vdd. Cf AN2606.

Debug Authentication

  • Discovery: yes.
  • Debug-reopening: only after Debug Authentication provisioning.
  • Regression: only after Debug Authentication provisioning.

2.2. Product state : Provisioning

  • This state is used during the provisioning.
  • The debug is only available when executing a nonsecure user application.
  • The Trust-Zone can be disabled or enabled (not available for STM32H503 devices).
  • Bootloader is usable.
  • Secure Firmware install can be launched in this state (not anymore possible in the following states).

2.3. Product state : Provisioned

  • In this state, the OEMiRoT or STiRoT code and datas are provisioned.
  • Debug is available only when executing a nonsecure user application.
  • Debug Authentication can be launched : Debug access for secure applications can be available by launching the Debug Authentication (see Debug Authentication setting).
  • The OEMiRoT or STiRoT can launch the bootloader if the verification of the code located in the next isolation level is failing (authentication, integrity, or missing code)

2.4. Product state : TZ-Closed

  • This product state is not available for STM32H503 devices.
  • The TZ-Closed state corresponds to an intermediate state of the product. All the secure firmware is installed, the non secure application can be developed, or loaded in a second instance.
  • The [STiRoT or OEMiRoT]+ uRoT (optional) + Secure user application code and data are provisioned.
  • uRoT(optional) can launch the bootloader if the verification of the code located in the next isolation level is failing (authentication, integrity, or missing code).
  • The debug is only available when executing a nonsecure user application.
  • Debug Authentication can be launched : Debug access for secure applications can be available by launching the Debug Authentication.
  • From this state, the non secure application can be updated using the firmware update mechanism, or directly programmed through the flash loader (embedded in the IDE).

2.5. Product state : Closed

  • This state occurs with the fully provisioned product.
  • Debug Authentication is allowed : The debug is fully closed but can be opened by launching the Debug Authentication (see Debug Authentication setting).

2.6. Product state : Locked

  • This state is used with the fully provisioned product without any more changes.
  • Locked is a final unchangeable product state. No method can modify the embedded firmware and product configuration.
  • The debug is definitively closed and cannot be reopened through debug authentication.
  • No regression is possible anymore

3. Lifecycle

The figure below shows the product states of the product during along the lifecycle phases :

  • Development phase, offering full debug capabilities to the developer.
  • Provisioning phase, the main asset areas are protected (no longer accessible)
  • Final phase, the product is in the field.
  • Maintenance phase, including field return management.
SECURITY H5 Lifecycle.png

4. References

  • RM0481 STM32H5x3/562 reference manual