Revision as of 16:36, 27 November 2023 by Registered User
This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or
pending task to finish installation of
Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. STM32WB-WBA - Connection Oriented Channel
A Connection Oriented Channel - COC allows the exchange of Bluetooth® Low Energy data at L2CAP layer without GATT layer. There is no notion of client/server, only central and peripheral.
To set a COC logical link, it is necessary to establish first a Bluetooth® Low Energy link.Over this Bluetooth® Low Energy link, one or several COC can be established.
The central or the peripheral may be COC initiator.
Bluetooth® LE architecture
|
|
1.1. General L2CAP Terminology
Bluetooth® LE General L2CAP Terminology
|
Term
|
Description
|
L2CAP channel
|
The logical connection between two endpoints in peer devices, characterized by their Channel Identifiers (CIDs)
|
SDU or L2CAP SDU
|
Service Data Unit: a packet of data that L2CAP exchanges with the upper layer and transports transparently over an L2CAP channel
|
PDU or L2CAP PDU
|
Protocol Data Unit: a packet of data containing L2CAP protocol information fields, control information, and/or upper layer information data
|
Maximum Transmission Unit (MTU)
|
The maximum size of payload data, in octets, that the upper layer entity can accept (that is, the MTU corresponds to the maximum SDU size).
|
Maximum PDU Payload Size (MPS)
|
The maximum size of payload data in octets that the L2CAP layer entity can accept (that is, the MPS corresponds to the maximum PDU payload size).
|
|
2. L2CAP COC commands and events overview
2.1. L2CAP COC establishment
ACI_L2CAP_COC_CONNECT : This command sends a Credit Based Connection Request packet on the specified connection.
L2CAP COC connect command
|
Parameter
|
Description
|
Connection_Handle
|
Connection handle for which the command applies
|
SPSM
|
Simplified Protocol/Service Multiplexer
|
MTU
|
Maximum Transmission Unit
|
MPS
|
Maximum payload size (in octets)
|
Initial_Credits
|
Number of K-frames that can be received on the created channel(s) by the L2CAP layer entity sending this packet
|
Channel_Number
|
Number of channels to be created. If this parameter is set to 0, it requests the creation of one LE credit based connection-oriented channel. Otherwise, it requests the creation of one or more enhanced credit based connection-oriented channels
|
|
ACI_L2CAP_COC_CONNECT_EVENT : This event is generated when receiving a valid Credit Based Connection Request packet.
L2CAP COC connect event
|
Parameter
|
Description
|
Connection_Handle
|
Handle of the connection where this event occurred
|
SPSM
|
Simplified Protocol/Service Multiplexer
|
MTU
|
Maximum Transmission Unit
|
MPS
|
Maximum payload size (in octets)
|
Initial_Credits
|
Number of K-frames that can be received on the created channel(s) by the L2CAP layer entity sending this packet
|
Channel_Number
|
Number of channels to be created. If this parameter is set to 0, it requests the creation of one LE credit based connection-oriented channel. Otherwise, it requests the creation of one or more enhanced credit based connection-oriented channels
|
|
ACI_L2CAP_COC_CONNECT_CONFIRM : This command sends a Credit Based Connection Response packet. It must be used upon receipt of a connection request through an ACI_L2CAP_COC_CONNECT_EVENT event.
L2CAP COC connect confirm command
|
Parameter
|
Description
|
Connection_Handle
|
Connection handle for which the command applies
|
MTU
|
Maximum Transmission Unit
|
MPS
|
Maximum payload size (in octets)
|
Initial_Credits
|
Number of K-frames that can be received on the created channel(s) by the L2CAP layer entity sending this packet
|
Result
|
This parameter indicates the outcome of the request. A value of 0x0000 indicates success while a non-zero value indicates the request is refused
|
|
ACI_L2CAP_COC_CONNECT_CONFIRM_EVENT : This event is generated when receiving a valid Credit Based Connection Response packet.
L2CAP COC connect confirm event
|
Parameter
|
Description
|
Connection_Handle
|
Handle of the connection where this event occurred
|
MTU
|
Maximum Transmission Unit
|
MPS
|
Maximum payload size (in octets)
|
Initial_Credits
|
Number of K-frames that can be received on the created channel(s) by the L2CAP layer entity sending this packet
|
Result
|
This parameter indicates the outcome of the request. A value of 0x0000 indicates success while a non-zero value indicates the request is refused.
|
Channel_Number
|
Number of created channels. It is the length of Channel_Index_List
|
Channel_Index_List
|
List of channel indexes for which the primitive applies
|
|
- MTU frames are fragmented into K-frames of MPS size at application level on transmitter side.
- MTU frames are reassembled at application level on receiver side.
- Initial Credits are handled at application level once they have been exchanged through both previous commands.
2.2. L2CAP COC data exchange
ACI_L2CAP_COC_TX_DATA : This command sends a K-frame packet on the specified connection-oriented channel.
L2CAP COC Tx Data command
|
Parameter
|
Description
|
Channel_Index
|
Index of the connection-oriented channel for which the primitive applies
|
Length
|
Length of Data (in octets)
|
Data
|
Information data
|
|
- Note: for the first K-frame of the SDU, the Information data shall contain the MTU Length coded on two octets followed by the K-frame information payload. For the next K-frames of the SDU, the Information data shall only contain the K-frame information payload.
- Application must handle MTU length, fragmentation in K-frame, length of current transmitted frame and credits number.
ACI_L2CAP_COC_RX_DATA_EVENT : This event is generated when receiving a valid K-frame packet on a connection-oriented channel.
L2CAP COC Rx Data event
|
Parameter
|
Description
|
Channel_Index
|
Index of the connection-oriented channel for which the primitive applies
|
Length
|
Length of Data (in octets)
|
Data
|
Information data
|
|
- Application must handle MTU length received in first K-frame, K-frame number, length of current received frame and credits number.
2.3. L2CAP COC flow control
ACI_L2CAP_COC_FLOW_CONTROL : This command sends a Flow Control Credit signaling packet on the specified connection-oriented channel.
L2CAP COC Flow Control command
|
Parameter
|
Description
|
Channel_Index
|
Index of the connection-oriented channel for which the primitive applies
|
Credits
|
Number of credits the receiving device can increment, corresponding to the number of K-frames that can be sent to the peer device sending the Flow Control Credit packet.
|
|
ACI_L2CAP_COC_FLOW_CONTROL_EVENT : This event is generated when receiving a valid Flow Control Credit signaling packet.
L2CAP COC Flow Control command
|
Parameter
|
Description
|
Channel_Index
|
Index of the connection-oriented channel for which the primitive applies
|
Credits
|
Number of credits the receiving device can increment, corresponding to the number of K-frames that can be sent to the peer device sending the Flow Control Credit packet.
|
|
Information
|
Application must handle credits number on transmitter and receiver side
|
3. Bluetooth® Low Energy connection and COC establishment initiated by the central
3.1. On central side
- Initiate a Bluetooth® Low Energy link: send aci_gap_create_connection
- Wait for HCI_LE_CONNECTION_COMPLETE_EVENT
- Initiate a CoC connection: ACI_L2CAP_COC_CONNECT
- Wait for ACI_L2CAP_COC_CONNECT_CONFIRM_EVENT (get channel_index_list)
Range of channel_index_list for the COC initiator: from 0 to 0x1F
3.2. On peripheral side
- Start advertising: send aci_gap_set_discoverable
- Wait for HCI_LE_CONNECTION_COMPLETE_EVENT
- Wait for ACI_L2CAP_COC_CONNECT_EVENT
- Send ACI_L2CAP_COC_CONNECT_CONFIRM
- In hci_command_complete_event, get Channel_number and Channel_Index_List values
Range of channel_index_list for the COC peripheral: from 0x20 to 0x3F
3.3. COC data exchange
3.3.1. On sender side
Send ACI_L2CAP_COC_TX_DATA (Channel_Index, length, data)
3.3.2. On receiver side
Reception of ACI_L2CAP_COC_RX_DATA_EVENT
3.4. Example of Bluetooth® Low Energy connection, COC establishment and data exchange
Bluetooth® Low Energy and COC link establishment
|
|
3.5. Code Example
A STM32WB COC code example has been shared on STM32-Hotspot [1]
A STM32WBA COC code example is available with BLE_SerialCom application
3.6. References