OEMiRoT OEMuRoT for STM32H7S

Revision as of 17:26, 23 November 2023 by Registered User (→‎Features list)


A device deployed in the field operates in an untrusted environment and it is therefore subject to threats and attacks. To mitigate the risk of attack, the goal is to allow only authentic firmware to run on the device. Allowing the update of firmware to fix bugs, or introducing new features or countermeasures, is commonplace for connected devices, but it is prone to attacks if not executed in a secure way.


This article gives an overview of the OEMiRoT solution integrated in STM32H7S. How to use it, step by step, is described in wiki pages How to start with OEMiRoT on STM32H7S

1. OEMiRoT presentation

1.1. Overview

OEMiRoT stands for OEM immutable (unchangeable) Root of Trust and acts as a first boot stage. OEMiRoT is an example based on the MCUboot open-source software (refer to [MCUboot]) provided with STM32CubeH7RS. OEMiRoT offers two services:

  • The Secure Boot (root of trust service) is an immutable code, which is always executed after a system reset. It checks static protections (Options Bytes), activates runtime protections and then verifies the authenticity and integrity of the user application code before every execution.
  • The Secure Firmware Update application is an immutable code that detects new firmware image candidate. It checks its version (version downgrade prevention), authenticity and integrity before installing it after decryption.

An OEM updatable RoT (OEMuRoT) can be generated by compiling OEMiRoT_Boot project with OEMUROT_ENABLE switch activated. OEMuRoT acts as a second boot stage after STiRoT and provides the same two services: Secure Boot and Secure Firmware Update. Both OEMiRoT and OEMuRoT examples are generated based on OEMiRoT_Boot project with the switch OEMUROT_ENABLE activated or not.


1.2. Protection measures and security strategy

Cryptography ensures integrity, authentication, and confidentiality. However, the use of cryptography alone is not enough: a set of measures and system-level strategies are needed for protecting critical operations and sensitive data (such as a secret key), and the execution flow, in order to resist against possible attacks. On STM32H7S, the security strategy is based on (see also STM32H7RS Reference manual for more description):

  • Product life cycle: product state CLOSED or LOCKED must be selected in order to ensure that the JTAG debugger cannot access the device, except to execute the DA process (see DA wiki article).
  • Boot configuration:
1 boot stage: IROT_SELECT option byte must be set to OEMiRoT, to boot on user flash where must be located the OEMiRoT code.
2 boot stages: IROT_SELECT option byte must be set to STiRoT, to boot on system flash.
  • Anti-tamper protection: the anti-tamper protection is activated at the start of OEMiRoT_Boot project and remains active during OEMiRoT_Appli execution. In case of tamper detection, sensitive data, caches, and cryptographic peripherals are immediately erased, and a reboot is forced. Both external active tamper pins and internal tamper events are used.
  • MPU: the MPU is configured to limit the surface execution to the code area during OEMiRoT_Boot project execution then extended to the application code area after verifying its integrity and its authenticity. This protection is dynamically managed at runtime.
  • HDP: HDP area is configured to cover the whole OEMiRoT_Boot project code area in order to prevent any execution out of the OEMiRoT_Boot execution. When jumping in the application, the temporal isolation (HDP level) is increased from HDPL1 to HDPL2 making the OEMiRoT_Boot project code no longer accessible.
  • OBkeys: HDPL1 OBkeys (HDPL2 OBkeys for OEMuRoT) are a protected and isolated enclave used to store secrets such as encryption and authentication cryptographic keys. This enclave is no longer accessible when switching from HDPL1 to HDPL2 or to HDPL3. Data stored in this enclave is encrypted with a HUK derivated key.
  • WRP: this protection is set on the whole OEMiRoT_Boot project code area to make it immutable.
  • RAM ECC: ECC is a mechanism to prevent external attacks. A reset is generated in case of RAM ECC detection.

Note: WRP and HDP protections cannot be activated when OEMUROT_ENABLE switch is activated.

Secure software coding techniques such as doubling critical tests, doubling critical actions, checking parameter values, and flow control mechanism, are implemented to resist to basic fault-injection attacks.


The OEMiRoT_Boot application example is delivered with following cryptographic scheme:

  • ECDSA-P256 asymmetric cryptography for image authentication.
  • AES-CTR-128 symmetric cryptography with key ECIES-P256 encrypted for image confidentiality.
  • SHA256 cryptography for image integrity check.
  • AES-ECB-128 symmetric cryptography for firmware encryption using MCE after installation in external flash memory.
  • AES-ECB-128 symmetric cryptography for firmware encryption using MCE after transfer in execution slot in external RAM memory (load and run configuration).


1.3. OEMxRoT activation

On STM32H7S, OEMxRoT activation is done by:

  • Configuring the IROT_SELECT option to boot on OEMiRoT or STiRoT.
  • Configuring OEMxRoT secrets. authentication and encryption keys used by OEMxRoT.
  • Building OEMiRoT_Boot binary in the selected configuration (OEMiRoT or OEMuRoT).

All these operations operations are part of the provisioning process. OEMxRoT is activated in two different uses cases:

  • One boot stage, OEMiRoT: OEMiRoT_Boot project binary is built in OEMiRoT configuration. OEMiRoT directly manages the user application binary.
  • Two boot stages, STiRoT + OEMuRoT: OEMiRoT_Boot project binary is built in OEMuRoT configuration. STiRoT integrated inside the STM32H7S manages an updatable boot stage (OEMuRoT) located in the user flash memory, which manages the user application binary.

See also Secure Boot for STM32H7RS article

1.3.1. One boot stage: OEMiRoT

OEMiRoT is generated by compiling OEMiRoT_Boot project with OEMUROT_ENABLE switch de-activated.

At reset, OEMiRoT, located in the user flash memory, is the first application executed in temporal isolation 1 (HDPL1). After a successful verification of the authenticity and the integrity of the user application code image, OEMiRoT executes the user application in HDPL3. In case of verification failure, a reset will be triggered except if OEMIROT_DEV_MODE compilation switch is activated during OEMiRoT_Boot project generation. In this case the execution will fall into an infinite loop.

The following figure illustrates the secure boot and the secure update process by showing all the steps required to boot the user application code image located in the installation slot of the external flash memory:


  1. In CLOSED or LOCKED state RSS jumps into OEMiRoT if IROT_SELECT option byte is configured to boot on OEMiRoT.
  1. OEMiRoT checks if a new user application is stored in the download slot. If any, OEMiRoT decrypts it and controls its integrity and its authenticity. If successful, the image is copied in the user application installation slot. The image is re-encrypted by the MCE with OEMiRoT encryption keys.
  1. OEMiRoT controls the integrity and the authenticity of the user application image from the installation slot of the external flash memory. If successful, OEMiRoT executes it from external flash memory or from RAM memories. In this case an additional copy is made before its execution.

Security H7S OEMiRoT 1bootstage.png


Note: To avoid any risk of attack, when OEMiRoT jumps into the user application, the MPU is configured to ensure that only the user application code area is allowed to be executed (execution surface controlled via MPU configuration). It is the user application responsibility to reconfigure the MPU to fit with its security needs.

1.3.2. Two boot stages: STiRoT + OEMuRoT

OEMuRoT is generated by compiling OEMiRoT_Boot project with OEMUROT_ENABLE switch activated. OEMuRoT (updatable Root of Trust) acts as a second boot stage.


At reset, STiRoT is the first application executed in temporal isolation 1 (HDPL1). Refer to [2] for more details on temporal isolation levels. After a successful verification of the authenticity and the integrity of OEMuRoT code image, STiRoT executes OEMuRoT in HDPL2 and in RAM memory. Then, OEMuRoT verifies the user application before executing it from external flash or external/internal RAM memories. In case of verification failure, a reset will be triggered except if OEMIROT_DEV_MODE compilation switch is activated during OEMiRoT_Boot project generation. In this case the execution will fall into an infinite loop. The following figure illustrates the main steps performed to execute a user application in the two boot stages configuration:

  1. In CLOSED or LOCKED state RSS jumps into STiRoT if IROT_SELECT option byte is configured to boot on STiRoT.
  2. After executing the secure firmware update process (refer to STiRoT_for_STM32H7S article for more details), STiRoT requests iLoader to load the OEMuRoT image from installation slot in the internal RAM memory.
  3. Then STiRoT controls its integrity and its authenticity. If successful, STIRoT executes OEMuRoT in internal RAM memory.
  4. OEMuRoT checks if a new user application is stored in the download slot. If any, OEMuRoT decrypts it and controls its integrity and its authenticity. If successful, the image is copied in the user application installation slot. The image is re-encrypted by the MCE with OEMuRoT encryption keys.
  5. OEMuRoT controls the integrity and the authenticity of the user application from the installation slot. If successful, OEMuRoT executes it from external flash memory or from RAM memories. In case of RAM memory execution (Load and Run use case) an additional copy is made before its execution with an MCE re-encryption for the external memory. Refer to [5] for more details on OEMuRoT execution modes.

Security H7S OEMiRoT 2bootstages.png

Note: To avoid any risk of attack, when OEMuRoT jumps into the user application, the MPU is configured to ensure that only the user application code area is allowed to be executed (execution surface controlled via MPU configuration). It is the user application responsibility to reconfigure the MPU to fit with its security needs.

2. Features list

The main features of the OEMiRoT/OEMuRoT are:

  • ECDSA-P256 asymmetric cryptography for image authentication.
  • SHA256 cryptography for image integrity check.
  • AES-CTR-128 cryptography for image encryption, with symmetric key encrypted in ECIES-P256 provided in the image itself.
  • AES-ECB-128 cryptography for firmware encryption with MCE after installation in external flash and after transfer in external RAM memory before its execution (load and run configuration). In both cases, a specific key derived from HUK is used.
  • Accelerated boot thanks to image hash reference management. Image verification mainly consists of verifying hash of the image (integrity check) and then verifying the signature of this hash (authentication check). If successful, the hash is stored as reference hash for next boot. At next boot, the signature verification is skipped if hash of the image match the reference hash stored in OBKeys. This feature brings performance optimization (under the MCUBOOT_USE_HASH_REF compilation switch).
  • Anti rollback version check based on image version counters in OBkeys.
  • Image installation resistant to asynchronous power down and reset.
  • Integration of the full entropy TRNG source (RNG hardware peripheral) for random numbers generation (boot seed generation, tamper protection) or random delays (FIH).
  • Configurable firmware image upgrade strategy, for primary and secondary slots mode:
  1. Overwrite strategy, for which the image in the secondary slot overwrites the image in the primary slot.
  2. Swap strategy, for which the image in primary and secondary slots are swapped. After the swap, the new image in the primary slot must be confirmed by the user application, else, at the next boot, the images are swapped back.
  • Memory configuration:
  1. Download and installation slots in external flash memory. Installation slot is encrypted with MCE based on key derived from HUK.
  2. Execution slot from external flash memory or from internal RAM, or external RAM memories (load and run configuration). External RAM memory slot is encrypted with MCE based on specific key derived from HUK. Load and run capability is configured with OEMIROT_LOAD_AND_RUN define.
  • Integration of hardware security peripherals and mechanisms in order to implement a root of trust. Product life cycle, IROT_SELECT, MPU, WRP, HDP, and TAMPER are combined to achieve the highest security level. When connected on the HW board, external tamper can be activated with OEMIROT_TAMPER_ENABLE define.
  • IDE integrated image tool to prepare the image, provided both as a Windows® executable and a Python™ source code.
  • Activation of ICACHE peripheral for internal flash memory access to improve boot time performance.

Features configurability in OEMiRoT based example in the STM32CubeH7RS MCU Package.

Feature OEMiRoT OEMuRoT

OEMiRoT/OEMuRoT generation

OEMUROT_ENABLE switch deactivated

OEMUROT_ENABLE switch activated

Image upgrade strategy

  • Overwrite only mode
  • Swap mode
  • Overwrite only mode
  • Swap mode

Flash memory configuration

  • External flash memory for download and installation slots
  • Execution slot definition depending on load and run configuration
  • External flash memory for download and installation slots
  • Execution slot definition depending on load and run configuration

Security peripherals

  • IROT_SELECT set to OEMiRoT
  • WRP and HDP activated
  • IROT_SELECT set to STiRoT

Antitamper

  • None
  • Internal tampers only
  • Internal and external tampers
  • None
  • Internal tampers only
  • Internal and external tampers


3. Memories layout

The STM32CubeH7RS OEMiRoT/OEMuRoT relies on memories layout defining several regions:

  • SCRATCH region: region used by OEMiRoT_Boot to store the image data temporarily during the image swap process (not used in overwrite-only mode).
  • OEMiRoT_Boot binary region: region to program the OEMiRoT_Boot code binary that manages the functions "Secure Boot" and "Secure Firmware Update”.
  • Installation (primary) slot region: region to program the image of an “active” firmware after installation.
  • Download (secondary) slot region: region to program the image of a “new” firmware, candidate for installation.
  • Execution slot region when load and run feature is activated.

Memories layout is as follow: Security H7S OEMiRoT layout.png Security H7S OEMuRoT layout.png

For both configuration, default values are :

Symbol Execute in place Load and run in external RAM Load and run in internal RAM
FLASH_AREA_0_OFFSET 0x00000000 0x00000000 0x00000000
FLASH_AREA_0_SIZE 0x00200000 0x00200000 0x00020000
IMAGE_PRIMARY_RUN_PARTITION_OFFSET NA 0x00000000 0x24040000
FLASH_AREA_SCRATCH_OFFSET 0x00400000 0x00400000 0x00040000
FLASH_AREA_SCRATCH_SIZE 0x00010000 0x00010000 0x00010000
FLASH_AREA_BL2_OFFSET 0x08000000 0x08000000 0x08000000
FLASH_AREA_BL2_SIZE 0x00010000 0x00010000 0x00010000
BL2_RAM_OFFSET* 0x24000000 0x24000000 0x24000000
BL2_RAM_SIZE* 0x00020000 0x00020000 0x00020000
BL2_DATA_OFFSET** 0x20000000 0x20000000 0x20000000
BL2_DATA_SIZE** 0x00020000 0x00020000 0x00020000
RAMECC_HANDLER_START 0x30004000 0x30004000 0x30004000
RAMECC_HANDLER_SIZE 0x40 0x40 0x40
CONF_FLAG_SIZE 0x20 0x20 0x20

*: specific to OEMiRoT
**: specific to OEMuRoT

4. Provisioning process

4.1. OEMiRoT provisioning process

The product provisioning to activate and configure OEMiRoT is done following the three steps below:

  1. Configuration of OEMiRoT. At this stage, the cryptographic keys for authentication and encryption are defined.
  2. Generation of the firmware image.
  3. Programing of the OBkeys, the option bytes, the application image in the device

Security H7S OEMiRoT provisioning.png

Note: A set of scripts is provided in Firmware/Projects/STM32H7S78-DK/ROT_Provisioning/OEMiRoT folder. It guides the user all along the provisioning process. Refer to How to start with OEMiRoT on STM32H7S article.

4.2. OEMuRoT provisioning process

The product provisioning to activate and configure OEMuRoT is done following the three steps below:

  1. Configuration of STiRoT. At this stage, the number of images managed (firmware code image only), the location of the image, and the STiRoT cryptographic keys are defined. Refer to article.
  2. Configuration of OEMuRoT. At this stage, the OEMuRoT cryptographic keys for authentication and encryption are defined.
  3. Generation of the OEMuRoT code images as well as the application code image.
  4. Programing of the OBkeys, the option bytes, the OEMuRoT code image and the application code image in the device

Security H7S OEMuRoT provisioning.png

Note: A set of scripts is provided in Firmware/Projects/STM32H7S78-DK/ROT_Provisioning/STiROT_OEMuROT folder. It guides the user all along the provisioning process. Refer to How to start with OEMuRoT on STM32H7S article.

4.3. OEMiRoT/OEMuRoT OBkeys configuration file

OEMiRoT/OEMuRoT OBkeys configuration file (OEMiROT_Config.obk, OEMuRoT_Config .obk) is generated using STM32TrustedPackageCreator with a template file listing all the different parameters (OEMiRoT_Config.xml, OEMuRoT_Config.xml) as input. The list of the configuration parameters is the following:

Parameter Description Additional constraints
Encryption key Key used to encrypt the firmware image When this key is regenerated, firmware image must be processed with TPC “Image Gen” tab (OEMiRoT_Code_Image.xml)
Authentication key Key used to authenticate the firmware image When this key is regenerated, firmware image must be processed with TPC “Image Gen” tab (OEMiRoT_Code_Image.xml)

A detailed presentation of the format of STiROT_Config.obk file is provided in Appendix 5.3 STiROT Config.obk file format.

5. Images generation

OEMiRoT manages an image at MCUBoot format including:

  • a header,
  • the encrypted firmware binary,
  • some metadata information (TLV format: Tags Length Value) allowing the control of the image (SHA256, encryption key …), and
  • a magic to trigger the installation.

Further information about the MCUBoot open-source software is available at mcuboot.com. A PC tool STM32TrustedPackageCreator is provided to generate both firmware and data images. These images are encrypted and signed using the keys configured in OBkeys configuration file. OEMiROT_Code_Image.xml contains all the parameters driving the image generation such as:

  • The authentication and encryption keys,
  • The version.

OEMiROT_Code_Image.xml can be edited with STM32TrustedPackageCreator in order to modify the version. Keys are directly inherited from OEMiROT_Config.xml file.

The following figure shows the firmware image generation: Security H7S OEMiRoT image.png

6. Appendix

6.1. OEMiRoT start-up sequence

Security H7S OEMiRoT startup.png

Note: When no valid firmware image is installed a reset will be triggered in loop. Debug authentication process must be executed to force the download of a new image. Refer to Debug Authentication for STM32H7RS article.

IDE Boot time (1Mb image)
IAR x ms
Keil x ms
STM32CubeIDE x ms

6.2. Application development phase

Merci Réjane :-)

6.3. OEMiRoT_Config.obk file format

Offset Size Type Description
0 1 uint8 sdp command header : destination OBKey index
1 1 uint8 sdp command header : destination OBKey HDP level
2 2 uint16 sdp command header : reserved
4 4 uint32 sdp command header : data size address
8 4 uint32 sdp command header : encryption disabled/enabled (0/1)
12 32 array SHA256 of the following data content (from offset 44 to xxx)
44 91 array Authentication public key (MCU Boot format)
135 70 array Encryption private key (MCU Boot format)
xx 31 array Reserved

Same applied for OEMuRoT_Config.xml

6.4. OEMiRoT_Code_image xml file format

Parameter Updatable Description
Authentication key Yes, through OEMiROT_Config.xml Private key inherited from OEMiROT_Config.xml file.
Encryption key Yes, through OEMiROT_Config.xml Public key inherited from OEMiROT_Config.xml file.
Endianness No Little endian.
Padding No Add an installation magic value at the end of the image to trigger image installation. Padding with 0xFF when required.
Firmware area size Yes Firmware slot size information. This value is updated during the provisioning process based on slot configuration from flash_layout.h
Header Size No 0x400 bytes
Padding Header No Padding the header with 0xFF to fulfil the 0x400 bytes.
Dependency with data image No This parameter is removed by setting the <enable> property to 0.
Write Option No This value is updated during the provisioning process based on the installation method: overwrite or swap.
Version Yes x.y.z firmware image version.
Security Counter No Security counter value automatically generated based on version information.
Align No 16 bytes alignment
Firmware download area offset Yes Used to generate .hex binary file format including the destination address. This value is updated during the provisioning process based on load and run configuration (execution from external flash extern, internal RAM or external RAM.
Firmware binary input file Yes Location of the firmware binary file. This parameter is updated during the provisioning process based on information from env.bat file.
Image output file Yes Location of the encrypted image generated. If changed, provisioning scripts must be updated accordingly.

Same applied for OEMuRoT_Code_Image.xml

6.5. Troubleshooting

Problem Possible solution
... ...