SFI STM32H5 How to Intro

Revision as of 17:47, 3 November 2023 by Registered User

SFI Step-by-step on STM32H573_DK MB1677Clock.png75min


Target description

This tutorial shows how to use SFI for installing an OEM application developed with STM32TRUSTEE on STM32H573_DK MB1677.

The process goes through three 'steps' at the Original Equipment Manufacturer (OEM) and Contract Manufacturer (CM) sites.

  • Development @ OEM: the application code that runs on STM32 is generated.
  • Secure Room @ OEM: code prepared during the development is encrypted and packaged to be sent for manufacturing. The Secure Room is isolated, and its resources are not visible outside of it.
  • Manufacturing @ CM: the encrypted code received by the OEM Secure Room is installed using SFI tools.


Prerequisites

  • Knowledge of STM32CubeProgrammer
  • Knowledge of JTAG

Hardware

  • STM32H573_DK MB1677[1] Discovery kit with STM32H573IIK3Q MCU
  • STM32-HSM[2] SAM for Secure Firmware Installation
  • Smartcard Reader
    • Laptop Built-in
    • External
  • 1 x USB cable Type-A to Micro-C

Software

  • STM32CubeProgrammer[3] Software programming tool for STM32 (v2.13 min)
    • Including STM32TrustedPackageCreator
  • STM32CubeH5[4] STM32Cube MCU Package for STM32H5 series
  • X-CUBE-SEC-M-H5[5] STM32Cube Expansion Package STM32TRUSTEE-SM for STM32H5 series


Literature

  • AN4992 STM32 MCUs secure firmware install (SFI) overview
  • UM2237 STM32CubeProgrammer software description
  • UM2238 STM32 Trusted Package Creator tool software description
  • AN5054 Secure programming using STM32CubeProgrammer
  • AN2606 STM32 microcontroller system memory boot mode
  • RM0481 STM32H563/H573 and STM32H562 Arm®-based 32-bit MCUs
  • UM2448 STLINK-V3SET debugger/programmer for STM8 and STM32



===> Go step by step now How to start with SFI on STM32H5

No categories assignedEdit