1. Introduction
In the context of the Secure Manager, an RTOS can be used. In this article, we will explore how an RTOS can be use with the Secure Manager, focused on the mechanism provided to ensure thread safe secure calls. We will now use FreeRTOS to show how the implementation is done.
2. Implementation example
2.1. Thread-safe secure calls
We will use mutexes to synchronize access to the PSA api and protect shared resources. For the implementation of the mutex it needs to be initialized and then used in the functions of the project interface. These functions are usually defined as "__weak" in the middleware part, but can be redefined in the project to use the mutex.
Declare a mutex and initialize it to 0:
static SemaphoreHandle_t nsIpcMutex = { 0 };
Create a function that creates the mutex and assigns it to the nsIpcMutex variable. If the mutex creation fails, log an error:
void tfm_ns_interface_init( void )
{
nsIpcMutex = xSemaphoreCreateMutex();
if(nsIpcMutex == NULL)
{
// Logging Error
}
}
Finally, implement the acquisition and release of the mutex in the ns_ipc_seq_begin and ns_ipc_seq_end functions, respectively. This will allow locking access when a thread calls the API, ensuring that shared resources are not accessed simultaneously:
void ns_ipc_seq_begin(const ns_ipc_seq_info_t* info)
{
/* Lock mutex */
if(nsIpcMutex != NULL)
{
xSemaphoreTake(nsIpcMutex, portMAX_DELAY );
}
….
}
void ns_ipc_seq_end(const ns_ipc_seq_info_t* info)
{
/* Unlock mutex */
if(nsIpcMutex != NULL)
{
xSemaphoreGive(nsIpcMutex);
}
….
}
For more concrete examples, real implementations can be found in X-Cube-AWS & X-Cube-Azure using the security manager with a real-time operating system.
2.2. Memory Management
SRAM 3 can be configured with heap RTOS configuration. The heap_5 implementation of FreeRTOS dynamic memory allocator is selected to use non-contiguous memory regions in SRAM1 and SRAM3. During initialization, prvInitializeHeap() needs to be set up.
This concludes the overview of using FreeRTOS with the Secure Manager to ensure thread safety and prevent concurrent access to shared resources.