Some recent STM32H747I-DISCO kits are shipping with an updated LCD controller (NT35510). This article describes how to run FP-AI-VISION1 projects on these kits. The latest LCD daughterboard is marked MB1166-A09, as seen in the image below.
Prerequisites:
1.
Steps: 1. Download and unzip NT35510 drivers from this zip file. Alternatively, up-to-date drivers can also be downloaded directly from the STM32CubeH7 GitHub repo [1] 2. Copy the entire nt35510 directory to ..\FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\ 3. Copy stm32h747i_discovery_lcd.c and stm32h747i_discovery_lcd.h , and paste them into ..\FP-AI-VISION1_V3.1.0\Drivers\BSP\STM32H747I-Discovery\ 4. Use a text editor to open ..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\Common\CM7\Inc\stm32h747i_discovery_conf.h. On line 34, make the following changes: /* LCD controllers defines */
- define USE_LCD_CTRL_NT35510 1U
- define USE_LCD_CTRL_OTM8009A 0U
- define USE_LCD_CTRL_ADV7533 0U
5. TODO: Drag/drop nt355510 to components directory in CubeIDE 6. Compile and flash