How to start with STM32CubeMX Secure Manager on STM32H57

Revision as of 15:59, 26 September 2023 by Registered User (→‎Boot path configuration)
Under construction.png Coming soon

The purpose of this article is to show an integration of Secure Manager in ecosystem using STM32CubeMX.


Read Secure Manager for STM32H5 before starting the practical example described below.


SECURITY SM Boot scheme.png

Prerequisites

To execute the example described below, you'll need an STM32H573I-DK discovery board:

Figure 2: STM32H573 DK MB1677

You'll also need the following tools:

  • STM32CubeMX_6.9.2 or later (see STM32CubeMX ST web page[1])
  • IAR Embedded Workbench rev 9.20.1 or later
  • STM32CubeProgrammer rev 2.14.0

Note:

  • STM32 Trusted Package Creator (TPC) is automatically installed during the STM32CubeMX installation. This TPC version is dedicated to STM32CubeMX and installed in the STM32CubeMX/utilities folder.
  • The latest STM32Cube_FW revision is installed through STM32CubeMX (see appendix).
  • If needed, set the Windows environment variable (see appendix). It is required in case the H5 doesn’t appear in the STM32CubeMX Access to MCU Selector


1. Introduction


2. Setting up the STM32CubeMX project

Launch STM32CubeMX

  1. Click on Access to MCU Selector (for this example, it's easier to enable only the necessary GPIOs, so it's advised to use the MCU selector instead of the board selector).
  2. From the Series column, select STM32H5, and select the device used in STM32H5-DK.
  3. Click start project.
  4. Enable TrustZone, as shown in Figure 3. (For the STiROT boot path, TrustZone needs to be enabled.)


SECURITY STM32CubeMX MCU selector.png


Create the STM32CubeMX project:

  1. Type the name of the project (if it doesn't already exist, the related folder will be created).
  2. Choose a folder for the project (avoid a long path).
  3. Check that both the Secure Project and Nonsecure Project checkboxes are checked (they should be checked by default).
  4. Select the relevant toolchain; for this example EWARM is used.
  5. Go to File > Save Project. The project folder (if it doesn't already exist) and the STM32H5_STiROT_SLed_NSLed.ioc file will be created.


SECURITY STM32CubeMX project parameters SM.png


SECURITY STM32CubeMX project non secure SM.png
SECURITY STM32CubeMX save pj SM 2.png

3. Boot path configuration

SECURITY STM32CubeMX boot path selection SM.png


SECURITY STM32CubeMX boot path SM.png



SECURITY STM32CubeMX boot path selection OK SM 2.png