Zigbee Certification Process for STM32WB and STM32WBA

Revision as of 11:50, 25 September 2023 by Registered User

1. Introduction

Zigbee is widely used in smart home, commercial and industrial applications. To ensure interoperability between Zigbee devices, the CSA has established a certification process that involves rigorous testing.
Depending on the scope of the certification, 2 types of certification are defined:

  • Platform Certification
    • Zigbee Compliant Platform (FFD/RFD)
  • End Product Certification
    • Zigbee 3.0 Certified Product (FFD/RFD)
    • Zigbee Smart Energy Product (FFD/RFD)

2. Zigbee Certification Process

The general steps of obtaining a certification are the following:

  1. Join the ZigBee Alliance.
  2. Select the certification type: The company must then select the type of certification they wish to pursue, such as Zigbee Platform Certification or End Product Certification.
  3. Prepare the product.
  4. Select an authorized test house and submit to product for testing.
  5. Address any issues: If the product fails any of the tests, the company must address the issues and resubmit the product for testing.
  6. Obtain certification: Once the product passes all the tests, the company will receive the appropriate certification.

3. Zigbee Platform Certification

Zigbee Platform Certification is a process that certifies the compliance of a specific hardware or software platform with the CSA standards and requirements for interoperability with other Zigbee devices. The certification process involves rigorous testing of the product's hardware, software, and functionality to ensure that it can communicate effectively with other Zigbee devices and operate within a Zigbee network. This certification is typically obtained by manufacturers of chips and software stacks.
Depending on device type (FFD/RFD), dedicated tests set applies.
Green Power Proxy tests (GPP) may be run as part of Zigbee Platform certification to ensure that the platform or device can support GPP functionality and can communicate with low-power devices using GPP.
802.15.4 MAC & PHY certification has to be performed before running Zigbee Compliant Platform certification tests.

4. End Product Certification

Is a process that certifies the compliance of a final product or device that incorporates Zigbee technology with the CSA standards and requirements. This certification is typically obtained by manufacturers of consumer/ commercial products that use Zigbee technology, such as smart home devices or lighting systems.

4.1. Zigbee 3.0 Certification

This certification intends to check Zigbee End Product interoperability & application middleware (ZCL cluster library / BDB)

Depending on device type (FFD/RFD), dedicated BDB tests set applies.

Zigbee Green Proxy cluster (GPP) is mandatory to get Zigbee 3.0 certificate in FFD device case.

Zigbee Compliant platform certification has to be performed before running Zigbee 3.0 certification tests.

Prior sending the product for testing, Zigbee 3.0 Test Tool (ZTT) is used for internal pre-testing, to avoid the delays and cost of multiple iterations with the test house. This is available for all Zigbee Alliance members.

Zigbee 3.0 Certification Process

4.2. Zigbee Smart Energy Certification

Zigbee SE Certification can only be performed with a real End Product with dedicated Hw such as Power Meter / Gas Meter. As a result, Zigbee SE Certification is not applicable to STM32WB.

2 flavours of SE certification are defined : ZigBee Smart Energy v1.2b / ZigBee Smart Energy v1.4

Zigbee SE certification intends to check Zigbee End Product interoperability & application middleware (ZCL cluster library / BDB)

Zigbee Compliant platform certification has to be performed before running Zigbee SE certification tests.

5. Certification Tools

5.1. Chai Tool ?

5.2. Zigbee Unified Test Harness (ZUTH)

It is the official CSA test tool for certification testing. It is used for formal testing by Alliance Authorized Test Laboratories (ATLs) and is also available to all Alliance members for pre-certification testing.

6. Acronyms and definitions

Term Definition
BDB Base Device Behavior
DUT Device Under Test
FFD Full Feature Device
RFD Reduced Feature Device
PICS Protocol Implementation Conformance Statement
PIXIT Protocol Implementation Extra Information for Testing
ZTT Zigbee Test Tool
ZCL ZigBee Cluster Library