![]() |
Coming soon |
This page contains information related to Bluetooth® Low Energy or regional (CE, FCC) certification.
It is assumed that reader is familiar with STM32WB and/or STM32WBA development. Otherwise please visit Introduction to Bluetooth® LE with STM32
guideline.
1. STMicroelectronics tools for certification
STMicroelectronics is providing a dedicated STM32WB/WBA firmware called "Transparent Mode" that could be used for certification purpose.
STMicroelectronics is also providing a dedicated GUI PC tool called STM32 Cube Monitor RF[1] that could be used for regional RF certifications.
1.1. Transparent mode FW
A set of commands/events are sent through the STM32WB/WBA UART or USB to control the Bluetooth® Low Energy stack via the transparent mode application.
1.1.1. STM32WB1x, STM32WB3x, STM32WB5x
STM32WB devices embed Arm Cortex-M4 and Arm Cortex-M0 network co-processors.
STM32WB-M0 embed the Bluetooth® smart protocol stack.
While, on external STM32WB-M4 a dedicated Transparent mode FW is available in STM32CubeWB [2] software package.
It is available in source code, and it must eventually be rebuilt according to customer HW configuration (UART interface used, SMPS used or not, etc.)
Please note, stm32wbxx_BLE_Stack_full_extended_fw binary is mandatory in STM32WB-M0 with STM32WB-M4 transparent mode FW .
if UART interface is used, refer FW example available in P-NUCLEO-WB55 Nucleo folder.
if USB interface is used, refer FW example available P-NUCLEO-WB55 USBDongle folder.
1.1.2. STM32WBA5x
It is available in STM32CubeWBA [3] software package.
Transparent mode FW is available in source code and it must eventually be rebuilt according customer HW configuration (UART interface used, SMPS used or not, etc.)
You can find more details on dedicated STM32WBA page STM32WBA_TransparentMode.
1.2. STM32 Cube Monitor RF PC tool
STM32 Cube Monitor RF [1] is a PC tool for quick testing the RF performance of STM32WB/WBA-based hardware devices.
Thanks to RF Tests panel, device under test can quickly be set in the required mode (Rx or Tx), modulation and power.
2. Bluetooth® certification
2.1. Bluetooth® Low Energy qualification process
All products using Bluetooth® technology must complete the Bluetooth® Qualification process. Please refer to below Bluetooth® SIG webpage :
Bluetooth® Qualification Process Overview [4].
Bluetooth® Qualification process is not a matter of putting Bluetooth® logo on product or not, it is a matter of using a licensed technology.
Two possible paths for qualification process:
No required testing
✓ I am designing a product based on a STMicroelectronics pre-certified module such as STM32WB5MMG or STM32WB1MMC
✓ I am designing a product using STM32WB and I follow recommendations as explained in AN5165 or STM32WBA chipset and I made no changes in schematics and layout.
Required testing
✓ I am designing a product based on a STMicroelectronics chipset such as STM32WB and I don't follow recommendations as explained in AN5165 or STM32WBA and I made changes in schematics or layout.
Launch Studio process flow
Launch studio process is described step by step in dedicated chapter.
Whatever STM32WB or STM32WBA chipset or associated modules, STMicroelectronics is not providing End Product devices so that Required Testing path should be used.
STMicroelectronics qualified its product as component [5] (Tested) to allow changes and maintenance to latest core functionality.
Below pictures is providing main qualification steps and associated costs.
All the certification fees are available at SIG Website [6]
RF PHY reports for STM32WB modules can be found on st.com:
- STM32WB5MMG (cutY) RF PHY test report [7]
- STM32WB5MMG (cutX) RF PHY test report[8]
- STM32WB1MMC (cutX) RF PHY test report[9]
Is SW testing required?
Whatever path selected, no SW testing is required except if using adopted standard profiles.
Where is done BT qualification?
If testing is required, qualification testing process must be done in an official Bluetooth® Qualification Test Facility (BQTF)
A Bluetooth® Qualification Test Facility (BQTF) is formally recognized by the Bluetooth® SIG as competent to perform those Bluetooth® qualification conformance tests.
List of official BQTF is available on Bluetooth® website: Qualification Test Facilities [10].
2.2. Available Qualified Design IDs (QDID)
Below tables are summarizing all available PHY and host stack QDIDs for STM32WB / STM32WBA family
When moving to certification, customers should select PHY and stack QDID depending on STM32WBx selected version or stack/features used.
As a reminder:
- You will need to start launch studio process from the latest mandatory TCRL
- It will ensure interoperability between a 5.1 device and 5.3 device for example
- All BLE features are optional so you will "pickup" features needed for your application
STM32WB PHY QDID
Package | Part number | Cut version | RF PHY QDID |
---|---|---|---|
QFN48 | STM32WB55Cx (BLE5.2 - 2Mbit/s) STM32WB50Cx (BLE5.2 - 1Mbit/s) STM32WB35Cx (BLE5.2 - 2Mbit/s) STM32WB30Cx (BLE5.2 - 1Mbit/s) |
Y or X | 161807 (TCRL 2021-1) |
STM32WB15CCU6E (BLE5.2 – 2Mbit/s) STM32WB10CCU5E (BLE5.2 – 1Mbit/s) |
Y or X | 164054 (TCRL 2020-1) | |
STM32WB15CXX6 (BLE5.2 – 2Mbit/s) STM32WB10CXX5 (BLE5.2 – 1Mbit/s) |
Y or X | 161969 (TCRL 2020-1) | |
QFN68 | STM32WB55Rx (BLE5.0 - 2Mbit/s) | Y | 127495 (TCRL 2023-1) |
CSP 100 | STM32WB5xVY (BLE5.1 - 2Mbit/s) | Y | 134665 (TCRL 2021-1) |
STM32WB55VY (BLE5.3 - 2Mbit/s) | X | 178970 (TCRL 2021-2) | |
BGA129 | STM32WB55Vxx (BLE5.2 - 2Mbit/s) | Y or X | 161808(TCRL 2021-1) |
WLCSP49 | STM32WB15CCY (BLE5.2 – 2Mbit/s) STM32WB10CCY (BLE5.2 – 1Mbit/s) |
Y or X | 170241 (TCRL 2020-1) |
Module 86-pin LGA | STM32WB5MMG (BLE5.2 – 2Mbits/s) | Y | 170767 (TCRL 2020-1) |
STM32WB5MMG (BLE 5.3 - 2Mbits/s) | X | 187035 (TCRL2021-2) | |
Module 77-pin LGA | STM32WB1MMC (BLE5.3 – 2Mbit/s) | 2.1 | 187042 (TCRL2023-1) |
STM32WB host stack QDID
Features | Host stack version | STM32WB_Copro_Wireless_Binaries | QDID |
---|---|---|---|
4.0 HCI LL |
STM32Cube_WB_BLE_HCI | stm32wb5x_BLE_HCI_AdvScan_fw.bin stm32wb5x_BLE_HCILayer_fw.bin stm32wb3x_BLE_HCI_AdvScan_fw.bin stm32wb3x_BLE_HCILayer_fw.bin stm32wb1x_BLE_HCI_AdvScan_fw.bin stm32wb1x_BLE_HCILayer_fw.bin |
160726 (TCRL 2023-1) BLE5.2 |
4.0 HCI LL, ATT, GAP, GATT, L2CAP, SMP |
STM32Cube_WB_BLE_FULL_STACK STM32Cube_WB_BLE_BASIC_STACK STM32Cube_WB_BLE_LIGHT_STACK |
stm32wb5x_BLE_Stack_full_fw.bin stm32wb5x_BLE_Stack_light_fw.bin stm32wb3x_BLE_Stack_full_fw.bin stm32wb3x_BLE_Stack_light_fw.bin stm32wb1x_BLE_Stack_full_fw.bin stm32wb1x_BLE_Stack_light_fw.bin |
160724 (TCRL 2023-1) BLE 5.2 |
4.0 HCI LL with extended advertising, ATT, GAP, GATT, L2CAP with Enhanced Connected Oriented Channel, SMP |
STM32CubeFW_WB_BLE_HCI_FULL_EXT STM32CubeFW_WB_BLE_STACK_FULL_EXT |
stm32wb5x_BLE_HCILayer_extended_fw.bin stm32wb3x_BLE_HCILayer_extended_fw.bin stm32wb1x_BLE_HCILayer_extended_fw.bin stm32wb5x_BLE_Stack_full_extended_fw.bin stm32wb3x_BLE_Stack_full_extended_fw.bin stm32wb1x_BLE_Stack_full_extended_fw.bin |
201968 (TCRL2023-1) BLE 5.3 216169 (TCRL2023-1) BLE 5.4 |
STM32WBA PHY QDID
Package | Part number | Cut version | RF PHY QDID |
---|---|---|---|
QFN48 | STM32WBA52 | 1.x | 197135 (TCRL 2022-2) BLE 5.4 |
STM32WBA Host stack QDID
Features | Host stack version | QDID |
---|---|---|
4.0 HCI LL with extended advertising, ATT, GAP, GATT, L2CAP with Enhanced Connected Oriented Channel, SMP |
STM32Cube_WBA_BLE_HCI_STACK STM32Cube_WBA_BLE_FULL_STACK |
198195 (TCRL 2022-1) BLE 5.3 |
2.3. Launch studio process
Please find Bluetooth® qualification process example wiki article, detailing all different steps to qualify our End Product. We will describe a specific example: Qualify your project "My first project with STM32WB55RG component"
2.4. Bluetooth® Low Energy PHY testing : How to?
In case PHY testing is required, below page contains information for preparing customer's HW and SW.
2.4.1. SW & HW recommendation for BLE RF testing
Customer should then prepare its device under test so that:
✓STM32WBx or STM32WBAx is flashed with transparent mode FW.
✓SMA RF cable is set instead of antenna (ensure solid grounding connection) as BLE RF PHY tests are done in conducted mode only.
2.4.2. Direct test mode
Direct Test Mode (Bluetooth® tester is sending HCI commands directly to device under test) is mandatory for BLE qualification.
This why customer product must be flashed with transparent mode FW (refer dedicated chapter on transparent mode FW).
2.4.3. Pixit
When moving to RF PHY tests, customer might need to provide test house few details about RF PHY of chipset.
Needed information for STM32WB are listed in below table.
- Note 1: Some information is product related and not chipset related (noted “Product dependent” in this table)
- Note 2: 2M tests should be set to “NA” if device is not supporting 2M modulation.
Needed information for STM32WBA are listed in below table.
- Note 1: Some information is product related and not chipset related (noted “Product dependent” in this table)
- Note 2: 2M tests should be set to “NA” if device is not supporting 2M modulation.
- Note 3: Direction finding parameters should be set to NA if not used.
3. Regional certification
In order to sell Bluetooth® Low Energy product in regional countries, equipment needs to comply with the associated RF regulatory requirements:
- FCC (Federal Communications Committee) for North America
- CE European Commission (Radio Equipment Directive)
- IC (Industry Canada).
- etc.
3.1. Module versus chipset
Chipset use case
- STM32WB chipsets are compliant with regional RF regulatory requirements.
- However, RF tests for regional certification are fully HW dependent (antenna, layout etc.)
→ Each customer product must go through RF tests for all regional certification.
Module use case
- STM32WBxMMx modules are RF pre-certified for various region.
Certificates and tests reports are available on st.com for STM32WB1M [11] and STM32WB5M [12].
- It means limited RF tests are requested on final product (Rx and Tx radiated tests).
→ RF tests costs are then reduced when using our certified modules.
→ Each customer product must go through remaining RF tests for all regional certification.
3.2. Regional testing : How to?
3.2.1. Test setup for regional RF testing
Customer should then prepare its DUT so that:
- STM32WB is flashed with transparent mode FW.
- Device under test is connected to STM32CubeMonitorRF [1] PC tool.
- RF test will be done in conducted and mainly radiated mode. For conducted tests RF cable should be implemented instead of antenna (ensure solid grounding connection).
Below picture is describing recommended test setup for performing regional RF testing.
3.2.2. RED - EN 300 328 prefilled document
Customers will be asked to fill up a form for EN 300 328 RED RF tests. Below are pre-filled suggested values when related to to STM32WB/WBA (to be completed with product related information)
3.2.3. Immunity tests
For regional certification, test house will check final product is able to sustain BLE communication under EMC stress.
Possible setup could be as below:
- Device under test is flashed with Transparent Mode FW and connected to STM32 Cube Monitor RF.
- STM32WB evaluation kit (for example) is also used outside anechoic chamber. It is flashed with Transparent Mode FW and connected also to STM32 Cube Monitor RF.
- Thanks to ACI Utilities panel, you can quickly establish a BLE link between DUT and ST eval kit. You can then check any disconnection during EMC stress test.
1) DUT Advertises
2) STM32WB Scans
3) STM32WB Connects
4) If RF link is broken with DUT, disconnection will appear.
4. References
- ↑ 1.0 1.1 1.2 STM32 Cube Monitor RF
- ↑ STM32CubeWB software package
- ↑ STM32CubeWBA software package
- ↑ Bluetooth® Qualification Process Overview
- ↑ Qualifying-With-a-Component
- ↑ Bluetooth® SIG Website
- ↑ STM32WB5MMG (cutY) RF PHY test report
- ↑ STM32WB5MMG (cutX) RF PHY test report
- ↑ STM32WB1MMC (cutX) RF PHY test report
- ↑ Qualification Test Facilities
- ↑ STM32WB5M
- ↑ STM32WB1M