This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.
1. Overview
This application provides an example of Matter bridge using the NUCLEO-H753ZI-Q board with Ethernet connectivity.
This prototype application demonstrates dynamic endpoint with device commissioning and cluster control. It adds the non-matter device as endpoints on a bridge that acts as a Matter device. In this example, 8 light devices supporting one on-off cluster have been added as endpoints.
System presentation |
---|
2. Boards Needed
- The bridge runs on:
3. Package content
You can download the necessary files on Github