SFI for STM32H5

Revision as of 13:14, 23 August 2023 by Registered User

1. introduction

The STM32H5 series provide a trusted execution environment security framework: the Secure Manager . It is aiming at simplifying the security development cycle of embedded applications by providing ready to use security services developed according to best practices.

The OEM can choose to develop its application with or without the Secure Manager.

2. OEM applications developed with Secure Manager

When the OEM wants to securely install its application (developed with the Secure Manager), there are several additional components to prepare and install.

Here is an overview of the preparation and installation flow:

Security Secure Manager ecosystem.png


ST provides the SFI solution to perform the preparation and installation flows.

2.1. Preparation flow

2.1.1. Overview

The purpose of this step is to:

  • Prepare the encrypted firmware image to install (called SFI mage). It is composed of the OEM application and additional components: OEM secrets, Secure Manager and modules.
  • Provision the OEM key within an HSM or a global license

2.1.2. SFI image

2.1.2.1. Overview
2.1.2.2. SFI image inputs description

The OEM must provide the following inputs:

2.1.2.2.1. OEM application

OEM must provide its application binary developed with the Secure Manager.

2.1.2.2.2. Secure Manager

The Secure Manager binary is available as an encrypted image from STM32TRUSTEE-SM[1].

2.1.2.2.3. Modules

Secure Manager offers the possibility to install secure modules. Module installation is possible by following the SFI procedure.
The SFI image modules inputs are the encrypted module binaries.

2.1.2.2.4. OEM secrets

OEM secrets are OEM data, OEM keys and also the OEM configuration of the Secure Manager.
OEM secrets are described in detail in the Secure Manager configuration.

During the SFI procedure, OEM shall pay attention on the following secrets:

  • Factory Internal Trusted Storage (ITS)
    • The OEM can change the factory ITS blob default content to include its own keys and data
  • Secure Manager keys
    • the OEM must update the default Secure Manager keys and use their own keys.
  • Secure Modules configuration
    • The OEM must set the license type for each module (no license, global license or chip specific license)
    • The OEM must set the licensed modules installation model (same model for all licensed modules)
    • The OEM must set the secure SRAM size used by the modules (one secure SRAM area shared between all the modules)
  • Option Bytes
Warning white.png Warning
The Flash Memory configuration to install via the SFI procedure must be the same than the one used during the OEM application development.
2.1.2.3. SFI image output description

The Trusted Package Creator encrypts the SFI images inputs with the OEM key and generates a SFI image. The SFI image is then an encrypted image containing the Secure Manager, the OEM application, the OEM secrets and the modules.

2.1.2.4. SFI image generation

In order to ease the creation of the SFI image used in manufacturing, the OEM must complete the nonsecure application development. To do so, the OEM must use the SMAK in production preparation phase.

The output of the SMAK production preparation phase is the SFI image ready to be install in manufacturing.

2.1.3. OEM key provisioning

The OEM (via the Trusted Package Creator) must program its OEM key in a HSM or in a global license.

By this way:

  • Only STMicroelectronics STM32 microcontrollers can securely install the SFI image.
  • Authenticity, integrity, and confidentiality of the SFI image content is ensured

Using HSM allows to count the number of STM32 chips to program.


2.2. Installation flow

There is one additional input compared to other platforms: the module license information
It indicates if the module is licensed or not.
In case the module is licensed, it either gives the module global license file or it indicates the module ID in HSM in case of module chip specific license.

The installation procedure is similar to generic SFI installation procedure deployed on other STM32 product when SFI is supported.


Info white.png Information
You can refer to AN4992 §6 "SFI image programming by OEMs or CMs" for an overview of the SFI image programming.

2.3. Step by Step SFI procedure

Please follow How to start SFI on STM32H5 with Secure Manager to run a SFI procedure on STM32H5 with Secure Manager.

3. OEM applications developed without Secure Manager

The SFI procedure on the STM32H5 series is similar to the SFI procedure applied on other platforms. Please follow SFI Step-by-step on STM32 boards to run an SFI procedure on STM32H5 without Secure Manager.

4. References