1. Introduction
The Secure Manager Access Kit (SMAK) provides an environment where users can:
- Develop nonsecure applications that use the Secure Manager services.
- Prepare the final encrypted images used for OEM secure manufacturing.
The SMAK details are described in the next chapters.
2. Architecture
2.1. Ecosytem Architecture
The SMAK ecosystem is composed of:
- The Secure Manager binary, available as an encrypted image from STM32TRUSTEE-SM[1].
- The image is delivered with the software license agreement SLA0048[2].
- It can be used for production purposes.
- The STM32Cube embedded firmware package available from STM32CubeH5 [3], containing:
- Scripts to configure and install the Secure Manager, relying on STM32TrustedPackageCreator and STM32CubeProgrammer tools.
- Template and example projects( for STM32CubeIDE [4], KEIL[5] and IAR[6]) to develop nonsecure application using Secure Manager services. They contain pre-integrated prebuild and postbuild scripts relying on STM32TrustedPackageCreator to generate signed and encrypted image, and download scripts relying on STM32CubeProgrammer to flash nonsecure application image.
- STM32TrustedPackageCreator and STM32CubeProgrammer[7], for above needs.
- STM32CubeMX[8], to generate nonsecure application projects for Secure Manager.
- IDEs (STM32CubeIDE[4], IAR[6] or KEIL[5])
The following diagram presents the SMAK ecosystem architecture.
2.2. Software architecture
The Secure Manager is executed in secure processing environment (SPE).
It is composed of the STiRoT, STuRoT plus the Secure Manager.
It is responsible for Secure Boot and Secure Firmware Update, and it provides secure services to nonsecure (NS) applications at runtime.
The Secure Manager is composed of:
- A 2-level Root of Trust
- An immutable Root of Trust (STiRoT)
- An updatable Root of Trust (STuRoT)
- The Secure Manager Core
- Secure Services such as
- Cryptography
- Initial attestation
- Trusted storage
- Firmware update
Additionally, trusted applications, also called Secure Modules, can be added by the user, but are not part of the Secure Manager.
The following figure describes the Secure Manager software architecture.
For more information about each Secure Manager components (STuRoT, Secure Manager Core...), please refer to Secure Manager components.
3. Security model
3.1. Stakeholders
The stakeholders involved in the security model are:
- STMicroelectronics, who owns the Secure Manager.
- The OEM who owns the nonsecure application and possibly Secure Modules, and is responsible for the system integration.
- Optionally, third-party Secure Module owners who own Secure Modules.
3.2. Asset confidentiality
The Secure Manager ensures stakeholders asset confidentiality by protecting:
- Secure Manager assets against the Secure Modules and nonsecure application.
- Secure Module assets against the nonsecure application and other Secure Modules.
- Nonsecure application assets against Secure Modules using the internal trusted storage (ITS) service.
3.3. Multi-tenant IP protection
The Secure Manager supports multi-tenant IP protection, meaning that each Secure Module (from the OEM or third-party) is isolated from the others using sandboxes.
3.4. PSA level 3 isolation
The security model is based on PSA level 3 isolation, ensuring that the secure domain is isolated from nonsecure domain. This means that the Secure Manager and Secure Modules are protected from access by any nonsecure applications (hardware and software).
This isolation also ensures that privileged secure domain is separated from unprivileged secure domain, meaning that the Secure Manager Core is protected from access by secure services and Secure Modules.
Additionally, it ensures that the secure partitions are fully isolated. This means that each secure partition (secure services and Secure Modules) is sandboxed and can only access its own resources. This protects each secure partition from access by other secure partitions, and it provides protection for the Secure Manager Core.
3.5. Type of assets
The following table describes which types of assets are protected.
Code asset | Volatile data asset | Nonvolatile data asset | ITS data | Peripherals | |
---|---|---|---|---|---|
Secure Manager | Yes | Yes | Yes | Yes | Yes |
Secure Module | Yes | Yes | Yes | Yes | Yes |
nonsecure application | Yes | Yes | Yes | Yes | Partially (see note below) |
4. Feature overview and secure services
The Secure Manager is responsible for supplying secure services at boot-time and runtime.
The boot-time services are available after a power-on or system reset and are responsible of secure boot and secure firmware update.
The runtime secure services can be used by nonsecure applications running on nonsecure domain, as well as other secure modules running on secure domain. These services are defined by the PSA standard.
The following services are supported:
- PSA cryptography: supplies cryptographic services, such as authentication or encryption, based on hardware cryptographic acceleration with side-channel resistance.
- PSA internal trusted storage (ITS): supplies services for storing the most important assets (such as keys and data) in the internal flash memory, ensuring integrity, and confidentiality. Be aware that ITS file system is encrypted.
- PSA attestation: supplies services to authenticate a device. To do this, a unique signed token is generated for each device, which can be later authenticated by a server.
- PSA firmware update: supplies services to download new firmware images and perform image updates.
The Secure Manager also supports firmware installations and updates, based on direct image download in the download slot (this feature must be enabled using OEM Secure Manager configuration parameter) instead of PSA firmware update API.
4.1. PSA services
4.1.1. PSA cryptography service
4.1.1.1. Description
This service provides an implementation of the PSA cryptography API as defined in the Arm PSA Cryptography API document[9].
Cryptographic algorithms implementation relies on cryptographic hardware accelerator peripherals of the device (PKA, SAES, HASH, TRNG) whenever possible. The table below lists the supported functionalities, as well as the protections they implement.
4.1.1.2. Services
The main services are:
- Library management
- Library (PSA cryptography service) initialization
- Key management
- Opaque key identifiers
- Key lifetimes (volatile, persistent)
- Key policy
- Key import, generation, derivation, and copy
- Symmetric cryptography
- Message digests (Hash)
- Message authentication codes (MAC)
- Encryption and decryption
- Authenticated encryption (AEAD)
- Key derivation
- Asymmetric cryptography
- Asymmetric encryption
- Hash and sign
- Key agreement
- Randomness
The following table describes the implemented operations, algorithms, and key lengths.
Operations | Algorithms | Key lengths | Modes | Implementation | SCA/DPA resistant | Fault resistant |
---|---|---|---|---|---|---|
Get entropy | TRNG | N/A | N/A | Hardware | N/A | N/A |
Encryption, decryption | AES | 128, 256 | ECB, CBC, CTR, CFB | Hardware | YES | YES |
Authenticated encryption, decryption | AES | 128, 256 | GCM, CCM | Hardware | YES | YES |
Cipher-based message authentication code | AES | 128 | CMAC | Hardware | YES | YES |
Cryptographic hash | SHA-11 | N/A | Digest 160-bit | Hardware | N/A | N/A |
Cryptographic hash | SHA-2 | N/A | SHA-224, SHA-256, SHA-384, SHA-512 | Hardware | N/A | N/A |
Keyed hashing for message authentication | HMAC-SHA2-224 | Short, long (>64 bytes) | N/A | Hardware | N/A | YES |
Keyed hashing for message authentication | HMAC-SHA2-256 | Short, long (>64 bytes) | N/A | Hardware | N/A | YES |
Keyed hashing for message authentication | HMAC-SHA2-384 | Short, long (>64 bytes) | N/A | Hardware | N/A | YES |
Keyed hashing for message authentication | HMAC-SHA2-512 | Short, long (>64 bytes) | N/A | Hardware | N/A | YES |
Asymmetric encryption | RSA | 2048, 3072 | RSAES-OAEP, RSASSA-PKCS1-V1_5 | Hardware | YES | YES |
Signature with hashing signature verification | RSA | 2048, 3072 | RSASSA-PKCS1-v1_5, RSASSA-PSS | Hardware | YES | YES |
Signature with hashing signature verification | ECDSA | Up to 521 | List of supported hardware ECC curves below2 | Hardware | YES | YES |
Key agreement | ECDH | Up to 521 | List of supported ECC curves below2 | Hardware | YES | YES |
Encryption, decryption | DES1 | 128, 256 | ECB, CBC | Software | NO | NO |
Encryption, decryption | Triple DES | 128, 256 | ECB, CBC | Software | NO | NO |
Key derivation | HMAC-based | N/A | N/A | Hardware | YES | YES |
- Weak - not recommended.
- The following elliptic curves are supported: secp224r1, secp256r1, secp384r1, secp521r1, secp256k1, bp256r1, bp384r1, and bp512r1. secp192r1 and secp192k1 are also supported, but not recommended.
Note:
All implementations that manipulate private keys are protected against side-channel and timing attacks.
4.1.1.3. Pre-provisioned DUA user key
To ease OEM manufacturing, STMicroelectronics has pre-provisioned STM32 devices with a unique asymmetric key pair for user purpose. This ECC key pair is accessible through the PSA crypto API using a specific key ID.
The following services are available:
- Sign with the DUA user private key.
- Export the DUA user public key.
4.1.2. PSA initial attestation service
4.1.2.1. Description
This service provides an implementation of the PSA initial attestation API, described in the PSA Attestation API document[10].
The service allows the application to prove the device identity during an authentication process to a verification entity. The initial attestation service can create a entity attestation token (EAT) on request, which contains a fix set of device specific data.
The EAT is encoded according to the CBOR format and signed according to COSE standard.
To ease OEM manufacturing, STMicroelectronics has pre-provisioned for each device an ECC asymmetric unique key pair and a certificate used for device unique authentication. It is called DUA initial attestation key. It is dedicated and used by the PSA initial attestation service to sign the token.
The table below lists the fields contained in the EAT.
Claim | Mandatory | Description | Value | Implemented |
---|---|---|---|---|
Auth challenge | Yes | Authenticated challenge is an input object of the caller (user who request the token). | 32, 48 or 64 bytes length. Value is provided by the caller. | Yes |
Instance ID | Yes | Unique identifier of the device instance. | Concatenation of 0x1 and the hash of the public key used for initial attestation (DUA initial attestation key). | Yes |
Verification service indicator | No | A hint used by a relying party to locate a validation service for the token | N.A. | No |
Profile definition | No | Name of a document that describes the profile of the report | N.A. | No |
Implementation ID | Yes | Unique identifier of the underlying immutable PSA RoT. | ST immutable firmware (ROM) version (32 bytes in STM32 system flash at address 0x0BF96000). | Yes |
Client ID | Yes | Partition ID of the caller (application who requested the token). | Signed 32-bits. -1 for NSPE firmwares. Application Service Identifier (ASID) of the secure service or secure module for SPE firmwares. | Yes |
Security life cycle | Yes | Current life cycle state of the PSA RoT. | Product state Closed (SL_SECURED) or TZ-Closed (SL_NON_PSA_ROT_DEBUG). | Yes |
Hardware version | No | Metadata linking the token to the GDSII that went to fabrication for this instance. | String encoded from the DBGMCU IDCODE register. | Yes |
Boot seed | Yes | Random value created at system boot time. | Random number. | Yes |
Software components | Yes | A list of software components that represent all software managed by the PSA RoT | See table below. | Yes |
The table below lists the fields contained in each Software component.
Software component fields | Mandatory | Description | Value | Implemented |
---|---|---|---|---|
Measurement type | No | A short string representing the role of this software component. | String. "BL" for STuRoT, "SPE" for Secure Manager, "ARoT" for a Secure Module, "NSPE" for nonsecure application | Yes |
Measurement value | Yes | The hash of the invariant software component in memory at startup time. | 32 bytes. SHA256 of the software component. | Yes |
Version | No | The issued software version in the form of a text string. | String encoded in CBOR. For example "1.0.0" | Yes |
Signer ID | No | The hash of a signing authority public key for the software component. | 32 bytes. SHA256 of this public key. | Yes |
Measurement description | No | Represents the way in which the measurement value of the software component is computed. | ASCII string. "SHA256" | Yes |
The following figure displays an example of a decoded token, using the iat-verifier tool from the trustedfirmware middleware. This token was generated with the configuration:
- Authenticated challenge from the user (caller): null value of 32 bytes
- Token get from the nonsecure application (caller): negative Client ID value ('-1')
- Product State TZ-Closed ('SL_NON_PSA_ROT_DEBUG')
- Components installed: STuRoT ('BL'), Secure Manager ('SPE'), nonsecure application ('NSPE') and an OEM module application ('ARoT')
4.1.2.2. Services
The main services are:
- Get token size (useful to allocate the right buffer size to get the token).
- Get token.
4.1.3. PSA internal trusted storage service
4.1.3.1. Description
This service provides an implementation of the PSA internal trusted storage (ITS) API defined in the Arm PSA Secure Storage API document [11].
It allows the writing of data in the microcontroller built-in flash memory region that is isolated from the nonsecure application and from other secure services by hardware security protection mechanisms. It provides a nonhierarchical storage model (like a file system), where a linearly-indexed list of metadata manages all the assets. The data are generally small pieces of data (such as private key, credentials).
ITS includes the following functionalities:
- Confidentiality: the data are located in a secure area, protected from unauthorized access by hardware isolation (TZ, MPU) of the flash memory access domain. Data are encrypted using a symmetric algorithm and a unique STMicroelectronics 256-bit key.
- Access control: a specific mechanism establishes the identity of the requester (a nonsecure entity, a secure entity, or a remote server).
- Integrity: the internal flash memory device provides resistance to hardware physical access attacks.
- Reliability: ITS provides resistance to power failure scenarios and incomplete write cycles.
- Configurability: ITS size can be configured by the OEM based on Secure Manager memory configuration selection. Additional ITS size are considered in ST roadmap.
4.1.3.2. Services
The main ITS services are:
- Set data in the ITS area (data are identified by a unique identifier (UID)).
- Get data from the ITS area.
- Remove data from the ITS area.
- Get data information (metadata).
Manipulated objects (data) can be data or keys. The metadata contain the data size and some attributes that define how they can be accessed (immutable, public...).
Each data is associated with a owner ID. The nonsecure application owner ID is 0xFFFFFFFF. The Secure Service (respectively Secure Module) owner ID is the ASID of the Secure Service (respectively Secure Module). The ASID is encoded with 32 bits.
A data can be accessed only by the data owner (Owner ID) unless the data is declared as public.
When data are provisioned using ITS builder tool, the supported key format is limited (for details, see ITS builder documentation in STM32CubeH5 [3] at ./Utilities/PC_Software/ITSbuilder/README.md).
4.1.3.3. ITS provisioning
The ITS can be provisioned in two ways:
- The first way is to use the PSA internal trusted storage API to provision data and keys in the ITS. In this case, it is the nonsecure application that performs the provisioning at runtime (generally during the OEM manufacturing phase).
- The second way is to use Factory Internal Trusted Storage provisioning. The OEM prepares the data and keys to provision, using the STMicroelectronics ITS builder tool (on a PC). This tool generates an encrypted and authenticated blob (using OEM keys used for nonsecure application preparation) containing the data and keys. The OEM can later install this blob in a secure way during production (the encrypted blob is programmed during production but blob installation and initialization in ITS filesystem is done at the first product power on).
For more information on ITS builder, refer to ITS builder documentation in STM32CubeH5 [3] at ./Utilities/PC_Software/ITSbuilder/README.md.
Notes:
- In the current Secure Manager memory configurations, the blob size is limited to 8 KB.
- The maximum data and key size is 2016 bytes.
- The installed data and keys can only be used by the nonsecure application, using the PSA internal trusted storage API.
4.1.4. PSA firmware update service
4.1.4.1. Description
This service provides an implementation of the PSA firmware update API defined in the PSA Firmware Update API document [12]. It provides a standard and platform agnostic interface for firmware updates.
The firmware update scheme is based on a dual slot: one active slot and one download slot. The active slot is used to execute the firmware and the download slot used to download the new image to be installed.
The following images can be updated:
- Nonsecure application
- STuRoT
- Secure Manager
- Secure Modules (each independently)
The installation flow is as follows:
- The nonsecure application (update agent) gets information about the installed images (name, installation status, version, etc.).
- It downloads the image to the secure download slot.
- It requests image installation
- It resets the device to execute the secure boot stages (STiRoT and STuRoT) that performs the installation in the active slot and jumps to the non-secure application.
- The non-secure application must accept the image using its specific acceptation criteria (non secure application dependent)
- If the acceptation criteria is met, the nonsecure application informs the firmware update service that the image is accepted.
- If the acceptation criteria is not met, the nonsecure application generates a reboot. The secure boot stages are executed, set the image to rejected state, and performs a rollback to the previous valid image which was swapped in the download slot.
During the installation, the image in active and download slots changes states. The possible states are:
State | Value | Description |
---|---|---|
UNDEFINED | 0x0 | Empty download slot. Or download slot containing a former image whereas new image on the active slot has been successfully installed. |
CANDIDATE | 0x1 | Image candidate present in the download slot. |
INSTALLED | 0x2 | Image accepted by the nonsecure application (update agent) in the active slot. |
REJECTED | 0x3 | Image not accepted by the nonsecure application (update agent), swapped back to download slot. |
PENDING_INSTALL | 0x4 | Image candidate in the active slot, waiting for image acceptance from the nonsecure application (update agent). |
REBOOT_NEEDED | 0x5 | Reboot is needed to finalize the image candidate swap from download slot to active slot. |
The image installation (swap) is resistant to asynchronous power down and system reset. Nevertheless, to be noticed that if a power down occurs whereas the new image has not been completely written to the download slot, the image installation process must be restarted.
4.1.4.2. Services
The services are:
- Get image information (state, version, digest) for an image ID.
- Write image to the download slot (staging area) (image state "CANDIDATE").
- Request the installation of the downloaded image and inform the client that a reboot is required to execute the secure boot stages (image state "REBOOT_NEEDED").
- Reboot the device to execute secure boot stages:
- If there is an image to install in the download slot, the secure boot stage installs the image (image state "PENDING_INSTALL") during the boot. If the image to install is not valid image, the image is not installed and is erased from the staging area (image state "UNDEFINED").
- Accept the image. The image is fully installed and becomes the new valid image (image state "INSTALLED").
An image ID is composed of a slot ID and a type ID.
The slot ID indicates if the image is located in the download or active slot.
The type ID indicates the type of image as described in below table.
Type ID | Description |
---|---|
NONSECURE | nonsecure application |
BL | STuRoT |
SECURE | Secure Manager |
MODULE0 | Secure Module 0 |
4.2. Other services
4.2.1. Power-on and system reset
After each product power-on or reset, the platform starts to execute the Secure Manager root of trust (STiRoT, STuRoT, and Secure Manager) that manages the secure initialization of the platform. If a candidate STuRoT image is present in the STuRoT download slot, STiRoT performs the installation in the STuRoT active slot. If a candidate Secure Manager, nonsecure application, or Secure Module image is present in the respective download slot, STuRoT performs the installation in the respective active slot.
4.2.2. Firmware update with direct writing to download slot
The OEM can configure the Secure Manager in a way that it jumps to the system bootloader when there is no valid image in at least one of the active slot (nonsecure application, STuRoT, Secure Manager, or Secure Module). In this case, the OEM can use the system bootloader to download an encrypted image in the download slot. After a reset, the Secure Manager detects the downloaded image and performs the installation if the image is valid.
This service can be used to update STuRoT, Secure Manager, the nonsecure application, or a Secure Module.
4.2.3. Certificate utility
Two STMicroelectronics certificates are provisioned in the STMicroelectronics device system flash memory. They are both used for the device unique authentication (DUA). The DUA initial attestation certificate is used for Initial Attestation purposes, for example the authentication with a cloud. The DUA user certificate is used for user purposed, for example create a secure communication (TLS).
The certificate utility supplies the following services:
- Get DUA certificate size based on certificate ID.
- Get DUA certificate (X509 format) based on certificate ID.
The X509 certificate can be visualized with openssl from a terminal. For X509 certificate details, please refer to rfc2459.
The table below lists the fields contained in the X509 certificate (DUA initial attestation or DUA user certificates).
Claim | Description |
---|---|
Version | Version of x509 format supported. |
Serial Number | Unique number that identify each certificate and is issued by a certificate authority (CA). |
Signature Algorithm | The value and algorithm of the certificate signature delivered by the certificate authority (CA). |
Issuer | Identifies the certification authority that issued the certificate. |
Validity | Validity period of the certificate with a start and end date. |
Subject | Identify the entity associated to the certificate. |
Public Key | Contains the public key of the entity associated to the certificate. |
Subject Public Key info | Information about the public key (size, curve, algorithm) |
Extension | Provides additional information about the certificate such as access permissions or usage restrictions. |
The figure below present an example of DUA Initial Attestation certificate visualized with openssl.
The figures below present an example of DUA User certificate visualized with openssl.
5. Interfaces
This chapter describes the interfaces supplied by the Secure Manager to develop a nonsecure application.
The details of the interfaces are described in the header files of the Secure Manager API middleware (./Middlewares/ST/secure_manager_api/) and in the Secure Manager API documentation (./Middlewares/ST/secure_manager_api/SecureManagerAPI.chm).
5.1. PSA interfaces
5.1.1. PSA cryptography service
5.1.1.1. Overview
The PSA cryptography service interface is described in the Arm PSA Cryptography API document[9].
To use this interface, the application must include the psa/crypto.h header file.
5.1.1.2. Function list
Function | Description | Comment |
---|---|---|
psa_aead_decrypt() | Process an authenticated decryption operation. | |
psa_aead_encrypt() | Process an authenticated encryption operation. | |
psa_aead_operation_init() | Return an initial value for an AEAD operation object. | |
psa_asymmetric_decrypt() | Decrypt a short message with a private key. | |
psa_asymmetric_encrypt() | Encrypt a short message with a public key. | |
psa_cypher_abort() | Abort a cipher operation(). | |
psa_cipher_decrypt() | Decrypt a message using a symmetric cipher. | |
psa_cipher_decrypt_setup() | Set the key for a multipart symmetric decryption operation. | |
psa_cipher_encrypt() | Encrypt a message using a symmetric cipher. | |
psa_cipher_encrypt_setup() | Set the key for a multipart symmetric encryption operation. | |
psa_cipher_finish() | Set the key for a multipart symmetric decryption operation. | |
psa_cipher_generate_iv() | Generate an initialization vector (IV) for a symmetric encryption operation. | |
psa_cipher_operation_init() | Return an initial value for a cipher operation object. | |
psa_cipher_set_iv() | Set the initialization vector (IV) for a symmetric encryption or decryption operation. | |
psa_cipher_update() | Encrypt or decrypt a message fragment in an active cipher operation. | |
psa_close_key() | Close a key handle. | |
psa_copy_key() | Make a copy of a key. | |
psa_crypto_init() | Library initialization. | |
psa_destroy_key() | Destroy a key. | |
psa_export_key() | Export a key in binary format. | |
psa_export_public_key() | Export a public key or the public part of a key pair in binary format. | |
psa_generate_key() | Generate a key or key pair. | |
psa_generate_random() | Generate random bytes. | |
psa_get_key_algorithm() | Retrieve the permitted algorithm policy from key attributes. | |
psa_get_key_attributes() | Retrieve the attributes of a key. | |
psa_get_key_bits() | Retrieve the key size from key attributes. | |
psa_get_key_id() | Retrieve the key identifier from key attributes. | |
psa_get_key_lifetime() | Retrieve the lifetime from key attributes. | |
psa_get_key_type() | Retrieve the key type from key attributes. | |
psa_get_key_usage_flags() | Retrieve the usage flags from key attributes. | |
psa_hash_abort() | Abort a hash operation. | |
psa_hash_clone() | Clone a hash operation. | |
pa_hash_compare() | Calculate the hash (digest) of a message and compare it with a reference value. | |
psa_hash_compute() | Calculate the hash (digest) of a message. | |
psa_hash_finish() | Finish the calculation of the hash of a message. | |
psa_hash_operation_init() | Return an initial value for a hash operation object. | |
psa_hash_setup() | Set up a multipart hash operation. | |
psa_hash_update() | Add a message fragment to a multipart hash operation. | |
psa_hash_verify() | Finish the calculation of the hash of a message and compare it with an expected value. | |
psa_import_key() | Import a key in binary format. | |
psa_key_attributes_init() | Return an initial value for a key attribute object. | |
psa_key_derivation_abort() | Abort a key derivation operation. | |
psa_key_derivation_get_capacity() | Retrieve the current capacity of a key derivation operation. | |
psa_key_derivation_input_bytes() | Provide an input for key derivation or key agreement. | |
psa_key_derivation_operation_init() | Return an initial value for a key derivation operation object. | |
psa_key_derivation_output_bytes() | Read some data from a key derivation operation. | |
psa_key_derivation_output_key() | Derive a key from an ongoing key derivation operation. | |
psa_key_derivation_set_capacity() | Set the maximum capacity of a key derivation operation. | |
psa_key_derivation_setup() | Set up a key derivation operation. | |
psa_mac_abort() | Abort a MAC operation. | |
psa_mac_compute() | Calculate the message authentication code (MAC) of a message. | |
psa_mac_operation_init() | Return an initial value for a MAC operation object. | |
psa_mac_sign_finish() | Finish the calculation of the MAC of a message. | |
psa_mac_sign_setup() | Set up a multipart MAC calculation operation. | |
psa_mac_update() | Add a message fragment to a multipart MAC operation. | |
psa_mac_verify() | Calculate the MAC of a message and compare it with a reference value. | |
psa_mac_verify_finish() | Finish the calculation of the MAC of a message and compare it with an expected value. | |
psa_mac_verify_setup() | Set up a multipart MAC verification operation. | |
psa_open_key() | Open a handle to an existing persistent key. | |
psa_purge_key() | Remove nonessential copies of key material from memory. | |
psa_reset_key_attributes() | Reset a key attribute object to a freshly initialized state. | |
psa_set_key_algorithm() | Declare the permitted algorithm policy for a key. | |
psa_set_key_bits() | Declare the size of a key. | |
psa_set_key_id() | Declare a key as persistent and set its key identifier. | |
psa_set_key_lifetime() | Set the location of a persistent key. | |
psa_set_key_type() | Declare the type of a key. | |
psa_set_key_usage_flags() | Declare usage flags for a key. | |
psa_sign_hash() | Sign an already-calculated hash with a private key. | |
psa_sign_message() | Sign a message with a private key. For hash-and-sign algorithms, this includes the hashing step. | |
psa_verify_hash() | Verify the signature of a hash or short message using a public key. | |
psa_verify_message() | Verify the signature of a message with a public key, using a hash-and-sign verification algorithm. |
5.1.1.3. Pre-provisioned DUA user key
The following interfaces are available to access this key:
Function | Description |
---|---|
psa_open_key() | Open a handle to an existing persistent key (DUA user key ID). |
psa_close_key() | Close a key handle. |
psa_export_public_key() | Export a public key. |
psa_sign_hash() | Sign an already-calculated hash with a private key. |
psa_sign_message() | Sign a message with a private key. For hash-and-sign algorithms, this includes the hashing step. |
5.1.1.4. Configuration
No specific configuration is required.
5.1.2. PSA initial attestation service
5.1.2.1. Overview
The PSA initial attestation service interface is described in the Arm PSA Attestation API document[10].
To use this interface, the application must include the psa/initial_attestation.h header file.
5.1.2.2. Function list
The following interface functions are implemented:
Function | Description |
---|---|
psa_initial_attestation_get_token() | Get the initial attestation token. |
psa_initial_attestation_get_token_size() | Get the size of the initial attestation token. |
5.1.2.3. Configuration
No specific configuration is required, because the EAT key (DUA initial attestation key) is pre-provisioned by STMicroelectronics.
5.1.3. PSA internal trusted storage service
5.1.3.1. Overview
The PSA internal trusted storage service interface is described in the Arm PSA Secure Storage API document[11].
To use this interface, the application must include a psa/internal_trusted_storage.h header file.
5.1.3.2. Function list
The following interface functions are implemented:
Function | Description |
---|---|
psa_its_set() | Create a new or modify an existing UID/value pair. |
psa_its_get() | Get data associated with a provided UID. |
psa_its_get_info() | Get the metadata for the provided UID. |
psa_its_remove() | Remove the UID and associated data. |
5.1.3.3. Configuration
No specific configuration is required.
5.1.3.3.1. ITS file system size
The ITS file system is in internal user flash memory. Its size must be a multiple of the flash memory sector size.
The Secure Manager predefined memory configuration defines the size of the Factory ITS area and the size of the ITS file system area.
The following table gives an estimation of the maximum ITS user data size, according to ITS file system area size.
ITS file system size (KB) | ITS user data size (KB) |
---|---|
40 | 19 |
The following table gives an estimation of the maximum ITS user data size, according to the Secure Manager predefined memory configuration.
Secure Manager memory configuration | ITS file system size (KB) | ITS user data size (KB) |
---|---|---|
SMAK_0 | 40 | 19 |
SMAK_1 | 40 | 19 |
5.1.3.4. Tips
- The maximum data size supported by the ITS is 2016 bytes.
- The maximum number of data supported by the ITS is 150.
- ITS service does not implement replay protection.
- The PSA storage API flags PSA_STORAGE_FLAG_NO_CONFIDENTIALITY and PSA_STORAGE_FLAG_NO_REPLAY_PROTECTION are not supported.
5.1.4. PSA firmware update service
5.1.4.1. Overview
The PSA firmware update service interface is described in the Arm PSA firmware update API document[12].
To use this interface, the application must include the psa/update.h header file.
5.1.4.2. Function list
The following interface functions are implemented:
Function | Description |
---|---|
psa_fwu_query() | Returns information for an image of a particular image ID. |
psa_fwu_write() | Writes an image to the staging area (download slot). |
psa_fwu_install() | Starts the installation of an image. |
psa_fwu_request_reboot() | Requests the platform to reboot. |
psa_fwu_accept | Indicates to the implementation that the upgrade was successful. |
psa_fwu_abort | Abort a firmware update procedure. |
5.1.4.3. Configuration
No specific configuration is required.
5.2. Other interfaces
5.2.1. Power-on and system reset
After each product power-on or reset, the platform starts to execute STiRoT, STuRoT, and the Secure Manager that manages the secure initialization of the platform. If a candidate STuRoT image is present in the STuRoT download slot, STiRoT installs it in the STuRoT active slot. If a candidate Secure Manager, nonsecure application, or Secure Module image is present in the respective download slot, STuRoT installs it in the respective active slot.
Method of use:
- Power-on the STM32H5 device.
- Or reset the STM32H5 device.
5.2.1.1. Interface description
Parameters:
- Not applicable.
Actions:
- Power-on or system reset.
- STiRoT is executed. STiRoT performs the installation of the STuRoT image (if required) and jumps to STuRoT after an integrity and authenticity verification. STuRoT installs the Secure Manager, Secure Module, and nonsecure application images (if required) and jumps to the Secure Manager after an integrity and authenticity verification.
- If the integrity and authenticity verification is passed, the Secure Manager jumps to the nonsecure application.
- If the integrity and authenticity verification fails, the Secure Manager jumps to the system bootloader or performs a system reset (depending on the OEM configuration).
Errors:
- The platform resets in the event of any of the following errors:
- Violation (unexpected value) of the STM32H5 option byte values related to platform security.
- STiRoT- or STuRoT-provisioned data error (data integrity failure or wrong value).
- Internal tamper event.
- If the "jump to system bootloader" configuration is disabled (OEM configuration as defined in Secure Manager configuration chapter), the platform resets in the event of any of the following errors:
- The STuRoT active slot image is not controlled successfully (authenticity and integrity).
- The Secure Manager active slot image is not controlled successfully (authenticity and integrity).
- The nonsecure application active slot image is not controlled successfully (authenticity and integrity).
- The module(s) active slot image is not controlled successfully (authenticity and integrity).
- If the "jump to system bootloader" configuration is enabled (OEM configuration as defined as Secure Manager configuration chapter), the platform jumps to the system bootloader in the event of any of the following errors:
- The STuRoT active slot image is not controlled successfully (authenticity and integrity).
- The Secure Manager active slot image is not controlled successfully (authenticity and integrity).
- The nonsecure application active slot image is not controlled successfully (authenticity and integrity).
- The module(s) active slot image is not controlled successfully (authenticity and integrity).
5.2.2. Firmware update with direct writing to download slot
The SMAK templates and examples generate two types of encrypted and signed binary.
First binary type (.bin) contains encrypted and signed binary without 16-bytes magic word neither pre-acceptation information. This binary is used for firmware installation using PSA firmware update API
Second binary type (.hex) contains encrypted and signed binary with 16-bytes magic word and pre-acceptation information. This type (.hex) also contains programming address. This binary is used for firmware update with direct writing to download slot. This binary type is the relevant one for this chapter.
5.2.2.1. STuRoT image download slot interface
This interface is only available if the integrator selects the Secure Manager configuration that enables the system bootloader to act as the local loader for STiRoT (see Secure Manager configuration chapter).
Method of use:
- To use the STuRoT image download slot, the system bootloader must be entered. For this, at least one of the STuRoT, Secure Manager, nonsecure application, or Secure Module active slots must contain an invalid image.
- The data must then be written in the correct image format in the STuRoT image download slot, and the 16-byte magic word must be written in the slot area end location. (This magic word is used by STiRoT to detect that an image to be processed is present in the download slot).
5.2.2.1.1. Interface description
Parameters:
- The candidate STuROT image to be written in the STuROT image download slot.
Actions:
- System reset:
- At each system reset, the Secure Manager (STiRoT) checks if a new STuROT candidate image is present in the STuROT image download slot. Only STMicroelectronics can generate a new valid STuROT image.
- When a new valid STuROT image is detected, the STiRoT component updates the STuROT image in the STuROT image active slot.
Errors:
- The STuROT candidate image is not installed in the STuROT image active slot and is erased from the STuROT image download slot in the event of any of the following errors:
- The STuROT image size is inconsistent.
- Flash memory reading errors (double ECC errors).
- Version check failure: the STuROT image version is lower than the previously installed image.
- STuROT image integrity failure.
- STuROT image signature failure (image not authentic).
- The candidate STuROT image is not installed in the STuROT image active slot and the platform resets in the event of the following error:
- Flash memory writing or erasing errors are reported by the flash memory driver used to write data in the STuROT image active slot area.
5.2.2.2. Secure Manager image download slot interface
This interface is only available if the integrator selects the STuROT configuration that enables the system bootloader to act as the local loader for STuROT (see Secure Manager configuration chapter).
Method of use:
- To use the Secure Manager image download slot interface, the system bootloader must be entered. For this, at least one of the STuROT, Secure Manager, nonsecure application, or Secure Module active slot must contain an invalid image.
- The data must then be written in the correct image format in the Secure Manager image download slot, and the 16-byte magic word must be written in the slot area end location.
5.2.2.2.1. Interface description
Parameters:
- The candidate Secure Manager image to be written in the Secure Manager download slot.
Actions:
- System reset:
- At each system reset, the platform (STuROT) checks if a new Secure Manager image is present in the Secure Manager image download slot. Only STMicroelectronics can generate a new valid Secure Manager image.
- When a new valid Secure Manager image is detected, the STuROT updates the Secure Manager image in the Secure Manager image active slot.
Errors:
- The Secure Manager candidate image is not installed in the Secure Manager image active slot in the event of the following error:
- Version dependency failure: the version of the Secure Manager image is incompatible with the version of another image (nonsecure application or Secure Module image).
- The candidate image is not installed in the Secure Manager image active slot and is erased from the Secure Manager image download slot in the event of any of the following errors:
- The Secure Manager image size is inconsistent.
- Flash memory reading errors (double ECC errors).
- Version check failure: the Secure Manager image version is lower than the previously installed image.
- Secure Manager image integrity failure.
- Secure Manager image signature failure (image not authentic).
- The candidate Secure Manager image is not installed in the Secure Manager image active slot, and the platform resets in the event of the following error:
- Flash memory writing or erasing errors are reported by the flash memory driver used to write data in the Secure Manager image active slot area.
5.2.2.3. nonsecure application image download slot interface
This interface is only available if the integrator selects the STuROT configuration that enables the system bootloader to act as the local loader for STuROT.
Method of use:
- The nonsecure application image download slot region is located according to the selected flash memory layout configuration.
- To use the nonsecure application image download slot interface, the system bootloader must be entered. For this, at least one of the STuROT, Secure Manager, nonsecure application, or Secure Module active slots must contain an invalid image.
- The data must then be written in the correct image format in the nonsecure application image download slot, and the 16-byte magic word must be written in the slot area end location.
5.2.2.3.1. Interface description
Parameters:
- The candidate nonsecure application image to be written in the nonsecure application download slot.
Actions:
- System reset:
- At each system reset, the platform (STuROT) checks if a new nonsecure application image is present in the nonsecure application image download slot. The PC tool STM32TrustedPackageCreator and the .xml file are delivered to the OEM for the generation of a nonsecure application binary image with the right format.
- When a new nonsecure application image is detected, STuRoT updates the nonsecure application image in the nonsecure application image active slot.
Errors:
- The nonsecure application candidate image is not installed in the nonsecure application image active slot in the event of the following error:
- Version dependency failure: the version of the nonsecure application image is incompatible with the version of another image (Secure Manager or Secure Module image).
- The candidate image is not installed in the nonsecure application image active slot and is erased from the nonsecure application image download slot in the event of any of the following errors:
- The nonsecure application image size is inconsistent.
- Flash memory reading errors (double ECC errors).
- Version check failure: the nonsecure application image version is lower than the previously installed image.
- nonsecure application image integrity failure.
- nonsecure application image signature failure (image not authentic).
- The candidate nonsecure application image is not installed in the nonsecure application image active slot and the platform resets in the event of the following error:
- Flash memory writing or erasing errors are reported by the flash memory driver used to write data in the nonsecure application image active slot area.
5.2.2.4. Modules image download slot interface
This interface is only available if the integrator selects the STuROT configuration that enables the system bootloader to act as the local loader for STuROT.
Method of use:
- The Secure Module image download slot region is located according to the selected flash memory layout configuration.
- To use the Secure Module image download slot interface, the system bootloader must be entered. For this, at least one of the STuROT, Secure Manager, nonsecure application, or Secure Module active slots must contain an invalid image.
- The data must then be written in the correct image format in the Secure Module image download slot, and the 16-byte magic word must be written in the slot area end location.
Parameters:
- The candidate Secure Module image to be written in the Secure Module download slot.
Actions:
- System reset
- At each system reset, the platform (STuROT) checks if a new Secure Module image is present in the Secure Module image download slot. The PC tool STM32TrustedPackageCreator and the xml file are delivered for the generation of a Secure Module binary image with the right format.
- When new Secure Module images are detected, the STuROT updates the Secure Module images in the Secure Module images active slot.
Errors:
- The Secure Module candidate images are not installed in the Secure Module image active slot in the event of the following error:
- Version dependency failure: the version of the Secure Module image is incompatible with the version of another image (Secure Manager or nonsecure application image).
- The candidate image is not installed in the Secure Module image active slot and is erased from the Secure Module image download slot in the event of any of the following errors:
- The Secure Module image size is inconsistent.
- Flash memory reading errors (double ECC errors).
- Version check failure: the Secure Module image version is lower than the previously installed image.
- Modules application image integrity failure.
- Modules application image signature failure (image not authentic).
- The candidate Secure Module image is not installed in the Secure Module image active slot and the platform resets in the event of the following error:
- Flash memory writing or erasing errors are reported by the flash memory driver used to write data in the Secure Module image active slot area.
5.2.3. X509 certificates for DUA
5.2.3.1. Overview
Two X509 certificates are provisioned in STMicroelectronics devices for DUA initial attestation and the DUA user. The interface is provided to access these certificates. The interface is described in ./Firmware/Utilities/Certificates/stm32_cert.h header file.
5.2.3.2. Function list
The following interface functions are implemented:
Function | Description | Comment |
---|---|---|
UTIL_CERT_GetCertificateSize() | Get certificate size. | DUA initial attestation or DUA user identifiers are used to select the certificate. |
UTIL_CERT_GetCertificate() | Get certificate (raw binary). | DUA initial attestation and DUA user are used to select the certificate. |
6. System consideration
This chapter describes the system requirements that must be met to develop a product based on the Secure Manager.
6.1. Resource sharing
The hardware resources (peripherals, memory) are shared between the nonsecure application, Secure Manager, and Secure Modules.
These resources can be:
- Allocated exclusively to the Secure Manager.
- Allocated exclusively to the nonsecure application.
- Allocated exclusively to a Secure Module (via the Secure Module header).
- Shared between the nonsecure application, Secure Manager, and Secure Module.
All resources not used by the Secure Manager are fully available for the nonsecure application, unless used by a Secure Module.
Note:
- It is the responsibility of the OEM to ensure that there are no conflicts between nonsecure application, Secure Manager, and Secure Modules.
6.1.1. Secure Manager resources
6.1.1.1. Memory
At boot time, the Secure Manager reserves some ranges of RAM and user flash for its own usage.
These ranges are allocated to Secure Manager up to next system reset, except:
- RAM buffer dedicated to shared communication between the secure and nonsecure domain which is dynamically swapped from secure to nonsecure for communication purpose.
- User flash download slot which is allocated to nonsecure domain when the Secure Manager (STiRoT or STuRoT) jumps to the system bootloader when an invalid image has been detected.
6.1.1.2. Peripheral
The Secure Manager is executed in the secure domain and reserves some resources for its own usage.
The table below describes the reserved resources by Secure Manager.
Peripheral | Allocated to Secure Manager | Accessible by nonsecure application through a Secure Manager API | Comment |
---|---|---|---|
SAU, MPU_S | Yes | No | |
SYSTICK_S, NVIC_S | Yes | No | |
GTZC | Yes | No | |
RNG | Yes | PSA Crypto API | |
TAMP | Partly | No | The TAMP resource (from TAMP peripheral) is controlled by the Secure Manager. Other TAMP peripheral resources (monotonic counter 1...) are controlled by nonsecure application. |
PKA | Yes | PSA Crypto API | |
AES | Yes | No | |
SAES | Yes | PSA Crypto API | |
HASH | Yes | PSA Crypto API | |
FLASH | Partly | PSA ITS API, PSA firmware update API | The FLASH secure registers are only accessible by the Secure Manager. The FLASH nonsecure registers are only accessible by nonsecure application. |
I-CACHE | Yes | No | |
RAMCFG | Yes | No |
All other peripherals are available to nonsecure application unless reserved by Secure Modules.
If a Secure Module requires only some part of a given peripheral to be reserved, the whole peripheral will be marked secure and allocated to this Secure Module.
Exceptions:
- For GPIO, pins may be independently configured as secure or non-secure (pin by pin allocated to nonsecure application or Secure Module)
If a nonsecure application accesses unauthorized registers, the policy will be read as zero, write ignored.
6.2. Clocking
6.2.1. Clocking during device initialization
The system clock speed is constant during the whole device initialization (until the nonsecure application is entered), and is configurable by user, depending on the voltage supply and the range of temperature supported.
When starting, the nonsecure application can reconfigure the clocks, taking into account below considerations.
6.2.2. Clocking versus Secure Manager resources
There are no constraint on the system clock speed for the Secure Manager execution.
The source clocks of peripherals used by the Secure Manager can not be modified by nonsecure application.
However, the HSI48 clock can be modified by the nonsecure application, but must be kept enabled to ensure proper Secure Manager execution, as RNG peripheral (used by Secure Manager) uses it as source clock.
To ensure correct RNG behavior, the clock requirement described in RM0481[13] (chapter 32.3.6) must also be met (dependency between AHB bus clock and RNG clock).
6.2.3. Clocking versus Secure Module
Changing the system clock configuration and the peripheral clock configuration (enable, disable, reset) in the nonsecure application can affect the Secure Module peripheral behavior. The OEM must ensure that the system clock dependency requirement between the nonsecure application and Secure Modules is met.
6.3. Product state
The OEM can configure the product state (in option bytes) between those possible values:
- TZ-Closed:
- Debug: a debug connection to the OEM’s nonsecure application is allowed natively. Then, the OEM allows the execution of one or several commands through the Debug Authentication service.
- Regression: the STM32H5 MCU fully erases the user flash memory and falls back to the product state Open.
- Closed: the OEM can allow the execution of one or several commands through the Debug Authentication service:
- Debug: the STM32H5 MCU grants a debug connection to the OEM’s nonsecure application.
- Regression: same as TZ-Closed.
- Partial regression: the STM32H5 device fully erases the nonsecure user flash memory (but keeps the secure user flash unchanged) and falls back to the product state TZ-Closed.
- Locked: the OEM forbids all Debug Authentication services listed above. In this product state, the user cannot leverage Debug Authentication features, such as Debug reopening and regressions.
The product state (option bytes) is controlled by the boot stage. The OEM can also configure the minimal product state allowed used for this control:
The boot stage will execute the application only if the product state programmed in option byte is equal or greater than the "Minimal product state allowed".
More constraining product states are in following increasing order:
- TZ-Closed
- Closed
- Locked
6.3.1. Development phase
In development phase, it is recommended to set the product state to TZ-Closed. In this case, the debugging of the nonsecure application is allowed natively (without a Debug Authentication service).
Product state can also be set to Closed. In this case, the debugging of the nonsecure application requires Debug Authentication.
Product state can also be set to Locked to test the final SW configuration but it shall be clear that this device can't be reopened anymore.
6.3.2. Production preparation phase
In production preparation phase, the OEM can set the product state to Closed (Debug opening controlled by Debug Authentication), or Locked (device can't be reopened anymore).
7. Memory mapping
7.1. Flash memory mapping
The user flash memory is composed of several areas for the Secure Manager, the secure module, and the nonsecure application execution (active slots).
It contains also download slots, to allow update of the Secure Manager, secure module, and nonsecure application over the air during application execution.
It also contains ITS storage area (ITS file system and ITS provisioning area).
To simplify Secure Manager usage, Secure Manager is used with some pre-defined flash memory mapping configurations. OEM shall choose predefined memory mapping during installation phase, according to its need regarding:
- nonsecure application size
- secure module number and size
- ITS size
The supported predefined flash layout are the following:
Once the pre-defined flash layout configuration has been selected, the OEM can customize it to reserve a nonsecure flash area for the nonsecure application, for non volatile data storage or file system purpose for example. The nonsecure reserved area is inserted between the nonsecure application active slot and download slot.
In this case, the nonsecure application flash area is implicitly reduced accordingly, by half of the nonsecure reserved area size.
Below schema describes the NS reserved area location for pre-defined flash memory config SMAK_0, as example. Same principle is applied for other flash memory configuration.
The flash memory mapping can no more be changed until device regression, and re-installation of the Secure Manager.
7.2. SRAM mapping
The static random access memory (SRAM) is composed of several areas for Secure Manager, Secure Modules, and nonsecure application.
SRAM mapping is independent from the flash memory configuration index (SMAK_0 or SMAK_1).
Secure Manager uses 140 KB of SRAM (whole SRAM2 and beginning of SRAM3).
Secure modules, if any, will use some configurable size of SRAM3 located just after Secure Manager SRAM. It shall be ensured that the module SRAM starts from 0x3006 3000 (corresponding to end of Secure Manager SRAM). In case of third-party module, the module provider shall provide the OEM with SRAM requirements for the secure module, so that OEM can configure secure SRAM end address accordingly.
A nonsecure/secure shared buffer area is located at end of SRAM1 for data buffer exchange between nonsecure application and Secure Manager. It shall be sized according to application needs. Indeed, if nonsecure application needs to manage big data in ITS or import/export big cryptography keys (ie RSA 3072 key), this buffer size may need to be increased else an error will be returned by psa api if too small.
The rest of SRAM (beginning of SRAM1 and end of SRAM3) is available for nonsecure application usage.
SRAM mapping (using NS memory aliases 0x2xxx xxxx by convention):
8. Performances
Secure Manager performances are described for selected use cases.
The performance figures (measurements) are given for the default Secure Manager configuration, more specifically:
- STM32 running at 250 MHz
UC category | Pre-conditions | Description | Value | Comment |
---|---|---|---|---|
Boot time | Time to boot up to nonsecure application (size: 584 kB) execution. No Secure Module. | 200 ms | ||
Boot time | Time to boot up to nonsecure application (size: 456 kB) execution. 1 Secure Module (size: 128kB). | 250 ms | ||
NSPE to SPE transition | SPE code executed in thread mode. | Time to call Secure Service (or Secure Module) from nonsecure application. | 37 μs | |
nonsecure IRQ | NSPE code executed in thread mode. | Time to execute non-secure IRQ interrupt handler while NSPE code is executed in thread mode. | 600 ns | |
nonsecure IRQ | SPE code executed in thread mode. | Time to execute non-secure IRQ interrupt handler while SPE code is executed in thread mode. | 4 μs |
Notes:
- These performance figures are nominal values.
9. Secure Manager configuration
Prior to its installation, the Secure Manager can be configured according to OEM product needs.
This configuration step can be skipped, so that the Secure Manager will be installed using ST default configuration.
As mentioned in the introduction, the Secure Manager Access Kit is used in two phases:
- Development: to develop a nonsecure application that uses the Secure Manager services.
- Production preparation: to prepare the encrypted images for OEM secure manufacturing.
These phases have different constraints for the installation.
For example, the debug may be open/permissive in the development phase to allow developers to debug their application, whereas it will be closed by default and strictly controlled by Debug Authentication in the production preparation phase.
9.1. Flash Memory configuration
9.1.1. Secure Manager pre-defined flash memory configuration
The OEM can select one of the following Secure Manager memory configurations
(see "Flash memory mapping"):
- SMAK_0 : nonsecure application 584 KB, no secure module, ITS physical size 40 KB
- SMAK_1 : nonsecure application 456 KB, one secure module 128 KB, ITS physical size 40 KB
9.1.2. Flash memory nonsecure reserved area
The OEM can customize the pre-defined flash memory configuration to reserve nonsecure flash area (see "Flash memory mapping"):
By default, there is no nonsecure reserved flash area. OEM can reserve some flash area with a granularity of 16 KB (2 flash sectors). In this case, the nonsecure application size is reduced by half of the value.
9.2. SRAM configuration
The OEM can configure the size of the nonsecure/secure shared buffer SRAM area (see "SRAM mapping").
The minimum size of this buffer is 4 KB, with a maximum of 248 KB. The size granularity is 1 KB. In default configuration, its size is 16 KB, matching the Secure Manager application example delivered in STM32H5 CubeFw package.
9.2.2. Secure SRAM
The OEM can configure the secure SRAM area depending on Secure module needs (if any).(see "SRAM mapping")
Secure SRAM configuration granularity is 4 KB.
By default, secure SRAM configuration reserves 24 KB in SRAM3 for secure module.
In case of flash mapping configuration SMAK_0, it is recommended to change this setting so that no SRAM3 is reserved for module, to avoid wasting SRAM3.
9.3. Minimal Product state
The OEM can configure the minimal product state allowed ((see "Product state").
It can be configured to TZ-closed, Closed or Locked.
By default, the minimal product state is set to TZ-Closed.
9.4. System clock
The OEM can configure the system clock speed during device initialization (see "Clocking during device initialization") among these values:
- 250 MHz (using PLL with HSI input).
- 200 MHz (using PLL with HSI input).
- 64 MHz (using HSI).
9.5. Authentication of Module with license (third-party module)
The Secure Manager supports two installation models for module with license (third-party module):
- Model #1: Modules with license shall not be signed by OEM
- Model #2: Modules with license shall be signed by OEM
The OEM must choose between Model #1 and Model #2.
9.6. System bootloader
When the device finds an invalid image right after reset, depending on the OEM's configuration, it can either reset or jump to the system bootloader that acts as the local loader.
The invalid image can be either a STuRoT, Secure Manager, nonsecure application, or module image.
Jumping to the system bootloader and using a PC host physically connected to the STM32H5 device, you can download a new valid image.
The OEM can configure the Secure Manager behavior to reset or to jump to the system bootloader as a response to invalid image detection.
This configuration is managed at two level:
- STiRoT level: managing STuRoT firmware image
- STuRoT level: managing Secure Manager, nonsecure application, and module image
9.7. Factory Internal Trusted Storage (ITS)
By default, a factory ITS blob containing dummy data is securely provisioned during Secure Manager installation.
The OEM can change the factory ITS blob content to include their own keys and data, which can be used by the application at runtime, through a secure ITS service.
The ITS blob can be customized by the OEM with keys and data using the STMicroelectronics ITS builder tool.
For more information on the ITS builder, refer to the ITS builder documentation in STM32CubeH5 [3] at ./Utilities/PC_Software/ITSbuilder/README.md.
9.8. Secure Manager keys
Secure Manager uses OEM keys for authentication and decryption of the firmware images.
- Encryption key: an asymmetric ECC secp256r1 private key. This key is used to decrypt the nonsecure application and secure modules images (except secure modules with license), using ECIES-P256 algorithm.
- Authentication key: an asymmetric ECC secp256r1 public key. This key is used to authenticate the nonsecure application and secure modules (except secure modules with license, not signed by OEM), using ECDSA-P256 algorithm..
In development phase, there are two possibilities:
- The OEM uses the default Secure Manager keys from ST.
- The OEM uses its own Secure Manager keys.
9.9. Debug Authentication configuration
Debug Authentication configuration contains a set of DA keys/certificates and permissions.
SMAK contains a default DA configuration by ST that can be used by OEM during development phase.
9.9.1. DA keys/certificates
The DA uses an asymmetric key to authenticate a genuine user with its credential (a certificate) when reopening a debug connection and/or performing a regression.
9.9.2. DA permissions
DA permission lists are restricted by the Secure Manager installation procedure.
The OEM must configure the permissions among:
- Full regression
- Partial regression (nonsecure domain only)
- Nonsecure application debug reopening.
Please refer to XXXXXXX(dedicated wiki ref)XXXXX for more information on Debug Authentication.
9.10. Secure Modules
The OEM can choose to add their own secure functions to a Secure Module or to add a third-party Secure Module inside the secure domain in the unprivileged part. The OEM must select a Secure Manager memory configuration compatible with the integrated module number and size.
The OEM uses the kernel APIs to access the Secure Manager and complies with the Secure Manager rules to export the new secure services API to the nonsecure application.
The integrated module can be licensed or not.
9.11. Option byte (OB) configuration
The OEM must configure the STM32H5 MCU option bytes to fit the device requirements.
The OEM can configure the option bytes mentioned in the table below. Other option bytes are not configurable in the Secure Manager context.
register | BitField | Description |
---|---|---|
OPTSR_PRG |
IWDG_STDBY |
independent watchdog counter active in Standby mode |
OPTSR2_PRG |
SRAM3_ECC |
SRAM3 error code correction |
The OEM must refer to RM0481[13] for more details regarding the option bytes mentioned in the table above.
10. Use cases
This chapter describes the main use cases available through SMAK.
UC category | UC name | Comment |
---|---|---|
Initial installation | ||
The OEM creates their encrypted firmware for the secure firmware installation (SFI). Limited firmware list. | Firmware from STMicroelectronics and OEM. Firmware list: Secure Manager, Secure Manager configuration, nonsecure application, device configuration (option bytes). | |
The OEM installs the firmware using SFI. Limited firmware list. | Firmware from STMicroelectronics and OEM. Firmware list: Secure Manager, Secure Manager configuration, nonsecure application, device configuration (option bytes). | |
The OEM creates their encrypted firmware (for SFI). Full firmware list. | Firmware from STMicroelectronics, OEM, and third party. Firmware list: Secure Manager, Secure Manager configuration, nonsecure application, device configuration (option bytes). Optional: Secure Modules and diversified data (ITS). | |
The OEM installs the firmware using SFI. Full firmware list. | Firmware from STMicroelectronics, OEM, and third party. Firmware list: Secure Manager, Secure Manager configuration, nonsecure application, device configuration (option bytes). Optional: Secure Modules and diversified data (ITS). | |
Installation and update | ||
The OEM gets the new STuRoT encrypted image from STMicroelectronics. | ||
The OEM updates the STuRoT. | ||
The OEM gets the new encrypted Secure Manager image from STMicroelectronics. | ||
The OEM updates the Secure Manager. | ||
The OEM creates their new encrypted nonsecure application. | ||
The OEM updates the nonsecure application. | ||
The OEM creates their new encrypted Secure Module. | ||
The OEM installs/updates the OEM Secure Module. | ||
The OEM installs/updates a third-party Secure Module (without image installation counting). | Third party can be STMicroelectronics, the OEM, or third-party company (owner of the module). | |
The OEM installs/updates a third-party Secure Module (with image installation counting, with STM32HSM). | Secure Module must be previously installed with SFI as it requires STM32HSM for Secure Module installation. | |
The OEM signs the third-party Secure Module with their own key. | ||
The OEM updates a third-party Secure Module (without image installation counting) with OEM authentication. | ||
The OEM updates a third-party Secure Module (with image installation counting, with STM32HSM) with OEM authentication. | Secure Module must be previously installed with SFI as it requires STM32HSM for Secure Module installation. | |
Debug reopening and regression | ||
The OEM performs a partial regression. | Firmware and data located in nonsecure domain (nonsecure application) are erased. Device in TZ-Closed product state. | |
The OEM performs a full regression. | Firmware and data located in nonsecure and secure domains are erased. Device in Open product state. | |
The OEM opens the nonsecure domain to debug their nonsecure application. | Firmware and data located in nonsecure domain are not erased. Device in TZ-Closed product state. | |
PSA services - Internal Trusted Storage | ||
The OEM uses PSA Internal Trusted Storage (ITS) to set and get data and keys in ITS. | Data and key confidentiality is ensured by encryption. | |
PSA services - Firmware update | ||
The OEM uses PSA firmware update API to download firmware. | Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules. | |
The OEM uses PSA firmware update API to request installation of firmware. | Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules. | |
The OEM uses PSA firmware update API to abort installation of firmware. | Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules. | |
The OEM uses PSA firmware update API to install or update firmware. | Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules. | |
The OEM uses PSA firmware update API to validate candidate firmware. | Firmware: Secure Manager, nonsecure application, Secure Modules. | |
PSA services - Cryptography | ||
The OEM uses PSA cryptography API to encrypt or decrypt data. | ||
The OEM uses PSA cryptography API to sign or verify data. | ||
The OEM uses PSA cryptography API to hash data. | ||
The OEM uses PSA cryptography API to generate random number of key. | ||
PSA services - Initial Attestation | ||
The OEM uses PSA initial attestation API to get an authenticated token and its size. | This token is used by the server to uniquely identify an STMicroelectronics device from the OEM. | |
ST DUA pre-provisioned key | ||
The OEM uses the STMicroelectronics CA initial attestation key pair to authenticate STMicroelectronics devices. | PSA initial attestation compliant. | |
The OEM uses the STMicroelectronics CA user key pair to authenticate STMicroelectronics devices. | ||
Internal Trusted Storage (ITS) provisioning | ||
The OEM uses the ITS builder tool to prepare an ITS blob. | ITS blob can be different for each STMicroelectronics device and is later provisioned on STMicroelectronics device using SFI procedure. | |
System bootloader - Firmware update | ||
The OEM uses the system bootloader to download firmware. | Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules. | |
The OEM uses a system reset after firmware download via the system bootloader to install or update firmware. | Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules. | |
The OEM uses the PSA firmware update API to validate candidate firmware. | Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules. |
10.1. UC category: ST DUA pre-provisioned key
10.1.1. UC name: The OEM uses STMicroelectronics CA initial attestation key pair to authenticate STMicroelectronics devices
To ease OEM manufacturing, STMicroelectronics has pre-provisioned each device with an ECC chip unique key and X509 certificates, used for device unique authentication during the initial attestation procedure. The ECC initial attestation private key is used by the PSA initial attestation service to sign the token.
The typical usage is described below.
During STMicroelectronics device manufacturing:
- STMicroelectronics provisions the DUA initial attestation chip private key and certificate for each device.
Between STMicroelectronics and OEM offices:
- STMicroelectronics delivers the STMicroelectronics CA DUA initial attestation certificate to the OEM. This CA certificate is delivered under license and must be requested from STMicroelectronics.
Two options are possible:
Option 1: the OEM builds the OEM device list at OEM manufacturing.
At OEM product manufacturing:
- The OEM gets the DUA initial attestation chip public key for each device to create an OEM device database.
In the field:
- The server requests the STMicroelectronics DUA initial attestation chip certificate from the device.
- The server authenticates this certificate using the STMicroelectronics CA DUA initial attestation certificate and gets the authenticated STMicroelectronics DUA initial attestation chip public key from this certificate.
- The server verifies that this key is part of the OEM device database.
- The server requests an initial attestation token from the device.
- The server authenticates this token using the STMicroelectronics DUA initial attestation chip public key.
- The server can now use the authenticated token (for example, to identify firmware versions and firmware measurements).
Option 2: the OEM authenticates the OEM device based on the authenticated initial attestation token field instance ID.
At OEM product manufacturing:
- The OEM does not create the OEM device database at OEM manufacturing, but uses the initial attestation procedure (in the field) to get the authenticated token claim (field Instance ID: hash of the initial attestation public key) to authenticate OEM devices
In the field:
- The server requests the STMicroelectronics DUA initial attestation chip certificate from the device.
- The server authenticates this certificate using the STMicroelectronics CA DUA initial attestation certificate and gets the authenticated STMicroelectronics DUA initial attestation chip public key from this certificate.
- The server requests an initial attestation token from the device.
- The server authenticates this token using the STMicroelectronics DUA initial attestation chip public key.
- The server uses this authenticated token (field instance ID: hash of the initial attestation public key) to authenticate that this STMicroelectronics device is an OEM device.
- The server can now use the authenticated token (for example to identify firmware versions and firmware measurements).
10.1.2. Use case: OEM uses the STMicroelectronics CA user key pair to authenticate 'STMicroelectronics devices
To ease OEM manufacturing, STMicroelectronics has pre-provisioned each device with an ECC chip private key and X509 certificate for user purposes. This ECC chip private key is used to sign some messages and is accessible through the PSA cryptography API using a key ID (opaque key). It can be used, for example, for TLS X509 mutual authentication (challenge, response).
The typical usage of this key and certificate is described below.
At STMicroelectronics device manufacturing:
- STMicroelectronics provisions the DUA user chip private key and certificate on each device.
Between STMicroelectronics and OEM offices:
- STMicroelectronics delivers the STMicroelectronics CA DUA user certificate to the OEM. This CA certificate is delivered by STMicroelectronics as part of STM32CubeFW.
At OEM product manufacturing:
- The OEM gets the DUA user chip public key for each device to create an OEM device database.
In the field:
- The server requests the STMicroelectronics DUA user chip certificate from the device.
- The server authenticates this certificate using the STMicroelectronics CA DUA user certificate and gets the authenticated STMicroelectronics DUA chip public key from this certificate.
- The server verifies that this key is part of its OEM device database.
- The server sends a hash to the device and requests a signature of this hash.
- The device performs the signature of this hash using the STMicroelectronics DUA user chip unique private key.
- The server authenticates this hash signature using the authenticated STMicroelectronics DUA user chip public key.
- The server is now sure to communicate with authentic STMicroelectronics devices from this OEM.
11. Secure Manager manufacturing
As we have seen in the introduction, SMAK is used in the manufacturing preparation phase to prepare the encrypted images for the OEM secure manufacturing (SFI).
Refer to SFI for STM32H5 to see how the output of the SMAK manufacturing preparation phase is used in the SFI procedure.
12. Debug
The STM32H5 device supports the PSA Authenticated Debug Access Control (ADAC) protocol.
After the Secure Manager installation, the STM32H5 device is set at least to the TZ-Closed product state, which means that the secure domain is not accessible via JTAG. Moreover, the OEM can decide to set the device to the Closed or Locked product state, which means the nonsecure application is no longer accessible via JTAG either.
In such states, it is no longer possible to debug the installed firmware (secure or nonsecure) via JTAG.
In the TZ-Closed product state, the OEM can use the ADAC protocol to:
- Perform a full regression (moving to an Open product state). This way, the OEM can reinstall the Secure Manager, Secure Modules, and a nonsecure application.
In the Closed product state, the OEM can use the ADAC protocol to:
- Reopen the nonsecure debug (moving to a TZ-Closed product state). This way, the OEM can debug their nonsecure application.
- Perform a partial regression of the nonsecure part (moving to a TZ-Closed product state). This way, the OEM can reinstall their nonsecure application.
- Perform a full regression (moving to an Open product state). This way, the OEM can reinstall the Secure Manager, Secure Modules, and a nonsecure application.
In the Locked product state, it is definitely not possible to reopen debugging or to perform regressions.
For more information on authenticated debug access protocol, refer to Debug Authentication for STM32H5.
13. Trace and log
13.1. nonsecure application
The OEM can implement their own trace and log in their nonsecure application (log in RAM, trace over UART, etc.).
13.2. Secure Manager
13.2.1. At boot time
If the Secure Manager detects an error at boot time, it generates a reset or jumps to the system bootloader (depending on a Secure Manager configuration parameter).
The boot error code is accessible via the STM32cubeProgrammer discovery command.
13.2.2. At runtime
The nonsecure application calls the Secure Manager functions at runtime. In the event of an error, the Secure Manager function returns an error code that can be used by the nonsecure application for debugging purposes.
14. Getting started
For the Secure Manager hardware and software environment setup, installation procedure, and step-by-step execution, refer to Secure Manager STM32H5 How to Intro.
15. To go further
For more details about Secure Manager environment setup, installation procedure and execution, refer to Secure Manager STM32H5 How to Intro.
For more details about Secure Manager manufacturing, refer to SFI for STM32H5.
16. Acronyms
See Security acronyms.
17. Definitions
See Security definitions.
18. References
- ↑ Secure Manager embedded software for STM32Cube
- ↑ SLA0048
- ↑ 3.0 3.1 3.2 3.3 STM32CubeH5
- ↑ 4.0 4.1 STM32CubeIDE
- ↑ 5.0 5.1 KEIL
- ↑ 6.0 6.1 IAR
- ↑ STM32CubeProgrammer
- ↑ STM32CubeMX
- ↑ 9.0 9.1 Arm PSA Cryptography API
- ↑ 10.0 10.1 Arm PSA Attestation API
- ↑ 11.0 11.1 Arm PSA Secure Storage API
- ↑ 12.0 12.1 PSA Firmware Update API
- ↑ 13.0 13.1 RM0481