This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Change propagation updates are pending (14 jobs estimated) and it is recommended to wait with modifications to a category until the process has been finalized to prevent intermediary interruptions or contradictory specifications.
Start with STM32 and Bluetooth® Low Energy |
Learn how to set up STM32 for Cellular connectivity applications |
Start with STM32 and LoRaWAN |
Learn how to set up STM32 for Thread connectivity applications |
Learn how to set up STM32 for Zigbee connectivity applications |
Subcategories
This category has the following 6 subcategories, out of 6 total.
Media in category "Connectivity"
The following 7 files are in this category, out of 7 total.
- Connectivity:Connectivity - Nucleo with J-LINK.png 575 × 169; 254 KB
- Connectivity:Connectivity - Nucleo with STLINK.png 624 × 218; 280 KB
- Connectivity:Connectivity - Segger patch adapter.png 1,307 × 857; 569 KB
- Connectivity:Connectivity - STDC14 and MIPI10 pin correspondance.png 759 × 453; 118 KB
- Connectivity:Connectivity Nucleo WBA55CG.png 560 × 560; 258 KB
- Connectivity:STM32WBA55G-DK1.jpg 2,039 × 1,405; 1.81 MB
- Connectivity:WBA Keil project location.png 979 × 553; 141 KB