SMAK for STM32H5

Revision as of 11:56, 16 August 2023 by Registered User (→‎Description)

1. Introduction

The Secure Manager Access Kit (SMAK) provides an environment where users can:

  • Develop nonsecure applications that use the Secure Manager services.
  • Prepare the final encrypted images used for OEM secure manufacturing.

The following diagram presents an overview of the SMAK ecosystem.

Security SMAK.png


The SMAK details are described in the next chapters.

2. Architecture

2.1. Ecosytem Architecture

The SMAK ecosystem is composed of:

  • The Secure Manager package binary, available as an encrypted image from STM32TRUSTEE-SM[1].
    • The image is delivered with the software license agreement SLA0048[2].
    • It can be used for production purposes.
  • The STM32Cube embedded firmware package available from STM32CubeH5 [3], containing:
    • Scripts to configure and install the Secure Manager package, relying on STM32TrustedPackageCreator and STM32CubeProgrammer tools.
    • Template and example projects (for STM32CubeIDE, KEIL and IAR) to develop nonsecure application using Secure Manager services. They contain pre-integrated prebuild and postbuild scripts relying on STM32TrustedPackageCreator to generate signed and encrypted image, and download scripts relying on STM32CubeProgrammer to flash nonsecure application image.
  • STM32TrustedPackageCreator and STM32CubeProgrammer[4], for above needs.
  • STM32CubeMX[5], to generate nonsecure application projects for Secure Manager.
  • IDEs (STM32CubeIDE, IAR or KEIL)




The following diagram presents the SMAK ecosystem architecture.


Security Secure Manager ecosystem.png

2.2. Software architecture

The Secure Manager package is executed in secure processing environment (SPE).
It is composed of the STuRoT plus the Secure Manager.
It is responsible for Secure Boot and Secure Firmware Update, and it provides secure services to nonsecure (NS) applications at runtime.

The Secure Manager package is composed of:

  • A 2-level Root of Trust
    • An immutable Root of Trust (STiRoT)
    • An updatable Root of Trust (STuRoT)
  • The Secure Manager core
  • Secure Services such as
    • Cryptography
    • Initial attestation
    • Trusted storage
    • Firmware update

Additionally, trusted applications, also called modules, can be added by the user, but are not part of the Secure Manager package.

The following figure describes the Secure Manager software architecture.


Security Secure Manager.png

Info white.png Information
Please note that the secure modules are not part of the Secure Manager package.

For details about each Secure Manager components (STuRoT, Secure Manager core...), please refer to Secure Manager components.

3. Security model

3.1. Stakeholders

The stakeholders involved in the security model are:

  • STMicroelectronics, who owns the Secure Manager and associated services.
  • The OEM who owns the nonsecure application and possibly Secure Modules, and is responsible for the system integration.
  • Optionally, third-party Secure Module owners who own Secure Modules.

3.2. Asset confidentiality

The Secure Manager ensures stakeholders asset confidentiality by protecting:

  • Secure Manager assets against the Secure Modules and nonsecure application.
  • Secure Module assets against the nonsecure application and other Secure Modules.
  • Nonsecure application assets against Secure Modules using the internal trusted storage (ITS) service.

3.3. Multi-tenant IP protection

The Secure Manager supports multi-tenant IP protection, meaning that each Secure Module (from the OEM or third-party) is isolated from the others using sandboxes.

3.4. PSA level 3 isolation

The security model is based on PSA level 3 isolation, ensuring that the secure domain is isolated from nonsecure domain. This means that the Secure Manager and Secure Modules are protected from access by any nonsecure applications (hardware and software).
This isolation also ensures that privileged secure domain is separated from unprivileged secure domain, meaning that the Secure Manager core is protected from access by secure services and Secure Modules.
Additionally, it ensures that the secure partitions are fully isolated. This means that each secure partition (secure services and Secure Modules) is sandboxed and can only access its own resources. This protects each secure partition from access by other secure partitions, and it provides protection for the Secure Manager core.

3.5. Type of assets

The following table describes which types of assets are protected.

Code asset Volatile data asset Nonvolatile data asset ITS data Peripherals
Secure Manager Yes Yes Yes Yes Yes
Secure Module Yes Yes Yes Yes Yes
nonsecure application Yes Yes Yes Yes Partially (see note below)
Info white.png Information
nonsecure application peripherals are accessible by a Secure Module if this peripheral is described in the Secure Module header. This means that the OEM must review the Secure Module header with the third-party module owner to ensure that this module cannot access any nonsecure application peripheral assets.

4. Feature overview and secure services

The Secure Manager package is responsible for supplying secure services at boot-time and runtime.

The boot-time services are available after a power-on or system reset and are responsible of secure boot and secure firmware update.

The runtime secure services can be used by nonsecure applications running on nonsecure domain, as well as other secure services running on secure domain. These services are defined by the PSA standard.

The following services are supported:

  • PSA cryptography: supplies cryptographic services, such as authentication or encryption, based on hardware cryptographic acceleration with side-channel resistance.
  • PSA internal trusted storage (ITS): supplies services for storing the most important assets (such as keys and data) in the internal flash memory, ensuring integrity, and confidentiality. Be aware that ITS file system is encrypted.
  • PSA attestation: supplies services to authenticate a device. To do this, a unique signed token is generated for each device, which can be later authenticated by a server.
  • PSA firmware update: supplies services to download new firmware images and perform image updates.

The Secure Manager package also supports firmware installations and updates, based on direct image download in the download slot (this feature must be enabled using OEM Secure Manager configuration parameter) instead of PSA firmware update API.

4.1. PSA services

4.1.1. PSA cryptography service

4.1.1.1. Description

This service provides an implementation of the PSA cryptography API as defined in the Arm PSA Cryptography API document[6].
Cryptographic algorithms implementation relies on cryptographic hardware accelerator peripherals of the device (PKA, SAES, HASH, TRNG) whenever possible. The table below lists the supported functionalities, as well as the protections they implement.

4.1.1.2. Services

The main services are:

  • Library management
    • Library (PSA cryptography service) initialization
  • Key management
    • Opaque key identifiers
    • Key lifetimes (volatile, persistent)
    • Key policy
    • Key import, generation, derivation, and copy
  • Symmetric cryptography
    • Message digests (Hash)
    • Message authentication codes (MAC)
    • Encryption and decryption
    • Authenticated encryption (AEAD)
    • Key derivation
  • Asymmetric cryptography
    • Asymmetric encryption
    • Hash and sign
    • Key agreement
  • Randomness

The following table describes the implemented operations, algorithms, and key lengths.

Operations Algorithms Key lengths Modes Implementation SCA/DPA resistant Fault resistant
Get entropy TRNG N/A N/A Hardware N/A N/A
Encryption, decryption AES 128, 256 ECB, CBC, CTR, CFB Hardware YES YES
Authenticated encryption, decryption AES 128, 256 GCM, CCM Hardware YES YES
Cipher-based message authentication code AES 128 CMAC Hardware YES YES
Cryptographic hash SHA-11 N/A Digest 160-bit Hardware N/A N/A
Cryptographic hash SHA-2 N/A SHA-224, SHA-256, SHA-384, SHA-512 Hardware N/A N/A
Keyed hashing for message authentication HMAC-SHA2-224 Short, long (>64 bytes) N/A Hardware N/A YES
Keyed hashing for message authentication HMAC-SHA2-256 Short, long (>64 bytes) N/A Hardware N/A YES
Keyed hashing for message authentication HMAC-SHA2-384 Short, long (>64 bytes) N/A Hardware N/A YES
Keyed hashing for message authentication HMAC-SHA2-512 Short, long (>64 bytes) N/A Hardware N/A YES
Asymmetric encryption RSA 2048, 3072 RSAES-OAEP, RSASSA-PKCS1-V1_5 Hardware YES YES
Signature with hashing signature verification RSA 2048, 3072 RSASSA-PKCS1-v1_5, RSASSA-PSS Hardware YES YES
Signature with hashing signature verification ECDSA Up to 521 List of supported hardware ECC curves below2 Hardware YES YES
Key agreement ECDH Up to 521 List of supported ECC curves below2 Hardware YES YES
Encryption, decryption DES1 128, 256 ECB, CBC Software NO NO
Encryption, decryption Triple DES 128, 256 ECB, CBC Software NO NO
Key derivation HMAC-based N/A N/A Hardware YES YES
  1. Weak - not recommended.
  1. The following elliptic curves are supported: secp224r1, secp256r1, secp384r1, secp521r1, secp256k1, bp256r1, bp384r1, and bp512r1. secp192r1 and secp192k1 are also supported, but not recommended.

Note:
All implementations that manipulate private keys are protected against side-channel and timing attacks.

4.1.1.3. Pre-provisioned DUA user key

To ease OEM manufacturing, STMicroelectronics has pre-provisioned STM32 devices with a unique asymmetric key pair for user purpose. This ECC key pair is accessible through the PSA crypto API using a specific key ID.

The following services are available:

  • Sign with the DUA user private key.
  • Export the DUA user public key.

4.1.2. PSA initial attestation service

4.1.2.1. Description

This service provides an implementation of the PSA initial attestation API, described in the PSA Attestation API document[7].

The service allows the application to prove the device identity during an authentication process to a verification entity. The initial attestation service can create a entity attestation token (EAT) on request, which contains a fix set of device specific data. The EAT is encoded according to the CBOR format and signed according to COSE standard. The EAT is signed using a DUA initial attestation key, pre-provisioned by STMicroelectronics in STM32H5 devices (distinct from DUA user key).

The table below lists the fields contained in the EAT.

Claim Mandatory Description Value Implemented
Auth challenge Yes Authenticated challenge. Value is provided by the user (caller) that request the token Yes
Instance ID Yes Unique identifier of the device instance. Concatenation of 0x1 and hash of the public key used for initial attestation (DUA initial attestation key). Yes
Verification service indicator No A hint used by a relying party to locate a validation service for the token N.A. No
Profile definition No Name of a document that describes the profile of the report N.A. No
Implementation ID Yes Unique identifier of the underlying immutable PSA RoT. ST immutable (ROM) firmware version (32 bytes at address 0x0BF96000). Yes
Client ID Yes Partition ID of the caller (application who requested the token). -1 for NSPE. ASID (4 bytes) of the secure module for SPE. Yes
Security life cycle Yes Current life cycle state of the PSA RoT. Product state Closed (SL_SECURED) or TZ-Closed (SL_NON_PSA_ROT_DEBUG). Yes
Hardware version No Metadata linking the token to the GDSII that went to fabrication for this instance String encoded from the DBGMCU IDCODE register. Yes
Boot seed Yes Random value created at system boot time. Random number. Yes
Software components Yes A list of software components that represent all software managed by the PSA RoT See table below. Yes

The table below lists the fields contained in each Software component.

Software component fields Mandatory Description Values Implemented
Measurement type No A short string representing the role of this software component. "BL" for STuRoT, "SPE" for Secure Manager, "ARoT" for a Secure Module, "NSPE" for nonsecure application Yes
Measurement value Yes The hash of the invariant software component in memory at startup time. SHA256 (32 bytes) of the software component. Yes
Version No The issued software version in the form of a text string. Encoded in CBOR representing a string such as "1.0.0" Yes
Signer ID No The hash of a signing authority public key for the software component. SHA256 (32 bytes) of the public key. Yes
Measurement description No Represents the way in which the measurement value of the software component is computed. ASCII string "SHA256" Yes


TO DO!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!!


4.1.2.2. Services

The main services are:

  • Get token size (useful to allocate the right buffer size to get the token).
  • Get token.
4.1.2.3. DUA initial attestation pre-provisioned key

To ease OEM manufacturing, STMicroelectronics has pre-provisioned for each device an ECC asymmetric unique key pair and a certificate used for device unique authentication. It is called DUA initial attestation key. It is dedicated and used by the PSA initial attestation service to sign the token.

4.1.3. PSA internal trusted storage service

4.1.3.1. Description

This service provides an implementation of the PSA internal trusted storage (ITS) API defined in the Arm PSA Secure Storage API document [8].

It allows the writing of data in the microcontroller built-in flash memory region that is isolated from the nonsecure application and from other secure services by hardware security protection mechanisms. It provides a nonhierarchical storage model (like a file system), where a linearly-indexed list of metadata manages all the assets. The data are generally small pieces of data (such as private key, credentials).

ITS includes the following functionalities:

  • Confidentiality: the data are located in a secure area, protected from unauthorized access by hardware isolation (TZ, MPU) of the flash memory access domain. Data are encrypted using a symmetric algorithm and a unique STMicroelectronics 256-bit key.
  • Access control: a specific mechanism establishes the identity of the requester (a nonsecure entity, a secure entity, or a remote server).
  • Integrity: the internal flash memory device provides resistance to hardware physical access attacks.
  • Reliability: ITS provides resistance to power failure scenarios and incomplete write cycles.
  • Configurability: ITS size can be configured by the OEM based on Secure Manager memory configuration selection. Additional ITS size are considered in ST roadmap.
4.1.3.2. Services

The main ITS services are:

  • Set data in the ITS area (data are identified by a unique identifier (UID)).
  • Get data from the ITS area.
  • Remove data from the ITS area.
  • Get data information (metadata).

Manipulated objects (data) can be data or keys. The metadata contain the data size and some attributes that define how they can be accessed (immutable, public...).
Each data is associated with a owner ID. The nonsecure application owner ID is 0xFFFFFFFF. The Secure Service (respectively Secure Module) owner ID is the ASID of the Secure Service (respectively Secure Module). The ASID is encoded with 32 bits.
A data can be accessed only by the data owner (Owner ID) unless the data is declared as public.
When data are provisioned using ITS builder tool, the supported key format is limited (for details, see ITS builder documentation in STM32CubeH5 [3] at ./Utilities/PC_Software/ITSbuilder/README.md).

4.1.3.3. ITS provisioning

The ITS can be provisioned in two ways:

  • The first way is to use the PSA internal trusted storage API to provision data and keys in the ITS. In this case, it is the nonsecure application that performs the provisioning at runtime (generally during the OEM manufacturing phase).
  • The second way is to use Factory Internal Trusted Storage provisioning. The OEM prepares the data and keys to provision, using the STMicroelectronics ITS builder tool (on a PC). This tool generates an encrypted and authenticated blob (using OEM keys used for nonsecure application preparation) containing the data and keys. The OEM can later install this blob in a secure way during production (the encrypted blob is programmed during production but blob installation and initialization in ITS filesystem is done at the first product power on).

For more information on ITS builder, refer to ITS builder documentation in STM32CubeH5 [3] at ./Utilities/PC_Software/ITSbuilder/README.md.

Notes:

  • In the current Secure Manager memory configurations, the blob size is limited to 8 KB.
  • The maximum data and key size is 2016 bytes.
  • The installed data and keys can only be used by the nonsecure application, using the PSA internal trusted storage API.

4.1.4. PSA firmware update service

4.1.4.1. Description

This service provides an implementation of the PSA firmware update API defined in the PSA Firmware Update API document [9]. It provides a standard and platform agnostic interface for firmware updates.
The firmware update scheme is based on a dual slot: one active slot and one download slot. The active slot is used to execute the firmware and the download slot used to download the new image to be installed.

The following images can be updated:

  • Nonsecure application
  • STuRoT
  • Secure Manager
  • Secure Modules (each independently)

The installation flow is as follows:

  • The nonsecure application (update agent) gets information about the installed images (name, installation status, version, etc.).
  • It downloads the image to the secure download slot.
  • It requests image installation
  • It resets the device to execute the secure boot stages (STiRoT and STuRoT) that performs the installation in the active slot and jumps to the non-secure application.
  • The non-secure application must validate the image using its specific validation criteria (non secure application dependent)
    • If the validation criteria is met, the nonsecure application informs the firmware update service that the image is valid.
    • If the validation criteria is not met, the nonsecure application generates a reboot. The secure boot stages are executed, set the image to rejected state, and performs a rollback to the previous valid image which was swapped in the download slot.

During the installation, the image in active and download slots changes states. The possible states are:

State Value Description
UNDEFINED 0x0 Empty download slot. Or download slot containing a former image whereas new image on the active slot has been successfully installed.
CANDIDATE 0x1 Image candidate present in the download slot.
INSTALLED 0x2 Image accepted by the nonsecure application (update agent) in the active slot.
REJECTED 0x3 Image not accepted by the nonsecure application (update agent), swapped back to download slot.
PENDING_INSTALL 0x4 Image candidate in the active slot, waiting for image acceptance from the nonsecure application (update agent).
REBOOT_NEEDED 0x5 Reboot is needed to finalize the image candidate swap from download slot to active slot.

The image installation (swap) is resistant to asynchronous power down and system reset. Nevertheless, to be noticed that if a power down occurs whereas the new image has not been completely written to the download slot, the image installation process must be restarted.

4.1.4.2. Services


The services are:

  • Get image information (state, version) for an image ID.
  • Write image to the download slot (staging area) (image state "CANDIDATE").
  • Install the image and inform the client that a reboot is required to execute the secure boot stages (image state "REBOOT_NEEDED").
  • Reboot the device to execute secure boot stages:
    • If there is an image to install in the download slot, the secure boot stages installs the image (image state "PENDING_INSTALL") and reboot. If there is no valid image in the active slot, the secure boot stages performs a rollback to the image located in the download slot and sets the invalid image state to "REJECTED".
  • Accept the image. The image is fully installed and becomes the new valid image (image state "INSTALLED").

An image ID is composed of a slot ID and a type ID.
The slot ID indicates if the image is located in the download or active slot.
The type ID indicates the type of image as described in below table.

Type ID Description
NONSECURE nonsecure application
BL STuRoT
SECURE Secure Manager
MODULE0 Secure Module 0

4.2. Other services

4.2.1. Power-on and system reset

After each product power-on or reset, the platform starts to execute the Secure Manager root of trust (STiRoT, STuRoT, and Secure Manager) that manages the secure initialization of the platform. If a candidate STuRoT image is present in the STuRoT download slot, STiRoT performs the installation in the STuRoT active slot. If a candidate Secure Manager, nonsecure application, or Secure Module image is present in the respective download slot, STuRoT performs the installation in the respective active slot.

4.2.2. Firmware update with direct writing to download slot

The OEM can configure the Secure Manager in a way that it jumps to the system bootloader when there is no valid image in at least one of the active slot (nonsecure application, STuRoT, Secure Manager, or Secure Module). In this case, the OEM can use the system bootloader download an encrypted image in the download slot. After a reset, the Secure Manager detects the downloaded image and performs the installation if the image is valid.
This service can be used to update STuRoT, Secure Manager, the nonsecure application, or a Secure Module.

4.2.3. Certificate utility

Two STMicroelectronics certificates are provisioned in the STMicroelectronics device system flash memory. They are both used for the device unique authentication (DUA), but one is used for Initial Attestation purposes and the other for user purposes.


The certificate utility supplies the following services:

  • Get DUA certificate size based on certificate ID.
  • Get DUA certificate (X509 format) based on certificate ID.

5. Interfaces

That is why we have to limit what is in the previous chapter which is more feature description/services that interface definition.}} This chapter describes the interfaces supplied by the Secure Manager to develop a nonsecure application.
The details of the interfaces are described in the header files of the Secure Manager API middleware (./Middlewares/ST/secure_manager_api/) and in the Secure Manager API documentation.

5.1. PSA interfaces

5.1.1. PSA cryptography service

5.1.1.1. Overview

The PSA cryptography service interface is described in the Arm PSA Cryptography API document[6].
To use this interface, the application must include the psa/crypto.h header file.

5.1.1.2. Function list
Function Description Comment
psa_aead_decrypt() Process an authenticated decryption operation.
psa_aead_encrypt() Process an authenticated encryption operation.
psa_aead_operation_init() Return an initial value for an AEAD operation object.
psa_asymmetric_decrypt() Decrypt a short message with a private key.
psa_asymmetric_encrypt() Encrypt a short message with a public key.
psa_cypher_abort() Abort a cipher operation().
psa_cipher_decrypt() Decrypt a message using a symmetric cipher.
psa_cipher_decrypt_setup() Set the key for a multipart symmetric decryption operation.
psa_cipher_encrypt() Encrypt a message using a symmetric cipher.
psa_cipher_encrypt_setup() Set the key for a multipart symmetric encryption operation.
psa_cipher_finish() Set the key for a multipart symmetric decryption operation.
psa_cipher_generate_iv() Generate an initialization vector (IV) for a symmetric encryption operation.
psa_cipher_operation_init() Return an initial value for a cipher operation object.
psa_cipher_set_iv() Set the initialization vector (IV) for a symmetric encryption or decryption operation.
psa_cipher_update() Encrypt or decrypt a message fragment in an active cipher operation.
psa_close_key() Close a key handle.
psa_copy_key() Make a copy of a key.
psa_crypto_init() Library initialization.
psa_destroy_key() Destroy a key.
psa_export_key() Export a key in binary format.
psa_export_public_key() Export a public key or the public part of a key pair in binary format.
psa_generate_key() Generate a key or key pair.
psa_generate_random() Generate random bytes.
psa_get_key_algorithm() Retrieve the permitted algorithm policy from key attributes.
psa_get_key_attributes() Retrieve the attributes of a key.
psa_get_key_bits() Retrieve the key size from key attributes.
psa_get_key_id() Retrieve the key identifier from key attributes.
psa_get_key_lifetime() Retrieve the lifetime from key attributes.
psa_get_key_type() Retrieve the key type from key attributes.
psa_get_key_usage_flags() Retrieve the usage flags from key attributes.
psa_hash_abort() Abort a hash operation.
psa_hash_clone() Clone a hash operation.
pa_hash_compare() Calculate the hash (digest) of a message and compare it with a reference value.
psa_hash_compute() Calculate the hash (digest) of a message.
psa_hash_finish() Finish the calculation of the hash of a message.
psa_hash_operation_init() Return an initial value for a hash operation object.
psa_hash_setup() Set up a multipart hash operation.
psa_hash_update() Add a message fragment to a multipart hash operation.
psa_hash_verify() Finish the calculation of the hash of a message and compare it with an expected value.
psa_import_key() Import a key in binary format.
psa_key_attributes_init() Return an initial value for a key attribute object.
psa_key_derivation_abort() Abort a key derivation operation.
psa_key_derivation_get_capacity() Retrieve the current capacity of a key derivation operation.
psa_key_derivation_input_bytes() Provide an input for key derivation or key agreement.
psa_key_derivation_operation_init() Return an initial value for a key derivation operation object.
psa_key_derivation_output_bytes() Read some data from a key derivation operation.
psa_key_derivation_output_key() Derive a key from an ongoing key derivation operation.
psa_key_derivation_set_capacity() Set the maximum capacity of a key derivation operation.
psa_key_derivation_setup() Set up a key derivation operation.
psa_mac_abort() Abort a MAC operation.
psa_mac_compute() Calculate the message authentication code (MAC) of a message.
psa_mac_operation_init() Return an initial value for a MAC operation object.
psa_mac_sign_finish() Finish the calculation of the MAC of a message.
psa_mac_sign_setup() Set up a multipart MAC calculation operation.
psa_mac_update() Add a message fragment to a multipart MAC operation.
psa_mac_verify() Calculate the MAC of a message and compare it with a reference value.
psa_mac_verify_finish() Finish the calculation of the MAC of a message and compare it with an expected value.
psa_mac_verify_setup() Set up a multipart MAC verification operation.
psa_open_key() Open a handle to an existing persistent key.
psa_purge_key() Remove nonessential copies of key material from memory.
psa_reset_key_attributes() Reset a key attribute object to a freshly initialized state.
psa_set_key_algorithm() Declare the permitted algorithm policy for a key.
psa_set_key_bits() Declare the size of a key.
psa_set_key_id() Declare a key as persistent and set its key identifier.
psa_set_key_lifetime() Set the location of a persistent key.
psa_set_key_type() Declare the type of a key.
psa_set_key_usage_flags() Declare usage flags for a key.
psa_sign_hash() Sign an already-calculated hash with a private key.
psa_sign_message() Sign a message with a private key. For hash-and-sign algorithms, this includes the hashing step.
psa_verify_hash() Verify the signature of a hash or short message using a public key.
psa_verify_message() Verify the signature of a message with a public key, using a hash-and-sign verification algorithm.
5.1.1.3. Pre-provisioned DUA user key

The following interfaces are available to access this key:

Function Description
psa_open_key() Open a handle to an existing persistent key (DUA user key ID).
psa_close_key() Close a key handle.
psa_export_public_key() Export a public key.
psa_sign_hash() Sign an already-calculated hash with a private key.
psa_sign_message() Sign a message with a private key. For hash-and-sign algorithms, this includes the hashing step.
5.1.1.4. Configuration

No specific configuration is required.

5.1.2. PSA initial attestation service

5.1.2.1. Overview

The PSA initial attestation service interface is described in the Arm PSA Attestation API document[7].
To use this interface, the application must include the psa/initial_attestation.h header file.

5.1.2.2. Function list

The following interface functions are implemented:

Function Description
psa_initial_attestation_get_token() Get the initial attestation token.
psa_initial_attestation_get_token_size() Get the size of the initial attestation token.
5.1.2.3. Configuration

No specific configuration is required, because the EAT key (DUA initial attestation key) is pre-provisioned by STMicroelectronics.

5.1.3. PSA internal trusted storage service

5.1.3.1. Overview

The PSA internal trusted storage service interface is described in the Arm PSA Secure Storage API document[8].
To use this interface, the application must include a psa/internal_trusted_storage.h header file.

5.1.3.2. Function list

The following interface functions are implemented:

Function Description
psa_its_set() Create a new or modify an existing UID/value pair.
psa_its_get() Get data associated with a provided UID.
psa_its_get_info() Get the metadata for the provided UID.
psa_its_remove() Remove the UID and associated data.
5.1.3.3. Configuration

No specific configuration is required.

5.1.3.3.1. ITS file system size

The ITS file system is in internal user flash memory. Its size must be a multiple of the flash memory sector size.
The Secure Manager predefined memory configuration defines the size of the Factory ITS area and the size of the ITS file system area. The ITS file system area can manage an amount of ITS user data size.

The following table gives an estimation of the maximum ITS user data size, according to ITS file system area size.

ITS file system size (KB) ITS user data size (KB)
32 11
40 19
48 27
5.1.3.4. Tips
  • The maximum data size supported by the ITS is 2016 bytes.
  • The maximum number of data supported by the ITS is 150.
  • ITS service does not implement replay protection.
  • The PSA storage API flags PSA_STORAGE_FLAG_NO_CONFIDENTIALITY and PSA_STORAGE_FLAG_NO_REPLAY_PROTECTION are not supported.

5.1.4. PSA firmware update service

5.1.4.1. Overview

The PSA firmware update service interface is described in the Arm PSA firmware update API document[9].
To use this interface, the application must include the psa/update.h header file.

5.1.4.2. Function list

The following interface functions are implemented:

Function Description
psa_fwu_query() Returns information for an image of a particular image ID.
psa_fwu_write() Writes an image to the staging area (download slot).
psa_fwu_install() Starts the installation of an image.
psa_fwu_request_reboot() Requests the platform to reboot.
psa_fwu_accept Indicates to the implementation that the upgrade was successful.
psa_fwu_abort Abort a firmware update procedure.
5.1.4.3. Configuration

No specific configuration is required.

5.2. Other interfaces

5.2.1. Power-on and system reset

After each product power-on or reset, the platform starts to execute STiRoT, STuRoT, and the Secure Manager that manages the secure initialization of the platform. If a candidate STuRoT image is present in the STuRoT secondary slot (also called download slot), STiRoT installs it in the STuRoT primary slot (also called active lot). If a candidate Secure Manager, nonsecure application, or Secure Module image is present in the respective secondary slot, STuRoT installs it in the respective primary slot.

Method of use:

  • Power-on the STM32H5 device.
  • Or reset the STM32H5 device.
5.2.1.1. Interface description

Parameters:

  • Not applicable.

Actions:

  • Power-on or system reset.
    • STiRoT is executed. STiRoT performs the installation of the STuRoT image (if required) and jumps to STuRoT after an integrity and authenticity verification. STuRoT installs the Secure Manager, Secure Module, and nonsecure application images (if required) and jumps to the Secure Manager after an integrity and authenticity verification.
    • If the integrity and authenticity verification is passed, the Secure Manager jumps to the nonsecure application.
    • If the integrity and authenticity verification fails, the Secure Manager jumps to the system bootloader or performs a system reset (depending on the OEM configuration).

Errors:

  • The platform resets in the event of any of the following errors:
    • Violation (unexpected value) of the STM32H5 option byte values related to platform security.
    • STiRoT- or STuRoT-provisioned data error (data integrity failure or wrong value).
    • Internal tamper event.
  • If the "jump to system bootloader" configuration is disabled (OEM configuration as defined in Secure Manager configuration chapter), the platform resets in the event of any of the following errors:
    • The STuRoT primary slot image is not controlled successfully (authenticity and integrity).
    • The Secure Manager primary slot image is not controlled successfully (authenticity and integrity).
    • The nonsecure application primary slot image is not controlled successfully (authenticity and integrity).
    • The module(s) primary slot image is not controlled successfully (authenticity and integrity).
  • If the "jump to system bootloader" configuration is enabled (OEM configuration as defined as Secure Manager configuration chapter), the platform jumps to the system bootloader in the event of any of the following errors:
    • The STuRoT primary slot image is not controlled successfully (authenticity and integrity).
    • The Secure Manager primary slot image is not controlled successfully (authenticity and integrity).
    • The nonsecure application primary slot image is not controlled successfully (authenticity and integrity).
    • The module(s) primary slot image is not controlled successfully (authenticity and integrity).

5.2.2. Firmware update with direct writing to secondary slot (also called download slot)

The SMAK templates and examples generate two types of encrypted and signed binary.
First binary type (.bin) contains encrypted and signed binary without 16-bytes magic word neither pre-acceptation information. This binary is used for firmware installation using PSA firmware update API
Second binary type (.hex) contains encrypted and signed binary with 16-bytes magic word and pre-acceptation information. This type (.hex) also contains programming address. This binary is used for firmware update with direct writing to download slot. This binary type is the relevant one for this chapter.

5.2.2.1. STuRoT image secondary slot interface

This interface is only available if the integrator selects the Secure Manager configuration that enables the system bootloader to act as the local loader for STiRoT.

Method of use:

  • To use the STuRoT image secondary slot, the system bootloader must be entered. For this, at least one of the STuRoT, Secure Manager, nonsecure application, or Secure Module primary slots must contain an invalid image.
  • The data must then be written in the correct image format in the STuRoT image secondary slot, and the 16-byte magic word must be written in the slot area end location. (This magic word is used by STiRoT to detect that an image to be processed is present in the secondary slot).
5.2.2.1.1. Interface description

Parameters:

  • The candidate STuROT image to be written in the STuROT image secondary slot.

Actions:

  • System reset:
    • At each system reset, the Secure Manager (STiRoT) checks if a new STuROT candidate image is present in the STuROT image secondary slot. Only STMicroelectronics can generate a new valid STuROT image.
    • When a new valid STuROT image is detected, the STiRoT component updates the STuROT image in the STuROT image primary slot.

Errors:

  • The STuROT candidate image is not installed in the STuROT image primary slot and is erased from the STuROT image secondary slot in the event of any of the following errors:
    • The STuROT image size is inconsistent.
    • Flash memory reading errors (double ECC errors).
    • Version check failure: the STuROT image version is lower than the previously installed image.
    • STuROT image integrity failure.
    • STuROT image signature failure (image not authentic).
  • The candidate STuROT image is not installed in the STuROT image primary slot and the platform resets in the event of the following error:
    • Flash memory writing or erasing errors are reported by the flash memory driver used to write data in the STuROT image primary slot area.


5.2.2.2. Secure Manager image secondary slot interface

This interface is only available if the integrator selects the STuROT configuration that enables the system bootloader to act as the local loader for STuROT.

Method of use:

  • To use the Secure Manager image secondary slot interface, the system bootloader must be entered. For this, at least one of the STuROT, Secure Manager, nonsecure application, or Secure Module primary slot must contain an invalid image.
  • The data must then be written in the correct image format in the Secure Manager image secondary slot, and the 16-byte magic word must be written in the slot area end location.
5.2.2.2.1. Interface description

Parameters:

  • The candidate Secure Manager image to be written in the Secure Manager secondary slot.

Actions:

  • System reset:
    • At each system reset, the platform (STuROT) checks if a new Secure Manager image is present in the Secure Manager image secondary slot. Only STMicroelectronics can generate a new valid Secure Manager image.
    • When a new valid Secure Manager image is detected, the STuROT updates the Secure Manager image in the Secure Manager image primary slot.

Errors:

  • The Secure Manager candidate image is not installed in the Secure Manager image primary slot in the event of the following error:
    • Version dependency failure: the version of the Secure Manager image is incompatible with the version of another image (nonsecure application or Secure Module image).
  • The candidate image is not installed in the Secure Manager image primary slot and is erased from the Secure Manager image secondary slot in the event of any of the following errors:
    • The Secure Manager image size is inconsistent.
    • Flash memory reading errors (double ECC errors).
    • Version check failure: the Secure Manager image version is lower than the previously installed image.
    • Secure Manager image integrity failure.
    • Secure Manager image signature failure (image not authentic).
  • The candidate Secure Manager image is not installed in the Secure Manager image primary slot, and the platform resets in the event of the following error:
    • Flash memory writing or erasing errors are reported by the flash memory driver used to write data in the Secure Manager image primary slot area.
5.2.2.3. nonsecure application image secondary slot interface

This interface is only available if the integrator selects the STuROT configuration that enables the system bootloader to act as the local loader for STuROT.

Method of use:

  • The nonsecure application image secondary slot region is located according to the selected flash memory layout configuration.
  • To use the nonsecure application image secondary slot interface, the system bootloader must be entered. For this, at least one of the STuROT, Secure Manager, nonsecure application, or Secure Module primary slots must contain an invalid image.
  • The data must then be written in the correct image format in the nonsecure application image secondary slot, and the 16-byte magic word must be written in the slot area end location.
5.2.2.3.1. Interface description

Parameters:

  • The candidate nonsecure application image to be written in the nonsecure application secondary slot.

Actions:

  • System reset:
    • At each system reset, the platform (STuROT) checks if a new nonsecure application image is present in the nonsecure application image secondary slot. The PC tool STM32TrustedPackageCreator and the .xml file are delivered to the OEM for the generation of a nonsecure application binary image with the right format.
    • When a new nonsecure application image is detected, STuRoT updates the nonsecure application image in the nonsecure application image primary slot.

Errors:

  • The nonsecure application candidate image is not installed in the nonsecure application image primary slot in the event of the following error:
    • Version dependency failure: the version of the nonsecure application image is incompatible with the version of another image (Secure Manager or Secure Module image).
  • The candidate image is not installed in the nonsecure application image primary slot and is erased from the nonsecure application image secondary slot in the event of any of the following errors:
    • The nonsecure application image size is inconsistent.
    • Flash memory reading errors (double ECC errors).
    • Version check failure: the nonsecure application image version is lower than the previously installed image.
    • nonsecure application image integrity failure.
    • nonsecure application image signature failure (image not authentic).
  • The candidate nonsecure application image is not installed in the nonsecure application image primary slot and the platform resets in the event of the following error:
    • Flash memory writing or erasing errors are reported by the flash memory driver used to write data in the nonsecure application image primary slot area.
5.2.2.4. Modules image secondary slot interface

This interface is only available if the integrator selects the STuROT configuration that enables the system bootloader to act as the local loader for STuROT.

Method of use:

  • The Secure Module image secondary slot region is located according to the selected flash memory layout configuration.
  • To use the Secure Module image secondary slot interface, the system bootloader must be entered. For this, at least one of the STuROT, Secure Manager, nonsecure application, or Secure Module primary slots must contain an invalid image.
  • The data must then be written in the correct image format in the Secure Module image secondary slot, and the 16-byte magic word must be written in the slot area end location.

Parameters:

  • The candidate Secure Module image to be written in the Secure Module secondary slot.

Actions:

  • System reset
    • At each system reset, the platform (STuROT) checks if a new Secure Module image is present in the Secure Module image secondary slot. The PC tool STM32TrustedPackageCreator and the xml file are delivered for the generation of a Secure Module binary image with the right format.
    • When new Secure Module images are detected, the STuROT updates the Secure Module images in the Secure Module images primary slot.

Errors:

  • The Secure Module candidate images are not installed in the Secure Module image primary slot in the event of the following error:
    • Version dependency failure: the version of the Secure Module image is incompatible with the version of another image (Secure Manager or nonsecure application image).
  • The candidate image is not installed in the Secure Module image primary slot and is erased from the Secure Module image secondary slot in the event of any of the following errors:
    • The Secure Module image size is inconsistent.
    • Flash memory reading errors (double ECC errors).
    • Version check failure: the Secure Module image version is lower than the previously installed image.
    • Modules application image integrity failure.
    • Modules application image signature failure (image not authentic).
  • The candidate Secure Module image is not installed in the Secure Module image primary slot and the platform resets in the event of the following error:
    • Flash memory writing or erasing errors are reported by the flash memory driver used to write data in the Secure Module image primary slot area.

5.2.3. X509 certificates for DUA

5.2.3.1. Overview

Two X509 certificates are provisioned in STMicroelectronics devices for DUA initial attestation and the DUA user. The interface is provided to access these certificates. To use the interface, the application must include the util_cert.h header file.

5.2.3.2. Function list

The following interface functions are implemented:

Function Description Comment
UTIL_CERT_GetCertificateSize() Get certificate size. DUA initial attestation or DUA user identifiers are used to select the certificate.
UTIL_CERT_GetCertificate() Get certificate (raw binary). DUA initial attestation and DUA user are used to select the certificate.

6. System consideration

This chapter describes the system requirements that must be met to develop a product based on the Secure Manager.

6.1. Resource sharing

The hardware resources (peripherals, memory) are shared between the nonsecure application, Secure Manager, and Secure Modules.
These resources can be:

  • Allocated exclusively to the Secure Manager.
  • Allocated exclusively to a Secure Module (via the Secure Module header).
  • Allocated exclusively to the nonsecure application.
  • Shared between the nonsecure application, Secure Manager, and Secure Module.

All resources not used by Secure part are fully available for NonSecure.

Note:

  • If the resource is shared, the OEM is responsible for ensuring that there is no conflict.

6.1.1. Secure Manager resources

The Secure Manager is executed in secure domain and reserves some resources for its own usage.
Reserved resources are controlled with different policies:

  • Exclusive control: the resource is reserved for the Secure Manager. The nonsecure application and Secure Modules can access some of these, only through the Secure Manager API.
  • Nonexclusive control: a part of the resource is reserved for the Secure Manager. The nonsecure application and Secure Modules can access only this part through the Secure Manager API.
  • Secure Manager API access: the nonsecure application and Secure Modules can access the reserved resource only through the Secure Manager API (Secure Manager middleware API for nonsecure applications or Secure Manager Core API for Secure Modules).

The table below describes the reserved resources of Secure Manager.

Peripheral Exclusive control Accessible via Secure Manager API Comment
UART x No ??? x configured by OEM through configuration parameters; can be disabled.
SAU, MPU_S Yes No
SYSTICK_S, NVIC_S Yes No
DMA 2 Yes* Yes *Yes only if a Secure Module uses one DMA2 channel.
GTZC Yes No
RNG Yes Yes
TAMP No No Only the tamper protection TAMP resource is controlled by the Secure Manager.
PKA Yes Yes
AES Yes No
SAES Yes Yes
HASH Yes Yes
FLASH No No The secure FLASH registers are only accessible by the Secure Manager (the secure registers are fixed by the hardware). The nonsecure FLASH registers are only accessible by the nonsecure domain. The nonsecure application can access ITS file system using PSA internal trusted storage API.
I-CACHE Yes No
RAMCFG Yes No
GPIO Yes* Yes* *Yes only if a Secure Module uses this GPIO pin, in which case it is controlled exclusively by the Secure Module.



6.1.2. Secure Module resources

In addition to the Secure Manager, some Secure Modules can use peripherals and declare them as nonsharable. The list of used peripherals is part of each Secure Module header, and is parsed by the Secure Manager at boot time. These peripherals are controlled exclusively by the Secure Manager core and are no longer accessible to other Secure Modules or the nonsecure application.
It is the responsibility of the system integrator (OEM) to ensure that there are no conflicts between the nonsecure application, Secure Manager, and Secure Modules.

The table below describes the reserved resources of Secure Manager.

Peripheral Exclusive control Accessible via Secure Manager API Comment
UART x No ??? x configured by OEM through configuration parameters; can be disabled.
SAU, MPU_S Yes No
SYSTICK_S, NVIC_S Yes No
DMA 2 Yes* Yes *Yes only if a Secure Module uses one DMA2 channel.
GTZC Yes No
RNG Yes Yes
TAMP No No Only the tamper protection TAMP resource is controlled by the Secure Manager.
PKA Yes Yes
AES Yes No
SAES Yes Yes
HASH Yes Yes
FLASH No No The secure FLASH registers are only accessible by the Secure Manager (the secure registers are fixed by the hardware). The nonsecure FLASH registers are accessible by the secure domain and nonsecure domain.
I-CACHE Yes No
RAMCFG Yes No
GPIO Yes* Yes* *Yes only if a Secure Module uses this GPIO pin, in which case it is controlled exclusively by the Secure Module.


6.2. Clocking

6.2.1. Clocking versus Secure Manager resources

6.2.1.1. RNG clocking

The RNG peripheral is owned by the Secure Manager and is used behind some cryptographic operations (based on PKA, SAES...).
To ensure correct RNG behavior, the clock requirement described in RM0481[10] (chapter 32.3.6) must be met (dependency between AHB bus clock and RNG clock).
The nonsecure application and Secure Module must ensure that this requirement is met. Generally, the non-secure application initializes the clock during its initialization phase.

6.2.2. Clocking in nonsecure application and Secure Module

Changing the system clock configuration (system clock selection) and the peripheral clock configuration (enable, disable, reset) in the nonsecure application can affect the Secure Module peripheral behavior. The OEM must ensure that the system clock dependency requirement between the nonsecure application and Secure Modules is met.

7. Memory mapping

7.1. User flash memory mapping

The user flash memory is composed of several areas. The main ones are the Secure Manager, Secure Modules, and nonsecure application.

The OEM must select the Flash Layout configuration index (see "Secure Manager Configuration").

The Flash Layout configuration is an index that select pre-defined flash mapping:

  • The ITS storage size (Factory ITS and ITS file system).
  • The number of modules and their size.
  • The nonsecure application size.

This configuration automatically defines the flash memory mapping described in the following table.

Flash layout configuration SMAK_0 SMAK_1
Factory ITS size (KB) 8 8
ITS file system size (KB) 40 40
Number of modules 0 1
Modules 0 size (KB) NA 128
Modules 0 address NA 0x806E000
nonsecure application size (KB)1 max 584 max 456
nonsecure application address 0x806E000 0x808E000
nonsecure reserved area size (KB)1 min 0 min 0
nonsecure reserved area address1 0x8100000 - nonsecure reserved area size 0x8100000 - (nonsecure reserved area size/2)


Notes:

  1. Once the flash layout configuration index has been chosen, the OEM must configure the nonsecure reserved area size (which implicitly defines the nonsecure application size). The nonsecure application size is reduced by half of the nonsecure reserved area size. Nonsecure reserved area can be used for nonsecure non-volatile data storage for example. (See "#Flash_memory_nonsecure_reserved_area")

7.2. SRAM mapping

The static random access memory (SRAM) is composed of several areas. The main areas are the Secure Manager, Secure Modules, and nonsecure application.

SRAM mapping is the same whatever the Secure Manager binary and Secure Manager memory configuration index.

The OEM must configure:

  • The SRAM size used for communication between the nonsecure application and Secure Manager (located at end of SRAM1): shared buffer area
  • The SRAM size used by each Secure Module (located in SRAM3, contiguously to Secure Manager SRAM).

See Secure Manager configuration chapter for details on SRAM configuration.

The table below describes the SRAM mapping.

SRAM address owner size (KB)
SRAM3 0x20063000 + Module 0 SRAM size nonsecure application 244 max
SRAM3 0x20063000 Module 0 0 min
SRAM2/3 0x20040000 Secure Manager 140
SRAM1 0x20040000 - Shared buffer area size Shared buffer area 4 min, 248 max
SRAM1 0x20000000 nonsecure application 256 - Shared buffer area size


8. Performances

TO BE COMPLETED
Time to boot
Time to install
Time to call SPE service from NSPE
Time to schedule a secure IRQ
Time to schedule a non-secure IRQ

9. Secure Manager configuration

Prior to its installation, the Secure Manager needs to be configured.

As mentioned in the introduction, the Secure Manager Access Kit is used in two phases:

  • Development, to develop a nonsecure application that uses the Secure Manager services.
  • Production preparation, to prepare the encrypted images for OEM secure manufacturing.

These phases have different constraints for the installation.

For example, the debug may be open/permissive in the development phase to allow developers to debug their application, whereas it will be closed by default and strictly controlled by Debug Authentication in the production preparation phase.

There may also be different memory configuration constraints between the development and production preparation phases.

The Secure Manager configuration is thus an important step.

Warning white.png Warning
The Secure Manager must be configured so as to be in line with the phase.

The phase constraints are listed in each configuration step below.

9.1. Configuration steps overview

The figure below shows an overview of the configuration steps.

Secure Manager configuration steps




































The following chapters provide more details regarding the different configuration steps.

9.2. Secure Manager package binary selection

9.2.1. Profile

A Secure Manager profile defines the features supported by the Secure Manager.
STM32H5 provides only the Secure Manager Large profile (supporting initial attestation, internal trusted storage, firmware update, cryptography with large number of algorithms...).

9.2.2. Mode

In SMAK, the Secure Manager mode is Manufacturing. The Module development mode is used in the Secure Manager Development Kit.

Info white.png Information
There is nothing to configure at this step; SMAK provides one Secure Manager package binary file (.ssfi).

9.3. Secure Manager package configuration

9.3.1. Memory configuration

The OEM defines the layout of the user flash memory by configuring the following items:

  • The Secure Manager pre-defined memory configuration
  • The nonsecure reserved area of the flash memory.
  • The SRAM secure/nonsecure interface.
  • The secure SRAM layout.
9.3.1.1. Secure Manager memory configuration

The OEM must select one of the following Secure Manager memory configurations (see Memory mapping chapter):

  • SMAK_0
  • SMAK_1
9.3.1.2. Flash memory nonsecure reserved area

The OEM must configure the size of the reserved non-secure flash area (to not be used by the nonsecure application code). This size has a granularity of 16 KB. For example, this area can be used by the nonsecure application to store some data. By default, the size is 0 KB.

This configuration impacts the size of the nonsecure application image:

  • The size of the nonsecure application active and download slots are reduced by the nonsecure flash memory reserved area size divided by two.
  • The nonsecure reserved area is inserted between the nonsecure application active slot and the nonsecure application download slot.















9.3.1.3. SRAM nonsecure /secure shared buffer

The nonsecure application and Secure Manager use a shared buffer located at the end of SRAM1 to share data between nonsecure application and Secure Manager. The minimum size of this buffer is 4 KB, with a maximum of 248 KB. The size granularity is 1 KB.

The OEM must configure the size of this shared SRAM buffer. The OEM tailors the nonsecure /secure shared buffer size to fit the secure services requirements used by their application.

9.3.1.4. Secure SRAM layout

The OEM must configure the SRAM allocated to secure domain (secure SRAM), considering that the Secure Manager and Secure Modules run within SPE.
The Secure Manager uses 140 KB of SRAM. This SRAM, allocated to STM32TRUSTEE, starts at the beginning of SRAM2 (0x30040000) and finishes at 0x030062FFF.
The OEM can extend the size of the secure SRAM by increasing the secure SRAM end address with a 4 KB granularity:

  • If the OEM chooses the flash memory layout configuration SMAK_0 (without modules), they can set the SRAM end address to 0x30062FFF.
  • If the OEM chooses the flash memory layout configuration SMAK_1 (with one module), they must set the SRAM end address to a value that fits the needs of the modules. The third-party module provider must provide the OEM with this value.

9.3.2. Minimal Product state

The OEM must configure the minimal product state. The boot stage will execute the application only if the product state programmed in option byte is equal or greater than the "Product state minimal allowed".
This minimal product state can be either:

  • TZ-Closed:
    • Debug: a debug connection to the OEM’s nonsecure application is allowed natively. Then, the OEM allows the execution of one or several commands through the Debug Authentication service:
    • Regression: the STM32H5 MCU fully erases the user flash memory and falls back to the product state Open.
  • Closed: the OEM can allow the execution of one or several commands through the Debug Authentication service:
    • Debug: the STM32H5 MCU grants a debug connection to the OEM’s nonsecure application.
    • Regression: same as TZ-Closed.
    • Partial regression: the STM32H5 device fully erases the nonsecure user flash memory (but keeps the secure user flash unchanged) and falls back to the product state TZ-Closed.
  • Locked: the OEM forbids all Debug Authentication services listed above. In this product state, the user cannot leverage Debug Authentication features, such as Debug reopening and regressions.
9.3.2.1. Development phase

The OEM must set the product state to TZ-Closed or Closed.
We recommend setting the product state to TZ-Closed. In this case, the debugging of the nonsecure application is allowed natively (without a Debug Authentication service).

Warning white.png Warning
In the development phase, the OEM must not sets the product state to Locked.
9.3.2.2. Production preparation phase
Warning white.png Warning
In the production preparation phase, the OEM must sets the product state to Closed or Locked. It can also use Locked for test purpose, but it will no more be possible to re-open the device.

9.3.3. System clock

By default, the system clock speed during the device initialization (until the nonsecure application is entered) is 250 MHz (using PLL with HSI input).

During the device initialization and depending on the voltage supply level and the range of temperature supported, the OEM can change the system clock speed to:

  • 200 MHz (using PLL with HSI input).
  • 64 MHz (using HSI).

When started, the nonsecure application can fully reconfigure the clocks according to its needs.

9.3.4. Authentication of Module with license

The Secure Manager supports two installation models for module with license (third-party):

  • Model #1: Modules with license (third party module) shall not be signed by OEM
  • Model #2: Modules with license (third party module) shall be signed by OEM

The OEM must choose between Model #1 and Model #2.

9.3.5. System bootloader

When the device finds an invalid image right after reset, depending on the OEM's configuration, it can either reset or jump to the system bootloader that acts as the local loader.
The invalid image can be either a STuRoT, Secure Manager, nonsecure application, or module image.
Jumping to the system bootloader and using a PC host physically connected to the STM32H5 device, you can download a new valid image.
The OEM can configure the Secure Manager behavior to reset or to jump to the system bootloader as a response to invalid image detection.
This configuration can be performed at two level:

  • STiRoT level: managing STuRoT firmware image
  • STuRoT level: managing Secure Manager, nonsecure application, and module image

9.3.6. Factory Internal Trusted Storage (ITS)

By default, the Secure Manager provisioning environment stores a factory ITS blob containing dummy data. This factory ITS blob is securely provisioned in the ITS area during the provisioning phase.
The OEM can change the factory ITS blob content to include their own keys and data, which can be used by the application at runtime, through a secure ITS service.

The ITS blob can be prepared using the STMicroelectronics ITS builder tool. For more information on the ITS builder, refer to the ITS builder documentation in STM32CubeH5 [3] at ./Utilities/PC_Software/ITSbuilder/README.md.

9.3.7. Secure Manager keys

The OEM must configure keys the Secure Manager uses for authentication and decryption of firmware images.

  • The Secure Manager encryption key: an asymmetric ECC secp256r1 private key. This key is used to decrypt the nonsecure application and modules (except modules with license) images.
  • The Secure Manager authentication key: an asymmetric ECC secp256r1 public key. This key is used to authenticate the nonsecure application and modules (except modules with license, not signed)
9.3.7.1. Development phase

There are two possibilities:

  • The OEM uses the default Secure Manager keys.
  • The OEM modifies the default Secure Manager keys to use their own keys.
9.3.7.2. Production preparation phase
Warning white.png Warning
In the production preparation phase, the OEM must update the default Secure Manager keys and use their own keys.

9.3.8. Debug Authentication configuration

The OEM provides the Debug Authentication (DA) configuration to be able to perform the DA procedure.

Warning white.png Warning
Without proper DA configuration, a target regression/update is impossible.

DA configuration contains a set of DA keys/certificates and permissions.

9.3.8.1. DA keys/certificates

The DA uses an asymmetric public key to authenticate a genuine user with its credential (a certificate) when reopening a debug connection and/or performing a regression.
The OEM must change the DA asymmetric public key to their own key.

9.3.8.2. DA permissions

DA permission lists are restricted by the Secure Manager installation procedure.

The OEM must configure the permissions among:

  • Full regression
  • Partial regression
  • nonsecure application debug reopening.

9.3.9. Modules

The OEM can choose to add their own secure functions to a Secure Module or to add a third-party Secure Module inside the secure domain in the unprivileged part. The OEM must select a Secure Manager memory configuration compatible with the integrated module number and size.
The OEM uses the kernel APIs to access the Secure Manager and complies with the Secure Manager rules to export the new secure services API to the nonsecure application.


The integrated module can be licensed or not.


9.4. Option byte (OB) configuration

The OEM must configure the STM32H5 MCU option bytes to fit the device requirements. The OEM can configure the option bytes mentioned in the table below: Other option bytes are configured by Secure Manager package and can not be changed by OEM.

register BitField
OPTSR_PRG

IWDG_STDBY
IWDG_STOP
IO_VDDIO2_HSLV
IO_VDD_HSLV
PRODUCT_STATE
NRST_STDBY
NRST_STOP
IWDG_SW
BORH_EN
BOR_LEV

OPTSR2_PRG

USBPD_DB_DIS
SRAM2_PAR
SRAM3_ECC
BKPRAM_ECC
SRAM1_3_RST


Warning white.png Warning
The OEM must configure the PRODUCT_STATE option byte in compliance with the configuration of minimal Product state.

More constraining product states are in following increasing order:

  • TZ-Closed
  • Closed
  • Locked

The OEM must refer to RM0481[10] for more details regarding the option bytes mentioned in the table above.

10. Use cases

This chapter describes the main use cases available through SMAK.

UC category UC name Comment
Initial installation
The OEM creates their encrypted firmware for the secure firmware installation (SFI). Simple configuration. Firmware from STMicroelectronics, OEM, and third party.
Firmware: Secure Manager package, Secure Manager package configuration, nonsecure application, device configuration (option bytes).
The OEM installs the firmware using SFI. Simple configuration. Firmware from STMicroelectronics, OEM, and third party.
Firmware: Secure Manager package, Secure Manager package configuration, nonsecure application, device configuration (option bytes).
The OEM creates their encrypted firmware (for SFI). Full configuration. Firmware from STMicroelectronics, OEM, and third party.
Firmware: Secure Manager package, Secure Manager package configuration, nonsecure application, device configuration (option bytes). Optional: Secure Modules and diversified data (ITS).
The OEM installs the firmware using SFI. Full configuration. Firmware from STMicroelectronics, OEM, and third party.
Firmware: Secure Manager package, Secure Manager package configuration, nonsecure application, device configuration (option bytes). Optional: Secure Modules and diversified data (ITS).
Installation and update
The OEM gets the new STuRoT encrypted image from STMicroelectronics.
The OEM updates the STuRoT.
The OEM gets the new encrypted Secure Manager image from STMicroelectronics.
The OEM updates the Secure Manager.
The OEM creates their new encrypted nonsecure application.
The OEM updates the nonsecure application.
The OEM creates their new encrypted Secure Module.
The OEM installs/updates the OEM Secure Module.
The OEM installs/updates a third-party Secure Module (without image counting). Third party can be STMicroelectronics, the OEM, or third-party company (owner of the module).
The OEM installs/updates a third-party Secure Module (with image counting). Secure Module must be previously installed with SFI
The OEM signs the third-party Secure Module with their own key.
The OEM updates a third-party Secure Module with OEM authentication (without image counting).
The OEM signs the third-party Secure Module with their own key.
The OEM updates a third-party Secure Module with OEM authentication (with image counting). Secure Module must be previously installed with SFI.
Debug reopening and regression
The OEM performs a partial regression. Firmware and data located in nonsecure domain (nonsecure application) are erased. Device in TZ-Closed product state.
The OEM performs a full regression. Firmware and data located in nonsecure and secure domains are erased. Device in Open product state.
The OEM opens the nonsecure domain to debug their nonsecure application. Firmware and data located in nonsecure domain are not erased. Device in TZ-Closed product state.
PSA services - Internal Trusted Storage
The OEM uses PSA Internal Trusted Storage (ITS) to set and get data and keys in ITS. Data and key confidentiality is ensured by encryption.
PSA services - Firmware update
The OEM uses PSA firmware update API to download firmware. Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules.
The OEM uses PSA firmware update API to request installation of firmware. Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules.
The OEM uses PSA firmware update API to abort installation of firmware. Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules.
The OEM uses PSA firmware update API to install or update firmware. Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules.
The OEM uses PSA firmware update API to validate candidate firmware. Firmware: Secure Manager, nonsecure application, Secure Modules.
PSA services - Cryptography
The OEM uses PSA cryptography API to encrypt or decrypt data.
The OEM uses PSA cryptography API to sign or verify data.
The OEM uses PSA cryptography API to hash data.
The OEM uses PSA cryptography API to generate random number of key.
PSA services - Initial Attestation
The OEM uses PSA initial attestation API to get an authenticated token and its size. This token is used by the server to uniquely identify an STMicroelectronics device from the OEM.
ST DUA pre-provisioned key
The OEM uses the STMicroelectronics CA initial attestation key pair to authenticate STMicroelectronics devices. PSA initial attestation compliant.
The OEM uses the STMicroelectronics CA user key pair to authenticate STMicroelectronics devices.
Internal Trusted Storage (ITS) provisioning
The OEM uses the ITS builder tool to prepare an ITS blob. ITS blob can be different for each STMicroelectronics device and is later provisioned on STMicroelectronics device using SFI procedure.
System bootloader - Firmware update
The OEM uses the system bootloader to download firmware. Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules.
The OEM uses a system reset after firmware download via the system bootloader to install or update firmware. Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules.
The OEM uses the PSA firmware update API to validate candidate firmware. Firmware: STuRoT, Secure Manager, nonsecure application, Secure Modules.

10.1. UC category: ST DUA pre-provisioned key

10.1.1. UC name: The OEM uses STMicroelectronics CA initial attestation key pair to authenticate STMicroelectronics devices

To ease OEM manufacturing, STMicroelectronics has pre-provisioned each device with an ECC chip unique key and X509 certificates, used for Device Unique Authentication during the initial attestation phase. The ECC private key is used by the PSA initial attestation service to sign the token.

The typical usage is described below.

During STMicroelectronics device manufacturing:

  • STMicroelectronics provisions the DUA initial attestation chip private key and certificate for each device.

Between STMicroelectronics and OEM offices:

  • STMicroelectronics delivers the STMicroelectronics CA DUA certificate to the OEM. This CA certificate is delivered under license and must be requested from STMicroelectronics.

Two options are possible:

Option 1: the OEM builds the OEM device list at OEM manufacturing.

At OEM product manufacturing:

  • The OEM gets the DUA chip public key for each device to create an OEM device database.

In the field:

  • The server requests the STMicroelectronics DUA chip certificate from the device.
  • The server authenticates this certificate using the STMicroelectronics CA DUA certificate and gets the authenticated STMicroelectronics DUA chip public key from this certificate.
  • The server verifies that this key is part of the OEM device database.
  • The server requests an initial attestation token from the device.
  • The server authenticates this token using the STMicroelectronics DUA chip public key.
  • The server can now use the authenticated token (for example, to identify firmware versions and firmware measurements).

Option 2: the OEM authenticates the OEM device based on the authenticated initial attestation token field instance ID.

At OEM product manufacturing:

  • The OEM does not create the OEM device database at OEM manufacturing, but uses the initial attestation procedure (in the field) to get the authenticated token claim (field Instance ID: hash of the initial attestation public key) to authenticate OEM devices

In the field:

  • The server requests the STMicroelectronics DUA chip certificate from the device.
  • The server authenticates this certificate using the STMicroelectronics CA DUA certificate and gets the authenticated STMicroelectronics DUA chip public key from this certificate.
  • The server requests an initial attestation token from the device.
  • The server authenticates this token using the STMicroelectronics DUA chip public key.
  • The server uses this authenticated token (field instance ID: hash of the initial attestation public key) to authenticate that this STMicroelectronics device is an OEM device.
  • The server can now use the authenticated token (for example to identify firmware versions and firmware measurements).
10.1.2. Use case: OEM uses the STMicroelectronics CA user key pair to authenticate 'STMicroelectronics devices

To ease OEM manufacturing, STMicroelectronics has pre-provisioned each device with an ECC chip private key and X509 certificate for user purposes. This ECC chip private key is used to sign some messages and is accessible through the PSA cryptography API using a key ID (opaque key). It can be used, for example, for TLS X509 mutual authentication (challenge, response).

The typical usage of this key and certificate is described below.

At STMicroelectronics device manufacturing:

  • STMicroelectronics provisions the DUA user chip private key and certificate on each device.

Between STMicroelectronics and OEM offices:

  • STMicroelectronics delivers the STMicroelectronics CA DUA user certificate to the OEM. This CA certificate is delivered by STMicroelectronics as part of STM32CubeFW.

At OEM product manufacturing:

  • The OEM gets the DUA user chip public key for each device to create an OEM device database.

In the field:

  • The server requests the STMicroelectronics DUA user chip certificate from the device.
  • The server authenticates this certificate using the STMicroelectronics CA DUA user certificate and gets the authenticated STMicroelectronics DUA chip public key from this certificate.
  • The server verifies that this key is part of its OEM device database.
  • The server sends a hash to the device and requests a signature of this hash.
  • The device performs the signature of this hash using the STMicroelectronics DUA user chip unique private key.
  • The server authenticates this hash signature using the authenticated STMicroelectronics DUA user chip public key.
  • The server is now sure to communicate with authentic STMicroelectronics devices from this OEM.


11. Secure Manager manufacturing

As we have seen in the introduction, SMAK is used in the manufacturing preparation phase to prepare the encrypted images for the OEM secure manufacturing (SFI).

Refer to SFI for STM32H5 to see how the output of the SMAK manufacturing preparation phase is used in the SFI procedure.

12. Debug

The STM32H5 device supports the PSA Authenticated Debug Access Control (ADAC) protocol.

After the Secure Manager installation, the STM32H5 device is set at least to the TZ-Closed product state, which means that the secure domain is not accessible via JTAG. Moreover, the OEM can decide to set the device to the Closed or Locked product state, which means the nonsecure application is no longer accessible via JTAG either.

In such states, it is no longer possible to debug the installed firmware (secure or nonsecure) via JTAG.

In the Closed product state, the OEM can use the ADAC protocol to:

  • Reopen the nonsecure debug (moving to a TZ-Closed product state). This way, the OEM can debug their nonsecure application.
  • Perform a partial regression of the nonsecure part (moving to a TZ-Closed product state). This way, the OEM can reinstall their nonsecure application.
  • Perform a full regression (moving to an Open product state). This way, the OEM can reinstall the Secure Manager, Secure Modules, and a nonsecure application.

In the Locked product state, it is definitely not possible to reopen debugging or to perform regressions.

For more information on authenticated debug access protocol, refer to Debug Authentication for STM32H5.

13. Trace and log

13.1. nonsecure application

The OEM can implement their own trace and log in their nonsecure application (log in RAM, trace over UART, etc.).

13.2. Secure Manager

13.2.1. At boot time

If the Secure Manager detects an error at boot time, it generates a reset or jumps to the system bootloader. The boot error code is accessible via the STM32cubeProgrammer discovery command.

13.2.2. At runtime

The nonsecure application calls the Secure Manager functions at runtime. In the event of an error, the Secure Manager function returns an error code that can be used by the nonsecure application for debugging purposes.

14. Getting started

For the Secure Manager hardware and software environment setup, installation procedure, and step-by-step execution, refer to how to start with Secure Manager on STM32H573.

15. Troubleshooting


16. Acronyms

See Acronyms.

17. References