STM32WB1M Discovery Kit Out Of Box Demonstration

Revision as of 13:58, 28 July 2023 by Registered User

1. Introduction

OOB WB1M Board Package
STM32StepByStep OOB WB1M Introduction Board Packaging.jpg




2. Setup Part

OOB WB1M Setup B-WB1M-WPAN1
STM32StepByStep OOB WB1M Setup B-WB1M-WPAN1.jpg


3. Hands On

3.1. Application Interface

To begin using your B-WB1M-WPAN1 board, you will require an interface for communication and interaction.

Here are two application interface solutions :

  • ST BLE Sensor, available on IOS and Android
  • ST Web Bluetooth App Interface, running on a compatible web browser
OOB WB1M System Presentation
STM32StepByStep OOB WB1M System Presentation.jpg


With one of these two solutions, you will be able to communicate with your BLE board and establish a connection.

For the rest of the demonstration, we will be using the Android application ST BLE Sensor.

3.2. Let's Get Started

Make sure the board is powered and running.
Open the ST BLE Sensor Application.

You should now see your WB1M board on the homepage. Note that the Bluetooth Device Address and the RSSI are stated just below. Click on your WB1M board to connect. If you don’t see it, try clicking the refresh button at the bottom.

Connection to the B-WB1M-WPAN1 board with ST BLE Sensor App
WB1M ST BLE Sensor Connection.jpg



3.2.1. Home Page

Here is the main page where you can find all the features implemented with the embedded application.

Now let's have a look at all the implemented services:

  • BLE Sensor (Environmental / Plot Data)
  • p2pServer (Led Control)
  • HeartRate

You can now click on them to play with.

ST BLE Sensor Features Page
SensorsLed ControlHearRateWB1M ST BLE Sensor Features Page.jpg


3.2.2. HearRate Service

In the HeartRate interface, Hear Rate and energy measurement are launched and displayed in graphs, you can reset the energy measurement.

For more information about it, click here : STM32WB_HeartRate

HeartRate
ST BLE Sensor HeartRate.jpg



3.2.3. Led Control

In the LED control panel, you can turn the LED on and off for your board. Additionally, you can receive a notification by clicking on the board's button.

You can find more information about ours Peer To Peer examples here : Peer_To_Peer

Led Control
ST BLE Sensor Led Control.jpg



3.2.4. Environmental and Motion Sensors

Now let’s have a look a the sensors panel.

For the environmental part you can find temperature and the humidity measured by the STTS22H sensor of your WB1M.

You can click on the button in the top right to switch between units, from degrees to Fahrenheit.

Environmental Sensor
ST BLE Sensor Environmental Sensor.jpg


Regarding the Plot Data tab:

puce1.png
Click on the dropdown arrow
puce2.png
Select a motion data sensor to view real-time data
Motion Sensor (1/2)
STM32StepByStep OOB WB1M ST BLE Sensor Motion Sensor 1 2.jpg


puce3.png
Click on the play/pause button
Motion Sensor (2/2)
STM32StepByStep OOB WB1M ST BLE Sensor Motion Sensor 2 2.jpg



4. What Next ?

4.1. How can I flash my WB1M board ?

No categories assignedEdit