Certification guideline with STM32WB and STM32WBA

Revision as of 10:38, 20 July 2023 by Registered User


This page contains information related to Bluetooth® Low Energy or regional (CE, FCC) certification.



1. STMicroelectronics tools for certification

STMicroelectronics is providing a dedicated FW called transparent FW that will be used for certification purpose.
We are also providing a dedicated GUI PC tool called Cube Monitor RF PC tool that will be used for regional RF certifications.

1.1. Transparent mode FW

A set of commands/events are sent though the STM32WB/WBA UART or USB to control the Bluetooth® Low Energy stack via the transparent mode application.

1.1.1. STM32WB1x, STM32WB3x, STM32WB5x

Transparent mode FW is available in STM32CubeWB software package.
It is available in source code and it must eventually be rebuilt according customer HW configuration (UART interface used, SMPS used or not, etc.)
Be careful, stm32wbxx_BLE_Stack_full_extended_fw binary is mandatory with transparent mode FW.

if UART interface is used, refer FW example available in P-NUCLEOWB55 Nucleo folder.
if USB interface is used, refer FW example available P-NUCLEOWB55 USBDongle folder.

1.1.2. STM32WBA5x

It is available in STM32CubeWBA software package.
Transparent mode FW is available in source code and it must eventually be rebuilt according customer HW configuration (UART interface used, SMPS used or not, etc.)



1.2. Cube Monitor RF PC tool

Cube Monitor RF is a PC tool for quickly testing the RF performance of STM32WB-based hardware devices.


Thanks to RF Tests panel, device under test can quickly be set in the required mode (Rx or Tx), modulation or power.


2. Bluetooth® certification

2.1. Bluetooth® Low Energy (BLE) qualification process

All products using Bluetooth® technology must complete the Bluetooth Qualification process. Please refer to below SIG webpage.
https://www.bluetooth.com/develop-with-bluetooth/qualification-listing
Bluetooth Qualification process is not a matter of putting BT logo on product or not, it is a matter of using a licensed technology.


2 possible paths for qualification process :
No required testing
✓ I am designing a product based on a STMicroelectronics pre-certified module such as STM32WB5MMG or STM32WB1MMC
✓ I am designing a product based on an already qualified design using STM32WB chipset and I made no change in schematics and layout.

Required testing
✓ I am designing a product based on a STMicroelectronics chipset such as STM32WB or STM32WBA


Launch studio Process flow
Launch studio process is described step by step in dedicated chapter.
Whatever STM32WB or STM32WBA chipset or associated modules, STMicroelectronics is not providing End Product devices so that Required Testing path should be used.
Below pictures is providing main qualification steps and associated costs.

RF PHY reports for STM32WB modules can be found on st.com:


Is SW testing required?
Whatever path selected, no SW testing is required except if using adopted standard profiles.


Where is done BT qualification?
If testing is required, qualification testing process must be done in an official Bluetooth Qualification Test Facility (BQTF)
A Bluetooth Qualification Test Facility (BQTF) is formally recognized by the Bluetooth SIG as competent to perform those Bluetooth qualification conformance tests.
List of official BQTF is available on Bluetooth website.
https://www.bluetooth.com/develop-with-bluetooth/qualification-listing/qualification-test-facilities.


2.2. Available QDIDs

Below tables are summarizing all available PHY and host stack QDIDs for STM32WB / STM32WBA family
When moving to certification, customers should select PHY and stack QDID depending STMM32WBx selected version or stack/features used.
As a reminder:

  • You will need to start launch studio process from the latest mandatory TCRL
  • It will ensure interoperability between a 5.1 device and 5.3 device for example
  • All BLE features are optional so you will "pickup" features needed for your application


STM32WB PHY QDID

Package Part number Cut version RF PHY QDID
QFN48 STM32WB55Cx (BLE5.2 - 2Mbit/s)
STM32WB50Cx (BLE5.2 - 1Mbit/s)
STM32WB35Cx (BLE5.2 - 2Mbit/s)
STM32WB30Cx (BLE5.2 - 1Mbit/s)
Y or X 161807 (TCRL 2021-1)
STM32WB15CCU6E (BLE5.2 – 2Mbit/s)
STM32WB10CCU5E (BLE5.2 – 1Mbit/s)
Y or X 164054 (TCRL 2020-1)
STM32WB15CXX6 (BLE5.2 – 2Mbit/s)
STM32WB10CXX5 (BLE5.2 – 1Mbit/s)
Y or X 161969 (TCRL 2020-1)
QFN68 STM32WB55Rx (BLE5.0 - 2Mbit/s) Y 127495 (TCRL 2023-1)
CSP 100 STM32WB5xVY (BLE5.1 - 2Mbit/s) Y 134665 (TCRL 2021-1)
STM32WB55VY (BLE5.3 - 2Mbit/s) X 178970 (TCRL 2021-2)
BGA129 STM32WB55Vxx (BLE5.2 - 2Mbit/s) Y or X 161808(TCRL 2021-1)
WLCSP49 STM32WB15CCY (BLE5.2 – 2Mbit/s)
STM32WB10CCY (BLE5.2 – 1Mbit/s)
Y or X 170241 (TCRL 2020-1)
Module 86-pin LGA STM32WB5MMG (BLE5.2 – 2Mbits/s) Y 170767 (TCRL 2020-1)
STM32WB5MMG (BLE 5.3 - 2Mbits/s) X 187035 (TCRL2021-2)
Module 77-pin LGA STM32WB1MMC (BLE5.3 – 2Mbit/s) 2.1 187042 (TCRL2023-1)


STM32WB host stack QDID

Features Host stack version STM32WB_Copro_Wireless_Binaries QDID
4.0 HCI
LL
STM32Cube_WB_BLE_HCI stm32wb5x_BLE_HCI_AdvScan_fw.bin
stm32wb5x_BLE_HCILayer_fw.bin
stm32wb3x_BLE_HCI_AdvScan_fw.bin
stm32wb3x_BLE_HCILayer_fw.bin
stm32wb1x_BLE_HCI_AdvScan_fw.bin
stm32wb1x_BLE_HCILayer_fw.bin
160726 (TCRL 2023-1) BLE5.2
4.0 HCI
LL, ATT, GAP, GATT, L2CAP, SMP
STM32Cube_WB_BLE_FULL_STACK
STM32Cube_WB_BLE_BASIC_STACK
STM32Cube_WB_BLE_LIGHT_STACK
stm32wb5x_BLE_Stack_light_fw.bin
stm32wb5x_BLE_Stack_light_fw.bin
stm32wb3x_BLE_Stack_full_fw.bin
stm32wb3x_BLE_Stack_light_fw.bin
stm32wb1x_BLE_Stack_full_fw.bin
stm32wb1x_BLE_Stack_light_fw.bin
160724 (TCRL 2023-1) BLE 5.2
4.0 HCI
LL with extended advertising, ATT,
GAP, GATT, L2CAP with Enhanced
Connected Oriented Channel, SMP
STM32CubeFW_WB_BLE_HCI_FULL_EXT
STM32CubeFW_WB_BLE_STACK_FULL_EXT
stm32wb5x_BLE_HCILayer_extended_fw.bin
stm32wb3x_BLE_HCILayer_extended_fw.bin
stm32wb1x_BLE_HCILayer_extended_fw.bin
stm32wb5x_BLE_Stack_full_extended_fw.bin
stm32wb3x_BLE_Stack_full_extended_fw.bin
stm32wb1x_BLE_Stack_full_extended_fw.bin
201968 (TCRL2023-1) BLE 5.3

216169 (TCRL2023-1) BLE 5.4


STM32WBA PHY QDID

Package Part number Cut version RF PHY QDID
QFN48 STM32WBA52 1.x 197135 (TCRL 2022-2) BLE5.4


STM32WBA Host stack QDID

Features Host stack version QDID
4.0 HCI
LL with extended advertising, ATT, GAP, GATT, L2CAP with
Enhanced Connected Oriented Channel, SMP
STM32Cube_WBA_BLE_HCI_STACK
STM32Cube_WBA_BLE_FULL_STACK
198195 (TCRL 2022-1) BLE 5.3

2.3. Launch studio process

Please find attached a link of a dedicated WIKI page detailing all different steps to qualify our End Product. We will describe a specific example: Qualify your project "My first project with STM32WB55RG component"


2.4. Bluetooth® Low Energy (BLE) PHY testing : How to?

In case PHY testing is required, below page contains information for preparing customer HW and SW.

2.4.1. SW & HW recommendation for BLE RF testing

Customer should then prepare its device under test so that:
✓STM32WBx or STM32WBAx is flashed with transparent mode FW .
✓SMA RF cable is set instead of antenna (ensure solid grounding connection) as BLE RF PHY tests are done in conducted mode only.

2.4.2. Direct test mode

Direct Test Mode (Bluetooth® tester is sending HCI commands directly to board under test) is mandatory for BLE certification.
This why customer product must be flashed with transparent FW (refer dedicated chapter on transparent FW).


2.4.3. Pixit

When moving to RF PHY tests, customer might need to provide test house few details about chipset RF PHY.
Needed information for STM32WB are listed in below table.


✓ Note 1 : Some information are product related and not chipset related (noted “Product dependent” in this table)
✓ Note 2 : 2M tests should be set to “NA” when device is not supporting 2M modulation.


Needed information for STM32WBA are listed in below table.

✓ Note 1 : Some information are product related and not chipset related (noted “Product dependent” in this table)
✓ Note 2 : 2M tests should be set to “NA” when device is not supporting 2M modulation.
✓ Note 2 : Direction finding parameters should be set to NA if not used..


3. Regional certification

In order to sell Bluetooth low energy product in regional countries, equipment needs to comply with the associated RF regulatory requirements:
✓ FCC (Federal Communications Committee) for North America
✓ CE European Commission (Radio Equipment Directive)
✓ IC (Industry Canada).
✓ etc.


3.1. Module versus chipset

Chipset use case
✓ STM32WB chipsets are compliant with regional RF regulatory requirements.
✓However, RF tests for regional certification are fully HW dependent (antenna, layout etc.)
→ Each customer product must go through RF tests for all regional certification.

Module use case
✓ STM32WBxMMx modules are RF pre certified for various region. Certificates and tests reports are available on st.com for STM32WB5M and STM32WB1M.
✓ It means limited RF tests are requested on final product (Rx and Tx radiated tests).
→ RF tests costs are then a bit lowered (few k$ savings for CE or FCC) when using our certified modules.
→ Each customer product must go through remaining RF tests for all regional certification.

3.2. Regional testing : How to?

3.2.1. Test setup for regional RF testing

Customer should then prepare its DUT so that:
✓STM32WB is flashed with transparent mode FW.
✓Device under test is connected to Cube Monitor RF PC tool.