Secure Manager for STM32H5

Revision as of 10:29, 2 June 2023 by Registered User (→‎Secure Manager)

1. Introduction

On the STM32H5 MCUs lots of new security features are provided : Product lifecycle, isolation, Debug Authentication, secure storage and secure boot.

You can use all these blocks by yourself if you have good security skills but you can also use a full solution owned and maintained by STMicroelectronics. This solution is certified SESIP 3 and also PSA certified which is the highest level of security certification that you can achieve with the general purpose MCUs.

2. Secure Manager overview

Secure Manager is a Trusted Execution Environment(TEE) integrating core security services.

SECURITY Secure Manager Global presentation.png

2.1. Secure Manager

Secure Manager is all what you see in blue. Secure Manager is composed of one software brick which is a binary encrypted and signed by STM. It is delivered by STM and user doesn't have access to this code. Secure Manager and ST iROT is only available on STM32H573 devices.

In blue and green correspond to all what is delivered by STM. In yellow it is the user application. User can call some security services which are standards defined by the PSA ARM.

  • ST iROT is the fisrt stage bootloader. It is installed inside your device when you buy it.
  • ST uROT is the second stage bootloader. It is possible to update this second stage bootloader.
  • Secure Manager Core is a secure OS which handle the security services that you have in your platform.
  • The services accessible by the PSA API are
    • Firmware update : The capability to update your firmware in a secure way
    • The secure storage : way to store securely some datas
    • Cryptography : in order to encrypt or decrypt something you want to check
    • Attestation : defined for the iOT. It allows to have an identifier to the full picture of your device.

2.2. Additional modules

If you need to add some security services you can define them by yourself and develop a secure module (in green). It can be done by a third party or by customer. This is a way to deliver a software API and ensure about its confidentiality. As is is delivered encrypted and signed it will be installed securely and then it is possible to access this API but it's not possible to access to the software by itself.

2.3. User application

Security is handled by the Secure Manager so for user it is as itf there is no security. There are some API to get access to security services but when user developps its application the only constraint is the size of the flash that is available. In fact Secure Manager is installed in the internal flash and a portion of RAM is locked by the Secure manager too.

2.4. Certification

Secure manager and Hardware are certified SESIP level 3 and PSA level 3 . If you want to have your platform certified you just have to take care about certification of your application or your secure module. The secure manager handle the isolation between the different services. It is needed to have this level of certification to ensure that one secure service can’t access the resources of the other secure services. It is PSA API compatible which means that this API has not been defined by ST, it is a standard defined by ARM. It is designed for long term support that means that if a weakness is found in the future ST will redelivered a new secure manager as it is updatable thanks to the different stage bootloader It is optimized for certification : you just have to focus on the certification of your application.

2.5. Booting mechanism

The secure storage is used to store some keys.
These keys will be used during the boot time to authenticate each brick of software before launching it.

After the provisioning and when we install the Secure Manager we also provision those keys in this secure storage.

At the reset we are on the ST iROT that will authenticate a second stage bootloader thanks to the keys that are inside the secure storage.

When this authentication is done we are sure this one is authenticated and has not been modified by a hacker or something else we jump on it thanks to the temporal isolation.

Temporal isolation is a mechanism which allow to ensure that a portion of code can’t be seen anymore by the system. The associated keys have the same isolation level. Once we jump to another level we remove access to the previous one and also to the associated keys.

The second stage bootloader will authenticate the secure Manager to ensure authenticity has not been modified from any hackers or something else. Then he will authenticate the different modules and each time the different keys because the keys owner are different and then the application to ensure this one is also authenticated and the integrity is guarantee . If every thing is ok he will jump to the secure manager.

The secure manager initialize by itself the core, and then jump to the application. After, we are in a “normal execution”:

The application could call some secure API and for example call an API to trusted storage in order to store some data.

The secure manager use the MPU to isolate the services that will be executed : during the execution of the secure storage it could not access to the resources of an other one. Secure manager jump on the Trusted storage, execute this API and then go back to the application All this is transparent for the user.

3. Links

For more details about Secure Manager you can refer to this article : Secure Manager

Secure Manager STM32H5 How to Intro Is an article which introduce the How to start article :

How to start with Secure Manager on H573 article is to experiment, to install and to try to use Secure Manager.