How to start with Secure Manager customized config on STM32H5

Revision as of 11:47, 31 May 2023 by Registered User

This article goal is to guide a STM32H573 user through first steps of using the Secure Manager. To learn what is the Secure Manager and why to use it please read introduction to Secure manager.

1. Installation

This section will walk you through provisioning with Secure Manager from product state open with clean STM32H57x (either a virgin or after full regression) and state where the Secure Manager is installed and the product is in TZ-Closed, ready for non-secure application with PSA API calls development.
There are several ways to install the Secure Manager, ranging from step-by-step meticulously following a checklist to simply executing a prepared batch. Very little is configurable in the SMAK form, only the arrangement of the non-secure application image slots.

1.1. Prerequisites

To use the Secure manager a compatible STM32 MCU is needed. At this moment only the STM32H573 line supports the Secure Manager.
On software side the STM32CubeMX toolset is needed, complete with STM32CubeProgrammer and the Trusted Package Creator. The STM32CubeMX will download the STM32H5 cube package, containing the HAL and examples.
There is no extra cost or licensing hurdle for the SMAK. To use SMDK the customer must contact ST to get qualified for signing an NDA.

2. Installing using batch

Automated installation using prepared script is ready for the STM32H573I-DK development kit in the STM32H5 Cube package.

2.1. Environment configuration

By default at the location of

C:\Users\***\STM32Cube\Repository\STM32Cube_FW_H5_V1.0.1\Projects\STM32H573I-DK\ROT_Provisioning

is a batch file called env.bat which needs to be modified first:

The env.bat contents

Correct the addresses and the communication virtual port number to continue with installation.

2.2. SMAK Keys configuration

The keys are in the SMAK/Keys sub-folder. Easiest way to modify the keys is to open the STM32 Trusted Package Creator tool. Select H5 in the leftmost pane and then OBkeys tab. Open key configuration file and regenerate the keys as needed.

  • SMAK authentication key - used to signed installed application
  • SMAK encryption key - used to provide confidentiality on the installed user application
The SMAK keys screen

2.3. Memory configuration

The memory layout and partitioning are also configurable. Basic settings are easily accessible by opening another xml file in the STM32 Trusted Package Creator tool:

Screen of the memory layout settings

2.4. DA configuration

Provisioning the Debug authentication keys and certificate is highly recommended step. Details of the process can be found in introduction to Debug Authentication
When modifying the default settings, consider the need to actually debug the NS application in the TZ-Closed state. Removing the debug certificate would block such development.

2.5. Installation process

In the basic scenario, all that is required is to execute the provisioning.bat and follow the instructions on the screen. The process will require you to manipulate the SW1 switch on the DK board to complete the provisioning correctly.
The batch file works in two steps. In step 1 it prepares the SFI package, consisting of:

  • Keys configuration
  • Layout configuration
  • DA configuration

All these are prepared in the STM32 Trusted Package Creator.
Environment configuration updated earlier will be used now to communicate with the STM32H573I-DK board and upload the SFI package. Pay attention to the instruction to manipulate the SW1 to assert correct state on the BOOT0 pin.
When finished, the Secure Manager is installed.

3. Using the Secure Manager

Now the Secure Manager is provisioned and the STM32H573 is in TZ-closed state. It's possible to code and debug in the non-secure domain of the MCU using the usual development tools, for example STM32CubeIDE. The STM32Cube package for STM32H5 contains a template called SMAK_Appli. Just add functionality and download using for example STM32CubeProgrammer.

3.1. Development of the user application

The SMAK_Appli template is by default available at the following path:

C:\Users\***\STM32Cube\Repository\STM32Cube_FW_H5_V1.0.1\Projects\STM32H573I-DK\Templates\ROT\SMAK_Appli\

The project is packed with batch files that automate necessary post-build actions and binary download using the CLI STM32CubeProgrammer.
One difference compared to the bare-metal development is that you need to manually place a breakpoint to your main to commence the debug session. The debug authentication session is valid while the debugger stays connected to the target.

3.2. The template application

The template application contains a user interface that works with terminal application on host PC and showcases the PSA funtionality provided by the Secure Manager, in service of the user application.

File:HowtoSecureManager-NSApp.png
Application terminal screen

4. Generating from STM32CubeMX

From the STM32CubeMX select the STM32H573xx and start a new project. A prompt will be displayed to choose whether TrustZone will be used. For development using the Secure Manager select "with TrustZone enabled."
Once the '*.ioc' project is saved, go to 'Project Manager' tab to select the boot path settings. the Secure Manager only works with underlying ST-iRoT and ST-uRoT selected. Configure your project in the STM32CubeMX as usual, selecting the peripherals used, assigning pins and configuring the clock tree. When the project is generated, it will have the linker files prepared to fit within the memory range assigned to the application by the Secure Manager.