This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Introduction
On the STM32H5 MCUs lots of new security features are provided : Product lifecycle, isolation, Debug Authentication, secure storage and secure boot.
You can use all these blocks by yourself if you have good security skills but you can also use a full solution owned and maintained by STMicroelectronics. This solution is certified SESIP level3 which is the highest level of security certification that you can achieve with the general purpose MCUs. Secure Manager is a Trusted Execution Environment(TEE) integrating core security services. The purpose of the How to start with Seecure Manager on H573 article is to experiment , to install and to try to use it.