Coming soon |
1. Bluetooth® Low Energy (BLE) Security - Out of Band Pairing method
The Out of Band (OOB) [1] mechanism is used to both discover the devices as well as to exchange or transfer cryptographic numbers used in the pairing process.
It needs to be effective from a security point of view and should be resistant to MITM attacks.
For LE Secure Connection Pairing, if Out Of Band pairing method is used, the public keys, nonces and confirmation values are all exchanged via a different wireless technology such as NFC.
For LE Legacy Pairing, if Out Of Band pairing method is used, the TK is exchanged using a different wireless technology such as NFC. The main advantage to this method is that a very large TK can be used, up to 128 bits.
2. OOB in LE Secure Connection Pairing via NFC
In the following description, it is considered the case where a smartphone connects a WB and WB provides OOB data
2.1. Commands sequence for pairing initialization, public key generation, generation and recovery of OOB data on WB
Sequence to be done in Ble_Hci_Gap_Gatt_Init function (in app_ble.c)
/* Initialize IO capability */
aci_gap_set_io_capability(0x00-display only)
/* Initialize authentication */
aci_gap_set_authentication_requirement(0x01- bonding, 0x00-no MITM, SC_Support=0x01, 0x00-fixed pin, 0x00000000-fixed pin value)
/* Sequence to force the regeneration of the EDCH_public key on OOB source device */
uint8_t ALL_EVENTS[8]={0xDF,0x1A,0x03,0x00,0x00,0x00,0x00,0x00};
hci_le_set_event_mask(ALL_EVENTS);
/* generation of a new P-256 public key */
Hci_le_read_local_p256_public_key()
/* Reception of META EVENT */
HCI_LE_READ_LOCAL_P256_PUBLIC_KEY_COMPLETE_EVENT
/* OOB data generation */
Aci_gap_set_oob_data(device_type=0x00, Address_type=0x00, address=0x00, oob_data_type=0, oob_data_len=0, oob_data=0)
/* OOB data recovery */
Aci_gap_get_oob_data(oob_data_type=0x01-random)
Aci_gap_get_oob_data(oob_data_type=0x02-confirm)
2.2. Pairing initialization commands on peripheral side
Pre-requisite before pairing request: initialization of pairing conditions with 2 commands:
aci_gap_set_io_capability(0x00-display only)
aci_gap_set_authentication_requirement(0x01- bonding, 0x00-no MITM, SC_Support=0x01, 0x00-fixed pin, 0x00000000-fixed pin value)
2.3. Public Key generation
The peripheral is the device where the OOB data will be extracted. The central is the device where OOB data will be set.
Following sequence is done before the connection:
On peripheral side:
Sequence to force the regeneration of the EDCH_public key on source device
First action: set LE Event Mask to require which LE events are generated by the HCI for the host.
hci_le_set_event_mask command is used to control which LE events are generated by the HCI for the Host.
Default value of this event mask is 0x0000000000031A5F. Refer to hci_le_set_event_mask command description.
To receive LE Read Local P-256 Public Key Complete Event, bitmask 0x80 is needed.
The new mask value is 0x0000000000031ADF.
uint8_t ALL_EVENTS[8]={0xDF,0x1A,0x03,0x00,0x00,0x00,0x00,0x00};
hci_le_set_event_mask(ALL_EVENTS);
Second action: generation of a new P-256 public key (first action necessary to receive the event)
Hci_le_read_local_p256_public_key()
HCI_LE_META_EVENT event received :
HCI_LE_READ_LOCAL_P256_PUBLIC_KEY_COMPLETE_EVENT
contains Local_P256_Public_Key field.
2.4. OOB data generation
Command used to generate OOB data on device data source:
Aci_gap_set_oob_data(device_type=0x00, Address_type=0x00, address=0x00, oob_data_type=0, oob_data_len=0, oob_data=0)
Previous command is sent with all data equal to zero.
2.5. OOB data recovery
For SC secure pairing:
Two commands used to recover the generated OOB data on device data source
First command:
Aci_gap_get_oob_data(oob_data_type=0x01-random)
HCI_COMMAND_COMPLETE_EVENT event received, contains following fields:
address_type
address
OOB_data_type 0x01 (Random SC)
OOB_data_length
OOB_data : RANDOM_DATA – local pairing data intended to the remote device to be sent via NFC
Second command:
Aci_gap_get_oob_data(oob_data_type=0x02-confirm)
HCI_COMMAND_COMPLETE_EVENT event received, contains following fields:
address_type
address
OOB_data_type 0x02 (Confirm SC)
OOB_data_length
OOB_data : CONFIRM_DATA – local pairing data intended to the remote device to be sent via NFC
RANDOM_DATA and CONFIRM_DATA generated by the BLE stack are written to ST25 (NFC shield).
2.6. OOB data written into NFC shield
Code example
Ndef_Bluetooth_OOB_t NdefBle = {
.LeOptionalMask = (NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_LE_SECURE_CONNECTIONS_CONFIRMATION_VALUE) |
NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_LE_SECURE_CONNECTIONS_RANDOM_VALUE)),
.LocalName = "ST25OOB",
.OptionalMask = NDEF_BLUETOOTH_OPTION(BLUETOOTH_EIR_COMPLETE_LOCAL_NAME),
.Type = NDEF_BLUETOOTH_BLE,
.Role = NDEF_BLE_ROLE_PERIPH_ONLY,
.DeviceAddressType = NDEF_BLE_PUBLIC_ADDRESS_TYPE
};
for(int i = 5; i >= 0; i --)
NdefBle.DeviceAddress[i] = bd_addr[5-i];
status = aci_gap_get_oob_data(1, &at,add,&len, rand);
status = aci_gap_get_oob_data(2, &at,add,&len, hash);
for(int i = 5; i >= 0; i --)
NdefBle.DeviceAddress[i] = add[5-i];
for(int i = 15; i >= 0; i --)
{
NdefBle.SimplePairingRandomizer[i] = rand[15-i];
NdefBle.SimplePairingHash[i] = hash[15-i];
}
NfcTag_SelectProtocol(NFCTAG_TYPE5);
NFC04A1_NFCTAG_Init(0);
NDEF_ClearNDEF();
NDEF_AppendBluetoothOOB(&NdefBle, NULL);
2.7. Transfer of OOB data through NFC
- RANDOM_DATA = rb
- CONFIRM_DATA = Cb
Random data and Confirm Data transferred through NFC |
---|
3. Bluetooth® Low Energy (BLE) pairing with Secure Connection Encryption
3.1. Secure Connection Encryption - Sequence
LE pairing with Secure Connection encryption - principle |
---|
3.2. Pairing Secure Connection
Pairing feature exchange, key generation method selection, authentication and LTK principle[2]
3.3. Authentication stage using OOB
- RANDOM_DATA : rb
- CONFIRM_DATA : Cb
- Pkb : Public Key provided by the peripheral
Authentication stage using OOB |
---|
4. OOB in LE Legacy Pairing
In the following description, it is considered the case where two WBs are connected and exchange OOB data via UART.
Both devices MUST set their OOB data flag if they want to use OOB for pairing.
In case of LE Legacy Pairing, only one device generates the TK, the both are using the same TK.
4.1. Commands sequence for pairing initialization, public key generation, generation and recovery of OOB data on WB
Sequence to be done in Ble_Hci_Gap_Gatt_Init function (in app_ble.c)
/* Initialize IO capability */
aci_gap_set_io_capability(0x00-display only)
/* Initialize authentication */
aci_gap_set_authentication_requirement(0x01- bonding, 0x00-no MITM, SC_Support=0x01, 0x00-fixed pin, 0x00000000-fixed pin value)
/* Sequence to force the regeneration of the EDCH_public key on OOB source device */
uint8_t ALL_EVENTS[8]={0xDF,0x1A,0x03,0x00,0x00,0x00,0x00,0x00};
hci_le_set_event_mask(ALL_EVENTS);
/* generation of a new P-256 public key */
Hci_le_read_local_p256_public_key()
/* Reception of META EVENT */
HCI_LE_READ_LOCAL_P256_PUBLIC_KEY_COMPLETE_EVENT
/* OOB data generation */
Aci_gap_set_oob_data(device_type=0x00, Address_type=0x00, address=0x00, oob_data_type=0, oob_data_len=0, oob_data=0)
/* OOB data recovery */
Aci_gap_get_oob_data(oob_data_type=0x00-TK)
4.2. Example of OOB data transfer in Legacy Pairing - central generates OOB data
OOB pairing sequence |
---|
5. ST example : STM32WB55 + NFC04A1 and Android smartphone
ST solution ST25DV-I2C Bluetooth® Low Energy out of band pairing solution[3] is presented on st.com.
A user manual[4] is also available describing the demonstration and a video[5] presents the demonstration.