1. Introduction
This wiki describes to an application developer how to integrate the STM32WBAxx Bluetooth® LE stack library.
This wiki covers only the Bluetooth® LE stack library integration, and it does not include the Link Layer integration aspects.
Acronym | Definition |
---|---|
HCI | Host Controller interface |
ACI | Application Controller Interface |
N/A | Not Applicable |
2. Bluetooth® LE Stack Overview
3. BLE Stack User interface
4. BLE Stack Porting
4.1. Stack Porting
5. References
6. Wiki syntax examples
Header text | Header text | Header text |
---|---|---|
Example | Example | Example |
Example | Example | Example |
Example | Example | Example |
Bluetooth® LE Health Thermometer Service specification | ||||||||||||||||||||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
ST Bluetooth® LE example project directory |
---|
ST Bluetooth® LE example project directory |
---|
Bluetooth®
texte - “doc” folder contains the current document and “STM32WBA_BLE_Wireless_Interface.html” which describes the BLE Application Commands Interface (ACI) and the Host Commands Interface (HCI).
- “include” folder contains the header files of the BLE stack library interface. These files contain some definitions of constants and types and the declarations of ACI and HCI functions. It also contains the declarations of some external modules’ functions used by the BLE stack (for more details see section 4.2)
- “lib” folder contains the 4 BLE stack library variants described in the following section.
BLA BLA BLA
ST Bluetooth® LE pour Nidhal |
---|
/**
******************************************************************************
* @file STM32WB_P2P_Server.ino
* @author WBL BLE Application Team
* @brief Arduino STM32WB P2P Server Application (Custom STM)
******************************************************************************