This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Introduction
Header text | Header text | Header text |
---|---|---|
Example | Example | Example |
Example | Example | Example |
Example | Example | Example |
Bluetooth® LE Health Thermometer Service specification | ||||||||||||||||||||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
ST Bluetooth® LE example project directory |
---|
ST Bluetooth® LE example project directory |
---|
2. BLE Stack Overview
texte - “doc” folder contains the current document and “STM32WBA_BLE_Wireless_Interface.html” which describes the BLE Application Commands Interface (ACI) and the Host Commands Interface (HCI).
- “include” folder contains the header files of the BLE stack library interface. These files contain some definitions of constants and types and the declarations of ACI and HCI functions. It also contains the declarations of some external modules’ functions used by the BLE stack (for more details see section 4.2)
- “lib” folder contains the 4 BLE stack library variants described in the following section.
3. BLE Stack User interface
4. BLE Stack Porting
4.1. Stack Porting
5. References