STM32CubeWBA: Low power management

Revision as of 14:09, 3 May 2023 by Registered User (→‎Standby dynamic view)


Under construction.png Coming soon

1. Introduction

STM32WBA CubeFW provides low power features that are integrated into the application framework.
Once the low power is enabled in the application, the system framework is responsible of choosing the lowest possible power mode that can be used. Serval parameters are taken into account such as the application use case or the radio activity.

2. Concepts

2.1. Low power general overview

STM32WBA SoC low power mode is determined by both Link Layer operating modes and SoC PWR modes.
Details are given in the next sections.

2.1.1. Link Layer operating modes

Link Layer operating modes are detailed in the table below.

Link Layer operating modes table
Operating mode Purpose
Active – Standby Link Layer is in active mode when the radio is operating.
Standby is used on active waiting of radio event (BLE IFS, RX on IDLE for 802.15.4).
Sleep This mode is used when there is no radio activity.
Baseband clock (active clock) has to be switched OFF. RXTX SRAM or sequence SRAM are not available.
HW Link Layer registers are accessible as long as bus clock remains ON.
Deep Sleep Deep Sleep mode is the lowest low power mode for Link Layer IP.
This mode is only available when the is no current/up-coming radio activity.
Baseband clock (active clock) is switched OFF.
All power domains are switched OFF except sleep timer one. Bus clock has to be ON for sleep timer registers access.

Deep sleep mode entry/exit is time consuming. Therefore, the next radio activity has to be far enough to power down the radio.
A threshold value is available in system framework and can be configured as needed. See RADIO_DEEPSLEEP_WAKEUP_TIME_US macro in system configuration.

2.1.2. SoC PWR power modes

STM32WBA SoC supports four main PWR power modes: run, sleep, stop and standby. Details are given below.

2.1.2.1. Run mode

The CPU and the system clock are running. It shall be used only when it is required to execute code.

2.1.2.2. Sleep mode

CPU clock is off (CPU stops fetching code), all peripherals including Cortex-M33 core such as NVIC and SysTick can run and wake up the CPU when an interrupt or an event occurs. This should be used when a peripheral (that does not have a kernel clock) requires the system clock to operate while the CPU is stopped.

Warning DB.png Important
Wake-up sources for Sleep mode are: any interrupt, any wakeup event.
The wake-up system clock is the same as before entering Sleep mode
2.1.2.3. Stop modes

Stop modes achieve the lowest power consumption while retaining the content of registers. The SRAM content can be selected to be retained or not. All clocks (except some autonomous peripherals bus and kernel clocks) in the Core domain are stopped (system clock, high-speed oscillators).
There are two stop modes:

  • stop0: This is the stop mode available when a kernel clock is enabled or a autonomous peripherals bus clock is requested.
    The 2.4GHz radio can still be active when in Stop 0 Range1. For this, the high-speed system clock and peripheral kernel clocks may be kept running.
  • stop1: Lowest stop mode available in WBA5x series where all bus and kernel clocks are off.
Warning DB.png Important
Wake-up sources for Stop modes are:
  • any EXTI line
  • autonomous peripherals
  • 2.4 GHz RADIO sleep timer event
  • IWDG event.
  • RTC event.
  • TAMP event.
  • WKUP event.
  • NRST external reset.
  • BOR reset.
  • HSECSS event for stop 0 only.

The system clock after wakeup is HSI 16 MHz.

2.1.2.4. Standby modes

The Standby mode is used to achieve the lowest power consumption. The internal regulator is switched off so that the Core domain is powered off. High-speed oscillators are off too (PLL, HSE and HSI). The LSE or LSI can still run.

When entering Standby mode, register contents are lost except for registers in the Backup domain and Standby circuitry. Regarding peripherals, only RTC, TAMP, and WKUP are retained. Standby mode exit leads to a SoC reset.

Warning DB.png Important
Standby mode requires the Link Layer to be in deep sleep mode.

The standby mode described above is Standby without retention.

Optionally, the user can retain the content of SRAMs. It is Standby with retention mode.

  • the full SRAM1 and/or SRAM2 can be retained in Standby mode, supplied by the low-power regulator.
  • the 2.4 GHz RADIO Sleep Timer, RXTXRAM and sequence SRAM can be retained in Standby mode, supplied by the low-power regulator.
Warning DB.png Important
Wake-up sources for Standby modes are:
  • IWDG event.
  • RTC event.
  • TAMP event.
  • WKUP event.
  • NRST external reset.
  • BOR reset.
  • 2.4 GHz RADIO sleep timer event only for Standby with retention.

The system clock after wakeup is HSI 16 MHz.

2.2. Low power in Connectivity applications

2.2.1. Low power manager Utility (LPM)

2.2.1.1. LPM Utility

The low power manager provides a simple interface to receive the input from up to 32 different users and computes the lowest possible power mode the system can use. Each LPM client can request a disablement (or re-enablement after deactivation) for stop and standby modes when necessary. The API to use is:

Low power Sleep mode is selected when Stop and Standby are disabled.

Info white.png Information
By default, when no LPM user request a disablement, the standby mode (lowest low power mode available) is selected.


Users can obtain the low power mode that is going to be selected at that time with UTIL_LPM_GetMode API.

2.2.1.2. Platform interfaces

Once it is time to enter in low power mode, application is responsible to call UTIL_LPM_EnterLowPower. According to the lowest low power mode available, LPM Utility will call appropriate interface to enter Sleep, Stop or Standby mode at SoC level. Those interfaces has to be defined at application level (system side).

Info white.png Information
UTIL_LPM_EnterLowPower also calls low power exit function.

Low power platform interfaces are:

Warning DB.png Important
Low power entry interfaces are responsible to call __WFI instruction to effectively enter in low power.

2.2.2. Low power Stop modes for Connectivity

Both stop0 and stop1 are supported. As a remainder:

  • when Link Layer is in active/standby mode, SoC can achieve stop0.
  • when Link Layer is in sleep mode, SoC can achieve stop1.
2.2.2.1. Low power Stop mode entry

Below is the mandatory system configuration before entering Stop modes (in order)

  • ICache IP shall be disabled.
  • FLASH latency: 3, SRAM1/2 latencies: 1.
  • CPU shall be in deep sleep mode.
  • PWR VOS shall be stable.
2.2.2.2. Low power Stop mode exit

At low power Stop mode exit, System Clock Manager (SCM) module is called to reconfigure the system clock as it was before entering low power.

See System Clock Manager for further information about this system module.

2.2.3. Low power Standby mode for Connectivity

2.2.3.1. Standby strategy

For Connectivity applications, the lowest low power mode achievable is Standby with retention. Indeed, the system has to retain

  • Link Layer configuration and context: Link Layer dedicated SRAM retained.
  • Application content: at least SRAM1 retained. If SRAM1 is not enough RAM for the application, SRAM2 shall be retained too.

As CPU is reset at standby exit, non-retained configuration (SRAMs content) shall be re-applied (e.g SoC register content). This concerns:

  • NVIC interrupts, system and user/application related.
    For system side, Link Layer high priority, Link Layer SW low priority, RCC, RTC interrupts are configured (priority) and enabled.
  • Link Layer peripheral clock (radio bus clock) is enabled.
  • SoC IP are re-initialized completely (including related NVIC interrupts if handled by HAL SW).
  • RTC peripheral clock. If RTC registers are retained as RTC IP is part of backup domain, peripheral clock is reset at Standby exit.
Info white.png Information
System clock is configured as it was before entering low power.
2.2.3.2. Save & restore mechanism
2.2.3.2.1. CPU context registers

Default behavior at standby exit - after CPU reset - is to execute Reset handler code. For connectivity applications, the goal is to execute the low power standby exit procedure (PWR_ExitOffMode function after __WFI) as system does for Stop mode.

Hereafter is the description of the mechanism implemented in WBA5 solution.

  • At Standby entry, system saves the CPU registers related to the execution context by calling CPUcontextSave. This concerns R4-R12, LR and SP general purpose registers that are backup in CPU stack.
  • Connectivity applications have a specific Reset handler (default Reset handler is overridden) that restores CPU context registers from the CPU stack if system resets from standby exit.
  • As a result, the next executed instruction is the one after __WFI in PWR_EnterOffMode.
Info white.png Information
Overridden Reset handler is located in the file System/Startup/stm32wbaxx_ResetHandler.S.
2.2.3.2.2. CPU peripherals registers

CPU peripheral registers are also maintained with backup_system_register and restore_system_register APIs.

Connectivity system backuped registers are

  • SCB CPACR (FPU related).
  • SysTick CTRL/LOAD/VAL.
Warning DB.png Important
If the user has any other CPU peripheral register to backup, it can be added to register_backup_table in System/Config/LowPower/user_low_power_config.c.
2.2.3.3. Standby dynamic view

Here is the steps the system performs to manage Standby mode (when application is IDLE):

Link Layer deep sleep entry

If there is enough time before the next radio event:

  1. Link Layer IP internal timer is programmed to wake-up before the next radio event with configurable threshold.
  2. Link Layer is switch to deep sleep mode.
Standby mode time
  1. Standby mode is entered at SoC level.
  2. Standby mode is exited from Link Layer IP timer interrupt.
  3. System side callback is called to exit the Link Layer from deep sleep mode (Link Layer mode is now sleep mode).
Stop mode time
  1. The system returns in IDLE state but Link Layer is not put in deep sleep as there is not enough time before the next radio event.
  2. As Link Layer is not in deep sleep, Stop mode is entered.

2.3. Low power concept summary

Here is a summary diagram of the STM32WBA5 low power features.

File:LowPower Overview.png
Low Power management concept

3. Interfaces

3.1. LPM Utility

UTIL_LPM_Init

Description

Initialize the LPM resources..
Syntax
void UTIL_LPM_Init( void );
Parameters
None
Return Value
None
UTIL_LPM_DeInit

Description

Un-initialize the LPM resources..
Syntax
void UTIL_LPM_DeInit( void );
Parameters
None
Return Value
None
UTIL_LPM_GetMode

Description

This API returns the Low Power Mode selected that will be applied when the system will enter low power mode if there is no update between the time the mode is read with this API and the time the system enters low power mode.
Syntax
UTIL_LPM_Mode_t UTIL_LPM_GetMode( void );
Parameters
None
Return Value
Type: UTIL_LPM_Mode_t
Description: LPM mode.
UTIL_LPM_SetStopMode

Description

This API notifies the low power manager if the specified user allows the Stop mode or not.
The default mode selection for all users is Stop Mode enabled.
Syntax
void UTIL_LPM_SetStopMode( UTIL_LPM_bm_t lpm_id_bm, UTIL_LPM_State_t state );
Parameters
[in] lpm_id_bm
Type: UTIL_LPM_bm_t
Description: Identifier of the user ( 1 bit per user )
[in] state
Type: UTIL_LPM_State_t
Description: Specify whether StopMode is allowed or not by this user
Return Value
None
UTIL_LPM_SetOffMode

Description

This API notifies the low power manager if the specified user allows the Standby mode or not.
The default mode selection for all users is Off mode enabled.
Syntax
void UTIL_LPM_SetOffMode( UTIL_LPM_bm_t lpm_id_bm, UTIL_LPM_State_t state );
Parameters
[in] lpm_id_bm
Type: UTIL_LPM_bm_t
Description: Identifier of the user ( 1 bit per user )
[in] state
Type: UTIL_LPM_State_t
Description: Specify whether Standby is allowed or not by this user
Return Value
None
UTIL_LPM_EnterLowPower

Description

System enters low power mode.
Syntax
void UTIL_LPM_EnterLowPower( void );
Parameters
None
Return Value
None

3.2. Low power platform interfaces

PWR_EnterSleepMode

Description

Interface to enter Sleep mode.
Syntax
void PWR_EnterSleepMode(void);
Parameters
None
Return Value
None
PWR_ExitSleepMode

Description

Interface to exit Sleep mode.
Syntax
void PWR_ExitSleepMode(void);
Parameters
None
Return Value
None
PWR_EnterStopMode

Description

Interface to enter Stop mode.
Syntax
void PWR_EnterStopMode(void);
Parameters
None
Return Value
None
PWR_ExitStopMode

Description

Interface to exit Stop mode.
Syntax
void PWR_ExitStopMode(void);
Parameters
None
Return Value
None
PWR_EnterOffMode

Description

Interface to enter Standby mode.
Syntax
void PWR_EnterOffMode(void);
Parameters
None
Return Value
None
PWR_ExitOffMode

Description

Interface to exit Standby mode.
Syntax
void PWR_ExitOffMode(void);
Parameters
None
Return Value
None

3.3. CPU context save & restore

CPUcontextSave

Description

Save Cortex general purpose registers on stack and call WFI instruction.
Syntax
void CPUcontextSave(void);
Parameters
None
Return Value
None
CPUcontextRestore

Description

Restore Cortex general purpose registers from stack.
Syntax
void CPUcontextRestore(void);
Parameters
None
Return Value
None

3.4. CPU peripherals save & restore

3.4.1. CPU peripheral register table

register_backup_table

Description

Table of CPU peripheral registers to backup/restore when standby mode available.
This table is present in System/Config/LowPower/user_low_power_config.c file.
const volatile uint32_t* const register_backup_table[] =
{
  &(SCB->CPACR),     /* FPU SCB->CPACR register */
  &(SysTick->CTRL),  /* SysTick CTRL register */
  &(SysTick->LOAD),  /* SysTick LOAD register */
  &(SysTick->VAL),   /* SysTick VAL register */

  /* USER CODE BEGIN RBL */

  /* USER CODE END RBL */
};

3.4.2. CPU peripheral save & restore functions

backup_system_register

Description

Backup CPU peripheral registers selected in register_backup_table
Syntax
void backup_system_register(void);
Parameters
None
Return Value
None
restore_system_register

Description

Restore CPU peripheral registers selected in register_backup_table
Syntax
void restore_system_register(void);
Parameters
None
Return Value
None

4. How to

4.1. Low power initialization & configuration

In Connectivity applications, low power is configured in Core/Inc/app_conf.h file where user can activate

  • CFG_FULL_LOW_POWER to deactivate incompatible features such as debugger and Nucleo LEDs.
  • CFG_LPM_SUPPORTED to activate low power manager Utility.
  • CFG_LPM_STDBY_SUPPORTED to activate standby mode support.

UTIL_LPM_Init is responsible for initializing low power manager Utility (in Core/Src/app_entry.c file). Once is done, user can dynamically enable or disable Stop/Standby mode with UTIL_LPM_SetStopMode/UTIL_LPM_SetOffMode APIs.

4.2. Low power entrance when IDLE

Low power can only be entered when application is in IDLE mode.
To do so, UTIL_LPM_EnterLowPower has to be called.