Debug Authentication for STM32H5

Revision as of 11:12, 27 April 2023 by Registered User (→‎Introduction)

1. Introduction

  • Debug authentication controls
    • Debug opening : Re-open Debug Access on the STM32 in a secured way.
    • Regressions : Perform regression to product states OPEN or TZ-CLOSED in a secured way, erasing user data in user Flash, SRAM and OBKeys.
  • It can be used
    • During development
    • During manufacturing
    • For field return analysis
  • Debug Authentication is only useful when STM32 is no more in product state OPEN
  • Features
    • When TZ disabled: usage of a password (very similar to U5). Only regression possible
    • When TZ enabled: usage of cryptography (certificates). Regressions and debug opening
  • Debug Authentication principle
    • Uses JTAG dedicated access point (ap0) to communicate with the chip
    • Secure protocol defined by ARM : ARM PSA ADAC V1.0. (Authenticated Debug Access Control)[1]
SECURITY Debug Authentication principle.png

2. Debug Authentication - STM32H503 device

SECURITY Lifecycle TZ disabled.png

Provisioning with password management

  • STM32H503 doesn't provide OB-Key area and uses OTP(One time programming) to store the provisioning data
  • Provisioning data is the HASH (SHA256) of the Password
  • STM32TrustedPackageCreator is used to generate the Hash of the password choosen by user (16 bytes) adding SHA256 to ensure integrity
SECURITY Provisioning H503.png

Debug Authentication allows to control

  • Full Regression thanks to the Debug Authentication password
  • Debug Authentication password has to be provisioned in OTP to allow this regression
SECURITY Regression TZ disabled.png

Getting started with Debug Authentication

You can refer to the following page for getting started example of DA access on STM32H503 devices :

How to start with DA access on STM32H503

3. Debug Authentication - STM32H563/573 device when TrustZone disabled

SECURITY Lifecycle TZ disabled.png

Provisioning with password management

  • the provisioning data is located at beginning of the OBK-HDPL1 area
  • Provisioning data is the HASH (SHA256) of the Password
  • STM32TrustedPackageCreator is used to generate the obk files containing the HASH of the Debug Authentication password adding SHA256 to ensure integrity
SECURITY Provisioning TZ disabled 2.png

Debug Authentication allows to control

  • Full Regression thanks to the Debug Authentication password
  • Debug Authentication password has to be provisioned in OBKeys to allow this regression
SECURITY Regression TZ disabled.png

Getting started with Debug Authentication

You can refer to the following page for getting started example of DA access when TrustZone is disabled:

How to start with DA access on STM32H573 – TrustZone disabled

4. Debug Authentication - STM32H563/573 device when TrustZone enabled

SECURITY Lifecycle TZ enabled.png

Provisioning with certificate management

  • the provisioning data is located at beginning of the OBK-HDPL1 area
  • Provisioning data contain
    • HASH (SHA256) of the root Certificate Public Key
    • SOC_PERMISSION: 16 bits defining the permissions authorized by default
  • STM32TrustedPackageCreator is used to generate the obk files containing the provisioning datas adding SHA256 to ensure integrity
SECURITY Provisioning TZ enabled.png

Debug Authentication allows to control

  • Re-enabling debug possibility
  • Partial or full regression

To perform Debug Authentication

  • the chip must be provisioned with
    • ECC public key
    • SOC_PERMISSION: 16 bits defining the permissions authorized by default
  • a certificate signed by a private ECC key has to be created to be able to authenticate, which embeds
    • ECC public key
    • PERM_MASK_CERT : which describes the capabilities associated with this certificate.
SECURITY Regression from closed TZ enabled 2.png

Getting started with Debug Authentication

You can refer to the following pages for getting started example of DA access when TrustZone is enabled:

5. Debug Authentication - Certificates

When debug authentication control is based on certificates (when TrustZone enabled (TZEN = 0xB4)), device must be provisioned with ECC public key and the SOC_PERMISSION which is a mask defining the different permissions allowed by the debug authentification (Full regression / Partial regression / debug secure / debug nonsecure).

5.1. Certificate for debug authentication access

To be able to connect to a closed device user needs a certificate which embeds

  • ECC public key
  • PERM_MASK_CERT : which describes the capabilities associated with this certificate.

This certificate should be created in a secure environment and is signed by a private ECC key to keep secret.

STM32TrustedPackageCreator is used to create the certificate. User enters the public root key and defines the 16-bytes permission mask which allows a lot of flexibility: Full or Partial regression, open the debug for non-secure or secure application (setting 1 gives the permission) :

SECURITY DA Permission Mask.png

STM32CubeH5 package provides certificates and public keys examples in
STM32Cube_FW_H5_V1.0.0\Projects\STM32H573I-DK\ROT_Provisioning\DA\Certificates,
STM32Cube_FW_H5_V1.0.0\Projects\NUCLEO-H563ZI\ROT_Provisioning\DA\Certificates,
STM32Cube_FW_H5_V1.0.0\Projects\STM32H573I-DK\ROT_Provisioning\DA\Keys and
STM32Cube_FW_H5_V1.0.0\Projects\NUCLEO-H563ZI\ROT_Provisioning\DA\Keys folders.

These default key pairs and certificates can be used to make a provisioning and a full or partial regression without crating a certificate.

5.2. Certificate chain

A certificate chain is used to delegate Debug Authentication access with the capability to restrict the possible permissions to an other stakeholder(OEM, third party, in the field).

5.2.1. Certificate chain composition

The permissions are handled through a certificate chain composed of three different certificates:

  • The root certificate : Define the permissions allowed to the owner of the root certificate.
  • The intermediate certificate : the owner of the root key defines the permission for the owner of the intermediate key. Intermediate certificate gives equal or less permissions than the root certificate.
  • The leaf certificate : the owner of intermediate private key defines the permission for the owner of the private leaf key. Leaf certificate gives equal or less permissions than the intermediate certificate.

5.2.2. Certificate chain use case

We can imagine 3 teams :

  • Team A : A secure development team which must have access to complete platform SW/HW
  • Team B : A non-secure development team which should have only access to non-secure resources
  • Team C : A field engineer who should only have the capability to do a regression to check HW

Team A tasks to create the debug authentication chain :

  • provision OB key and the permission mask
  • create his certificate called ROOT certificate which allows Full and partial regression, secure and nonsecure debug
  • Create a certificate for Team B allowing debug non-secure code and regressions : LEAF certificate 1
  • Create an intermediate certificate which allows Team B to create certificate to Team C

Team B tasks to create the debug authentication chain :

  • Create a certificate for Team C allowing only full regression thanks to the intermediate certificate delivered buy Team A. : LEAF certificate 2

Team B certificate is delivered by Team A: Leaf Certificate 1 - Regressions and non secure debug is allowed

Team C certificate is delivered by Team B. Team C will only be allowed to do a full regression with the Leaf certificate 2.

This team use case in an example that user can adapt.
In practice you can refer to these articles to create a chain certificate :

6. References

No categories assignedEdit