STM32WB and STM32WBA GATT caching

Revision as of 18:00, 21 April 2023 by Registered User (→‎GATT Caching new capabilities)

1. GATT caching feature

GATT Caching feature is a BLE 5.1 standard feature: it is implemented for STM32WB and STM32WBA.
GATT Caching is able to speed up the connection of the devices that have been connected previously.
Each time the two devices connect, the two devices exchange information on what other devices support.
In Bluetooth 5.0, GATT clients perform service discovery at each connection.
In Bluetooth 5.1, if the information has not changed from the initial pairing, the required data is checked against the cache, which uses less power.

1.1. GATT Caching new capabilities

The GATT caching feature brings the following changes in the STM32WB and STM32WBA BLE stack.
GATT server implementation:

  • At GATT initialization, two new characteristics to the GATT service are added:
    • Client Supported Features (for “Robust Caching”)
    • Database Hash
  • New GATT error codes may be generated upon client requests:
    • database out-of-sync (for “Robust Caching”)
    • value not allowed (for “Robust Caching”)
  • New GATT information stored in NVM:
    • Client supported features (for “Robust Caching”)
    • Client “change aware/unaware” state (for “Robust Caching”)

1.2. Changes introduced in BLE stack by the introduction of EATT

If EATT is enabled, at GATT initialization, two new characteristics are added to the GATT service:

Client Supported Features (for "Enhanced ATT bearer" and "Multiple Handle Value Notifications)
Server Supported Features (for "EATT Supported")

New GATT information are stored in NVM:

Client Supported Features (for "Enhanced ATT bearer" and "Multiple Handle Value Notifications)

Enhancement of existing GATT commands/events and addition of new GATT commands/events.

1.3. New events

ACI_GATT_EATT_BEARER_EVENT

ACI_GATT_EATT_BEARER_EVENT


ACI_GATT_MULT_NOTIFICATION_EVENT

ACI_GATT_MULT_NOTIFICATION_EVENT



1.4. New commands

ACI_GATT_READ_MULTIPLE_VAR_CHAR_VALUE

Connectivity EATT READ MULT VAR CHAR VALUE


ACI_GATT_SEND_MULT_NOTIFICATION

Connectivity EATT SEND MULT NOTIF


1.5. Enhancement of existing GATT commands and events

Backward compatibility is maintained.
Signification of "Connection Handle" parameter is extended.


1.6. Existing GATT commands supporting the enhancement

Client commands
ACI_GATT_DISC_ALL_PRIMARY_SERVICES
ACI_GATT_DISC_PRIMARY_SERVICE_BY_UUID
ACI_GATT_FIND_INCLUDED_SERVICES
ACI_GATT_DISC_ALL_CHAR_OF_SERVICE
ACI_GATT_DISC_CHAR_BY_UUID
ACI_GATT_DISC_ALL_CHAR_DESC
ACI_GATT_READ_CHAR_VALUE
ACI_GATT_READ_USING_CHAR_UUID
ACI_GATT_READ_LONG_CHAR_VALUE
ACI_GATT_READ_MULTIPLE_CHAR_VALUE
ACI_GATT_READ_LONG_CHAR_DESC
ACI_GATT_READ_CHAR_DESC
ACI_GATT_WRITE_CHAR_VALUE
ACI_GATT_WRITE_LONG_CHAR_VALUE
ACI_GATT_WRITE_CHAR_RELIABLE
ACI_GATT_WRITE_LONG_CHAR_DESC
ACI_GATT_WRITE_CHAR_DESC
ACI_GATT_WRITE_WITHOUT_RESP
ACI_GATT_CONFIRM_INDICATION

Server commands
ACI_GATT_UPDATE_CHAR_VALUE_EXT
ACI_GATT_WRITE_RESP
ACI_GATT_ALLOW_READ
ACI_GATT_DENY_READ

1.7. Existing GATT events supporting the enhancement

Client events
ACI_GATT_PROC_COMPLETE_EVENT
ACI_ATT_FIND_INFO_RESP_EVENT
ACI_ATT_FIND_BY_TYPE_VALUE_RESP_EVENT
ACI_ATT_READ_BY_TYPE_RESP_EVENT
ACI_ATT_READ_RESP_EVENT
ACI_ATT_READ_BLOB_RESP_EVENT
ACI_ATT_READ_MULTIPLE_RESP_EVENT
ACI_ATT_READ_BY_GROUP_TYPE_RESP_EVENT
ACI_ATT_PREPARE_WRITE_RESP_EVENT
ACI_ATT_EXEC_WRITE_RESP_EVENT
ACI_GATT_ERROR_RESP_EVENT
ACI_GATT_DISC_READ_CHAR_BY_UUID_RESP_EVENT
ACI_GATT_INDICATION_EVENT
ACI_GATT_INDICATION_EXT_EVENT
ACI_GATT_NOTIFICATION_EVENT
ACI_GATT_NOTIFICATION_EXT_EVENT

Server events
ACI_GATT_SERVER_CONFIRMATION_EVENT
ACI_GATT_READ_PERMIT_REQ_EVENT
ACI_GATT_READ_MULTI_PERMIT_REQ_EVENT
ACI_GATT_WRITE_PERMIT_REQ_EVENT
ACI_GATT_PREPARE_WRITE_PERMIT_REQ_EVENT

1.8. Flag configuration on STM32WB

To enable EATT feature on STM32WB:
Use SHCI_C2_BLE_INIT_OPTIONS_ENHANCED_ATT_SUPPORTED to configure CFG_BLE_OPTIONS_EXT in app_conf.h

Feature available only in "full extended" ble stack and certified in Cube 1.16.

1.9. Flag configuration on STM32WBA

To enable EATT feature on STM32WB:
Use BLE_OPTIONS_ENHANCED_ATT to initialize "options" field in pInitParams structure in app_ble.c

1.10. how to implement on STM32WB and STM32WBA applications

1. Set the flag and build the application.

2. Set the variable CFG_BLE_NUM_LINK to 1 (BLE link) + Channel_Number (parameter in ACI_L2CAP_COC_CONNECT command).
This Channel_Number corresponds to the number of "bearers" we want to establish.

3. Pairing and bonding of BLE link.

4. Establish a Connection Oriented Channel (COC) over the BLE link.

5. If condition 2. is filled, Channel_Number x ACI_GATT_EATT_BEARER_EVENT are received on central and peripheral sides.

On central side, Channel_Index (in ACI_GATT_EATT_BEARER_EVENT) is included between 0x00 and 0x1F.

On peripheral side, Channel_Index (in ACI_GATT_EATT_BEARER_EVENT) is included between 0x20 and 0x3F.

To address separately each bearer:
The connection handle to apply is between 0xEA00 and 0xEA1F for the central.

The connection handle to apply is between 0xEA20 and 0xEA3F for the peripheral.

2. Example of EATT feature including 5 bearers and data exchange

BLE and COC link establishment with EATT (SPSM=0x0027)


EATT bearers events


GATT data exchange


3. References