Getting started with STM32H5 security

Revision as of 18:32, 14 April 2023 by Registered User


A set of practical trainings is proposed to get an overview and to understand the STM32H5 security solutions.
These trainings are based on the boards, tools and code examples provided by ST.
This article gives an overview of these proposed trainings.
For the examples listed below, each step to be done is described in detail.
It is advised to start with these examples before making your own trials or using other security related examples available in the STM32Cube_FW_H5.


In this article you will access the following security features of the STM32H5

Security functions embedded on: STM32H503 picto.png STM32H563 picto.png STM32H573 picto.png
Secure boot and firmware update YES YES YES
SBSFU legacy YES NO NO
SBSFU by mcuboot NO YES YES
STiROT NO YES YES
Isolation YES YES YES
HDP YES YES YES
TF-M NO YES YES
Secure manager NO NO YES
IP protection YES YES YES
Secure provisioning YES YES YES
Initial attesation YES YES YES
SMAK NO NO YES
SMDK NO NO YES
Cryptography YES YES YES
ST crypto lib YES YES YES
Crypto libraries YES YES YES
Crypto lib usage YES YES YES
Silicon device life cycle YES YES YES
Legacy RDP NO NO NO
Secure manufacturing YES YES YES
SFI YES YES YES
SFIx YES YES YES
Provisioning YES YES YES
Secure storage NO YES YES
Attestation YES YES YES

1. Secure Boot

The STM32CubeMX can be used to set the wanted bootpath and to generate the related firmware frame.


2. Debug Authentication

It is key to well understand how to set the Debug Authentication in order to define the wanted rights to reopen the debugger once closed.

3. OEMiROT

4. STiROT

5. Secure Manager

rrrr

No categories assignedEdit