STM32WBA Bluetooth® LE – Data throughput measurement

Revision as of 15:53, 6 April 2023 by Registered User (→‎References)

1. Enhanced ATT feature

New Enhanced Attribute Protocol (EATT) capabilities and benefits:
• EATT modifies the sequential transaction model, making concurrent ATT transactions possible when conducted over distinct enhanced ATT bearers.
• EATT uses the L2CAP Enhanced Connection-Oriented Channels mode. This L2CAP mode provides flow control so that EATT can be regarded as reliable.
• MTU values at the ATT layer and L2CAP layer have been made independently configurable, and this may reduce latency experienced by some applications that share the BLE stack with other applications.

This is a BLE 5.2 standard feature: it is implemented for STM32WB and STM32WBA.

1.1. how to implement on STM32WB

1.2. how to implement on STM32WBA

• Issue: the Enhanced ATT feature “can provide an improved user experience on devices where there are multiple applications using the BLE stack”. • Solution: we have introduced a new static GATT mode: • BLE_OPTIONS_ENHANCED_ATT This mode along with new commands and events implements the Enhanced ATT feature (see next slides). • Implemented: in tag 111 only for “full extended” stack (included as “enabled” in WB cube release 1.15, and as “certified” in release 1.16)

2. References

No categories assignedEdit