How to start with OEMiRoT on STM32H573 and 563–TrustZone enabled

Revision as of 11:10, 27 February 2023 by Registered User (→‎Step 5 : Regression)

How to start with OEM-iROT on STM32H573 - TrustZone enabledClock.png85min

Target description

Through this practical example the user will learn how to perform the following operations

  • Run the OEMiROT example of the CubeFW
    • Provisioning preparation
    • Code and data compilation and encrypted image generation
    • Perform the provisioning and install the firmware and data files
    • Execute the installed firmware
    • Perform a full regression
  • Debug Authentication
    • Create a certificate chain
    • Perform a regression using the leaf certificate of the certificate chain
    • Debug opening (Secure and non Secure) using root certificate
    • Attach CubeProgrammer and attach an IDE once debugger is open
    • Read Secure and non secure firmware
    • Perform a partial regression and download new code and data non secure


This OEMiROT Step by step tutorial is divided in two main parts

  • Provisioning
    • Configuration
    • Device Provisioning
    • Application code execution
    • Full regression
  • Debug Authentication
    • Certificate chain
    • Debug opening (Secure and Non Secure)
    • Regression (partial and full)

Prerequisites

  • knowledge of STM32CubeProgrammer
  • knowledge of JTAG / SWD interface

Hardware

  • Discovery board STM32H573I-DK.


Required tools

  • STM32Cube_FW_H5_1.0.0 or later
  • STM32CubeProgrammer_rev2.13.0 or more recent with STM32TrustedPackageCreator selected at installation
Info white.png Information
TPC installed together with CubeProgrammer in bin folder located in default STM32CubeProgrammer path : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin You can pin this tool to task bar to simplify the OEMiROT Getting started process :

Security PinToTask.png

  • IAR Embedded Workbench rev 9.20.1 or later
  • Tera Term / Putty or equivalent terminal emulator


Literature

  • UM2237 STM32CubeProgrammer software description
  • UM2238 STM32 Trusted Package Creator tool software description
  • AN5054 Secure programming using STM32CubeProgrammer
  • AN2606 STM32 microcontroller system memory boot mode


Environment setup

Before starting, the first step is to prepare the environment to be able to go through the OEM-iROT process.

  • Download the STM32CubeFW_H5 Cube firmware

A directory STM32H573I-DK is included in the Projects directory

Security PATH STM32Cube FW H5 V1.0.0.png
Warning white.png Warning
Place STM32CubeFW_H5 Cube firmware close to the C: root to avoid long windows path.


  • STM32CubeProgrammer default folder is : C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer

In case the STM32CubeProgrammer has not been installed in the default folder, the customized installation paths need to be updated in the following script :Projects\STM32H573I-DK\ROT_Provisioning\env.bat

:: ==============================================================================
::                               General
:: ==============================================================================
:: Configure tools installation path
set stm32programmercli="C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe"
set stm32tpccli="C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32TrustedPackageCreator_CLI.exe"


1. OEMiROT Step by step : Provisioning / Code execution / Regression

1.1. Step 1 : OEMiROT and Debug Authentication configuration

1.1.1. OEMiROT configuration

At this step the file (OEMiRoT_Config.obk) used to configure the OEMiROT will be generated. A default file is provided in the example that can be used without modification for a first trial in this path : Projects\STM32H573I-DK\ROT_Provisioning\OEMiROT\Binary

Security Path Config OEMiROT fleches.png

Trusted Package Creator will be used to setup this file using the OEMiRoT_Config.xml as input located in Config folder : Projects\STM32H573I-DK\ROT_Provisioning\OEMiROT\Config

The following parameters can be defined at this step:

  • ECDSA-256 encryption key
  • ECDSA-256 authentication secure key
  • ECDSA-256 authentication non secure key

To generate a customized configuration file proceed as follow:

  • Open Trusted Package Creator and select H5
  • Open Obkey tab
  • Select the OEMiROT_Config.xml file in folder ROT_Provisioning\OEMiROT\Config
  • Update the parameters if needed
  • The default keys can be regenerated
Security OEMiROT Config-TPC with marker.png
  • Generate the file :
    Security GenerateOBKeyIcon.png

The OEMiROT_Config.obk file is generated. The modified parameters are saved in Binary \OEMiROT_Config.obk

1.1.2. Debug Authentication configuration

At this step the file DA_Config.obk will be generated in DA\Binary folder. This file is used to configure the conditions to reopen a protected device and the debugger. A default file is provided in the STM32CubeFW_H5 example that can be used without modification for a first trial.

Trusted Package Creator will be used to setup this file using the DA_Config.xml as input located in DA\Config path.

Security Path Config DA fleches.png

The following parameters can be defined at this step

  • Hash (SHA256) of the root private key
  • Permissions list (full regression, partial regression, debug opening (HDPL1 S/NS, HDPL2 S/NS, HDPL3)

Two files are included in the DA directory:

  • DA_Config.xml : configuration based on certificates for H5 crypto parts (this file is used for this tutorial)
  • DA_ConfigWithPassword : configuration based on password : when TrustZone is disabled
Warning white.png Warning
The device will be blocked if password provisioning is done during this tutorial since TrustZone is enabled


To generate a customized configuration file, proceed as follow:

  • Open Trusted Package Creator and select H5
  • Open Obkey tab
  • Select the DA_Config.xml file
  • Update the parameters if needed. For a first trial we recommend to keep the default key, because in the regression step we will use the default certificate that is linked to the default DA keys.
Warning white.png Warning
If a customized DA key is generated here, make sure the customized root key file is well saved/kept because they will be used later on for debug reopening and regression. If this key is lost, the device might be lock forever.
Security DA Config-TPC.png
  • Generate the file :Security GenerateOBKeyIcon.png

1.2. Step 2 : Code and data image generation

1.2.1. STM32CubeFW provided code compilation

1.2.2. Firmware and data encrypted image generation

1.2.2.1. Code compilation

Check that the STM32H5 IAR provided patch is correctly installed and check that your IAR Embedded Workbench version is recent enough.

Two code examples for IAR Embedded Workbench are provided

  • OEMiROT_Boot corresponds to the Secure Boot.

It performs authenticity and integrity checks of the project firmware and data images.

  • OEMiROT_Appli_TrustZone is an example of secure and non secure application managed by OEMiROT
Security Applis path withFleches.png

OEMiROT_Boot project compilation

  • Open the Project.eww located in the EWARM directory : ..\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Boot\EWARM
  • Open Project -> Option -> General Options : The device and CPU core should be automatically recognized and you should see the following windows
Security IAR Device.png

If the device is not recognized, check that the STM32H5 IAR provided patch is correctly installed check that your IAR Embedded Workbench version is recent enough

  • Perform: Project -> Rebuild all (don’t upload the code, only perform a compilation)

The following binary is created:…..\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Boot\EWARM\STM32H573I_DK\Exe\Project.bin

OEMiROT_Appli_TrustZone project compilation –Secure Project

  • Open the Project.eww located in the EWARM directory :

..\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Appli_TrustZone\EWARM

  • Select the Project secure :
Security Pj Secure withFlech.png
  • Open Project -> Option -> General Options

The device and CPU core should be automatically recognized.

  • Open Project -> Option -> Build Actions

Here is the command line which will create an image of the code with STM32Cube Package Creator:

Security postbuild Secure.png
  • Perform: Project -> Rebuild all (don’t upload the code, only perform a compilation)

The following image is created: …..\ Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Appli_TrustZone\Binary\rot_tz_s_app_enc_sign.hex Don’t close the EWARM project .

OEMiROT_Appli_TrustZone project compilation –Non-Secure Project

  • Select Non Secure Project
Security Pj NonSecure withFlech.png
  • Open Project -> Option -> Build Actions Check the correct paths for the command line
Security Postbuild non secure.png

This postbuild command will create an image of the compiled non secure code thanks to STM32Cube Package Creator.

  • Perform: Project -> Rebuild all (don’t upload the code, only perform a compilation)

The following image is created:…..\ Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Appli_TrustZone\Binary\rot_tz_ns_app_enc_sign.hex

1.2.2.2. Code image generation

During this step two image files will be created from secure and non secure binary code files.

In the previous steps secure and non secure code images have been created directly from EWARM post build command (rot_tz_ns_app_enc_sign.hex and rot_tz_s_app_enc_sign.hex), but you can also create code images manually:

Security Images Path withFlech.png

This tutorial shows an example for two code two data images installation, but other configurations are also possible.

We show here how to perform manually an encrypted / signed code image (equivalent to what the postbuid command has executed)

  1. Open Trusted Package Creator select H5
  2. Open tab ImageGen
  3. Select the template for the relevant image: OEMiRoT_S_Code_Image.xml (ROT_Provisioning\OEMiROT\Images directory)
  4. Update the default configuration if required
  • Update the Firmware area size
  • Update the version number
  • Enable the dependency with the other (Data) image when simultaneous installation is required for compatibility reasons.
  • Select the binary file to be used as input file
  • Select the output file to be filled with the signed and encrypted binary (hex format)
  1. Launch the generation
  2. An encrypted signed file will be created : rot_tz_s_app_enc_sign.hex
Security Code Image creation.png

Resume to 1. and select OEMiRoT_NS_Code_Image.xml template in order to generate rot_tz_ns_app_enc_sign.hex image.

1.2.2.3. Data image generation

During this step two image files will be created from secure and non secure data files.

Security data binaries path with fleches.png

The provided data files s_data.bin and ns_data.bin are just example files for this tutorial but have no meaning and not used for the code execution.

This tutorial shows an example for two code two data images installation, but other configurations are also possible.

To generate images of secure and non secure data you must :

  1. Open Trusted Package Creator select H5
  2. Open tab ImageGen
  3. Select the template for the relevant image: OEMiRoT_S_Data_Image.xml (ROT_Provisioning\OEMiROT\Images directory)
  4. Update the default configuration if required
  • Update the version number
  • Enable the dependency with the other Data image when simultaneous installation is required for compatibility reasons.
  • Select the binary file to be used as input file
  • Select the output file to be filled with the signed and encrypted binary (hex format)
  1. Launch the generation
  2. An encrypted signed file will be created : s_data_enc_sign.hex


Resume to 3. and select OEMiRoT_NS_Data_Image.xml template in order to generate ns_data_enc_sign.hex image.

1.3. Step 3 : Device provisioning, code and data image download into Flash, product state setting

The provided “provisioning” script will

  • Set the option bytes of the device
  • Configure the OEMiROT and the DA on the device
  • Install the images (code and data)
  • Set the final chosen product state according user selection
Security Provisioning path withFleches.png

Before launching the script , connect STM32CubeProgrammer and check that the device is in open state. Security OPEN STATE STM32CubeProgrammer.png

If it’s not the case refer to the step 5 explaining the regression. If the flash is not erased, the provisioning script will anyway erase it.

  • Connect the board, with BOOT0 pin not connected to VDD (check that the CubeProgrammer is disconnected)
  • Open folder OEMiROT in : Projects\STM32H573I-DK\ROT_Provisioning\OEMiROT
  • Run the provided provisioning.bat script (double click)
  • Steps 1 and step 2 have been previously executed : press any key to continue until Step 3
  • Step 3 : The script will proceed with the option byte programming and flashing the code and data image

The product state can be chosen (OPEN or PROVISIONED or TZ-CLOSED or CLOSED or LOCKED) Before setting the product state to TZ-CLOSED/CLOSED or LOCKED, it is advised to set the PROVISIONED state and to try out the regression. Then to redo the complete provisioning starting step by step from the beginning and only then set one of the more closed states.

Warning white.png Warning
Reminder that LOCKED is a definitive product step that can’t be changed anymore.

Make a first trial setting the product in PROVISIONED state and complete the tutorial till the end.

1.4. Step 4 : Execute the installed firmware

  • Open PUTTY(or another terminal emulator)
  • Select “Serial" and the COMxx port
  • Set speed to 115200
  • Click: Open
Security PuTTY Configuration.png

Reset the board (SW reset button on the board) : The code installed during previous steps will be executed

The menu of the installed code has two options

  • The menu 1 will launch the standard bootloader located in the system flash
  • The menu 2 will display the first 8 bytes and the last 8 bytes of the ns_data.bin

1.5. Step 5 : Regression

  • A full regression will erase the user stored contents and secrets.
    • Erase the user flash content
    • Erase the obkeys
    • Reset the secure option bytes to their default value
    • Set the product in open state
  • If the product is in Open state, a full regression is not needed since the device is not secured and changes can be done without any authentication. In case the regression script is executed, it will indicate some errors
  • If the product is not in Open state, the only way to change the OEMiROT is to first do a full regression


Warning white.png Warning
If DA key has been regenerated in Debug_Authentication_configuration, please follow section Certificate Chain generation (ROOT certificate) using STM32 Trusted Package Creator to generate Root certificate which will be needed for regression. If DA key has not been regenerated you can continue the exercise.

1.5.1. Full regression from Provisioned state using script (included in the STM32CubeFW)

The regression can be done using the provided script or using CubeProgrammer

To preform a full regression

  • Launch the regression script
Security PATH Regression Script with F.png
  • “The Trustzone feature is enabled?” answer “Yes”
  • If the regression has succeeded the following message should be displayed :
Security DA Success Message.png
  • Connect STM32CubeProgrammer. Check that the flash content is well erased and that the option bytes and product state are at default values.

1.5.2. Full regression from Closed state using STM32CubeProgrammer

  • Disconnect STM32CubeProgrammer
  • Redo the exercise starting at step3, set the “closed” state
  • Click Security DA ICON STM32CubeProgrammer.png in CubeProgrammer and select “Debug Authentication”
  • Click “Discover” the information window will be filled
SECURITY Discover Display State Closed.png
  • Enter the path for the key and the certificate(example with a certificate chain will be shown later, in this example only a single certificate is used (ROOT)):
Security Key and Certificate paths CubePragrammer.png
  • Click Continue
  • The opening method and permission are selected. Only the opening method defined by the certificate mask (during provisioning) will be possible
Security DA Permissions CubeProgrammer.png
  • Click Execute and you have the Success Message :
Security DA Success Message w CubeProgrammer.png
  • Check with CubeProgrammer that the flash content is well erased and that the option bytes and product state are at default values.
  • The TZ will stay enabled and can be disabled using CubeProgrammer

2. OEMiROT Step by step : Debug Authentication

2.1. Certificate chain generation

  • Perform a full regression (if not already done at step 5), disconnect/reconnect the USB cable
  • Check Step 0 and do/redo Step 1.1
  • Open Trusted Package Creator, select H5 and select the tab DA CertifGen
  • The example is provided with one root, one intermediate and one leaf key pair
  • The first certificate to generate is the ROOT certificate
  • This certificate defines the permission defined by the owner generating the certificates.

The second certificate to generate is the intermediate certificate, chained with the ROOT certificate The owner for instance an OEM is defining the permission of this intermediate certificate The last certificate to generate is the leaf certificate, chained with the intermediate certificate To use the certificate chain for debug opening or regression, the Leaf certificate is used as input for STM32CubeProgrammer (since this certificate is the last of the chain), but the permission is defined by the aggregation of all mask permissions. For instance, if the debug opening in L3 is not allowed in one of the mask of the chain, this debug opening will not be allowed (even if allowed in the leaf mask) The root certificate can also be used by the owner of the root key for debug opening or regression according to the permission defined during the root certificate generation

Certificate Chain generation (ROOT certificate) using STM32 Trusted Package Creator

  • Select STM32H5 and ROOT; enter the path for the private key, the public root key and where the certificate will be stored (overwrite the default stored certificate)
  • Set the permission mask for the ROOT : Setting 1 will give the permission
Security TPC-CertifGenROOT.png
  • ClickSecurity Icon-TPC GenerateCertif.png

Certificate Chain generation (INTERMEDIATE certificate)

  • Select INTERMEDIATE and enter the path for the private root key and the intermediate public keys.

One intermediate certificate for this example, but the same step can be done several time to add several intermediate certificates, each with his own key pair and permission mask

  • Set the permission mask for the INTERMEDIATE certificate;
Security TPC-CertifGenINTERMEDIATE withFleches.png
  • ClickSecurity Icon-TPC GenerateCertif.png
Info white.png Information
Reminder: every added certificate of the chain can have equal or less permission than the previous certificate of the chain


Certificate Chain generation (LEAF certificate)

  • Select LEAF and enter the path for the private intermediate key and the for the public leaf key.

This certificate is the last of the chain

  • Set the permission mask for the LEAF certificate;
Security TPC-CertifGenLEAF withFleches.png
Info white.png Information
The LEAF certificate can have equal or less permission than the intermediate certificate chained with the LEAF

2.2. Secure Debug Opening

  • Redo the exercise starting at step3, set the “closed” state
  • Click Security DA ICON STM32CubeProgrammer.png in CubeProgrammer and select “Debug Authentication”
  • Click “Discover” the information window will be filled
SECURITY Discover Display State Closed.png
  • Enter the path for the key and the certificate(example with a certificate chain will be shown later, in this example only a single certificate is used (ROOT)):
SECURITY Key and Certificate paths CubePragrammer.png
  • Click Continue

2.2.1. Secure Debug opening using STM32CubeProgrammer and ROOT certificate

Info white.png Information
For the OEMiROT example the application code is in HDPL3

A SECURE debug opening in Level 2 or in level 3 will make the secure application visible

  • Select Secure Intrusive Debug (level 3)
Security Permision Secure Debug CubeProgrammer.png
  • Click Execute and you have the Success Message :
Security DA Success Message w CubeProgrammer.png
  • Disconnect STM32CubeProgrammer
  • Now that the debug is open the secure flash content can be read out
Warning white.png Warning
! Don’t power on /off the board it will close the debugger
  • With STM32CubeProgrammer : Connect the board
  • Secure part of the flash is now visible @0x0C012400
Security Read Secure Flash STM32CubeProgrammer.png
Info white.png Information
The memory mapping of the non secure code is detailed in Project_s.map located in:

C:\STM32Cube_FW_H5_V1.0.0\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Appli_TrustZone\EWARM\Secure\STM32H573I-DK_S\List

2.2.2. Secure Debug opening, attach IAR, read flash content and code execution

To attach an IDE:

  • Disconnect STM32CubeProgrammer
  • Open the Project.eww located in the EWARM directory :

..\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Appli_TrustZone\EWARM

  • Select the Project secure :
Security Pj Secure withFlech.png
  • Select: Project -> Attach to running target
  • Open the main.c
  • Set a break point, the execution will stop at this point
  • Reset the board (SW reset, black button)
  • Select: View Memory1 -> enter the flash address
  • Secure code visible @ 0x0C012400
Security IAR Secure Flash debug.png

2.2.3. Close the debugger through hardware reset

  • Close the debug in IARSECURITY IAR close Debug Mode.png
  • Disconnect/reconnect the USB cable / A hardware reset will close again the debugger
  • Click Security DA ICON STM32CubeProgrammer.png in CubeProgrammer and select “Debug Authentication”
  • Click “Discover” the information window is filled again showing that the state is closed.
SECURITY Discover Display State Closed.png

2.3. Non Secure Debug Opening

2.3.1. Non Secure Debug opening using STM32CubeProgrammer and ROOT certificate

  • Enter the path for the root private key and certificate
SECURITY Key and Certificate paths CubePragrammer.png
  • Click Continue
Info white.png Information
For the OEMiROT example the application code is in HDPL3

A NON-SECURE debug opening in Level 2 or in level 3 will make the secure application visible

  • Select Non Secure Intrusive debug (level 3)
SECURITY Permission Non Secure Debug CubeProgrammer.png
  • Click execute and you have the success message :
Security DA Success Message w CubeProgrammer.png
  • Now that the debug is open the secure flash content can be read out
Warning white.png Warning
! Don’t power on /off the board it will close the debugger
  • Connect the board to STM32CubeProgrammer if it has not been automatically done
  • The Non Secure part of the flash is now visible @ 0x08018400
Info white.png Information
The memory mapping of the non secure code is detailed in Project_ns.map located in:

C:\STM32Cube_FW_H5_V1.0.0RC1\Projects\STM32H573I-DK\Applications\ROT\OEMiROT_Appli_TrustZone\EWARM\NonSecure\STM32H573I-DK_NS\List

SECURITY View Non Secure part of Flash CubeProgrammer.png
Info white.png Information
If you try to read the Secure Part of the Flash @ 0x0C012400 you have an error message :
SECURITY Error Message Data Read Failed CubeProgrammer.png

2.3.2. Non Secure Debug opening, attach IAR, read flash content and code execution

To attach an IDE:

  • Disconnect STM32CubeProgrammer
  • Open the Project.eww located in the EWARM
  • Select Non Secure project
SECURITY IAR Non Secure Project Select.png
  • Select: Project -> Attach to running target
  • Open the main.c
  • Set a break point, the execution will stop at this point
  • Select: View->Memory-> Memory1 and enter the flash address => Non secure code is visible @ 0x08018400
SECURITY IAR View Non Secure Part of Flash.png

2.3.3. Close the debugger through hardware reset

  • Close the debug in IARSECURITY IAR close Debug Mode.png
  • Disconnect/reconnect the USB cable / A hardware reset will close again the debugger
  • Click Security DA ICON STM32CubeProgrammer.png in CubeProgrammer and select “Debug Authentication”
  • Click “Discover” the information window is filled again showing that the state is closed.
SECURITY Discover Display State Closed.png

2.4. Partial Regression

2.4.1. Partial Regression using the leaf key and certificate chain

  • Enter the path for the leaf private key and leaf chain certificate
SECURITY LEAF Key and Certificate paths CubeProgrammer.png
  • Click Continue
Warning white.png Warning
Partial regression must be forbidden with leaf certificate : mask chosen for leaf certificate doesn’t give permission

to a partial regression :

SECURITY Permission Leaf Certif.png
  • Select Partial regression
SECURITY Permision PARTIAL REGRESSION CubeProgrammer.png
  • Click Execute

The partial regression has not been allowed by the leaf mask (only a full regression allowed) and you have the Error Message :

SECURITY Error Message Debug Authentication.png
  • Click on “Discover” the window state is filled again
SECURITY Discover Display State Closed.png

2.4.2. Partial Regression using the root key and certificate

2.4.2.1. Partial regression ->TZ-CLOSED State
  • Enter the path for the root private key and certificate
SECURITY Key and Certificate paths CubePragrammer.png
  • Click Continue
  • Select Partial regression
SECURITY Permision PARTIAL REGRESSION CubeProgrammer.png
  • Click execute and you have the success message :
Security DA Success Message w CubeProgrammer.png
  • Disconnect from CubeProgrammer.

The product is now in TZ-CLOSED

2.4.2.2. Run the code
  • Open PUTTY(or another terminal emulator)
  • Select “Serial" and the COMxx port
  • Set speed to 115200
  • Click: Open
Security PuTTY Configuration.png
  • Reset the board (SW reset button on the board)

-> Only the Boot code is displayed :

SECURITY PUTTY BOOT CODE DISPLAY.png
  • Non Secure code and data have been erased during partial regression
  • Debug is not possible anymore
  • New code and datas can be downloaded
2.4.2.3. Download a new application code
  • Open the project OEMiROT_Appli_TrustZone
  • Select Non Secure project
  • Change const uint8_t UserAppId = 'A' line 61 in main.c file by :
const uint8_t UserAppId = B; 
SECURITY Download new Non Secure App.png
  • Select: Project-> Rebuild all
  • Open CubeProgrammer and Connect the board
  • Select SECURITY ICON Erasing and Programming CubeProgrammer.png“Erasing & Programming” tab
  • Browse non secure encrypted code image .hex file that we previously generated in folder Application\ROT\OEMiROT_Appli_TrustZone\Binary
SECURITY Download new Non Secure App CubeProgrammer.png
  • Click Start Programming
  • Browse non secure encrypted data image .hex file in folder ROT_Provisioning\OEMiROT\Binary
SECURITY Download new Non Secure Data CubeProgrammer.png
  • Click Start Programming
Warning white.png Warning
!!! A partial regression erases code and data non secure.

It is necessary to download Code AND Data to visualize new firmware in the terminal

  • Disconnect STM32CubeProgrammer
  • Open PUTTY(or another terminal emulator)
  • Select “Serial" and the COMxx port
  • Set speed to 115200
  • Click: Open
Security PuTTY Configuration.png
  • Reset the board (SW reset button on the board)
    • Boot Code and new firmware are displayed
    • Non secure debug is possible
SECURITY PUTTY BOOT CODE and Non Secure Code Display.png

Non secure debug :

  • Disconnect STM32CubeProgrammer
  • Open the Project.eww located in the EWARM
  • Select Non Secure project
SECURITY IAR Non Secure Project Select.png
  • Select: Project -> Attach to running target
  • Open the main.c
  • Set a break point, the execution will stop at this point
  • Select: View->Memory-> Memory1 and enter the flash address => Non secure code is visible @ 0x08018400
SECURITY IAR View Non Secure Part of Flash.png
Warning white.png Warning
!! If code is jumping to secure code, it will still work but user can’t debug / see secure world

2.5. Full Regression using leaf key and certificate

  • Close the debug in IARSECURITY IAR close Debug Mode.png
  • Click Security DA ICON STM32CubeProgrammer.png in CubeProgrammer and select “Debug Authentication”
  • Click “Discover”
  • Enter the path for the leaf private key and leaf chain certificate
SECURITY LEAF Key and Certificate paths CubeProgrammer.png
  • Click Continue
  • Select Full Regression :
Security DA Permissions CubeProgrammer.png
  • Click Execute and you have the Success Message :
Security DA Success Message w CubeProgrammer.png
  • Check with CubeProgrammer that the flash content is well erased and that the option bytes and product state are at default values.
No categories assignedEdit