Click here for Bluetooth® Low Energy Overview
1. Introduction
The STM32CubeWBA MCU Package[1] provides software components running on STM32WBA Series MCUs.
For all examples provided with the package, the following integrated development environments are supported:
- STMicroelectronics integrated development environment for STM32 products (STM32CubeIDE)
- IAR Systems® IAR Embedded Workbench® for Arm® (EWARM)
- Keil® Microcontroller Development Kit (MDK-ARM)
2. STM32WBA Bluetooth® LE software architecture
The single Core Arm® Cortex®-M33 STM32WBA Bluetooth® low energy solution is designed to develop application firmware including Profiles & Services on top of the Bluetooth® Low Energy Firmware Stack (Controller & Host) handling the link layer up to the generic attribute profile and generic access profile layers
- more information regarding STM32WBA SW Architecture
STM32WBA Bluetooth® LE architecture |
---|
3. STM32WBA Bluetooth® LE application
The following Bluetooth® LE applications are delivered as source code
- To build and install them, follow the steps described in Bluetooth® LE Build and Install Application page
Application | Description | |
---|---|---|
Bluetooth® LE SIG | BLE_Beacon | Application advertising different types of beacon: ibeacon, eddystone (tlm, uuid, url) |
BLE_HealthThermometer | Application supporting the Health Thermometer Sensor as specified by the Bluetooth® SIG | |
BLE_HeartRate | Application supporting the Heart Rate Sensor as specified by the Bluetooth® SIG. | |
Operating System | BLE_HeartRate_ThreadX | Application supporting the Heart Rate Sensor with ThreadX implementation |
Bluetooth® LE ST proprietary | BLE_p2pServer & Multi Slave BLE_p2pClient | Simple ST proprietary applications to manipulate proprietary Services & Characteristics with single connection or multi slave connections |
BLE_p2pRouter | ST proprietary application to use the STM32WBA as a GAP Central & Peripheral" and "GATT Client & Server with multi link connection | |
BLE_DataThroughput | ST proprietary application to measure data throughput between 2 STM32WBA or with the dedicated ST Bluetooth® LE toolbox smartphone application (Android and IOS) | |
BLE_Fuota (Firmware Update Over The Air) | ST proprietary application to upgrade the STM32WBA firmware | |
BLE_SerialCom | ST proprietary application to simulate the previous Bluetooth® protocol "Serial Port Profile". The application is based on L2CAP Connection Oriented Channel (CoC) | |
BLE_p2pServer_Ext | Application to configure up to 8 advertising extended sets | |
BLE_p2pClient_Ext | Application to scan the extended advertising frames with extended API’s | |
BLE_TransparentMode | ST proprietary application to support the Direct Test Mode for RF certification. Standard host controller interface (HCI) and application (vendor) controller interface (ACI) can be sent by means of STM32CubeMonitor-RF |
4. Going further based on available application
Application | Description | |
---|---|---|
Bluetooth® LE Feature | power consumption Measurement | Explanation how to measure the power consumption with NUCLEO-WBA52CG development board |
BlueST SDK v2 | ||
|
5. Manufacturer Advertising Data & BlueST SDK v2
5.1. Background and motivations
BlueST SDK v1 development has started in 2015 and it has grown over time with the addition of more and more functionalities that enable microcontroller firmware to advertise its capabilities and exchange data with mobile applications as well as industrial gateways via Bluetooth Low Energy.
BlueST SDK is shared as opensource code on multiple github repositories for Android, iOS and Python.
The STMicroelectronics vendor-specific advertisement allows declaring characteristics that are implemented by the device. A 4 byte feature mask is a bitfield where each bit represents a feature, e.g. accelerometer, temperature, freefall, compass etc. In the vendor-specific advertisement, 1 byte is used to indicate the evaluation board model.
As firmware packages and board models grow in number and supported functionalities, a new mechanism is needed to overcome the 4 bytes feature mask limitations.
The main purpose of the BlueST SDK v2 protocol is allowing a client to recognize the board type and the firmware capabilities of the board in proximity and be future proof.
The mapping between Device ID / Firmware ID and the actual description of the firmware capabilities relies on a JSON document.
BlueST SDK v2 ^ BlueST SDK v1 |
---|
5.2. BlueST SDK v2 & STM32WBA Bluetooth® LE Applications
The following STM32WBA Bluetooth® LE Applications use the BlueST SDK v2 protocol
BlueST SDK v2 protocol & STM32WBA Bluetooth® LE Applications | ||||||||||||||||||||||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
6. References