Introduction to Thread

Revision as of 12:22, 20 February 2023 by Registered User
Under construction.png Coming soon

1. Introduction

Thread is an IPv6-based, low power and secure mesh networking protocol for IoT developed and supported by Thread Group [1]. It is designed specifically for Home Automation applications.
The Thread standard is based on IEEE 802.15.4 MAC and physical layer operating at 250 kbps in 2.4 GHz band. OpenThread is an open-source implementation of Thread released by Google [2].
The STM32WB [3] is a certified component for whatever Full Thread Device (FTD) or Minimal Thread Device (MTD) type of role is intended.

2. Thread Specification

Thread is a networking layer based on IPv6. Thread specification is based on 7 layers as shown in the figure below. It uses the IEEE 802.15.4 PHY and MAC layers for link layer communication. MAC layer supports a maximum packet size of 127 bytes. IPv6 requires a minimum of 1280 bytes of MTU. For that, 6LoWPAN performs IP packet fragmentation and header compression to fit in 127 bytes.

Thread Specification
Connectivity Thread Spec.png

3. Thread Border Router

A Thread Border Router (TBR) is a specific router that connects a Thread network to others IPv6-based networks like Wi-Fi or Ethernet.
A Thread network can contain one or more TBRs.

Thread Border Router
Connectivity Thread BorderRouter.png

4. Acronyms and definitions

Term Definition
DTLS Datagram Transport Layer Security
FTD Full Thread Device
MAC Media Access Control
MTD Minimal Thread Device
PHY Physical
REED Router Eligible End Device
UDP User Datagram Protocol

5. References