FP-AI-MONITOR2 getting started

Sensing is a major part of the smart objects and equipment, for example, condition monitoring for predictive maintenance, which enables context awareness, production performance improvement, and results in a drastic decrease in the downtime due to preventive maintenance.

The FP-AI-MONITOR2 function pack is a multi-sensor AI data monitoring framework on the wireless industrial node, for STM32Cube. It helps to jump-start the implementation and development of sensor-monitoring-based applications designed with the X-CUBE-AI, an Expansion Package for STM32Cube, or with the NanoEdge™ AI Studio, an autoML tool for generating AI models for tiny microcontrollers. It covers the entire design of the Machine Learning cycle from the data set acquisition to the integration and deployment on a physical node.

The FP-AI-MONITOR2 runs learning and inference sessions in real-time on the SensorTile Wireless Industrial Node development kit box (STEVAL-STWINBX1), taking data from onboard sensors as input. The FP-AI-MONITOR2 implements a wired interactive CLI to configure the node and manage the learn and detect phases. For simple in the field operation, a standalone battery-operated mode is also supported, that allows basic controls through the user button, without using the console.

The STEVAL-STWINBX1 has an STM32U585AIIxQ microcontroller, which is an ultra-low power Arm® Cortex®-M33 MCU, with FPU and TrustZone at 160 MHz, 2 Mbytes of Flash memory and 786 Kbytes of SRAM. In addition, the STEVAL-STWINBX1 embeds industrial-grade sensors, including 6-axis IMU, 3-axis accelerometer and vibrometer, and analog microphones to record any inertial, vibrational and acoustic data on the field with high accuracy at high sampling frequencies.

The rest of the article discusses the following topics:

  • The required hardware and software,
  • Pre-requisites and setup,
  • FP-AI-MONITOR2 console application,
  • Running a human activity recognition (HAR) application for sensing on the device,
  • Running an anomaly detection application using NanoEdge™ AI libraries on the device,
  • Running an n-class classification application using NanoEdge™ AI libraries on the device,
  • Running an advance dual model on the device, which combines anomaly detection using NanoEdge™ AI libraries based on vibration data and CNN based n-class classification based on ultrasound data,
  • Performing the vibration and ultrasound sensor data collection using a prebuilt binary of FP-SNS-DATALOG2,
  • Button operated modes, and
  • Some links to useful online resources, to help the user better understand and customize the project for her/his own needs.

This article is just to serve as a quick starting guide and for full FP-AI-MONITOR2 user instructions, readers are invited to refer to FP-AI-MONITOR2 User Manual.

Info white.png Information
NOTE: The NanoEdge™ library generation itself is out of the scope of this function pack and must be generated using NanoEdge™ AI Studio.

1. Hardware and software overview

1.1. STWIN.box - SensorTile Wireless Industrial Node Development Kit

The STWIN.box (STEVAL-STWINBX1) is a development kit and reference design that simplifies prototyping and testing of advanced industrial sensing applications in IoT contexts such as condition monitoring and predictive maintenance.

It is powered with Ultra-low-power Arm® Cortex®-M33 MCU with FPU and TrustZone at 160 MHz, 2048 kBytes Flash memory (STM32U585AI)

It is an evolution of the original STWIN kit (STEVAL-STWINKT1B) and features a higher mechanical accuracy in the measurement of vibrations, an improved robustness, an updated BoM to reflect the latest and best-in-class MCU and industrial sensors, and an easy-to-use interface for external add-ons.

The STWIN.box kit consists of an STWIN.box core system, a 480mAh LiPo battery, an adapter for the ST-LINK debugger, a plastic case, an adapter board for DIL 24 sensors and a flexible cable.

STEVAL-STIWINBX1.png

Other features:

  • MicroSD card slot for standalone data logging applications
  • On-board Bluetooth® low energy v5.0 wireless technology (BlueNRG-M2), Wi-Fi (EMW3080) and NFC (ST25DV04K)
  • Option to implement authentication and brand protection secure solution with STSAFE-A110
  • Wide range of industrial IoT sensors:
    • Ultra-wide bandwidth (up to 6 kHz), low-noise, 3-axis digital vibration sensor (IIS3DWB)
    • 3D accelerometer + 3D gyro iNEMO inertial measurement unit (ISM330DHCX) with Machine Learning Core
    • High-performance ultra-low-power 3-axis accelerometer for industrial applications (IIS2DLPC)
    • Ultra-low power 3-axis magnetometer (IIS2MDC)
    • High-accuracy, high-resolution, low-power, 2-axis digital inclinometer with Embedded Machine Learning Core (IIS2ICLX)
    • Dual full-scale, 1.26 bar and 4 bar, absolute digital output barometer in full-mold package (ILPS22QS)
    • Low-voltage, ultra low-power, 0.5°C accuracy I²C/SMBus 3.0 temperature sensor (STTS22H)
    • Industrial grade digital MEMS microphone (IMP34DT05)
    • Analog MEMS microphone with frequency response up to 80 kHz (IMP23ABSU)
  • Expandable via a 34-pin FPC connector

1.2. Software architecture

The top-level architecture of the FP-AI-MONITOR2 function pack is shown in the following figure.

BlockDiagram FP-AI-MONITOR2.png

2. Prerequisites and setup

2.1. HW prerequisites and setup

To use the FP-AI-MONITOR2 function pack on STEVAL-STWINBX1, the following hardware items are required:

  • STEVAL-STWINBX1 development kit board,
  • a microSD™ card and card reader to log and read the sensor data,
  • Windows® powered laptop/PC,
  • One USB C-type cable, to connect the sensor board to the PC
  • One USB micro B cable, for the STLINK-V3MINI, and
  • an STLINK-V3MINI.
FP-AI-MONITOR2-hardware.png

2.2. Software requirements

2.2.1. FP-AI-MONITOR2

  • Download the latest version of the FP-AI-MONITOR2, package from ST website, extract and copy the .zip file contents into a folder on the PC. The package contains binaries, source code and utilities for the sensor board STEVAL-STWINBX1.

2.2.2. IDE

Info white.png Information
All the steps presented in this document are carried out with STM32CubeIDE, but any of the other two IDEs could have been used.

2.2.3. STM32CubeProgrammer

  • STM32CubeProgrammer is an all-in-one multi-OS software tool for programming STM32 products. It provides an easy-to-use and efficient environment for reading, writing, and verifying device memory through both the debug interface (JTAG and SWD) and the bootloader interface (UART, USB DFU, I2C, SPI, and CAN). STM32CubeProgrammer offers a wide range of features to program STM32 internal memories (such as Flash, RAM, and OTP) as well as external memory. Download the latest version of the STM32CubeProgrammer. The FP-AI-MONITOR2 is tested with the STM32CubeProgrammer version 2.12.0.
  • This software is available from STM32CubeProg.

2.2.4. Tera Term

  • Tera Term is an open-source and freely available software terminal emulator, which is used to host the CLI of the FP-AI-MONITOR2 through a serial connection.
  • Users can download and install the latest version available from Tera Term website.

2.2.5. STM32CubeMX

STM32CubeMX is a graphical tool that allows a very easy configuration of STM32 microcontrollers and microprocessors, as well as the generation of the corresponding initialization C code for the Arm® Cortex®-M core or a partial Linux® Device Tree for Arm® Cortex®-A core), through a step-by-step process. Its salient features include:

  • Intuitive STM32 microcontroller and microprocessor selection.
  • Generation of initialization C code project, compliant with IAR™, Keil® and STM32CubeIDE (GCC compilers) for Arm®Cortex®-M core
  • Development of enhanced STM32Cube Expansion Packages thanks to STM32PackCreator, and
  • Integration of STM32Cube Expansion packages into the project.

FP-AI-MONITOR2 requires STM32CubeMX V 6.7.0 or later (tested on 6.7.0). To download the STM32CubeMX and obtain details of all the features please visit st.com.

2.2.6. X-CUBE-AI

X-CUBE-AI is an STM32Cube Expansion Package part of the STM32Cube.AI ecosystem and extending STM32CubeMX capabilities with automatic conversion of pre-trained Artificial Intelligence models and integration of generated optimized library into the user project. The easiest way to use it is to download it inside the STM32CubeMX tool (version 7.3.0 or newer) as described in the user manual Getting started with X-CUBE-AI Expansion Package for Artificial Intelligence (AI) (UM2526). The X-CUBE-AI Expansion Package offers also several means to validate the AI models (both Neural Network and Scikit-Learn models) both on desktop PC and STM32, as well as to measure performance on STM32 devices (Computational and memory footprints) without ad-hoc handmade user C code.

2.2.7. Python 3.7.3

Python is an interpreted high-level general-purpose programming language. Python's design philosophy emphasizes code readability with its notable use of significant indentation. Its language constructs, as well as its object-oriented approach, aim to help programmers write clear, logical code for small and large-scale projects. To build and export AI models the reader requires to set up a Python environment with a list of packages. The list of the required packages along with their versions is available as a text file in /FP-AI-MONITOR2_V1.0.0/Utilities/requirements.txt directory. The following command is used in the command terminal of the anaconda prompt or Ubuntu to install all the packages specified in the configuration file requirements.txt:

pip install -r requirements.txt
Info white.png Information
NOTE: The FP-AI-MONITOR2 is tested with exactly the same versions of all the libraries. We noticed that different versions of few dependencies can cause some problems. In addition we recommend to use pip version 20.2.4 or 21.2.4.

2.2.8. NanoEdge™ AI Studio

NanoEdge™ AI Studio is a new Machine Learning (ML) technology to bring true innovation easily to the end-users. In just a few steps, developers can create optimal ML libraries using a minimal amount of data, for:

  • Anomaly Detection,
  • Classification, and
  • Extrapolation.

This function pack supports only the Anomaly Detection and n-Class Classification libraries generated by NanoEdge™ AI Studio .

FP-AI-MONITOR2 is tested using NanoEdge™ AI Studio V3.2.0.

NanoEdge™ AI Studio is a new Machine Learning (ML) technology to bring true innovation easily to the end-users. In just a few steps, developers can create optimal ML libraries for Anomaly Detection, 1-class classification, n-class classification, and extrapolation, based on a minimal amount of data.

2.3. Installing the function pack

2.3.1. Getting the function pack

The first step is to get the function pack FP-AI-MONITOR2 from ST website. Once the pack is downloaded, unpack/unzip it and copy the content to a folder on the PC. The steps of the process along with the content of the folder are shown in the following image.

FP-AI-MONITOR2-Pack-Struct.png

2.3.2. Flashing the application on the sensor board

This section explains how to select a binary file for the firmware and program it into the STM32 microcontroller. A precompiled binary file is delivered as part of the FP-AI-MONITOR2 function pack. It is located in the FP-AI-MONITOR2_V1.0.0\Projects\STWIN.box\Applications\FP-AI-MONITOR2\Binary\ folder. When the STM32 board and PC are connected through the USB cable on the STLINK-V3E connector, the STEVAL-STWINBX1 appears as a drive on the PC. The selected binary file for the firmware can be installed on the STM32 board by simply performing a drag and drop operation as shown in the figure below. This creates a dialog to copy the file and once it is disappeared (without any error) this indicates that the firmware is programmed in the STM32 microcontroller.

FP-AI-MONITOR2 flash.png

3. FP-AI-MONITOR2 console application

FP-AI-MONITOR2 provides an interactive command-line interface (CLI) application. This CLI application equips a user with the ability to configure and control the sensor node, and to perform different AI operations on the edge including, learning and anomaly detection (for NanoEdge™ AI libraries), n-Class classification (NanoEdge™ AI libraries), dual (combination of NanoEdge AI detection and CNN based classification), and human activity recognition using CNN. The following sections provide a small guide on how to install this CLI application on a sensor board and control it through the serial connection from TeraTerm.

3.1. Setting up the console

Once the sensor board is programmed with the binary of the project, the next step is to set up the serial connection of the board with the PC through TeraTerm. To do so, start TeraTerm, select the proper connection, featuring the [USB Serial Device]. For the screenshot below this is COM5 but it could vary for different users.

FP-AI-MONITOR2 teraterm new connection.svg

Set the Terminal parameters:

FP-AI-MONITOR2 teraterm terminal setup.svg

Restart the board by pressing the RESET button. The following welcome screen is displayed on the terminal.

FP-AI-MONITOR2 Console Welcome Message

From this point, start entering the commands directly or type help to get the list of available commands along with their usage guidelines.

3.2. Configuring the sensors

Through the CLI interface, a user can configure the supported sensors for sensing and condition monitoring applications. The list of all the supported sensors can be displayed on the CLI console by entering the command sensor_info. This command prints the list of the supported sensors along with their ids as shown in the image below. The user can configure these sensors using these ids. The configurable options for these sensors include:

  • enable: to activate or deactivate the sensor,
  • ODR: to set the output data rate of the sensor from the list of available options, and
  • FS: to set the full-scale range from the list of available options.

The current value of any of the parameters for a given sensor can be printed using the command,

$ sensor_get <sensor_id> <param>

or all the information about the sensor can be printed using the command:

$ sensor_get <sensor_id> all

Similarly, the values for any of the available configurable parameters can be set through the command:

$ sensor_set <sensor_id> <param> <val>

The snippet below shows the complete example of getting and setting these values along with old and changed values.

$ sensor_info
imp34dt05  ID=0 , type=MIC
iis2iclx   ID=1 , type=ACC
stts22h    ID=2 , type=TEMP
ilps22qs   ID=3 , type=PRESS
iis2dlpc   ID=4 , type=ACC
imp23absu  ID=5 , type=MIC
iis2mdc    ID=6 , type=MAG
ism330dhcx ID=7 , type=ACC
ism330dhcx ID=8 , type=GYRO
ism330dhcx ID=9 , type=MLC
iis3dwb    ID=10, type=ACC
-------
11 sensors supported

$ sensor_get 10 all
enable = false
nominal ODR = 26667.00 Hz, latest measured ODR = 0.00 Hz
Availabe ODRs:
26667.00 Hz
fullScale = 16.00 g
Available fullScales:
2.00 g
4.00 g
8.00 g
16.00 g

$ sensor_set 10 enable 1
sensor 10: enable

$ sensor_set 10 FS 4
sensor FS: 4.00

$ sensor_get 10 all
enable = true
nominal ODR = 26667.00 Hz, latest measured ODR = 0.00 Hz
Availabe ODRs:
26667.00 Hz
fullScale = 4.00 g
Available fullScales:
2.00 g
4.00 g
8.00 g
16.00 g

4. Inertial data classification with STM32Cube.AI

The CLI application comes with a prebuilt Human Activity Recognition model. This functionality is started by typing the command:

$ start har

Note that the provided HAR model is built with a dataset created using the IHM330DHCX_ACC sensor with ODR = 26, and FS = 4. To achieve the best performance, the user must set these parameters to the sensor configuration using the sensor_set command as provided in the Command Summary table. Running the $ start har command starts doing the inference on the accelerometer data and predicts the performed activity along with the confidence. The supported activities are:

  • Stationary,
  • Walking,
  • Jogging, and
  • Biking.

The following figure is a screenshot of the normal working session of the har command in the CLI application.

FP-AI-MONITOR2 har use case.png

5. Anomaly detection with NanoEdge™ AI library

FP-AI-MONITOR2 includes a pre-integrated stub which is easily replaced by an AI condition monitoring library generated and provided by NanoEdge™ AI Studio. This stub simulates the NanoEdge™ AI-related functionalities, such as running learning and detection phases on the edge.

The learning phase is started by issuing a command $ start neai_learn from the CLI console or by long-pressing the [USR] button. The learning process is reported either by slowly blinking the green LED light on STEVAL-STWINBX1 or in the CLI as shown below:

$ NanoEdge AI: learn
CTRL:! This is a stubbed version, please install the NanoEdge AI library!
{"signal": 1, "status": "need more signals"},
{"signal": 2, "status": "need more signals"},
:
:
{"signal": 10, "status": success}
{"signal": 11, "status": success}
:
:
End of execution phase

The CLI shows that the learning is being performed and at every signal learned. The NanoEdge AI library requires to learn for at least ten samples, so for all the samples until ninth sample a status message saying 'need more signals' is printed along with the signal id. Once, ten signals are learned the status of 'success' is printed. The learning can be stopped by pressing the ESC key on the keyboard or simply by pressing the [USR] button.

Similarly, the user starts the condition monitoring process by issuing the command $ start neai_detect. This starts the inference phase. The anomaly detect phase checks the similarity of the presented signal with the learned normal signals. If the similarity is less than the set threshold default: 90%, a message is printed in the CLI showing the occurrence of an anomaly along with the similarity of the anomaly signal. The process is stopped by pressing the ESC key on the keyboard or pressing the [USR] button. This behavior is shown in the snippet below:

$ start neai_detect
NanoEdgeAI: starting detect phase...

$ NanoEdge AI: detect
CTRL: ! This is a stubbed version, please install NanoEdge AI library !
{"signal": 1, "similarity": 0, "status": anomaly},
{"signal": 2, "similarity": 1, "status": anomaly},
{"signal": 3, "similarity": 2, "status": anomaly},
:
:
{"signal": 90, "similarity": 89, "status": anomaly},
{"signal": 91, "similarity": 90, "status": anomaly},
{"signal": 102, "similarity": 0, "status": anomaly},
{"signal": 103, "similarity": 1, "status": anomaly},
{"signal": 104, "similarity": 2, "status": anomaly},
End of execution phase

Other than CLI, the status is also presented using the LED lights on the STEVAL-STWINBX1. Fast blinking green LED light shows the detection is in progress. Whenever an anomaly is detected, the orange LED light is blinked twice to report an anomaly. If not enough signals (at least 10) are learned, a message saying "need more signals" with a similarity value equals to 0 appears.

NOTE : This behavior is simulated using a STUB library where the similarity starts from 0 when the detection phase is started and increments with the signal count. Once the similarity is reached to 100 it resets to 0. One can see that the anomalies are not reported when similarity is between 90 and 100.

Info white.png Information
Note : The message CTRL:! This is a stubbed version, please install the NanoEdge AI library! shows that the library embedded in the function pack is just a stub and a real library is not present. This message is replaced by a new message saying CTRL:! Powered by NanoEdge AI Library! once a real library is embedded.

5.1. Additional parameters in condition monitoring

For user convenience, the CLI application also provides handy options to easily fine-tune the inference and learning processes. The list of all the configurable variables is available by issuing the following command:

$ neai_get all
signals     = 0
sensitivity = 1.00
threshold   = 90
timer       = 0 ms
sensor      = 7

Each of the these parameters is configurable using the neai_set <param> <val> command.

This section provides information on how to use these parameters to control the learning and detection phase. By setting the "signals" and "timer" parameters, the user can control how many signals or for how long the learning and detection is performed (if both parameters are set the learning or detection phase stops whenever the first condition is met). For example, to learn 10 signals, the user issues this command, before starting the learning phase as shown below.

$ neai_set signals 10
signals set to 10

$ start neai_learn
NanoEdgeAI: starting learn phase...

$ NanoEdge AI: learn
CTRL: ! This is a stubbed version, please install NanoEdge AI library !
{"signal": 1, "status": "need more signals"},
{"signal": 2, "status": "need more signals"},
...
{"signal": 9, "status": "need more signals"},
{"signal": 10, "status": "success"},
End of execution phase

If both of these parameters are set to "0" (default value), the learning and detection phases run indefinitely.

The threshold parameter is used to report any anomalies. For any signal which has similarities below the threshold value, an anomaly is reported. The default threshold value used in the CLI application is 90. Users can change this value by using neai_set threshold <val> command.

Finally, the sensitivity parameter is used as an emphasis parameter. The default value is set to 1. Increasing this sensitivity means that the signal matching is to be performed more strictly, reducing it relaxes the similarity calculation process, meaning resulting in higher matching values.

Info white.png Information
Note: For the best performance, the user must expose all the normal conditions to the sensor-board during the learning and library generation process, for example in the case of motor monitoring, the required speeds and ramps that need to be monitored must be exposed.

For further details on how NanoEdge™ AI libraries work users are invited to read the detailed documentation of NanoEdge™ AI Studio.

5.1. n-class classification with NanoEdge™ AI

This section provides an overview of the classification application provided in FP-AI-MONITOR2 based on the NanoEdge™ AI classification library. FP-AI-MONITOR2 includes a pre-integrated stub which is easily replaced by an AI classification library generated using NanoEdge™ AI Studio. This stub simulates the NanoEdge™ AI-classification-related functionality, such as running the classification by simply iterating between two classes for ten consecutive signals on the edge.

Unlike the anomaly detection library, the classification library from the NanoEdge™ AI Studio comes with static knowledge of the data and does not require any learning on the device. This library contains the functions based on the provided sample data to best classify one class from another and rightfully assign a label to it when performing the detection on the edge. The classification application powered by NanoEdge™ AI can be simply started by issuing a command $ start neai_class as shown in the snippet below.

 
$ start neai_class
NanoEdgeAI: starting classification phase...

$ CTRL: ! This is a stubbed version, please install the NanoEdge AI library!
NanoEdge AI: classification
{"signal": 1, "class": Class1}
{"signal": 2, "class": Class1}
:
:
{"signal": 10, "class": Class1}
{"signal": 11, "class": Class2}
{"signal": 12, "class": Class2}
:
:
{"signal": 20, "class": Class2}
{"signal": 21, "class": Class1}
:
:
End of execution phase

The CLI shows that for the first ten samples the class is detected as "Class1" while for the upcoming ten samples "Class2" is detected as the current class. The classification phase can be stopped by pressing the ESC key on the keyboard or simply by pressing the [USR] button.


NOTE : This behavior is simulated using a STUB library where the classes are iterated by displaying ten consecutive labels for one class and then ten labels for the next class and so on.

Info white.png Information
Note : The message CTRL: ! This is a stubbed version, please install the NanoEdge AI library! shows that the library embedded in the function pack is just a stub and a real library is not present. Once a real library is embedded, this message is replaced by another message saying CTRL:!Powered by NanoEdge AI Library! .

5.2. Dual-mode application with STM32Cube.AI and NanoEdge™ AI

In addition to the three applications described in the sections above the FP-AI-MONITOR2 also provides an advanced execution phase which we call the dual application mode. This mode uses anomaly detection based on the NanoEdge™ AI library and performs classification using a prebuilt ANN model based on an analog microphone. The dual-mode works in a power saver configuration. A low power anomaly detection algorithm based on the NanoEdge™ AI library is always running based on vibration data and an ANN classification based on a high-frequency analog microphone pipeline is only triggered if an anomaly is detected. Other than this both applications are independent of each other. This is also worth mentioning that the dual-mode is created to work for a USB fan when the fan is running at the maximum speed and does not work very well when tested on other speeds. The working of the applications is very simple.

To start testing the dual application execution phase, the user first needs to train the anomaly detection library using the $ start neai_learn at the highest speeds of the fan. Once the normal conditions have been learned the user can start the dual application by issuing a simple command as $ start dual as shown in the below snippet:

FP-AI-MONITOR2 dual use case.png

Whenever there is an anomaly detected, meaning a signal with a similarity of less than 90%, the ultrasound-based classifier is started. Both applications run in asynchronous mode. The ultrasound-based classification model takes almost one second of data, then preprocesses it using the mel-frequency cepstral coefficients (MFCC), and then feeds it to a pre-trained neural network. It then prints the label of the class along with the confidence. The network is trained for four classes [ 'Off', 'Normal', 'Clogging', 'Friction' ] to detect fan in 'Off' condition, or running in 'Normal' condition at max speed or clogged and running in 'Clogging' condition at maximum speed or finally if there is friction being applied on the rotating axis it is labeled as 'Friction' class. As soon as the anomaly detection detects the class to be normal, the ultrasound-based ANN is suspended.

6. Generating the AI models

6.1. Anomaly detection with NanoEdge™ AI

The following section shows how to generate an anomaly detection library using NanoEdge™ AI Studio and install and test it on STEVAL-STWINBX1 using FP-AI-MONITOR2. The steps are provided with brief details in the following figure.

FP-AI-MONITOR1 neai lib generation flow.png

6.1.1. Data logging for normal and abnormal conditions

The details on how to acquire the data are provided in the section data logging using HSDatalog.

Info white.png Information
Note: For the best performances, the user must expose the solution to the normal and abnormal behaviors, that are expected in real use (few signals only). For detailed information, the users are invited to read the detailed documentation of the NanoEdge™ AI Studio here.

6.1.2. Data preparation for library generation

The data logged through the datalogger is in the binary format and is not user readable nor compliant with the NanoEdge™ AI Studio format as it is.

Using the provided Python™ utility scripts on the path /FP-AI-MONITOR2_V1.0.0/Utilities/AI-resources/NanoEdgeAi/.

  • The Jupyter Notebook NanoEdgeAI_Utilities.ipynb provides a complete example of data preparation for a three-speed fan library generation running in normal and clogged conditions. In addition, there is a HSD_2_NEAISegments.py script provided if the user wants to prepare segments for given data acquisition. This script is used by issuing the following command for data acquisition with ISM330DHCX_ACC sensor.
  • >> python HSD_2_NEAISegments.py ../Datasets/HSD_Logged_Data/Fan12CM/ISM330DHCX/normal/1000RPM/ command generates a file named as ISM330DHCX_Cartesiam_segments_0.csv using the default parameter set. The file is generated with segments of length 1024 and stride 1024 plus the first 512 samples are skipped from the file.
  • If multiple acquisitions are used to acquire the data for the normal and abnormal conditions once the files *_Cartesiam_segments_0.csv are generated for different acquisitions, all the files for normal can be combined in a single file, and all the files for the abnormal in another file. This way the user has to provide only one normal and abnormal file to Studio.

6.1.3. Library generation using NanoEdge™ AI Studio

Running the scripts in FP-AI-MONITOR2_V1.0.0/Utilities/AI_Resources/NanoEdgeAi/NanoEdgeAI_Utilities.ipynb generates the normal_WL1024_segments.csv and clogged_WL1024_segments.csv files in FP-AI-MONITOR2_V1.0.0/Utilities/AI_Resources/Datasets/HSD-Logged_Data/Fan12CM/ISM330DHCX/. This section describes how to generate the libraries using these normal and abnormal files.

The NanoEdge™ AI Studio can generate libraries for four types namely:

  • Anomaly Detection
  • 1-Class Classification
  • n-Class Classification
  • Extrapolation.

To generate the anomaly detection library the first step is to create the project by clicking on the button for AD as shown in the figure below. The text shows the information on what Anomaly Detection is good for, and the project can be created by clicking on the CREATE NEW PROJECT button.

FP-AI-MONITOR2 NanoEdge DA .png

The process to generate the anomaly detection library consists of seven steps as described in the figure below:

FP-AI-MONITOR2 NanoEdge project settings.png
  1. Project Settings
    • Choose a project name and description.
    • Hardware Configurations
      • Choosing the target STM32 microcontroller type: select STM32U5 from the list provided in the drop-down menu under Target.
      • Maximum amount of RAM to be allocated for the library: Usually, a few Kbytes is enough (but it depends on the data frame length used in the process of data preparation, 32 Kbytes is a good starting point).
      • Putting a limit or no limits for the Maximum Flash budget
      • Sensor type: select 3-axis accelerometer from the list in the drop-down under Sensor type.
    • Click on SAVE & NEXT
  2. Providing the sample contextual data for normal segments to adjust and gauge the performance of the chosen model. Two options are available:
    • Provide directly an acquisition directory generated from the HSDatalog, (with all the *****.dat and DeviceConfig.json files unchanged), or
    • Provide the normal_WL1024_segments.csv generated using Jupyter notebook,
  3. Providing the sample contextual data for abnormal segments to adjust and gauge the performance of the chosen model. Two options are available:
    • Provide directly an acquisition directory generated from the HSDatalog, (with all the *****.dat and DeviceConfig.json files unchanged), or
    • Provide the clogged_WL1024_segments.csv generated using Jupyter notebook,
  4. Benchmark the available models and choose the one that complies with the requirements and provides the best performance. At the end of the process, the best library is selected for the setup under experimentation. At this stage, an indication of the minimum number of samples to learn is also provided. To get stable results user must run neai_learn for at least this many signals.
  5. Emulator can optionally be used to test this specific NanoEdge AI Library directly inside the Studio.
  6. Validating the model for learning and testing through the provided emulator which emulates the behavior of the library on the STM32 target.
  7. The final step is to compile and download the libraries. In this process, the flag "Float abi" has to be checked for using libraries with hardware FPU. All the other flags can be left to the default state.
Info white.png Information
For using the library with μKeil also check -fshort-wchar in addition to Float abi

Detailed documentation on the NanoEdge™ AI Studio.

6.2. n-class classification with NanoEdge™ AI

The following describes how to generate the NanoEdge™ AI-based classification library and download it. The figure below shows a full flow of generating the library, integrating and installing it with the firmware, and testing it on the sensor-tile to classify different conditions.

FP-AI-MONITOR1 neai class lib generation flow.png

6.2.1. Data logging for different conditions

The details on how to log the data are provided in the section Datalogging using HSDatalog. Using these steps the user needs to a separate acquisitions for each of the conditions/classes the user wants to monitor. For the simplicity purposes FP-AI-MONITOR2 provides the sample data for a USB fan in four different conditions namely [ Off, Normal, Clogging, Friction]. This data is measured using ISM330DHCX and IMP23ABSU sensors and can be found in FP-AI-MONITOR2_V1.0.0/Utilities/AI_Resources/Datasets/HSD_Logged_Data/Fan12CM/ISM330DHCX+IMP23ABSU directory. For the configurations we used ACC subsensor of ISM330DHCX running at ODR = 1666 samples/sec and FS = 4G, and IMP23ABSU running at ODR = 192,000 samples/sec.

6.2.2. Data preparation for n-class classification with NanoEdge™ AI Studio

The data logged through the datalogger is in the binary format and is not user readable nor compliant with the NanoEdge™ AI Studio format as it is.

To convert this data to a useful form, for the ease of the users we provided Python™ utilities to prepare this data to be ready to generate the n-class classification libraries using NanoEdge™ AI Studio. These scripts are provided in the form of a Jupyter Notebook and can be found in /FP-AI-MONITOR2_V1.0.0/Utilities/AI-resources/Training Scripts/Anomaly Classification/NanoEdgeAI_ACC/DataPreparation.ipynb.

Running all the sections of this notebook generates the NanoEdge™ AI segments for all the acquisitions in the datalog folders which can be inputted to the NanoEdge™ AI Studio in the next step.

6.2.3. Library generation using NanoEdge™ AI Studio

Running the scripts in Jupyter Notebook generates the ISM330DHCX_Cartesiam_segments_0.csv csv files in each of the four datalog folders. This section describes how to use these files to generate the n-class classification library with NanoEdge™ AI Studio.

To generate the classification library the first step is to create the project by clicking on the button for nC. This modifies the display and shows what n-Class Classification libraries are good for and how it works. Create a new project by clicking on the CREATE NEW PROJECT button.

FP-AI-MONITOR2-nclass-sel.png

The process to generate the anomaly classification library consists of six steps as described in the figure below:

FP-AI-MONITOR2-nclass.png
  1. Project Settings
    • Choose a project name and description.
    • Hardware Configurations
      • Choosing the target STM32 microcontroller type: select STM32U5 from the list provided in the drop-down menu under Target.
      • Maximum amount of RAM to be allocated for the library: Usually, a few Kbytes is enough (but it depends on the data frame length used in the process of data preparation, 32 Kbytes is a good starting point).
      • Putting a limit or no limits for the Maximum Flash budget
      • Sensor type: select 3-axis accelerometer from the list in the drop-down under Sensor type.
    • Click on SAVE & NEXT
  2. Providing the sample data for all four classes. Two options are available:
    • Provide directly an acquisition directory generated from the HSDatalog, (with all the *****.dat and DeviceConfig.json files unchanged), select ISM330DHCX>ACC from the sensor list and enter 1024 in the signal length field. Press CONTINUE button and then IMPORT button. Or
    • Provide the ISM330DHCX_Cartesiam_segments_0.csv generated using Jupyter notebook, directly
    NOTE: Assign a class label to the imported data in the Name field once the data is imported. This label is used to differentiate the classes and is used in the emulation to show the predicted class.
    • Repeat the process for all four classes.
  3. Benchmark the available models and choose the one that complies with the requirements and provides the best performance.
  4. Emulator can optionally be used to test this specific NanoEdge AI Library directly inside the Studio.
  5. Validating the model performance through the provided emulator which emulates the behavior of the library on the STM32 target.
  6. The final step is to compile and download the libraries. As in FP-AI-MONITOR2, we support multiple NanoEdge™ AI libraries, this step requires a few precise settings to work with FP-AI-MONITOR2:
    • Check the Multi-library check-box and provide ncc in the suffix name field. (ncc = n-Class Classification)
    • Check the "Float abi" flag for using libraries with hardware FPU. All the other flags can be left to the default state.
Info white.png Information
For using the library with μKeil also check -fshort-wchar in addition to Float abi

Detailed documentation on the NanoEdge™ AI Studio.

6.3. X-CUBE-AI models

This section explains how to generate the code for a pre-trained AI models using STM32 X-CUBE-AI. As the FP-AI-MONITOR2 runs two pre-trained AI models namely, USC and HAR, for the simplification and optimization purposes, the code is generated for both pre-trained models at the same time. We can either generate the code for the combination of har_IGN.h5 and usc_4_class.tflite or har_svc.onnx and usc_4_class.tflite. These pre-trained models are available in FP-AI-MONITOR2_V1.0.0/Utilities/AI_Resources/models directory. As the package already contains the code for the HAR_SVC + USC combination, in the section below a step-by-step process is provided for the code generation for the HAR_IGN and USC combination.

Step1 : Open the STM32CubeMX and click on the ACCESS TO BOARD SELECTOR button as shown in the image below.

FP AI MONITOR2 step 1 start new project.png

Step2 : Create a new project for STEVAL-STWINBX1:

  1. Confirm the board selector tab is selected,
  2. Search for the right board, and in our case it is the STEVAL-STWINBX1, by typing the name in the search bar,
  3. Select the board by clicking on either the board image or the name of the board,
  4. Start Project, and
  5. Chose NO for the Peripheral initialization option as this is not required for our purpose.
FP AI MONITOR2 step 2 1 board select.png

and check "without TrustZone activated" option

FP AI MONITOR2 step 2 2 trust zone.png

Step3 : Configuring hardware

  1. Click on the connectivity option in the left menu
  2. Select USART2
  3. Enable the "Asynchronous mode" by selecting it in the drop-down menu.
  4. check PD5 and PD6 pins are selected
FP AI MONITOR2 step 3 1 setup usart.png
  1. Click on the Power end Thermal option in the left menu
  2. Select PWR
  3. Enable the "SMPS" by selecting it in the drop-down menu.
FP AI MONITOR2 step 3 2 setup smps.png
  1. Click on the System Core option in the left menu
  2. Select ICACHE
  3. Enable the "2-ways set associative cache" by selecting it in the drop-down menu.
FP AI MONITOR2 step 3 3 setup cache.png

Step4 : Add the X-CUBE-AI in the software packs for the project

  1. Click on the Software Packs, and select the Select Components option
  2. Click on the STMicroelectronics X-CUBE-AI. Use Version 7.3.0 as preference but any version from 7.3.0 or later can be used,
  3. Click on checkbox in front of Core to add the X-CUBE-AI code in the software stack.
  4. Expand the Device Application menu and from the drop-down menu under selection column select SystemPerformance.
  5. Click OK button to finish the addition of the X-CUBE-AI in the project.
FP AI MONITOR2 step 4 select comp.png

Step 5 : Platform Settings

  1. Click on Software Packs,
  2. Choose STMicroelectronics.X-CUBE-AI,
  3. Confirm clock and peripherals settings for best perfomance
FP AI MONITOR2 step 5 1 platform settings.png
  1. Select the the Platform Settings tab,
  2. Select USART: Asynchronous option for the COM Port,
  3. Select USART2 in "Found Solutions" drop-down.
FP AI MONITOR2 step 5 2 platform settings.png

Step6 : Adding the networks for code generation This step require the users to add two networks. HAR and USC. This can be done using following steps

  • Adding HAR model
    1. Click on the add network button,
    2. In the first text field provide the text har_network as the network name. This is used to differentiate the name space of the model when code for multiple models is generated at once.
    3. From drop down select the type of the network. X-CUBE-AI allows the user to generate code for the Keras, ONNX, and TFLite models. For using har_IGN.h5 file select the Keras option.
    4. Click on the Browse button to select the model.
    5. The har_IGN.h5 is located under FP-AI-MONITOR2_V1.0.0/Utilities/AI_Resources/models . Select the model and click Select.
FP AI MONITOR2 step 6 1 har.png
  • Adding USC model
    1. Click on the add network button,
    2. In the first text field provide the text usc_network as the network name. This is used to differentiate the name space of the model when code for multiple models is generated at once.
    3. From drop down select the type of the network as TFLite model.
    4. Click on the Browse button to select the model.
    5. The usc_4_class.tflite is located under FP-AI-MONITOR2_V1.0.0/Utilities/AI_Resources/models . Select the model and click OK.
FP AI MONITOR2 step 6 2 USC.png

Step7 : Generating the C-code

  1. Go to Project Manager
  2. Assign a "Project Name", in the figure below it is AI-Code-Gen
  3. Choose a Project Location, in the figure below it is C:/Temp/
  4. Under Toolchain/IDE option select STM32CubeIDE (or your required toolchain), and
  5. Click on the GENERATE CODE button. A progress bar starts and shows progress across the different code generation steps.
  6. Upon completion of the code generation process the user sees a dialog as in the figure below. This shows completion of the code generation. Click on the Open Folder button to open the project with the generated code.
  7. The files present for the network model that have to be replaced in the provided project are located in the following directory: FP-AI-MONITOR2_V2.1_AI-Code-Gen/X-CUBE-AI/App/ as shown in the figure below.
FP AI MONITOR2 step 7 generate.png

The next section shows how these files are used to replace the existing model embedded in the FP-AI-MONITOR2 software step-by-step and install it on the sensor board.

7. Updating the AI models

7.1. Anomaly detection with NanoEdge™ AI

Once the libraries are generated and downloaded from NanoEdge™ AI Studio, the next step is to link these libraries to FP-AI-MONITOR2 and run them on the STWIN.Box. The FP-AI-MONITOR2, comes with the library stubs in the place of the actual libraries generated by NanoEdge™ AI Studio. This is done to simplify the linking of the generated libraries. In order to link the actual libraries, the user needs to copy the generated libraries and replace the existing stub/dummy libraries and header files NanoEdgeAI.h, and libneai.a files present in the folders Inc, and lib, respectively. The relative paths of these folders are /FP-AI-MONITOR2_V1.0.0/Middlewares/ST/NanoEdge_AI_Library/ .

Warning white.png Warning
If the project is being built using Keil IDE, the file libneai.a is to renamed as libneai.lib, before copying.

Once these files are copied, the project must be rebuilt and programmed on the sensor board to link the libraries correctly. For this, the user must open the project file in STM32CubeIDE located in the /FP-AI-MONITOR2_V1.0.0/Projects/STWIN.box/Applications/FP-AI-MONITOR2/STM32CubeIDE/ folder and double click .project file .

To build and install the project click on the play button and wait for the successful download message as shown in the section Build and Install Project.

Once the sensor board is successfully programmed, the welcome message appears in the CLI (Tera Term terminal). If the message does not appear try to reset the board by pressing the RESET button.

Info white.png Information
NOTE: To be absolutely sure that a new software is installed in STEVAL-STWINBX1, user can issue command info . This shows the compile time and the user can confirm if the sensor board is programmed with a new or old binary code.

7.1.1. Testing the anomaly detection with NanoEdge™ AI

Once the STWIN is programmed with the FW containing a valid library, the condition monitoring libraries are ready to be tested on the sensor board. The learning and detection commands can be issued and now the user does not see the warning of the stub presence.

To achieve the best performance, the user must perform the learning using the same sensor configurations which were used during the contextual data acquisition. For example in the snippet below users can see commands to configure ISM330DHCX sensor with sensor_id 2 with following parameters:

  • enable = 1
  • ODR = 1666,
  • FS = 4.
$ sensor_set 2 enable 1
sensor 2: enable

$ sensor_set 2 ODR 1666
nominal ODR = 1666.00 Hz, latest measured ODR = 0.00 Hz

$ sensor_set 2 FS 4
sensor FS: 4.00

Also, to get stable results in the neai_detect phase the user must perform learning for all the normal conditions to get stable results before starting the detection. In the case of running the detection phase without performing the learn first, erratic results are displayed. An indication of minimum signals to be used for learning is provided when a library is generated in the NanoEdge™ AI Studio in Step 4 of library generation.

Info white.png Information
Note: The NanoEdge™ AI library comes with an incremental learning capability, so the learning and detection phases can be toggled if the user does not get good results or if new normal states are to be added. The incremental learning capability means that the new normal states are learned without forgetting the previous learning.

7.2. n-class classification with NanoEdge™ AI

The FP-AI-MONITOR2, comes with the library stubs in the place of the actual libraries generated by NanoEdge™ AI Studio. This is done to simplify the linking of the generated libraries. In n-Class classification library the features for the classes are learned and required in the form of the knowledge.h file in addition to .h and .a files. So unlike the anomaly detection library, in order to link the classification libraries, the user needs to copy two header files NanoEdgeAI_ncc.h and knowledge_ncc.h, and the library libneai_ncc.a file to replace the already present files in the folders Inc, and lib, respectively. The relative paths of these folders are /FP-AI-MONITOR2_V1.0.0/Middlewares/ST/NanoEdge_AI_Library/.

Warning white.png Warning
If the project is being built using Keil IDE, the file libneai_ncc.a is to renamed as libneai_ncc.lib, before copying.

In addition to this the user is required to add the labels of the classes to expect during classification process by updating the sNccClassLabels array in FP-AI-MONITOR2_prj/Application/Src/AppController.c file:

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms that can be found here for the component: Application.
/**
 * Specifies the label for the two classes of the NEIA Class demo.
 */
static const char* sNccClassLabels[] = {
  "Unknown",
  "Off",
  "Normal",
  "Clogging",
  "Friction"
};

Note that the first label is "Unknown" and it is required to be left as it is. The real labels for the classification come after this. The order of the labels [Off, Normal, Clogging, Friction] has to be the same as was used to provide the data in the process of library generation in NanoEdge™ AI Studio.

Info white.png Information
The order of the labels for the n-Class Classification library can be found in the NanoEdgeAI_ncc.h file. The users can simply copy and paste this array.

After this step, the project must be rebuilt and programmed on the sensor board to link the libraries correctly. To build and install the project click on the play button and wait for the successful download message as shown in the section Build and Install Project.

Once the sensor board is successfully programmed, the welcome message appears in the CLI (Tera Term terminal). If the message does not appear try to reset the board by pressing the RESET button.

7.2.1. Testing the n-class classification with NanoEdge™ AI

Once the STWIN.Box is programmed with the FW containing a valid n-class classification library, it is ready to be tested.

To achieve the best performance, the user must perform the datalogging and testing in the same sensor configurations. For example in the snippet below users can see commands to configure ISM330DHCX sensor with sensor_id 2 with following parameters:

  • enable = 1
  • ODR = 1666,
  • FS = 4.
$ sensor_set 2 enable 1
sensor 2: enable

$ sensor_set 2 ODR 1666
nominal ODR = 1666.00 Hz, latest measured ODR = 0.00 Hz

$ sensor_set 2 FS 4
sensor FS: 4.00

After the configurations of the sensor are completed, the user can start the NEAI classification by issuing the command, $ start neai_class.

7.3. X-CUBE-AI models

The CLI example has two prebuilt models integrated with it. One for HAR and another for the USC. Following the steps below the user can update these models. As described in the code generation process, for sake of simplicity, the code for both models is generated at once. In this example the provided code for the combination of SVC and USC models(USC_4_Class_+_SVC_4_Class) is replaced with the prebuilt and converted C code from the HAR (CNN) and USC CNN models provided in the /FP-AI-MONITOR2_V1.0.0/Utilities/AI_Resources/models/USC_4_Class_+_IGN_4_Class/ folder.

To update the model, the user must copy and replace the following files in the /FP-AI-MONITOR2_V1.0.0/Projects/STWIN.box/Applications/FP-AI-MONITOR2/X-CUBE-AI/App/ folder:

  • app_x-cube-ai.c,
  • app_x-cube-ai.h,
  • har_network.c,
  • har_network.h,
  • har_network_config.h,
  • har_network_data.h,
  • har_network_data.c,
  • har_network_generate_report.txt,
  • usc_network.c,
  • usc_network.h,
  • usc_network_config.h,
  • usc_network_data.h,
  • usc_network_data.c, and
  • usc_network_generate_report.txt.

After the files are copied, the user must open the project with the CubeIDE. To do so, go to the /FP-AI-MONITOR2_V1.0.0/Projects/STWIN.box/Applications/FP-AI-MONITOR2/STM32CubeIDE/ folder and double click .project file. Once the project is opened, go to FP-AI-MONITOR2_V1.0.0/Projects/STWIN.box/Application/FP-AI-MONITOR2/X-CUBE-AI/App/app_x-cube-ai.c file and comment the following lines of the code as shown below:

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms that can be found here for the component: Application.
#include "app_x-cube-ai.h"
//#include "bsp_ai.h"
//#include "aiSystemPerformance.h"
#include "ai_datatypes_defines.h"

/* USER CODE BEGIN includes */
/* USER CODE END includes */

/* IO buffers ----------------------------------------------------------------*/

//DEF_DATA_IN
//
//DEF_DATA_OUT
/* Activations buffers -------------------------------------------------------*/

AI_ALIGNED(32)
static uint8_t pool0[AI_USC_NETWORK_DATA_ACTIVATION_1_SIZE];

ai_handle data_activations0[] = {pool0};
ai_handle data_activations1[] = {pool0};

/* Entry points --------------------------------------------------------------*/

//void MX_X_CUBE_AI_Init(void)
//{
//    MX_UARTx_Init();
//    aiSystemPerformanceInit();
//    /* USER CODE BEGIN 5 */
//    /* USER CODE END 5 */
//}
//
//void MX_X_CUBE_AI_Process(void)
//{
//    aiSystemPerformanceProcess();
//    HAL_Delay(1000); /* delay 1s */
//    /* USER CODE BEGIN 6 */
//    /* USER CODE END 6 */
//}

7.3.1. Building and installing the project

Then build and install the project on the STWIN sensor board by pressing the play button as shown in the figure below.

FP AI MONITOR2 build install.png

A message saying Download verified successfully indicates the new firmware is programmed in the sensor board.

Info white.png Information
NOTE: To be absolutely sure that a new software is installed in STEVAL-STWINBX1, user can issue command info . This shows the compile time and the user can confirm if the sensor board is programmed with new or old binary.

8. FP-AI-MONITOR2 Utilities

For the ease of the users FP-AI-MONITOR2 comes with a set of utilities to record and prepare the datasets, and generate the AI models for different supported AI applications. These utilities are in the FP-AI-MONITOR2_V1.0.0/Utilities/ directory and contain two sub-directories,

  • AI_Resources (all the Python resources related to AI), and
  • DataLog (binary and helper scripts for High-Speed Datalogger).

This following section briefly describes the contents of the AI_Resources folder.

8.1. AI_Resources

FP-AI-MONITOR2 comes equipped with four AI applications, and AI_Resources contains the Python™ scripts, the sample datasets, dataset placeholders, and the code to prepare these datasets for generating the AI models supported in this function pack.

In the AI_Resources directory, there are following subdirectories:

  • Dataset: Contains different datasets/holders for the datasets, used in the function pack
  • AST, a small subsample from an ST proprietary dataset for HAR.
  • HSD_Logged_Data, different datasets logged using High-speed Datalogger binary.
    • Fan12CM, Datasets logged on 12CM USB fan using different on-board sensors of STEVAL-STWINBX1.
    • HAR, Human activity recognition dataset acquired using the STEVAL-STWINBX1.
  • WISDM, a placeholder for downloading and placing the WISDM dataset for HAR.
  • models: Contains the pre-generated and trained models for HAR and USC along with their C-code
  • USC_4_Class_+_IGN_4_Class contains a combination of CNN for HAR and CNN for USC.
  • USC_4_Class_+_SVC_4_Class contains a combination of SVC for HAR and CNN for USC.
  • NanoEdgeAi: Contains the helper scripts to prepare the data for the NanoEdge™ AI Studio from the HSDatalogs to generate the anomaly detection libraries.
  • signal_processing_lib: Contains the code for various signal processing modules (there is equivalent embedded code available for all the modules in the function pack)
  • Training Scripts: Contains the Python scripts for HAR and AnomalyClassification.
  • HAR subdirectory at the path FP-AI-MONITOR2_V1.0.0/Utilities/AI_Resources/Training Scripts/HAR/ contains three Jupyter notebooks:
    • HAR_with_CNN.ipynb (a complete step-by-step code to build a sample HAR model based on Convolutional Neural Networks),
    • HAR_with_SVC.ipynb (a complete step-by-step code to build a sample HAR model based on Support Vector Machine Classifier), and
    • HAR_with_NEAI.ipynb (a complete step-by-step code to build NanoEdge™ AI Studio compliant files for all activities to generate n-Class classification libraries).
  • AnomalyClassification contains two subdirectories for two different usecases to perform anomaly classification.
    • Ultrasound directory contains the Python scripts to prepare the dataset and create a CNN based model for the anomaly classification using the ultrasound data logged through IMP23ABSU sensor (an analog microphone).
    • NanoEdgeAI_ACC contains the python code to prepare the .csv files for ACC data for different conditions on the fan for the anomaly classification library generation from NanoEdge™ AI Studio.
Info white.png Information
NOTE: The examples provided here are for the USB Fan and HAR models, but it is worth mentioning that using this pathway the readers can build any AI application or use case of their choosing. Also, the preprocessing chain can be changed to match the user's needs and requirements, as a full set of preprocessing modules is available along with equivalent C-code implementation to facilitate the users.

9. Data collection

The data collection functionality is out of the scope of this function pack, however, to simplify this for the users this section provides the step-by-step guide to logging the data on STEVAL-STWINBX1 using the high-speed data logger.

Step 1: Program the STEVAL-STWINBX1 with the HSDatalog FW

In the scope of this function pack and article, the STEVAL-STWINBX1 can be programmed with HSDatalog firmware using the binary provided in the function pack. To simplify the task of the users and to allow them the possibility to perform a data log, the precompiled HSDatalog.bin file for FP-SNS-DATALOG2 is provided in the Utilities directory, which is located under path /FP-AI-MONITOR2_V1.0.0/Utilities/Datalog/. The sensor tile can be programmed by simply following the drag-and-drop action shown in section 2.3.

Step 2: Place a DeviceConfig.json file on the SD card

The next step is to copy a DeviceConfig.json on the SD card. This file contains the sensors configurations to be used for the data logging. The users can simply use one of the provided sample .json files in the package in FP-AI-MONITOR2_V1.0.0/Utilities/Datalog/STWIN_config_examples/ directory.

Note : The configuration files are to be precisely named DeviceConfig.json or the process does not work.

Step 3: Insert the SD card into the STWIN board

Insert an SD card in the STEVAL-STWINBX1.

Note : For data logging using the high speed datalogger user needs a FAT32-FS formatted microSDTM card.

Step 4: Reset the board

Reset the board. Orange LED blinks once per second. The custom sensor configurations provided in DeviceConfig.json are loaded from the file.

Step 5: Start the data log

Press the [USR] button to start data acquisition on the SD card. The orange LED turns off and the green LED starts blinking to signal sensor data is being written into the SD card.

Step 6: Stop the data logging

Press the [USR] button again to stop data acquisition. Do not unplug the SD card, turn the board off or perform a [RESET] before stopping the acquisition otherwise the data on the SD card are corrupted.

Step 7: Retrieve data from SD card

Remove the SD card and insert it into an appropriate SD card slot on the PC. The log files are stored in STWIN_### folders for every acquisition, where ### is a sequential number determined by the application to ensure log file names are unique. Each folder contains a file for each active sub-sensor called SensorName_subSensorName.dat containing raw sensor data coupled with timestamps, a DeviceConfig.json with specific information about the device configuration (confirm if the sensor configurations in the DeviceConfig.json are the ones you desired), necessary for correct data interpretation, and an AcquisitionInfo.json with information about the acquisition.

Info white.png Information
For details on how to use all the features of the provided HSDatalog.bin binary the users are invited to refer to the user manual of FP-SNS-DATALOG2.

9.1. DeviceConfig.json file

The DeviceConfig.json file contains the configurations of all the onboard sensors of STEVAL-STWINBX1 as JSON format. The object consists of three attributes deviceInfo, sensor, and tagConfig.

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms that can be found here for the component: Application.
{
    "UUIDAcquisition": "287cddd8-3f95-4449-9350-799d16296c2b",
    "JSONVersion": "1.1.0",
    "device": {
    "sensor": [ ],
    "tagConfig": { }
    }
}

deviceInfo identifies the device.

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms that can be found here for the component: Application.
{
    "UUIDAcquisition": "287cddd8-3f95-4449-9350-799d16296c2b",
    "JSONVersion": "1.1.0",
    "device": {
        "deviceInfo": {
            "serialNumber": "000900115652500420303153",
            "alias": "STWIN_001",
            "partNumber": "STEVAL-STWINBX1",
            "URL": "www.st.com\/stwin",
            "fwName": "FP-SNS-DATALOG2",
            "fwVersion": "1.2.0",
            "dataFileExt": ".dat",
            "dataFileFormat": "HSD_1.0.0",
            "nSensor": 9
    "sensor": [ ],
    "tagConfig": { }
    }
}

sensor is an array of attributes to describe all the sensors available on-board. Each sensor has a unique ID a name and sensorDescriptor and sensorStatus.

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms that can be found here for the component: Application.
"sensor": [
        {
            "id": 0,
            "name": "IIS3DWB",
            "sensorDescriptor": { },
            "sensorStatus": { }
        },
        {
            "id": 1,
            "name": "HTS221",
            "sensorDescriptor": { },
            "sensorStatus": { }
        },
        :
        :

sensorDescriptor describes the main information about the single sensors through the list of its subSensorDescriptor. Each element of the subSensorDescriptor describes the main information about the single sub-sensor, such as the name, data type, sensor type, odr and full scale available, samples per unit of time supported, and measurement unit.

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms that can be found here for the component: Application.
{
      "id": 0,
      "name": "IIS3DWB",
      "sensorDescriptor": {
      "subSensorDescriptor": [
              {
                    "id": 0,
                    "sensorType": "ACC",
                    "dimensions": 3,
                    "dimensionsLabel": [
                           "x",
                           "y",
                           "z"
                    ],
                    "unit": "g",
                    "dataType": "int16_t",
                     "FS": [
                            2,
                            4,
                            8,
                            16
                     ],
                     "ODR": [
                            26667
                      ],
                     "samplesPerTs": {
                             "min": 0,
                             "max": 1000,
                             "dataType": "int16_t"

sensorStatus describes the actual configuration of the related sensor through the list of its subSensorStatus. Each element of subSensorStatus describes the actual configuration of the single subsensor, meaning whether the sensor is active or not, the actual odr(output data rate), fs (full scale), etc.).

This snippet is provided AS IS, and by taking it, you agree to be bound to the license terms that can be found here for the component: Application.
"sensorStatus": {
       "subSensorStatus": [
               {
                      "ODR": 26667,
                      "ODRMeasured": 0,
                      "initialOffset": 0,
                      "FS": 16,
                      "sensitivity": 0.000488,
                      "isActive": false,
                      "samplesPerTs": 1000,
                      "usbDataPacketSize": 3000,
                      "sdWriteBufferSize": 43520,
                      "wifiDataPacketSize": 0,
                       "comChannelNumber": -1,
                       "ucfLoaded": false
                }
            ]
       }

For us the only important configurations are isActive, odr, and fs. For details readers are invited to refer to the user manual of FP-SNS-DATALOG2 package.

10. Documents and related resources