1. Introduction
OTA is a feature that allows to update Zigbee devices Over-The-Air. Typically, the OTA server offers/presents an upgrade binary, and an OTA client downloads it. The implementation of the OTA feature uses the Exegin OTA Cluster.
See the Getting started with Zigbee® on STM32WB Series Application note [1].
2. STM32WB OTA use case
Zigbee OTA requires at least two STM32WBxx boards running Zigbee protocol with specific applications:
- one board (Server) running ZigBee_Ota_Server application (ZbZclOtaServer cluster allocated)
- one or more boards (Clients) running ZigBee_Ota_Client application (ZbZclOtaClient cluster allocated)
First, the binary to download must be flashed on the “FREE” memory region on the Server side, by using STM32CubeProgrammer for example. In our use-case, it is flashed at the address 0x08030000.
Then, the server initiates an OTA provisioning process and clients may or not request it. Multiple clients can be updated at the same time.
The binary should be transferred and flashed on the “FREE” memory region of the client. In our case it will be flashed at the address 0x08030000.
OTA Server/Client model |
---|
During application update, the server transfers the binary to the client. Upon the reception of all the frames of the binary, the device will reboot.
The binary could be either for M4 application or for M0 coprocessor wireless binary.
2.1. Application update (M4)
The OTA verify that the downloaded binary is for M4 and check the integrity code: if it is OK, the OTA launch the new application firmware (here On/Off app).
Application update |
---|
2.2. Coprocessor wireless binary update (M0)
If the downloaded binary is for coprocessor M0, the OTA check the integrity code and reboot on FUS if it is OK. The wireless coprocessor install the secure binary and reboot on the OTA. The OTA is now ready to receive the new M4 firmware which should be always updated and flashed after an M0 update.
Coprocessor wireless binary update |
---|
3. OTA Upgrade statements/description/assumptions
The OTA upgrade is based on a specific file format composed of :
- OTA header
- OTA sub-elements (Upgrade image tag + associated binary firmware data)
OTA Upgrade Diagram |
---|
4. OTA Cluster APIs Functions
The following table lists some examples of APIs used with OTA cluster.
Function | Description |
---|---|
ZbZclOtaClientAlloc | Create new OTA client cluster |
ZbZclOtaServerAlloc | Create new OTA server cluster |
ZbZclOtaClientDiscover | Discover OTA server |
ZbZclOtaClientDiscoverForced | Set the OTA Server directly |
ZbZclOtaClientImageTransferResume | Resume an OTA upgrade transfer |
ZbZclOtaClientImageTransferStart | Initiate an OTA transfer |
5. Resuming a partial download
The download of the binary could be interrupted due to network issues or losing connection with the server or other reason. The application can resume the transfer depending on the reason of the interruption. If the OTA server turns off, the application waits until the reestablishment of the connection and resume the transfer by calling ZbZclOtaClientImageTransferResume. If the OTA client turns off, after receiving and saving a part of the firmware, the transfer can be resumed from the previous download using the FileOffset attribute.