Cellular hardware setup

Revision as of 12:32, 27 January 2022 by Registered User

Click here for Cellular overview

1. Introduction

This wiki article contains information to help users with their hardware setups.
X-CUBE-CELLULAR supports different types of hardware setups.
Some are based on a module that contains both an STM32 and modem while some others are based on two boards, an STM32 board associated with a separate modem board.
If the STM32 board has no STMod+ connector, use an ARDUINO® / STMod+ adaptor. This is the case for the B-L4S5I-IOT01A[1].
Separate STM32 and modem boards are sometimes available as one pack composed of two boards in the same blister. This is the case for the P-L496G-CELL02[2].
In case of issue, do not forget to check the ST-LINK firmware version and upgrade it if needed. Use for instance the STM32CubeProgrammer tool (STM32CubeProg[3]) for this purpose.
Depending on users PC's OS a USB driver could be needed.
Note when GM01Q-STMOD[4] is mentioned it could be replaced by GMS01Q-STMOD[5]
Note that all the hardware setup listed are not available for all the software version. See Release Note associated to the software release note to have the complete information.

2. Modem FW version

The modem factory FW version in user's HW may not be compliant any longer with the latest X-CUBECELLULAR version. The Cellular modem RN indicates which modem FW version must be used. The modem FW version must be checked in the serial terminal trace and updated if needed.

3. B-L462E-CELL1[6]

3.1. Boards and ST-LINK USB cable connections

B-L462E-CELL1

The red USB cable from the PC is used to power and interact with the STM32.

4. P-L496G-CELL02 [2]

4.1. Boards and ST-LINK USB cable connections

P-L496G-CELL02

The red USB cable from the PC is used to power and interact with the STM32.

5. B-U585I-IOT02A[7] + GM01Q-STMOD[4] or STEVAL-STMODLTE[8]

5.1. Boards and ST-LINK USB cable connections

Cellular_B-U585I-IOT02A + GM01Q-STMOD or STEVAL-STMODLTE

The red USB cable from the PC is used to power and interact with the STM32.

6. B-L4S5I-IOT01A[1] + X-NUCLEO-STMODA1[9] + GM01Q-STMOD[4] or STEVAL-STMODLTE[8]

6.1. Boards and ST-LINK USB cable connections

B-L4S5I-IOT01A + X-NUCLEO-STMODA1 + GM01Q-STMOD or STEVAL-STMODLTE

The red USB cable from the PC is used to power and interact with the STM32.

7. 32L496GDISCOVERY[10] + GM01Q-STMOD[4] or STEVAL-STMODLTE[8]

7.1. Boards and ST-LINK USB cable connections

32L496GDISCOVERY + GM01Q-STMOD or STEVAL-STMODLTE

The red USB cable from the PC is used to power and interact with the STM32.

8. STEVAL-STWINKT1B[11] + GM01Q-STMOD[4] or STEVAL-STMODLTE[8]

8.1. Boards and ST-LINK USB cable connections

STEVAL-STWINKT1 + GM01Q-STMOD or STEVAL-STMODLTE

The red USB cable (not provided) from the PC is used to interact with the STM32 through the STLINK-V3. This STLINK-V3 is provided in the blister.
A second USB cable (not provided) is needed to power the STEVAL-STWINKT1B[11] through its USB connector.

9. Previous X-CUBE-CELLULAR versions before V6.0.0

The former X-CUBE-CELLULAR versions support other hardware setups such as P-L496G-CELL01[12] (similar to P-L496G-CELL02[2] but with the UG96 Quectel 2G/3G modem), and B-L475E-IOT01A[13].
UG96 is no more used because, nowadays, LTE Cat M and NB-IoT networks are available and much more low-power friendly than 3G.
B-L475E-IOT01A[13] (also known as "IoT node V1") is replaced with B-L4S5I-IOT01A[1] (also known as "IoT node V1.5").

10. References