![]() |
Coming soon |
Click here for BLE overview
1. Introduction
The STM32CubeWB MCU Package[1] provides software components running on the STM32WB Series MCU.
For all examples provided with the package, the following integrated development environments are supported:
- STMicroelectronics integrated development environment for STM32 products (STM32CubeIDE)
- IAR Systems® IAR Embedded Workbench® for Arm® (EWARM)
- Keil® Microcontroller Development Kit (MDK-ARM)
The Firmware Package for the STM32WB series is also available on STM32CubeWB github[2].
2. STM32WB Bluetooth® LE Software Architecture
The STM32WB Bluetooth® Low Energy architecture separates the Bluetooth® Low Energy Profile and Application, running on the application Cortex-M4, from the Bluetooth® Low Energy real-time aspects residing in the Bluetooth® Low Energy peripheral.
The Bluetooth® Low Energy peripheral incorporates a Cortex-M0+ processor containing the Bluetooth® Low Energy STACK handling the link layer up to the Generic Attribute Profile and Generic Access Profile layers.
STM32WB BLE Architecture |
---|
Regarding the Bluetooth® LE Software Architecture more information is available on the Application Note Building wireless applications with STM32WB Series microcontrollers[3]
3. STM32WB Bluetooth® LE application
The following Bluetooth® LE applications are delivered as source code.
Application | Description | |
---|---|---|
Bluetooth® LE SIG | BLE_Beacon | Application advertising different types of beacon : ibeacon, eddystone (tlm, uuid, url) |
BLE_BloodPressure | Application supporting the Blood Pressure sensor as specified by the Bluetooth® SIG | |
BLE_HealthThermometer | Application supporting the Health Thermometer sensor as specified by the Bluetooth® SIG | |
BLE_HeartRate | Application supporting the Heart Rate sensor as specified by the Bluetooth® SIG | |
BLE_Hid | Application supporting the Human interface device services for mouse & keyboard as specified by the Bluetooth® SIG | |
BLE_Proximity | Application supporting the Find Me and Proximity services as specified by the Bluetooth® SIG | |
Bluetooth® LE ST Proprietary | BLE_AT_Server | AT Command Server |
BLE_CableReplacement | Cortex-M4 | |
BLE_DataThroughput | Cortex-M3 | |
BLE_Ota | Firmware Update Over The Air (FUOTA) | |
BLE_p2pServer | Cortex-M3 | |
BLE_p2pClient | Cortex-M3 | |
BLE_p2pRouter | Cortex-M3 | |
BLE_Peripheral_Lite | Cortex-M3 | |
RF & Flash Activities | Cortex-M3 | |
Transparent mode | Cortex-M3 | |
Bluetooth® LE Mesh | Mesh Lighting Proxy Relay Friend node | examples |
Mesh Lighting Low Power node | Cortex-M4 | |
Mesh Lighting Embedded Provisioner | Cortex-M3 |
4. Going further based on available application
- https://wiki.st.com/stm32mcu/wiki/STM32WB_-_Bluetooth%C2%AE_LE_Fast_FUOTA
- https://wiki.st.com/stm32mcu/wiki/STM32WB_-_Bluetooth%C2%AE_LE_Additional_Advertising
- https://wiki.st.com/stm32mcu/wiki/STM32WB_-_Bluetooth%C2%AE_LE_%26_Arduino
- https://wiki.st.com/stm32mcu/wiki/Sensor_Server_Measurement_on_Sensor_Client_Request
- https://wiki.st.com/stm32mcu/wiki/Vendor_Model_Demonstration