This article is describing how to allocate more Flash memory to the Cortex M7 of the STM32H747 Discovery board.
The STM32H747 microcontroller is a dual core Cortex M7 / Cortex M7 with 2 MB of Flash. By default half of the Flash is allocated to the Cortex M7 and the other half to the Cortex M4. With a neural network and using STM32Cube.AI to generate STM32 code, the weights are stored by default in internal Flash. It might be require to allocate more Flash to the Cortex M7 if the required size is above 1 MB (or on the contrary to the Cortex M4 depending on the selected core). This article show how to change the Flash allocation, the tutorial is showing how to allocate 1984 KB of Flash to the Cortex M7 and the rest of the Flash, 64 KB to the Cortex M4.
1. Prerequisites
1.1. Hardware
- STM32H747I-DISCO
- A Micro-USB to USB cables
1.2. Software
2. Modify the boot addresses
The Cortex M7 is booting by default at the address 0x08000000 whereas the Cortex M4 boot at the address 0x08100000. This should be modified:
- Connect the board to the PC thanks to the USB cable using the USB STLink connector
- Open the STM32CubeProgrammer tool and connect to the board.
- Click on OB (Option Bytes) to modify the BOOT_CM4_ADD0
- Modify the CM4 boot address bytes to 0x81F0000 address instead of 0x8100000. You simply have to modify the value from 0x810 to 8x1f.
The initial configuration is as below:
The final configuration shall be as below:
2.1. Generate the code with STM32Cube.AI
Generate the project for your model as usual with STM32Cube.AI. Do not use the one click validation feature from the UI, it will take the default memory allocation. Instead use the Project Manager. Make sure to select the application in the menu when selecting the X-CUBE-AI software package:
Then use the Generate Project feature (make sure to enter a name for your project as well as selecting your IDE).
2.2. Modify the linker scripts
Once the The linker script shall reflect the new memory allocation, the linker scripts shall be modified as follow. Make sure the full RAM of 512 KB is allocated stm32h747xi_flash_cm7.ld {{Snippet | category=AI | component=Application | snippet=
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 512K /* Memory is divided. Actual start is 0x24000000 and actual length is 512K */
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1984K /* Memory is divided. Actual start is 0x08000000 and actual length is 1984K */
…
stm32h747xi_ram_cm7.ld : {{Snippet | category=AI | component=Application | snippet=
/* Memories definition */
MEMORY
{
RAM (xrw) : ORIGIN = 0x24000000, LENGTH = 512K /* Memory is divided. Actual start is 0x24000000 and actual length is 512K */
FLASH (rx) : ORIGIN = 0x08000000, LENGTH = 1984K /* Memory is divided. Actual start is 0x8000000 and actual length is 1984K */
….
stm32h747xi_flash_cm4.ld: {{Snippet | category=AI | component=Application | snippet=
/* Specify the memory areas */
MEMORY
{
FLASH (rx) : ORIGIN = 0x081F0000, LENGTH = 64K
RAM (xrw) : ORIGIN = 0x10000000, LENGTH = 288K
}