FP-AI-MONITOR1 user manual

Revision as of 16:49, 5 August 2021 by Registered User (→‎Autonomous and button-operated modes)
Under construction.png Delivery for this distribution is being prepared

Sensing and condition monitoring are two of the major components of the IoT and predictive maintenance systems, allowing context awareness, production performance improvement, maintenance cost reduction and a drastic decrease of the downtime due to routine maintenance.

The FP-AI-MONITOR1 function pack helps to jump-start the implementation and development of classification and condition monitoring applications designed with X-CUBE-AI Expansion package for STM32Cube and with the NanoEdge™ AI Studio solution.

FP-AI-MONITOR1 supports on device learning for the anomaly detection using NanoEdge AI libraries and on device inference for both classification problems based on classical machine learning and Neural Networks as well as for the anomaly detection using NanoEdge AI studio. The evaluation board supported is a sensor node STEVAL-STWINKT1B with STM32L4R9ZI ultra-low power microcontroller. It covers the entire design of the Machine Learning cycle from the data set acquisition to the integration on a physical node.

FP-AI-MONITOR1 implements a wired interactive CLI to configure the node, and manage the learn and detect phases. In addition to this for simple operation in the field, a standalone battery-operated mode is also supported, which allows basic controls through the user button, without using the console.

This article provides an overview of the following topics:

  • The required hardware and software,
  • Setting up the hardware and software components,
  • Performing the vibration sensor data collection using a prebuilt binary of FP-SNS-DATALOG1,
  • Running a One-class SVM model for anomaly detection on the device
  • Building the model using Scikit-learn,
  • Exporting as onnx model using onnx-runtime,
  • Generating C code using X-CUBE-AI, and
  • Running on STEVAL-STWINKT1B .
  • Generating the library using NanoEdgeTM AI Studio, Installing, and testing the NanoEdge™ AI machine learning libraries on the STEVAL-STWINKT1B using the provided function pack, and
  • Some links to useful online resources, to help a user to better understand and customize the project for his own needs.

For full user instructions of the FP-AI-MONITOR1 please refer to this article.

Info white.png Information
NOTE: The NanoEdge™ library generation itself is out of the scope of this function pack and must be generated using NanoEdge™ AI Studio.

1. General information

The FP-AI-NANOEDG1 function pack runs on STM32L4+ microcontrollers based on Arm® cores.

Info white.png Information
Note: Arm® is a registered trademark of Arm Limited (or its subsidiaries) in the US and/or elsewhere.

1.1. Feature overview

The FP-AI-NANOEDG1 function pack features:

  • Complete firmware to program an STM32L4+ sensor node for condition monitoring and predictive maintenance applications
  • Stub for replacement with a Cartesiam Machine Learning library generated using the NanoEdge™ AI Studio for the desired AI application
  • Configuration and acquisition of STMicroelectronics (IIS3DWB) 3-axis digital vibration sensor, and (ISM330DHCX) 6-axis digital accelerometer and gyroscope iNEMO inertial measurement unit (IMU) with machine learning core
  • Data logging on a microSD™ card
  • Embedded file system utilities
  • Interactive command-line interface (CLI) for:
    - Node and sensor configuration
    - Data logging
    - Management of learning and detection phase of the NanoEdge™ library
  • An extended configurable autonomous mode, controlled by the user button and the configuration files stored in the microSD™ card
  • Easy portability across STM32 microcontrollers by means of the STM32Cube ecosystem
  • Free and user-friendly license terms

1.2. Software architecture

The STM32Cube function packs leverage the modularity and interoperability of STM32 Nucleo and expansion boards running STM32Cube MCU Packages and Expansion Packages to create functional examples representing some of the most common use cases in certain applications. The function packs are designed to fully exploit the underlying STM32 ODE hardware and software components to best satisfy the final user application requirements.

Function packs may include additional libraries and frameworks, not present in the original STM32Cube Expansion Packages, which enable new functions and create more targeted and usable systems for developers.

STM32Cube ecosystem includes:

  • A set of user-friendly software development tools to cover project development from the conception to the realization, among which are:
    • STM32CubeMX, a graphical software configuration tool that allows the automatic generation of C initialization code using graphical wizards
    • STM32CubeIDE, an all-in-one development tool with peripheral configuration, code generation, code compilation, and debug features
    • STM32CubeProgrammer (STM32CubeProg), a programming tool available in graphical and command-line versions
    • STM32CubeMonitor (STM32CubeMonitor, STM32CubeMonPwr, STM32CubeMonRF, STM32CubeMonUCPD) powerful monitoring tools to fine-tune the behavior and performance of STM32 applications in real-time
  • STM32Cube MCU & MPU Packages, comprehensive embedded-software platforms specific to each microcontroller and microprocessor series (such as STM32CubeL4 for the STM32L4+ Series), which include:
    • STM32Cube hardware abstraction layer (HAL), ensuring maximized portability across the STM32 portfolio
    • STM32Cube low-layer APIs, ensuring the best performance and footprints with a high degree of user control over the HW
    • A consistent set of middleware components such as FreeRTOS™, USB Device, USB PD, FAT file system, Touch library, Trusted Firmware (TF-M), mbedTLS, Parson, and mbed-crypto
    • All embedded software utilities with full sets of peripheral and applicative examples
  • STM32Cube Expansion Packages, which contain embedded software components that complement the functionalities of the STM32Cube MCU & MPU Packages with:
    • Middleware extensions and applicative layers
    • Examples running on some specific STMicroelectronics development boards

To access and use the sensor expansion board, the application software uses:

  • STM32Cube hardware abstraction layer (HAL): provides a simple, generic, and multi-instance set of generic and extension APIs (application programming interfaces) to interact with the upper layer applications, libraries, and stacks. It is directly based on a generic architecture and allows the layers that are built on it, such as the middleware layer, to implement their functions without requiring the specific hardware configuration for a given microcontroller unit (MCU). This structure improves library code reusability and guarantees easy portability across other devices.
  • Board support package (BSP) layer: supports the peripherals on the STM32 Nucleo boards.

The top-level architecture of the FP-AI-MONITOR1 function pack is shown in the following figure.

FP-AI-MONITOR1 architecture.png

1.3. Folder structure

FP-AI-MONITOR1 folder structure

The figure above shows the contents of the function pack folder. The contents of each of these subfolders are as follows:

  • Documentation: contains a compiled .chm file generated from the source code, which details the software components and APIs.
  • Drivers: contains the HAL drivers, the board-specific part (BSP) drivers for each supported board or hardware platform (including the onboard components), and the CMSIS vendor-independent hardware abstraction layer for the Cortex®-M processors.
  • Middlewares: contains libraries and protocols for ST parts as well as for the third parties. From ST parts it includes the eLoom libraries, NanoEdgeTM AI library stub, Audio Processing library, FFT library and USB Device library.
  • Projects: contains a sample application software, which can be used to program the sensor-board for classification and anomaly detection applications using the data from the motion sensors and manage the learning and detection phases of Cartesiam Machine Learning solution provided for the STEVAL-STWINKT1B platforms through the STM32CubeIDE development environment.
  • Utilities: contains python scripts and sample datasets. These python scripts can be used to create Human Activity Recognition (HAR) models using Convolutional Neural Networks (CNN) or Support Vector machine based Classifier (SVC). The FP-AI-MONITOR1 also enables a user to prepare the data logged from the HSDatalog.bin for the Cartesiam library generation.

1.4. Terms and definitions

Acronym Definition.
API Application programming interface
BSP Board support package
CLI Command line interface
FP Function pack
GUI Graphical user interface
HAL Hardware abstraction layer
LCD Liquid-crystal display
MCU Microcontroller unit
ML Machine learning
ODE Open development environment
Acronyms used in this article.

1.5. References

References Description Source
[1] X-CUBE-AI X-CUBE-AI
[2] Cartesiam website cartesiam.ai
[3] STEVAL-STWINKT1B STWINKT1B
References

1.6. Prerequisites

Warning white.png Warning
confirms the versions from Laurent and Stefano.
  • FP-AI-MONITOR1 can be deployed on the following operating systems:
    • Windows® 10
    • Ubuntu® 18.4 and Ubuntu® 16.4 (or derived)
    • macOS® (x64)

Note: Ubuntu® is a registered trademark of Canonical Ltd. macOS® is a trademark of Apple Inc. registered in the U.S. and other countries.

Info white.png Information
NOTE : In this document all the steps presented are carried out with STM32CubeIDE but the same can also be done with the other two IDEs.

1.7. Licenses

FP-AI-MONITOR1 is delivered under the Mix Ultimate Liberty+OSS+3rd-party V1 software license agreement (SLA0048).

The software components provided in this package come with different license schemes as shown in the table below.

Software component Copyright License
Arm® Cortex®-M CMSIS Arm Limited Apache License 2.0
FreeRTOS™ Amazon.com, Inc. or its affiiates MIT
STM32L4xxx_HAL_Driver STMicroelectronics BSD-3-Clause
Board support package (BSP) STMicroelectronics BSD-3-Clause
STM32L4xx CMSIS Arm Limited - STMicroelectronics Apache License 2.0
Parson Krzysztof Gabis MIT
Applications STMicroelectronics Proprietary
Python TM scripts STMicroelectronics BSD-3-Clause
Dataset STMicroelectronics Proprietary
FP-AI-MONITOR1 Console application STMicroelectronics Proprietary
High-Speed Data Log Core application STMicroelectronics Proprietary
Warning white.png Warning
Fix the license table with Laurent, Stefano, and Ludo's help.

2. Hardware and firmware setup

2.1. Presentation of the Target STM32 board

The STWIN SensorTile wireless industrial node (STEVAL-STWINKT1B) is a development kit and reference design that simplifies the prototyping and testing of advanced industrial IoT applications such as condition monitoring and predictive maintenance. It is powered with Ultra-low-power Arm® Cortex®-M4 MCU at 120 MHz with FPU, 2048 kbytes Flash memory (STM32L4R9). Other than this, STWIN SensorTile is equipped with a microSD™ card slot for standalone data logging applications, a wireless BLE4.2 (on-board) and Wi-Fi (with STEVAL-STWINWFV1 expansion board), and wired RS485 and USB OTG connectivity, as well as Brand protection secure solution with STSAFE-A110. In terms of sensor, STWIN SensorTile is equipped with a wide range of industrial IoT sensors including:

  • an ultra-wide bandwidth (up to 6 kHz), low-noise, 3-axis digital vibration sensor (IIS3DWB)
  • a 6-axis digital accelerometer and gyroscope iNEMO inertial measurement unit (IMU) with machine learning (ISM330DHCX)
  • an ultra-low-power high-performance MEMS motion sensor (IIS2DH)
  • an ultra-low-power 3-axis magnetometer (IIS2MDC)
  • a digital absolute pressure sensor (LPS22HH)
  • a relative humidity and temperature sensor (HTS221)
  • a low-voltage digital local temperature sensor (STTS751)
  • an industrial-grade digital MEMS microphone (IMP34DT05), and
  • a wideband analog MEMS microphone (MP23ABS1)

Other attractive features include:

– a Li-Po battery 480 mAh to enable standalone working mode
STLINK-V3MINI debugger with programming cable to flash the board
stlink v3 mini.jpg
– a Plastic box for ease of placing and planting the SensorTile on the machines for condition monitoring. For further details, the users are advised to visit this link

2.2. Connect hardware

To start using FP-AI-NANOEDG1, the user needs:

  • A personal computer with one of the supported operating systems, (Windows® 10, Ubuntu® 18.4 and Ubuntu® 16.4, or macOS® x64)
  • One USB cable to connect the sensor node to the PC through STLINK-V3MINI
microBusb.png
  • An STEVAL-STWINKT1B board
STWINKt1.png
  • One microSD™ card formatted as FAT32 FileSystem.
microSdCard.png

Follow the next two steps to connect hardware:

  1. Connect the STM32 sensor board to the computer through the STLINK with the help of a USB micro cable. This connection will be used to program the STM32 MCU.
  2. Connect another micro USB cable to the STWIN USB connector. This connection will be used for the communication between the CLI console and the sensor node.
  3. Insert the microSD™ card into the dedicated slot to store the data from the HSDatalog.bin binary.
Info white.png Information
NOTE: microSDTM card is only required when using HSDatalog.bin for datalogging.

Note : Before connecting the sensor board to a Windows® PC through USB, the user needs to install a driver for the ST-LINK-V3E (not required for Windows 10®). This software can be found on the ST website. The power source for the board can either be a battery for standalone operations or a USB cable connection to the USART interface.

2.3. Program firmware into the STM32 microcontroller

This section explains how to select binary firmware and program it into the STM32 microcontroller. Binary firmware is delivered as part of the FP-AI-MONITOR1 function pack. It is located in the FP-AI-MONITOR1/Projects/STM32L4R9ZI-STWIN/Applications/FP-AI-MONITOR1/Binary/ folder. When the STM32 board and PC are connected through the USB cable on the STLINK-V3E connector, the related drive is available on the PC. Drag and drop the chosen firmware into that drive. Wait a few seconds for the firmware file to disappear from the file manager: this indicates that firmware is programmed into the STM32 microcontroller.

FP-AI-MONITOR1 drag drop installation.png

2.4. Using the serial console

A serial console is used to interact with the host board (Virtual COM port over USB). With the Windows® operating system, the use of the Tera Term software is recommended. Following are the steps to configure the Tera Term console for CLI over a serial connection.

2.4.1. Set the serial terminal configuration

Start Tera Term, select the proper connection (featuring the STMicroelectronics name),

tera term connection port choice.png

Set the parameters:

  • Terminal
    • [New line]:
      • [Receive]: CR
      • [Transmit]: CR
tera term connection new line.png
  • Serial
    The interactive console can be used with the default values.

2.4.2. Start FP-AI-MONITOR1 firmware

Restart the board by pressing the RESET button. The following welcome screen is displayed on the terminal.

FP-AI-MONITOR1 Console Welcome Message

From this point, start entering the commands directly or type help to get the list of available commands along with their usage guidelines.

Note: The provided firmware is generated with a HAR model based on SVC and users can test it right away out of the box. However for the NanoEdgeTM AI Library a stub is provided in place of the library. The user must generate the library with the help of the NanoEdge™ AI Studio, replace the stub with it, and rebuild firmware. These steps will be provided in details in the article later.

3. Button-operated modes

This section provides details of the button operated mode for FP-AI-MONITOR1. The purpose of the extended mode is to enable the users to operate the FP-AI-MONITOR1 on STWIN even in the absence of the CLI console.

In button operated mode, the sensor node can be controlled through the user button instead of the interactive CLI console. The default values for node parameters and settings for the operations during auto-mode are provided in the FW. Based on these configurations different modes (ai, neai_detect, and neai_learn) can be started and stopped through the user-button on the node.

3.1. Interaction with user

The button operated mode can work with or without the CLI and is fully compatible and consistent with the current definition of the serial console and its Command Line Interface (CLI).

The supporting hardware for this version of the function-pack (STWIN) is fitted with three buttons:

  1. User Button, the only SW usable,
  2. Reset Button, connected to STM32 MCU reset pin,
  3. Power Button connected to power management,

and three LEDs:

  1. LED_1 (green), controlled by Software,
  2. LED_2 (orange), controlled by Software,
  3. LED_C (red), controlled by Hardware, indicates charging status when powered through a USB cable.

So, the basic user interaction for button-operated operations is to be done through two buttons (user and reset) and two LEDs (Green and Orange). Following we provide details on how these resources are allocated to show the users what execution phases are active or to report the status of the sensor-node.

Warning white.png Warning
Check with stefano the options for the LED allocation.

3.1.1. LED Allocation

In the function pack four execution phases exist:

idle: the system waits for a specified amount of time.
ai: sensor(s) output data are streamed onto an SD card.
learn: all data coming from the sensor(s) are passed to the NanoEdge AI library to train the model.
detect: all data coming from the sensor(s) are passed to the NanoEdge AI library to detect anomalies.

At any given time, the user needs to be aware of the current active execution phase. We also need to report the outcome of the detection when the detect execution phase is active, telling the user if an anomaly has been detected. In addition, if a fatal error occurs and consequently the FW has stopped, the user needs to be notified, either to debug or to reset the node.

In total, we need the interaction mechanism to code six different states with the two available LEDs, so we need at least three patterns in addition to the traditional On-OFF options. At any given time the LED can be in one of the following states:

Pattern Description
OFF the LED is always OFF
ON the LED is always ON
BLINK the LED alternates ON and OFF periods of equal duration (400 ms)
BLINK_SHORT the LED alternates short (200 ms) ON periods with a short OFF period (200 ms)
BLINK_LONG the LED alternates long (800 ms) ON periods with a long OFF period (800 ms)

These patterns of each of the LEDs indicate the state of the sensor-node. Following table describes the state of the sensor-node for any of the patterns:

Pattern Green Orange
OFF Power OFF
ON idle System error
BLINK Data logging MicroSD™ card missing
BLINK_SHORT Detecting, no anomaly Anomaly detected
BLINK_LONG Learning, status OK Learning, status FAILED

3.1.2. Button Allocation

In the extended autonomous mode, the user can trigger any of the four execution phases. The available modes are:

  1. idle: the system waits for a command.
  2. ai: run the X-CUBE-AI library and print the results of the live inference on the CLI (if CLI is available).
  3. neai_learn: all data coming from the sensor are passed to the NanoEdgeTM AI library to train the model.
  4. neai_detect: all data coming from the sensor are passed to the NanoEdgeTM AI library to detect anomalies.

For triggering these phases the FP-AI-NANOEDG1 is equipped with the support of the user button. In the STEVAL-STWINKT1B sensor-node, there are two software usable buttons:

  1. The user button: This button is fully programmable and is under the control of the application developer.
  2. The reset button: This button is used to reset the sensor-node and is connected to the hardware reset pin, thus is used to control the software reset. It resets the knowledge of the NanoEdge AI libraries and reset all the context variables and sensor configurations to the default values.

In order to control the executions phases, we need to define and detect at least three different button press modes of the user button.

Following are the types of the press available for the user button and their assignments to perform different operations:

Button Press Description Action
SHORT_PRESS The button is pressed for less than (200 ms) and released Start AI inferences for X-CubeAI model.
LONG_PRESS The button is pressed for more than (200 ms) and released Starts the learning for NanoEdgeTM AI Library.
DOUBLE_PRESS A succession of two SHORT_PRESS in less than (500 ms) Starts the inference for NanoEdgeTM AI Library.
ANY_PRESS The button is pressed and released (overlaps with the three other modes) Stops the current running execution phase.

4. Command line interface

The command-line interface (CLI) is a simple method for the user to control the application by sending command line inputs to be processed on the device.

4.1. Command execution model

The commands are grouped into four main sets:

  • (CS1) Generic commands
    This command set allows the user to get the generic information from the device like the firmware version, UID, date, etc. and to start and stop an execution phase.
  • (CS2) AI commands
    This command set contains commands which are PdM specific. These commands enable users to work with the NanoEdge™ AI libraries for predictive maintenance.
  • (CS3) Sensor configuration commands
    This command set allows the user to configure the supported sensors and to get the current configurations of these sensors.
Info white.png Information
Warning: These commands are not a full implementation of a standard shell and only provide basic functionality to facilitate for some tasks.

4.2. Execution phases and execution context

The four system execution phases are:

  • Datalogging: data coming from the sensor are logged onto the microSD™ card.
  • NanoEdge™ AI learning: data coming from the sensor are passed to the NanoEdge™ AI library to train the model.
  • NanoEdge™ AI detection: data coming from the sensor are passed to the NanoEdge™ AI library to detect anomalies.
  • Idle: This is a special execution phase, available only in auto-mode.

Each execution phase (except 'idle' mode) can be started and stopped with a user command issued through the CLI. An execution context, which is a set of parameters controlling execution, is associated with each execution phase. One single parameter can belong to more than one execution context.

The CLI provides commands to set and get execution context parameters. The execution context cannot be changed while an execution phase is active. If the user attempts to set a parameter belonging to any active execution context, the BUSY status is returned, and the requested parameter is not modified.

4.3. command summary

Command name Command string Note
CS1 - Generic Commands
help help Lists all registered commands with brief usage guidelines. Including the list of applicable parameters.
info info Shows firmware details and version.
uid uid Shows STM32 UID.
reset reset Resets the MCU System.
start start <"ai", "neai_learn", or "neai_detect" > Starts an execution phase according to its execution context, i.e. ai, neai_learn or neai_detect.
CS2 - AI Specific Commands
neai_init neai_init (Re)initializes the AI model by forgetting any learning. Used in the beginning and/or to create a new NanoEdge AI model.
neai_set neai_set <param> <val> Sets a PdM specific parameters in an execution context.
neai_get neai_get <param> Displays the value of the parameters in the execution context.
CS3 - Sensor Configuration Commands
sensor_set sensor_set <sensorID>.<subsensorID> <param> <val> Sets the ‘value’ of a ‘parameter’ for a sensor with sensor id provided in ‘id’.
sensor_get sensor_get <sensorID>.<subsensorID> <param> Gets the ‘value’ of a ‘parameter’ for a sensor with sensor id provided in ‘id’.
sensor_info sensor_info Lists the type and ID of all supported sensors.
Available commands in Command Line Interface (CLI) Application of FP-AI-MONITOR1

5. Generating a Machine Learning library with NanoEdge™ AI Studio

Refer to [1] for the full NanoEdge™ AI Studio documentation.

5.1. Generating contextual data

In order to choose the right libraries for the problem under consideration, the user needs to present NanoEdge™ AI Studio to work on selecting the best algorithm and optimizing its hyperparameters. The [cartesiam-neaidocs.readthedocs-hosted.com/studio/studio.html documentation] of NanoEdge™ AI Studio provides the following guidelines for the preparation of the contextual data:

  • The Regular signals file corresponds to nominal machine behavior that includes all the different regimes, or behaviors, that the user wishes to consider as nominal.
  • The Abnormal signals file corresponds to abnormal machine behavior, including some anomalies already encountered by the user, or that the user suspects could happen.
Info white.png Information
Note: Although the behavior of the generated libraries heavily depends on this initial signal selection step, it does not contain any a priori knowledge when added to FP-AI-NANOEDG1 firmware on the sensor node. That needs to be acquired during the learning phases the user will carry out on the field.

FP-AI-NANOEDG1 comes equipped with the data logging capabilities for embedded sensors on the STM32 sensor board.

To proceed with data acquisition:

  • Make sure that a microSD™ card is inserted, and the USB cable is plugged in.
  • List the supported sensors with the sensor_info command and collect their IDs using the command $ sensor_info as shown in the figure below.
stwin supported sensors.png
Info white.png Information
MLC (Machine Learning Core) is not supported.
  • Select the desired sub-sensor, the accelerometer for instance, with the sensor_set command:
$ sensor_set 0.0 enable 1
sensor 0.0: enable.enable
  • You can further configure other parameters (Output Data Rate and full-scale settings) using sensor_set and sensor_get commands.
  • Configure and run the device you want to monitor in normal operating conditions and start the data logging.
  • Start data acquisition with the start datalog command
$ start datalog
  • Stop data acquisition when enough data is collected with the stop command (or even more conveniently with hitting the ESC key)
$ stop
  • Configure the monitored device for abnormal operation, start it .and repeat steps 6. and 7. During each data acquisition cycle, a new folder is created with the name STM32_DL_nnn. The suffix nnn increments by one each time a new folder is created, starting from 001. This means that if no STM32_DL_nnn directory pre-exists, directories STM32_DL_001 and STM32_DL_002 are created for normal and abnormal data respectively. Each created directory contains following files:
    • DeviceConfig.json: the configurations used for the sensors to acquire data.
    • AcquisitionInfo.json: File containing the information on the acquisition.
    • SensorName_SubsensorMode.dat: the sensor acquisition data.

Alternatively, the data acquisitions can be made using the auto-mode provided in extended autonomous modes of the FP-AI-NANOEDG1. To achieve this, the user has to provide the required configurations of the sensors either through the default values in the Firmware or through a DeviceConfig.json file in at the root of microSD™ card, and an execution_config.json file to configure the settings of the auto mode. An example file for auto-mode to log the data is provided below.

{
	"info": {
		"version": "1.0",
		"auto_mode": true,
		"phases_iteration": 3,
		"start_delay_ms": 2000,
		"execution_plan": [
			"datalog",
			"idle"
		],
		"learn": {
			"signals": 0,
			"timer_ms": 0
		},
		"detect": {
			"signals": 0,
			"timer_ms": 0,
			"threshold": 90,
			"sensitivity": 1.0
		},
		"datalog": {
			"timer_ms": 30000
		},
		"idle": {
			"timer_ms": 10000
		}
	}
}

This file assumes the data logging will start after 2 seconds of power-up or reset. Then this configuration file will perform three iterations for the data logging, with 10-second long idle breaks which can be used to change the configurations of the monitoring machine, such as the speed of a motor or load on a motor.

5.2. Exporting the data collection to NanoEdge™ AI Compliant Data format

FP-AI-NANOEDG1 comes with utility Python™ scripts located in /FP-AI-NANOEDG1_V2.0.0/Utilities/AI_ressources/DataLog to export data from the STWIN datalog application to the NanoEdge™ AI Studio compliant format.

The datalogs generated with FP-AI-NANOEDG1 datalog are in the binary format as .dat files along with the DeviceConfig.json and AcquisitionInfo.json files. The .dat as it is are not human-readable and can not be used for the library generation. The script STM_DataParser.py parses the binary .dat files, and create .csv human-readable files. This function takes in input the path to a data directory that contains all the .dat files. Following are the example calls:

python STM_DataParser.py Sample-DataLogs/STM32_DL_001
python STM_DataParser.py Sample-DataLogs/STM32_DL_002

As a result, a .csv file is added to each directory.

These .csv files contain data, in human-readable format, so they can be interpreted, cleaned, or plotted. Another step is needed to export them to NanoEdge™ AI Studio required format as explained in cartesiam-neai-docs.readthedocs-hosted.com/studio/studio.html#expected-file-format. This is done using script, PrepareNEAIData.py. The script converts the data stream into frames of equal length. The length, which depends on the use case and features to be extracted, must be given as a parameter along with the good and the bad data folders (respectively STM32_DL_001 and STM32_DL_002 in the example) as follows:

python PrepareNEAIData.py Sample-DataLogs/STM32_DL_001 Sample-DataLogs/STM32_DL_002 -seqLength 1024

As a result, two .csv files are created:

# normalData.csv
# abnormalData.csv
Info white.png Information
Note: Option mfloatabi is to be checked for hardware FPU to be used. All other flags can be left unchecked.
Info white.png Information
NOTE: When multiple acquisitions are made for normal and abnormal behaviors of the machine, the user is expected to collect all the normal data files in a single folder and all the abnormal files in another folder. The script Prepare NEAIData.py can handle the multiple files and create a single .csv file for both normal and abnormal cases, irrespective of the number of .csv present in normal and abnormal data folders.

Detailed script usage instructions and examples are provided in a Jupyter™ notebook located in the datalog directory (FP-AI-NANOEDG1-HSD-Utilities.ipynb). Samples of vibration dataset is provided provided in Utilities/AI_ressources/DataLog/Sample-DataLogs.

5.3. NanoEdgeTM AI Library Generation

The process of generating the libraries with Cartesiam NanoEdge AI studio consists of five steps.

  1. Hardware description
    1. Choosing the target platform or a microcontroller type: STEVAL-STWINKT1B Cortex-M4
    2. Maximum amount of RAM to be allocated for the library: Usually a few Kbytes will suffice (but it depends on the data frame length used in the process of data preparation, you can start with 32 Kbytes).
    3. Sensor type : 3-axis accelerometer
  2. Providing the sample contextual data to adjust and gauge the performance of the chosen model. This step will require data for:
    1. Nominal or normal case (normalSegments.csv)
    2. Abnormal case (abnormalSegments.csv)
  3. Benchmarking of available models and choose the one that complies with the requirements.
  4. Validating the model for learning and testing through the provided emulator which emulates the behavior of the library on the edge.
  5. The final step is to compile and download the libraries. In this process, the flag "-mfloat-abi" has to be checked for using libraries with hardware FPU. All the other flags can be left to the default state.

Detailed documentation on the NanoEdge AI Studio.

Info white.png Information
NanoEdgeTM AI libraries can be freely generated for the evaluation purposes for STEVAL-STWINKT1B Cortex-M4, NUCLEO-F401RE Cortex-M4,NUCLEO-L432KC Cortex-M4, and STM32L562QE-DK Cortex-M33)

.

5.4. Installing the NanoEdge™ library

Once the libraries are generated and downloaded from NanoEdge™ AI Studio, the next step is to incorporate these libraries into FP-AI-NANOEDG1. The FP-AI-NANOEDG1 function pack comes with the library stubs replacing the current libraries generated by NanoEdge™ AI Studio. This makes it easy for users to link the generated libraries and have a place holder for the libraries that are generated as described in Section 4.2 Exporting the data collection to NanoEdge. To link the current libraries, the user must copy the generated libraries and replace the existing stub/dummy libraries libneai.a and header files NanoEdgeAI.h, present in the lib and inc respectively. The relative path of these folders is ./FP-AI-NANOEDG1_v2.0.0/Middlewares/Third_Party/Cartesiam_NanoEdge_AI_Library as shown in the figure below.

replace libraries and header file.png

Once these files are copied, the project must be reconstructed and programmed on the sensor board to link the libraries. To perform these operations,

the user must open the .project file from the FP-AI-NANOEDG1 folder located at FP_AI_NANOEDG1_V2.0.0/Projects/STM32L4R9ZI-STWIN/Applications/NanoEdgeConcole/STM32CubeIDE/ as shown in the figure below.

open the cubeIDE project.png

To install new firmware after linking the library, connect the sensor board, and rebuild the project using the play button highlighted in the following figure. Build and download the project in STM32CubeIDE.

build and download the package in cubeide.png

See the console for the outputs and wait for the build and download success message as shown in the following figure.

downloaded successfully.png

6. Building and programming

Once a new binary is generated through the build process with a Machine Learning library using NanoEdge™ AI Studio, the user can install it on the sensor node and start testing it in real conditions. To install and test it onto the target, the below steps are to be followed.

  • Connect the STWIN board to the personal computer through an ST-LINK using a USB cable. This will make the STWIN board appear as a drive in the drive list of the computer, named something as STLINK_V3M.
  • Drag and drop the newly generated NanoEdgeConsoleSTWIN.bin file onto the drive STLINK_V3M.
  • When the programming process is complete, connect the STWIN through the console and you should see a welcome message confirming that the stub has been replaced with the Cartesiam libraries as shown in the figure below.
welcome screen cartesiam powered.png
Info white.png Information
Note: Even though the libraries are generated using the contextual data, they have zero knowledge when they are flashed to the STWIN board. Also, every time a reset of the board is performed all the learned knowledge of the libraries vanish also.
  • To use these libraries for condition monitoring, the user must provide some learning data of the nominal condition. To do so, place the machine to be monitored in nominal conditions, and start the learning phase, either through the CLI console or by performing a long press on the user button, and observe the screen as shown in the following figure (if the console is attached), or the LED blinking pattern1 as indicated in the autonomous mode to show the learning has started.
learn phase started console mode.png

The signals used for learning are counted. During the benchmark phase, a graph shows the number of signals to be used for learning in the form of minimum iterations. It is suggested to use between 3 to 10 times more signals than this number.

Info white.png Information
Note: For good performance, users are advised to expose all the possible nominal conditions to the library. Any condition not exposed during the learning phase might be wrongfully detected as an anomaly.
  • Once the desired number of signals are learned, press the user button again to stop the process. The learning can also be stopped by pressing Esc button or simply by entering stop command in the console. Upon stopping the phase, the console will show a message saying NanoEdge AI: stopped.
  • The anomaly detection mode can be started either through the console or by performing a short press on the user button. In the detection mode, the NanoEdge™ calculates the similarity between the observed signal and the nominal signals it has seen before. For normal conditions, the similarity is very high. However, for abnormal signals the similarity is low. If the similarity is low compared to a preset value, the signal is considered an anomaly, and the console shows the number of the bad signal along with the similarity calculated. However, the similarity for the normal signals is not shown.
detect phase started console mode.png
Info white.png Information
Note: By default the value for the neai_threshold is 90 but can be set to any value between 0 to 100.
  • The detect phase can be stopped by pressing the user button again if the sensor node is being used in autonomous mode. When the console is connected the detect phase can be stopped also by pressing Esc button on the keyboard or by entering stop command in the console. Upon stopping console shows a message saying NanoEdge AI: stopped.

Note: Some practical use cases (such as ukulele, coffee machine, and others) and tutorials are available from the Cartesiam website:

  • cartesiam-neai-docs.readthedocs-hosted.com/tutorials/ukulele/ukulele.html
  • cartesiam-neai-docs.readthedocs-hosted.com/tutorials/coffee/coffee.html

7. Documents and related resources

Warning white.png Warning
Note: Need to fix the links once available and checked with Laurent.
  • FP-AI-MONITOR1: Artificial Intelligence (AI) Sensing and monitoring function pack for STM32Cube
  • User Manual : User Manual for FP-AI-MONITOR1
  • STEVAL-STWINKT1B
  • STM32CubeMX : STM32Cube initialization code generator
  • X-CUBE-AI  : expansion pack for STM32CubeMX
  • NanoEdge AI Studio: NanoEdge AI™ by Cartesiam the first Machine Learning Software, specifically developed to entirely run on microcontrollers.
  • DB4345: Data brief for STEVAL-STWINKT1B.
  • UM2777: How to use the STEVALSTWINKT1B SensorTile Wireless Industrial Node for condition monitoring and predictive maintenance applications.