Click here for Cellular overview
1. Introduction
This wiki article contains information to help the user navigate ST Cellular software.
2. General description
The X-CUBE-CELLULAR Expansion Package only provides software components running on the host STM32 MCU. Cellular modem firmware is not in the scope of this document. The following integrated development environments are supported:
- STMicroelectronics integrated development environment for STM32 products (STM32CubeIDE)
- IAR Systems® IAR Embedded Workbench® for Arm® (EWARM)
- Keil® Microcontroller Development Kit (MDK-ARM)
3. X-CUBE-CELLULAR versions
Since the initial version V1.0.0 in mid-2018, the software content and hardware support have increased continuously.
Versions 1.0.0 to 5.2.0 progressively encompassed new features, applications, and hardware. The Cellular middleware however was part of X-CUBE, which is not sufficiently independent.
Therefore, V6.0.0 is reworked to provide standalone Cellular middleware that is easier to integrate into existing applications. Therefore the boot menu has been removed but command line calls are still available. The Cellular middleware API is also redesigned to ease/clarify its usage by application. Finally, V6.0.0 is the first delivery that introduces low power modem features for some modems (BG96 and Murata).
The current version, V6.0.0, supports the following hardware configurations:
- P-L496G-CELL02 (pack with a screenless 32L496GDISCOVERY associated with an STMod+ BG96 Quectel modem)
- B-L4S5I-IOT01A (STM32L4+ Discovery kit IoT node)
- 32L496GDISCOVERY (Discovery kit with STM32L496AG MCU)
- STEVAL-STWINKT1B (STWIN SensorTile Wireless Industrial Node development kit and reference design for industrial IoT applications)
- B-L462E-CELL1 (Discovery board with T1SE Murata module (STM32 L462, ST4SIM, ALT1250 modem))
- X-NUCLEO-STMODA1 (STMod+ connector expansion board for ARDUINO® connectors)
- STEVAL-STMODLTE (LTE connectivity expansion board for STMod+ connector compatible evaluation boards, based on the Quectel BG96 modem, the same modem board in the P-L496G-CELL02 pack described above)
- GM01Q-STMOD or GMS01Q-STMOD (Monarch from Sequans, GMS01Q is a GM01Q that also contains an internal SIM with a prepaid data plan).
P-L496G-CELL02 and B-L462E-CELL1 are standalone setups.
For other STM32 boards (B-L4S5I-IOT01A, 32L496GDISCOVERY, STEVAL-STWINKT1B), just plug in the STEVAL-STMODLTE or GM01Q-STMOD modem boards.
Note: for B-L4S5I-IOT01A, an X-NUCLEO-STMODA1 (ARDUINO® / STMod+ adapter) must be used.
For the complete description of deliveries (software and supported hardware), please refer to the release notes included in the X-CUBE package.
4. Modem socket versus LwIP
Either modem socket or LwIP can be used for the IP stack:
- Modem socket: the IP stack runs in modem FW
- LwIP: the LwIP stack runs on the STM32 side
This option is selected in software through a #define used during the compilation process.
Note:Only IPV4 is supported.
If LwIP is selected, the communication between host and modem is done through the PPP layer. There is a PPP client on the host side, and a PPP server on the modem side. PPPoSIF adapts the LwIP stack to a serial IF, while LwIP usually uses Ethernet interfacing.
5. What is X-CUBE-CELLULAR?
X-CUBE-CELLULAR (or XCC) allows applications to send and receive data on the cellular network using BSD API sockets.
Remember that the official web page on X-CUBE-CELLULAR on www.st.com provides access to multiple resources (software, documents, and so on).
X-CUBE-CELLULAR consists of a set of libraries and application examples for STM32L4 Series MCUs acting as hosts for cellular connectivity applications.
The colors highlight the different parts, Light Green for applications, light Blue for Middlewares, dark Blue for HAL, Purple for hardware.
L4 family STM32 MCUs are currently scoped, and more families are to be added in the future. However it is easy to port the Cellular middleware on other STM32 MCU families.
6. Software architecture
6.1. API description
The X-CUBE-CELLULAR API of the cellular package is defined by two components.
- Cellular management (Ctrl): initialization/starting of cellular features. It also represents
the control plane.
- Com: data communication API based on the BSD API. It represents the data plane.
6.2. Component description
7. Applications provided
A single application, Cellular App, is provided with examples of all the supported hardware configurations. It allows the Cellular middleware to be tested, and contains the following features:
- ECHO to provide an example of connection and data exchanges using the TCP or UDP (connected or not-connected mode) socket protocols. By default one instance of ECHO is started but a second one can be started to test multiple-socket configurations
- PING to test the access to a remote machine
- Performance to test throughput.
At boot, after hardware initialization, Cellular App is started and this then starts the Cellular middleware.
X-CUBE-CELLULAR also contains a command tool (to interact with the firmware through a terminal on a connected PC)
The following hardware setup (B-L462E-CELL1) embeds more than the others. It also brings BSP for sensors and display, and a complete IoT application: displays information on the screen, reads humidity, pressure, temperature sensors, and uses Cellular middleware to exchange with the network (Echo, Ping).
8. Run-time configuration
During firmware execution, the command-line interface (CLI) is entered by pressing the [return] key. For example, the help command lists all available components.
Command | Object |
---|---|
help | Help command |
cellularapp | Cellular App commands |
echoclient | Echo client commands |
ping | Ping commands |
trace | Trace management |
csp | Power management |
comlib | Com library commands |
cst | Cellular service task management |
atcmd | Send an AT command |
modem | Modem configuration management |
Command examples:
- cst info: provides information about cellular network
- trace off : stops the trace
- echo off: stops the Echo application
The CLI and traces are displayed on the same terminal.
9. Board support package
The X-CUBE-CELLULAR targets 2 goals, the first is to demonstrate the Cellular middleware based on multiple hardware setups. The second is to demonstrate the B-L462E-CELL1.
In the X-CUBE-CELLULAR the BSP is only available for B-L462E-CELL1 boards.
For users who need to develop an application that uses sensors on supported hardware setups other than B-L462E-CELL1, please refer to the Cube FW deliveries to copy/paste/adapt for cellular usage.
The B-L462E-CELL1 BSP is composed of 2 parts, the board part (Drivers/BSP/B-L462E-CELL1) and the component part (Drivers/Components/).
All the required component drivers are listed below:
- hts221 (capacitive digital sensor for relative humidity and temperature) from STMicroelectronics
- lps22hh (260-1260 hPa absolute digital output barometer) from STMicroelectronics
- lsm303agr (Ultra-low-power 3D accelerometer and 3D magnetometer) from STMicroelectronics
- ssd1315 (display driver for 0.96-inch 128 x 64 OLED / SPI Ref=9OL9935701000)
- M24128 (128-Kbit serial I²C bus EEPROM) from STMicroelectronics
- w25q80ew (8 Mbit-bit hence 1 MByte Serial Flash Memory) from Winbond
- mt25qu512 (MT25Q Serial NOR Flash, 512 Mbit hence 64 MByte) from Micron.
Notes:
- An EEPROM driver is not needed because the board BSP uses the HAL API directly
- The w25q80ew QSPI is internal Flash memory located in the Murata module
- The mt25qu512 QSPI is an external Flash memory soldered on the board outside the module
- The 2 QSPIs are exclusive and the default is the internal one. To use external QSPI soldering is needed, information about this is available in the board user manual.
QSPI drivers are to be provided into next delivery, X-CUBE-CELLULAR V6.1.0.
10. X-CUBE-CELLULAR dynamics
The following sequence diagram shows the Cellular middleware setup from an application, more sequence diagrams are to be provided soon.
11. Folder structure
- STM32CubeExpansion_CELLULAR_V6.0.0
- Drivers\
- BSP\
- B-L462E-CELL1\
- Components\
- Common\
- hts221\
- lps22hh\
- ...
- X_STMOD_PLUS_MODEMS\
- BG96\
- MONARCH\
- TYPE1SC\
- CMSIS\
- STM32L4xx_HAL_Driver\
- BSP\
- Middlewares\ (Internal and external middleware)
- ST\ (STMicroelectronics (internal) middleware)
- STM32_Cellular\
- Third_Party\ (Third-party (external middleware)
- FreeRTOS\
- LwIP\
- ST\ (STMicroelectronics (internal) middleware)
- Projects\ (Projects, one directory per board supported)
- 32L496GDISCOVERY\ (One of the supported board)
- B-L462E-CELL1\ (One of the supported board)
- Demonstrations\
- Cellular\
- Binaries\
- Core\
- IDE\ (Supported IDEs)
- EWARM\
- MDK-ARM\
- STM32CubeIDE\
- STM32_Cellular\
- Config\
- Target\
- CellularIoT\
- Cellular\
- Demonstrations\
- B-L4S5I-IOT01A\ (One of the supported board)
- Misc\
- Cmd\
- RTOS\
- Samples\
- Cellular\
- CellularIoT\
- Cellular\
- STWINKT1\ (One of the supported board)
- Utilities\
- Fonts\
- LCD\
- Modem_FW\ (material to allow modem FW update)
- Drivers\
12. Real network or simulator
Users must ensure that network coverage with the target technology is available at their location. Indeed, 2G, LTE Cat M and NB-IoT are not available worldwide. If the live network is not available for the target technology, the users can use a network simulator such as Amarisoft’s. To run the example, it is assumed that a network connection is possible with the device.
13. Miscellaneous information
To support low power, the application must close the socket before entering low power mode.