Introduction to Cellular LTE CatM / NBIoT

Revision as of 17:11, 1 April 2021 by Registered User

This page contains application examples, document references, tips and tricks and so on related to STM32 cellular.

1. What are Cellular LTE CatM and NBIoT?


Technologies


LTE CatM and Narrowband Internet of Things (NBIoT) are low-power wide-area network (LPWAN) radio technology standards developed by 3GPP to enable a wide range of cellular devices and services.
NBIoT focuses specifically on the indoor coverage, low cost, long battery life, and high connection density.
The advantage of LTE CatM over NBIoT is its higher data rate, mobility, and voice over the network. However it requires more bandwidth and is more costly.

Check GSMA's NBIoT / LTE CatM world wide coverage information


2. Wiki MCU / Cellular : pages breakdown

3. Getting started with STM32 and Cellular LTE Cat M and NBIoT


On hardware point of view, STMicroelectronics offers various possibilities to setup a STM32 MCU with the Cellular connectivity solution. In case STM32 board supports STMod+ connector, the easiest way, just connect the STMod+ modem boards. Another possibility for STM32 boards that do not have STMod+ connector is to use an ARDUINO® / STMod+ adapter (X-NUCLEO-STMODA1) in between.
To have a complete setup there are multiple possibilities, either to get a pack that includes the STM32 and modem boards or to get on one hand a STM32 board and in the other hand the modem board. For more information check hardware setup page.
Note that for each version of the Cellular middleware software there is a set of supported hardware. See details in the hardware setup page too.

On software side, the X-CUBE-CELLULAR (X-CUBE Expansion Package) provides a software solution to allow customers to quickly and easily develop their own Firmware:

  • Based on FreeRTOS
  • Users can choose whether to use either the IP stack in the modem or in the STM32 (LwIP)
  • Command line through Virtual COM UART over USB ST-LINK to configure the cellular connectivity parameters (technology selection, bands, APN, and others), and the connection to the cloud IoT platform
  • Easy to support a new modem.

Several applications are provided as examples.

For more information check X-CUBE-CELLULAR page on this wiki MCU.

New hardware setups and new software features in X-CUBE-CELLULAR are to be provided to customers over time.

4. How to ...

This part is a guideline that describes how to perform the main activities with X-CUBE-CELLULAR. All the information is merged in the Cellular How To Wiki page

5. FAQ

All the frequently-asked questions are listed in the dedicated Cellular F.A.Q Wiki page

6. Video related to Cellular LTE CatM and NBIoT

pc videol.png

Zigbee 3.0 mesh to cloud over cat-M with BLE 5.0 user control (MWC/EW 2020)

pc videol.png

ST at CES 2019 - LTE IoT Starter Kits

pc videol.png

STM32 Cellular to Cloud Discovery Packs: 2G/3G and Espruino JS, LTE IoT! Embedded World 2018

7. Specific tools

STMicroelectronics’ STM32 Power Shield to power and analyze current consumption
Network simulator for both LTE CatM & NBIoT