This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.Click here for Cellular overview
1. Introduction
This wiki page contains information to help the user to use this hardawre setup.
X-CUBE-CELLULAR V6.0.0 support different types of hardware setups.
Some are based on Module that contains STM32 and modem, some are based on 2 boards, one STM32 board associated to a modem board.
In case the STM32 board do not have STMod+ connector, an Arduino / STMod+ adaptor must be used.
Also note in case of STM32 and modem board sometime it is a pack (2 boards in the same blister)
2. Integrated module : B-L462E-CELL1
3. 3 separate boards : B-L4S5I-IOT01A + X-NUCLEO-STMODA1 + GM01Q-STMOD or STEVAL-STMODLTE
4. 2 separate boards : 32L496GDISCOVERY + GM01Q-STMOD or STEVAL-STMODLTE
5. 2 boards in a pack : STEVAL-STWINKT1 + GM01Q-STMOD or STEVAL-STMODLTE
6. Before X-CUBE-CELLULAR V6.0.0