STM32WB-WBA Zigbee memory requirements

Revision as of 14:25, 2 July 2024 by Registered User (→‎Memory consideration)


1. Introduction

The STM32WB Zigbee stack is a software component designed to enable Zigbee communication on the STM32WB microcontroller. Like any software, the stack requires memory to operate. There are two main types of memory that are relevant to the stack: RAM and Flash memory.

RAM (Random Access Memory) is a type of volatile memory that is used for temporary storage of data and program code. The stack uses RAM to store data structures, variables, and other runtime objects. The amount of RAM required by the stack will depend on the application and the used features.
Flash memory, on the other hand, is a type of non-volatile memory that is used for long-term storage of program code and data. The stack uses Flash memory to store the code and data that make up the stack itself. The amount of Flash memory required by the stack will depend on.

Memory Types in Microcontrollers
Connectivity Types of memory in Microontroller.png

Another important concept to understand is memory allocation. The stack uses a heap to allocate memory dynamically at runtime. This means that the stack can allocate memory as needed, rather than requiring a fixed amount of memory to be allocated at compile time. However, this also means that the stack requires some amount of overhead to manage the heap.
Developers should carefully consider their application's requirements and consult the stack's documentation to determine the appropriate memory requirements.

2. Memory Layout of C Code

Microcontrollers Flash memory contains different segments of application code such as, interrupt vector table, code segment, initialized data segment, uninitialized data segment, constant data segment etc. The linker script file defines where each of these segments will store in flash memory.
These are the typical sections of a given C binary:

  1. Text Section: This section contains the machine code of the compiled C program. It is read-only and contains the instructions that the processor executes.
  2. Data Section: This section contains the initialized global and static variables of the program. It is writable and read-only.
  3. BSS Section: This section contains the uninitialized global and static variables of the program. It is writable and read-only.
  4. Heap Section: This section is dynamically allocated by the program during runtime. It is used for dynamic memory allocation. The heap area begins at the end of the BSS segment and grows upwards to higher memory addresses.
  5. Stack Section: This section is used for storing local variables and function parameters. It grows and shrinks as functions are called and returned. On the standard x86 architecture it grows downwards to lower addresses.
Simple Memory Layout of C Program
Connectivity memory organization.png

Heap is not automatically managed and should be explicitly allocated using malloc() for example, and deallocated using free(). So it is managed by the programmer.
Later, we will focus on heap memory and we will give formula to compute it on STM32WB for a given Zigbee application.

3. Startup File and Linker Script

The startup file and the linker script allow to initialize the microcontroller's hardware and link the various sections of the code together. The startup file includes functions that set up the stack, initialize the memory, and configure the clock and other peripherals so that the user application can run. The linker script determines how the code and data are organized in memory, it defines the ROM_start, ROM_end, RAM_start and RAM_end for example.

The following figure shows the memory map representation of the On/Off STM32WB55.Nucleo application example of the STM32Cube MCU Package. We have two separate linker files, the first for M4 and the second for M0, which is common and necessary to ensure that the code and data are placed in the correct memory regions for each core.

Connectivity Zigbee Memory map file example.png

4. STM32WB series

4.1. STM32WB Zigbee software architecture

As a reminder, the STM32WB MCUs are built with two separate cores, Arm® Cortex®-M4 and Arm® Cortex®-M0+ cores. The architecture is depicted in the figure below. Mainly, the M0 core contains the Zigbee stack, and the M4 core contains clusters and the developer’s application.

STM32WB Zigbee architecture
Connectivity Zigbee MCU STM32WB.png

STM32WB contains up to 1 Mbyte of flash memory single bank architecture, can be accessed starting from address 0x0000 0000 or 0x0800 0000, internal SRAM1 (up to 192 KB) and internal SRAM2a (32 KB) + SRAM2b (32 KB).
From system point of view, there are 2 heaps:

  • one on M4 side
  • one on M0 side to be used by Zigbee stack

4.2. STM32WB stack memory requirements

4.2.1. STM32WB stack heap size

The stack allocates run-time objects, such as packets, timers, and endpoints, using a heap. The application can configure the size of the heap using the ZbInit struct ZbInitTblSizesT parameters, specifically heapPtr and heapSz. The heap memory is allocated from the M4 core, allowing any memory, such as packets, passed between the M0 and M4 to be accessed and modified by either core.
M0 heap is included in M4 heap and allocated using ZbMalloc when ZbInit is called.

If ZbInit is called providing a NULL heapPtr, M0 heap will be allocated with default size depending on SW type:

  • FFD SW: 32 KB
  • RFD SW: 16 KB

4.2.2. STM32WB stack tables size

The following table describes the impact on memory usage for each additional entry:

Entry Type Memory Usage Per Entry (bytes)
Network Neighbor Table entry (nwkNeighborTblSz) 144
Network Routing Table entry (nwkRouteTblSz) 28
Network Address Mapping Table (nwkAddrMapTblSz) 24
APS Link Key Table (apsPeerLinkKeyTblSz) 48

Default network topology in FFD SW is:

  • ZB_NWK_NEIGHBOR_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLME_ADDRMAP_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLME_ROUTE_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLDE_BTT_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLME_RREQ_TABLE_DEFAULT_SIZE=4U
  • ZB_APS_DEVICE_KEY_PAIR_DEFAULT_COUNT=16U

With such configuration, overall M4 heap consumption is close to 52 KB with 32 KB allocated for M0 heap + fixed M0 allocation + variable memory size depending on topology.

To compute M4 heap requirement for a given topology, you can use below formula:

M4 heap size= (32+16)*1024 + neighb_table_size*144 + routing_table_size*28 + address_mapping_table_size*24 + aps_link_key_table_size*48
Info white.png Information
Formula is accurate +/-10%

4.2.3. Device Configuration And Memory Usage

Description nwkNeighborTblSz nwkRouteTblSz nwkAddrMapTblSz apsPeerLinkKeyTblSz Heap kB Total Memory kB
Coordinator, 30 Devices, 30 Neighbors / Children 30 30 30 30 32 54
Coordinator, 100 Devices, 40 Neighbors / Children 40 30 100 100 32 60
Coordinator, 200 Devices, 40 Neighbors / Children 40 30 200 200 32 67
Router, 30 Neighbors / Children 30 30 4 4 32 52
Router, 100 Neighbors / Children 100 30 4 4 32 61
End-Device, 8 Neighbors 8 0 2 2 8 14.5

Note: Total Memory includes some items with constant overhead, which are not listed in this table.

5. STM32WBA series

5.1. STM32WBA Zigbee software architecture

As a reminder, the STM32WBA MCUs are built with Arm® Cortex®-M33 core. The architecture is depicted in the figure below.

STM32WBA Zigbee architecture
Connectivity Zigbee MCU STM32WBA.png

STM32WBA5xxG devices contain a 1 Mbyte flash memory from address offset 0x00 0000 to 0x0F FFFF, and 128 KB of SRAM defined below:

  • SRAM1 region start = 0x20000000
  • SRAM1 region end = 0x2000FFFF
  • SRAM2 region start = 0x20010000
  • SRAM2 region end = 0x2001FFFF

STM32WBA6x devices contain a 2 Mbyte flash memory, and 512 KB of as defined below:

  • SRAM1 region start = 0x20000000
  • SRAM1 region end = 0x2003FFFF
  • SRAM2 region start = 0x20040000
  • SRAM2 region end = 0x2007FFFF

5.2. STM32WBA stack memory requirements

5.2.1. Memory consideration

Some aspects of Zigbee stack must be runtime configurable, such as table sizes which depend on device capabilities and network topology. These values depend on the use case which is targeted. This is the reason why dynamic memory allocation is being used inside the stack.
Inside the Zigbee stack, two functions are used to allocate memory : ZIGBEE_PLAT_HeapMalloc() and ZIGBEE_PLAT_ZbMalloc()

  • ZIGBEE_PLAT_HeapMalloc() is used to allocate memory from the system during stack initialization (ZbInit), and it is not freed until ZbDestroy().
  • ZIGBEE_PLAT_ZbHeapMalloc() is used to allocate memory during the run-time operation of the stack. These are mostly short-lived memories, such as packets, timers, etc. Once the memory is no longer needed, it is freed by calling ZbHeapFree().

By default, these memory allocation APIs are linked to the ST memory manager. The relevant functions, including ZIGBEE_PLAT_ZbHeapInit(), ZIGBEE_PLAT_ZbHeapMalloc(), ZIGBEE_PLAT_ZbHeapFree(), ZIGBEE_PLAT_ZbInit(), ZIGBEE_PLAT_ZbMalloc(), and ZIGBEE_PLAT_ZbFree(), are defined within the Zigbee_plat.c file. These APIs are customizable and can be redefined to meet specific application requirements if necessary.

5.2.2. STM32WBA stack heap size

The size of memory buffer is provided by heapPtr. If heapSz is set to zero, then a default value of 32 kB for FFD or 16 kB for RFD is chosen, and memory will be allocated through ZbMalloc().

5.2.3. STM32WBA stack tables size

The following table describes the impact on memory usage for each additional entry:

Entry Type Memory Usage Per Entry (bytes)
Network Neighbor Table entry (nwkNeighborTblSz) 136
Network Routing Table entry (nwkRouteTblSz) 32
Network Address Mapping Table (nwkAddrMapTblSz) 24
APS Link Key Table (apsPeerLinkKeyTblSz) 88

Default network topology in FFD SW is:

  • ZB_NWK_NEIGHBOR_TABLE_DEFAULT_SIZE=32U
  • ZB_NWK_NLME_ADDRMAP_TABLE_DEFAULT_SIZE=64U
  • ZB_NWK_NLME_ROUTE_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLDE_BTT_TABLE_DEFAULT_SIZE=16U
  • ZB_NWK_NLME_RREQ_TABLE_DEFAULT_SIZE=4U
  • ZB_APS_DEVICE_KEY_PAIR_DEFAULT_COUNT=64U

6. Acronyms and definitions

Term Definition
APS Application Support Sublayer
RAM Random Access Memory
FFD Full Function Device
RFD Reduced Function Device

7. References


[[Category:Getting_Started_with_STM32WB-WBA_and_Zigbee|10]]

No categories assignedEdit