Bluetooth® Low Energy audio - Hearing Access Profile

Revision as of 16:30, 24 May 2024 by Registered User


1. Introduction

The Hearing Access Profile is a Bluetooth® Low Energy Audio Profile specified by the Bluetooth SIG. It is categorized as a "use-case profile", meaning that it is a high-layer profile designed for a specific use case. The complete specification can be found on the Bluetooth SIG website[1]. Location of TMAP inside Bluetooth® Low Energy Audio Profiles architecture The HAP addresses the use-case of Hearing Aids control over Bluetooth® Low Energy. It specifies audio preset control, immediate alert notification and requirements for LE Audio profiles.

2. Roles

The HAP introduces four different roles:

  • Hearing Aid (HA): Role implemented by hearing aids. Can receive audio stream as Unicast Server and implement Hearing Access Service as Server to allow remote devices to control local audio presets.
  • Hearing Aid Unicast Client (HAUC): Connects to hearing aids to stream audio data as Unicast Client. Examples of device implementing this role are smartphones, laptops, media players, TV, tablets, and PCs.
  • Hearing Aid Remote Controller (HARC): Connects to hearing aids and control audio presets, volume and microphone status. Implements Hearing Access Service as Client role. Examples of device implementing this role are smartphones, tablets and remote controllers.
  • Immediate Alert Client (IAC): Connects to hearing aids to emit alert notification to capture the attention of the hearing aid wearer. Example of devices implementing this role are smartphone , tablets, laptops and home appliances.

The requirements for the four roles are the following:

HAP Role CAP Roles BAP Roles GAP Roles VCP Roles
Hearing Aid (HA) Acceptor Unicast Server Peripheral Volume Renderer
Hearing Aid Unicast Client (HAUC) Initiator Unicast Client Central None
Hearing Aid Remote Controller (HARC) Commander None Central Volume Controller
Immediate Alert Client (IAC) None None None None

3. HAP Advertising

A device implementing HAP with HA role shall put the Hearing Access Service UUID in the Service UUID AD Type field of it's advertising data.

4. Hearing Access Service (HAS)

A device implementing the HA role shall implement the GATT server role with one instance of Hearing Access Service. This service permits remote HARC to control local Audio Presets when connected.

5. Hearing Access Profile application APIs

The following section lists and describes the APIs typically used in a HAP application.

5.1. HAP HA APIs

The following APIs are available for the HAP in HA Role:

HAP_Init Initialize the Hearing Access Profile with the selected role(s)
HAP_HA_BuildAdvPacket Build HAP HA advertising packet with the concatenation of CAP Advertising data, HAS UUID and Appearance
HAP_HA_SetHearingAidFeatures Set the local Hearing Aids Features value
HAP_HA_AddPreset Add a new local preset
HAP_HA_RemovePreset Remove a local preset
HAP_HA_SetPresetAvailability Set the availability value of a local preset
HAP_HA_EditPreset Edit a local preset
HAP_HA_SetActivePresetIndex Set the local Active Preset Index value
HAP_HA_DB_IsPresent Indicate if HAP HA Database is saved in NVM
HAP_HA_DB_RemoveServicesRecord Remove the record of the HAP HA stored in NVM

5.2. HAP HAUC APIs

There are no HAP HAUC specific APIs, refer to CAP Unicast Client APIs.

5.3. HAP HARC APIs

The following APIs are available for the HAP in HARC Role:

HAP_Init Initialize the Hearing Access Profile with the selected roles
HAP_Linkup Link Up the HAP Client roles with remote HAP HA
HAP_HARC_ReadHAFeatures Read the remote Hearing Aid Features
HAP_HARC_ReadActivePresetIndex Read the remote Active Preset Index
HAP_HARC_ReadPresetsRequest Send a requests to read remote HAP Server presets
HAP_HARC_WritePresetName Send a Write Preset Name command
HAP_HARC_SetActivePreset Set preset with specified index on remote HAP Server
HAP_HARC_SetNextPreset Set next preset on remote HAP Server
HAP_HARC_SetPreviousPreset Set previous preset on remote HAP Server
HAP_HARC_DB_IsPresent Indicate if HAP HARC Database is saved in NVM
HAP_HARC_DB_RemoveServicesRecord Remove the record of the HAP HARC stored in NVM

5.4. HAP IAC APIs

The following APIs are available for the HAP in HA Role:

HAP_Init Initialize the Hearing Access Profile with the selected roles
HAP_Linkup Link Up the HAP Client roles with remote HAP HA
HAP_IAC_SetAlertLevel Set Alert Level on remote Immediate Alert Server
HAP_IAC_DB_IsPresent Indicate if HAP IAC Database is saved in NVM
HAP_IAC_DB_RemoveServicesRecord Remove the record of the HAP IAC stored in the NVM

5.5. HAP initialization

1. First initialize the use-case device management module:

USECASE_DEV_MGMT_Init();

2. Then, initialize the HAP with a HAP_Role_t bitfield:

HAP_Role_t role = HAP_ROLE_HEARING_AID;
HAP_Init(role);

5.5.1. Linkup remote HAP server

To perform linkup on a remote HAP server as HAP HARC, use the dedicated API. If a database is already present, use the Restore mode.

/* Check if HAP link is present in NVM from a previous connection*/
if (HAP_DB_IsPresent(p_conn->Peer_Address_Type,p_conn->Peer_Address) == 0)
{
  HAP_Linkup(ConnHandle, HAP_LINKUP_MODE_COMPLETE);
}
else
{
  HAP_Linkup(pNotification->ConnHandle,HAP_LINKUP_MODE_RESTORE);
}

During the linkup process, the HAP_LINKUP_COMPLETE_EVT, HAP_HARC_HA_FEATURES_EVT and HAP_HARC_ACTIVE_PRESET_INDEX_EVT events are generated:

void HAP_Notification(HAP_Notification_Evt_t *pNotification)
{
  switch(pNotification->EvtOpcode)
  {
    case HAP_LINKUP_COMPLETE_EVT:
    {
      break;
    }

    case HAP_HARC_HA_FEATURES_EVT:
    {
      HAP_HA_Features_t ha_features = pNotification->pInfo[0];
      break;
    }
    case HAP_HARC_ACTIVE_PRESET_INDEX_EVT:
    {
      uint8_t active_preset_index = pNotification->pInfo[0];
      break;
    }
  }
}

6. HAP demonstrator using STM32WBA

The STM32WBA cube firmware allows to easily build and deploy HAP Peripheral and HAP Central applications.

6.1. Project architecture

The figure below represents the firmware architecture of the HAP Peripheral/Central example projects inside STM32CubeWBA MCU package. TMAP projects file architecture

6.2. HAP demonstrator menus

The two HAP projects present in STM32WBA cube firmware implement a menu displayed on the OLED Screen of the STM32WBA55G-DK.

6.2.1. HAP Peripheral screens

The following diagram show and describes the screens on the HAP Peripheral application: TMAP Peripheral screens

6.2.2. HAP Central Screens

The following diagram show and describes the screens on the HAP Central application: TMAP Central Screens

6.2.3. Audio streaming state screen

On the two HAP applications, the screens displays the status of the audio stream when connected. The following table describes each possible screen:

No stream screen Displayed when a remote device is connected but no audio stream is established
Unidirectional Sink stream screen Displayed when a unidirectional stream is established with sink role
Unidirectional source stream screen Displayed when a unidirectional stream is established with source role
Bidirectional stream screen Displayed when a bidirectional stream is established (source + sink)

6.3. Unicast Demo using two STM32WBA

6.3.1. Hardware required

This demonstrator requires the following hardware:

  • 2x STM32WBA55G-DK boards
  • 1x Headphones/Headset with a 3.5mm jack cable, optionally with a microphone in which case the jack is 4-pin.

Additionally, as an audio source on the HAP Central side, one of the following can be used:

  • 1x music source with a 3.5mm jack output (Laptop or smartphone with a jack output). If the music source is powered using a power supply, use a Ground Loop isolator device or run the laptop on a battery to avoid Ground Loop issues
  • 1x headset with microphone

6.3.2. Setup

The setup is as following: HAP demonstrator setup (two STM32WBA)

6.3.3. Operate demonstrator

The two projects integrate a menu permitting to operate the demonstrator.

1. To establish the connection between the two STM32WBAs, press the right direction on the joystick of the HAP Peripheral and select "Start Adv." to start advertising, then press the right direction on the joystick of the HAP Central and select "Start Scan" to start scanning. Select your device in the list and press the right direction to initiate the connection.

2. Once the linkup is done on each side, access the menu using the right direction of the joystick

  • To start or stop an audio stream, navigate to the “Audio stream” submenu on the HAP Central target and select the desired item list
  • To operate the HAP Central volume, navigate to the “Local volume” on the HAP Central target
  • To operate the HAP Peripheral volume, navigate to the “Remote Volume” submenu on the HAP Central target, or navigate to the “Volume” submenu on the HAP Peripheral target
  • To control the HAP Peripheral microphone mute status, navigate to the “Microphone” submenu on the HAP Central or Peripheral target
  • To control the HAP Peripheral active preset, navigate to the “Preset” submenu on the HAP Central or Peripheral target

The following configurations are used in the HAP Central project:

Configuration BAP audio configuration Legend Codec configuration
Media 4 ------->> 24_2
Telephony 3 <-------> 16_2

7. References