How to start with DA access on STM32H7S
Literature
- Wiki pages:
- STiRoT STM32H7S How to intro article.
- STiRoT_for_STM32H7RS article
- How to start with OEMiRoT on STM32H7S article.
- How to start with STiRoT on STM32H7S article.
- Debug Authentication for STM32H7RS article.
- UM2237 STM32CubeProgrammer software description
- UM2238 STM32 trusted package creator (TPC) tool software description
- AN5054 Secure programming using STM32CubeProgrammer
- ANxxx Getting started with STiRoT for STM32H7S MCUs
Target description
The purpose of this article is to explain step by step how to use the Debug Authentication STM32CubeFW example provided by ST, using the STM32H7S NUCLEO board.
The user application flashed during the provisioning is the GPIO_IOToggle example from STM32CubeFW, installed in external memory.
Introduction
Two examples are provided in the STM32Cube_FW:
In this "getting started" a simple way to flash a user application in external memory and to provision the chip are shown based on the example provided in STM32CubeFW.
Through this practical example you will learn:
- How to use the STM32CubeFW example which is provided.
- How to configure the debug authentication for this example.
- What the device provisioning is and how to perform the setup of the device.
- How the user application is installed.
- How to perform a regression to retrieve an empty board.
Prerequisites
- Hardware
- NUCLEO-H7S3L8 board: the STM32H7S devices have all the available security features, including the HW crypto accelerator (the HW cryptographic acceleration is not support for STM327R devices).
- NUCLEO-H7S3L8 board: the STM32H7S devices have all the available security features, including the HW crypto accelerator (the HW cryptographic acceleration is not support for STM327R devices).
- Required tools
- STM32Cube_FW_H7RS_V1.0.0 or later
- STM32CubeProgrammer_rev2.16.0 or more recent (with trusted package creator (TPC) selected at installation).
- IAR Embedded Workbench® rev 9.20.1 or later.
- Tera Term / Putty or equivalent terminal emulator.
- STM32Cube Firmware
- Download the STM32Cube_FW_H7RS Cube firmware (advise is to place it close form the C: in order to avoid long windows paths)
- A directory NUCLEO-H7S3L8 is included in "STM32Cube_FW_H7RS\Projects"
- Open the env.bat file
- If the STM32CubeProgrammer has not been installed in the default folder:C:\Program Files\STMicroelectronics\STM32Cube\STM32CubeProgrammer, the customized installation path needs to be updated.
- Option bytes programming
The STM32CubeFW example GPIO_IOToggle used in this step by step is running in external memory and it is necessary to configure the option byte XSPI2_HSLV to make it work :
- Open STM32CubeProgrammer
- Connect the Nucleo board and configure the OB as follow :
- Disconnect STM32CubeProgrammer
1. Debug authentication configuration
This chapter explains how to start with the provisioning script.
It is used to configure the debug authentication.
1.1. Preliminary stage
- The different steps to configure the DA are based on a script provided in the STM32CubeFW: Projects\NUCLEO-H7S3L8\ROT_Provisioning\DA\provisioning.bat.
- The following documentation is a guide through all the steps of this script, and explains how to perform each of them.
- The figure below shows where the script is located in the STM32CubeFW.
- Launch the script: provisioning.bat (double click) and keep it running during all the following steps.
- Type the product state: CLOSED (don't use LOCKED for this tutorial, this state is used only to set a final product state)
- Type the chosen Debug Authentication: CERTIFICATE (for explanation about certificate and password refer to intro article)
- Launch the script: provisioning.bat (double click) and keep it running during all the following steps.
1.2. Debug Authentication configuration
Press a key on terminal window and the script guide you to perform DA configuration :
- Using STM32TrustedPackageCreator
- Warning: for a commercial product, it is important to define your own key. But for trials it is advised to use the default provided, to avoid blocked regression due to lost password.
- According to the path specified in the DA_Config.xml, a DA_Config.obk file is generated in Projects\NUCLEO-H7S3L8\ROT_Provisioning\DA\Binary folder. This file will be used by the script during the provisioning step.
1.3. Provisioning
The step 2 corresponds to the provisioning of the OBKeys and the programming of the option bytes. This is automatically doe by the script :
1.4. Images flashing
Next step is the programming of the images.