How to perform people counting using FP-AI-VISION1 and STM32H747XI

Revision as of 14:43, 31 January 2024 by Registered User

This article shows how to run FP-AI-VISION1 function pack projects on STM32H747I-DISCO Discovery kits by using the people counting demo as an example. For the STM32H747I-DISCO Discovery kits shipped with the version A09 of the MB1166 LCD daughterboard, an additional step to update the drivers is also described. Further, if you only get static on the LCD as shown below, this article might be helpful.

Figure 1: Static on LCD


1. Prerequisites

1.1. Hardware

  • A USB Type-A or USB Type-C® to Micro-B cable
  • B-CAMS-OMV camera module bundle
  • STM32H747I-DISCO Discovery kit with LCD daughterboard

1.2. Software

2. Hardware setup

Connect the B-CAMS-OMV camera to the STM32H747I-DISCO Discovery kit using the flexible flat cable (FFC). Ensure that the FFC is securely attached to both ZIF connectors, and that the orientation is as shown in the figure below (highlighted in yellow).

Next, attach the USB cable to the USB port labelled "STLINK-V3E", as shown in the figure below (highlighted in blue).

Figure 2: Hardware setup


3. Project import

If the goal is to run the project on the STM32H747I-DISCO without any modifications, simply drag and drop the file ..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\PeopleCounting\Binary\STM32H747I-DISCO_PeopleCounting_Quant8_IntFps_IntFlash_V310.bin onto the STM32H747I-DISCO mass storage device as shown below.

Flash dragndrop
Figure 3: Drag and drop the binary file to program the MCU
Info white.png Information
Programming the existing binary file does not work for the STM32H747I-DISCO kits with the version A09 of the MB1166 LCD daughterboard. To run the project on such Discovery kits, follow the rest of the guide, including #Driver update (required only when using MB1166 version A09).

3.1. Project import into STM32CubeIDE

The project can be imported into STM32CubeIDE by simply opening the .project file located at ..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\PeopleCounting\STM32CubeIDE\.project and following the steps below:

  1. Double-click on the .project file
  2. STM32CubeIDE prompts for a workspace directory, as shown below. Select an appropriate location and press "Launch".
    Figure 4: Select workspace

    STM32CubeIDE prompts again once the project is successfully imported. Press "OK" to proceed.
    Figure 5: Prompt after successful import
  3. The project is visible under the project explorer.
Figure 6: Project directory listing

3.2. Directory overview

This project is being deployed on the STM32H747XI microcontroller, which is a dual-core Arm® Cortex®-M7 and Cortex®-M4 MCU. In this project, we only use the Cortex®-M7 core and therefore are only working with the CM7 directory. This directory contains the source code specific to the people counting project. Detailed information about the organization of this directory is available in the section 3.2 of the Artificial Intelligence (AI) and computer vision function pack for STM32H7 microcontrollers user manual UM2611.

4. Driver update (required only when using MB1166 version A09)

The drivers for the LCD daughterboard MB1166 version A09 (pictured below) are currently not included in the FP-AI-VISION1 function pack. To deploy the project on the STM32H747I-DISCO Discovery kits equipped with the version A09 of the MB1166 LCD daughterboard, follow the steps below to install the drivers.

Figure 7: STM32H747I-DISCO with MB1166 version A09


  1. If you already have STM32CubeH7 v1.11.1 or above installed, locate the directory at C:\users\<username>\STM32Cube\repository\STM32Cube_FW_H7_V1.11.1\Drivers\BSP\Components\nt35510 and jump to step 3.

    If it is not the case, download the drivers from the (1) STM32CubeH7 GitHub repo by clicking on (2) "Code", and then (3)"Download ZIP", as shown in the figurebelow.
    Figure 7: Download ZIP from GitHub
  2. Extract the contents of STM32CubeH7-master.zip to a local directory.
  3. Copy the directory ..\STM32CubeH7-master\Drivers\BSP\Components\nt35510 to ..\FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\
  4. Copy the files ..\STM32CubeH7-master\Drivers\BSP\STM32H747I-DISCO\stm32h747i_discovery_lcd.c and ..\STM32CubeH7-master\Drivers\BSP\STM32H747I-DISCO\stm32h747i_discovery_lcd.h, and paste both files into the ..\FP-AI-VISION1_V3.1.0\Drivers\BSP\STM32H747I-Discovery\ directory
  5. Use a text editor to open ..\FP-AI-VISION1_V3.1.0\Projects\STM32H747I-DISCO\Applications\Common\CM7\Inc\stm32h747i_discovery_conf.h. On line 34, add a #define for NT35510, and change the OTM8009A #define to 0, as follows:
    /* LCD controllers defines */ 
    #define USE_LCD_CTRL_NT35510                1U 
    #define USE_LCD_CTRL_OTM8009A               0U 
    #define USE_LCD_CTRL_ADV7533                0U
    
  6. From the FP-AI-VISION1_V3.1.0\Drivers\BSP\Components\nt35510 directory, select the four source files as shown in the figure below. Then, drag and drop the selected files into the components directory in STM32CubeIDE.
    Figure 8: Drag and drop all four files into components directory

    Then, in the pop-up window, keep “Link to files” and click "OK".
    Figure 9: Select "Link to files" and click "OK"

    The drivers are now indexed into the project
    Figure 10: Drivers are indexed

5. Building and programming

Right-click the project, then (1) clean and (2) build the project. It is now possible to click on the (3) run icon to program and execute the project.

Figure 10: Clean, build, and program the project

Once the execution starts, the screen displays a live output from the camera along with the number of people detected in the frame, as shown below.

Figure 12: Final output showing the people counting demo on STM32H747XI


6. References

Vision Pack Video Application Notes

UM2611: Artificial Intelligence (AI) and computer vision function pack for STM32H7 microcontrollers