Debug Authentication STM32H7RS How to Introduction

DA and FW update How to Introduction

1. Debug Authentication

Debug authentication controls debug opening and regressions. It can be used during development, manufacturing and for field return analysis.

  • Features
    • the usage of a password method allow only full regression (from closed state to open state).
    • the usage of cryptography (certificates) can be used for full regressions ,debug opening and firmware update from a closed device.
  • Debug authentication principle
    • Use of JTAG dedicated access point (ap0) to communicate with the chip.
    • Secure protocol defined by ARM : ARM PSA ADAC V1.0. (Authenticated Debug Access Control)[1]
SECURITY Intro to DA for H7S.png

2. Debug Authentication for STM32H7S with password method

SECURITY Product lifecycle H7S password method.png

Provisioning with password management

  • Provisioning data is located at beginning of the OBKeys-HDPL1 area.
  • Provisioning data is the HASH (SHA256) of the password.
  • STM32TrustedPackageCreator is used to generate the OBKeys files containing the HASH of the Debug authentication password adding SHA256 to ensure integrity.
SECURITY Provisioning TZ disabled 3.png

* For further details on OBKeys access per HDP level, refer to Table 45. Option-byte key area of RM0481 STM32H5x3/562 Reference Manual.

Debug authentication controls

  • Full regression with the Debug authentication password.
  • Debug authentication password has to be provisioned in OBKeys to allow this regression.
SECURITY Regression TZ disabled.png

Getting started with Debug authentication

Refer to the following page for an example on getting started with Debug authentication access when TrustZone© is disabled:

How to start with Debug authentication access on STM32H573 when TrustZone© is disabled

3. Debug Authentication for STM32H7S with certificate method

SECURITY Product lifecycle H7S certif method.png