This message will disappear after all relevant tasks have been resolved.
Semantic MediaWiki
There are 1 incomplete or pending task to finish installation of Semantic MediaWiki. An administrator or user with sufficient rights can complete it. This should be done before adding new data to avoid inconsistencies.1. Using the example
To ease the example generation and loading, a script is provided in the STM32Cube package. The script called “provisioning” is available in \Projects\NUCLEO-U083RC\ROT_Provisioning\OEMiSB.
The script execution is following steps:
- 1. Configuration management'
- RDP selection
- 0: In this case the development mode is enabled
- 1: Production mode is enabled, and debug is possible
- 2: Production mode is enabled, and debug is not possible
- Data size selection
- RDP selection
- 2. Image generation
- Compilation of the application and generating binary file.
- Editing boot header files automatically.
- Computing application HASH and generating hash area binary.
- Compilation of the boot.
- 3. Provisioning
- Remove old protections and initialize option bytes.
- Perform mass erase.
- Download application, boot and hash.
- Hardening by enabling HDP and WRP.
The script is useful to automate hash generation, which would have to be manually imported into the binary on each build.