Zigbee Realistic Use Case Window Covering

Revision as of 18:40, 14 December 2023 by Registered User (→‎Zigbee Implementation)

1. Introduction

This implementation can be seen as a simple extension of the Wiki: Zigbee RUC Lighting [1], adding another Zigbee cluster for the Home automation aspect.
In the aim to test and verify various functionality and ensure proper functioning, this approach mixes and maintains several Device with different clusters without logical interaction on the same network.

RUC Window Covering


2. Getting started

From the Wiki: Zigbee RUC Lighting network [1], this project adds new Router (ZR) and End Device (ZED) with Window covering features.

Hardware requirements
P-NUCLEO-WB55 Pack [2] and STM32WB5MM-DK[3] are required to set up the demonstration.
For more information, please visit STM32WB Development ecosystem

P-NUCLEO-WB55 STM32WB5MM-DK
Connectivity nucleo-description.png
Connectivity DK board.png


Additionally, it uses an Arduino Motor Shield Control (AMS) [4] based on the ST dual full-bridge driver L298P [5] to drive a DC motor, enabling the real opening and closing of a window covering.

Arduino Motor Shield


Software and system requirements
For more information to build Zigbee application, please visit STM32WB Build Zigbee Project
To check messages from the board, use any convenient terminal software via the UART Interface, please visit Wiki: Zigbee Log via UART
One driver was created for Arduino Motor Shield, please see below Server cluster side for more information.

3. Zigbee Implementation

In this example, the topology added is a Window Covering Device as ZR and one window covering controller device as ZED.
In addition, the ZR and ZED will use the Zigbee cluster Window Covering [6].

Window Covering cluster usage


3.1. Server cluster side

The server is based on a STM32WB5MM-DK [3], which has a slot to put an Arduino board to expand its functionality.
It uses an Arduino Motor Shield Control (AMS) [4] based on the ST dual full-bridge driver L298P [5] to drive a DC motor, enabling the real opening and closing of a window covering.

One driver was created to enable the following functionalities:

  • Adjust the motor’s speed by modifying the duty cycle of a PWM (driven by a GPIO connected to a timer).
  • Change the rotation direction (driven by a GPIO).
  • Set a break (also driven by a GPIO)
  • Current sensing, with that possibility, this feature detects when the window covering is stuck and stops the motor.

3.2. Client cluster side

The client is based on a P-NUCLEO-WB55 [2]
where Switch 1/2/3 can be seen like command Up/Stop/Down.

The client cluster of the window covering implements 7 commands but only three commands are used.

  • Up / Open
  • Down / Close
  • Stop

As with the previous example, theses commands are associated with callbacks functions on the server side. When a UP comand is sent, the corresponding callback function on the server side, initiating the motor rotation to open the window covering.

3.3. Binding and Report process

This example reuse the same process of Zigbee RUC Lighting.
For more information please visit it.

3.4. Extension possible

A potential extension is to add the Alarms cluster [7] to notify when the shutter is blocking and flash the LEDs controller to warn User.
To better understood a first approach implemented, please find below a process used.

4. Acronyms and definitions

Term Definition
ZC Zigbee Coordinator
ZR Zigbee Router
ZED Zigbee End Device
RUC Realistic Use Case
AMS Arduino Motor Shield
GPIO General Purpose Input Output
PWM Pulse Width Modulation

5. References