OEMiRoT stands for Original Equipment Manufacturer immutable Root of Trust. The users can develop OEMiRoT on all the STM32H7S devices.
1. Introduction
This wiki article describes OEMiRoT process steps developed in STM32CubeH7RS firmware and to read before the How to articles about OEMiRoT :
For more informations about OEMiRoT please refer to OEMiRoT for STM32H7S
2. OEMiRoT services
- 1) The secure boot (Root of Trust services):
- It is an immutable code that runs after every system reset. It activates STM32 runtime protections and verifies the authenticity and integrity of the application code before every execution.
- Integrity: to ensure that no corrupted or maliciously modified firmware is about to run.
- Authenticity: to verify that firmware comes from a trusted and known source to prevent unauthorized entities from installing and executing code.
- Integrity: to ensure that no corrupted or maliciously modified firmware is about to run.
- It is an immutable code that runs after every system reset. It activates STM32 runtime protections and verifies the authenticity and integrity of the application code before every execution.
- 2) The Secure Firmware Update:
- It is an immutable code that detects if a new firmware image is available, checks its authenticity and verifies the integrity of the code before installing it after decryption.
3. OEMiRoT process in STM32CubeH7RS firmware examples
In the STM32CubeH7RS firmware package an OEMiRoT use case is given as example.
In this example OEMiRoT boot path is automatically configured in a provisioning script.
For more details about the different configurations for OEMiRoT you can refer to OEMiRoT for STM32H7RS
For more details about the use case developped in STM32CubeH7RS package go to the One boot stage example described in OEMiRoT for STM32H7RS - One boot stage
The figure below illustrates the boot scheme that is followed in the OEMiRoT example.
- At reset RSS jumps from system flash to OEMiRoT in Internal Flash (Option Byte IROT_SELECT is configured in the script to boot on OEMiRoT)
- OEMiRoT checks if a new user application is stored in the download slot in external Flash.
If any, OEMiRoT decrypts it then controls its integrity, its authenticity and the anti-rollback version. If successful, the image is copied in the user application installation slot. The image is re-encrypted (AES) with MCE_1 encryption key.
- If the user application is not yet installed: OEMiRoT controls its integrity and its authenticity. If successful, OEMiRoT decrypts and install the
OEMiRoT-Appli in the external flash. The OEMiRoT application is stored after re-encryption with the MCE OEMiRoT key.
3.1. OEMiRoT provisioning steps
3.1.1. Step 1 – Preliminary stage
3.1.1.1. Define product state value
The following figure shows the possible product state.
The provided script Provisioning.bat given as an example in STM32CubeH7RS firmware guides the user during this phase.
At the begining of the provisioning script execution, the user can choose the product state can be chosen that automatically sets the corresponding option byte.
The product state is chosen depending on the user application development phase and the wanted security level.
- Open:
- This state is mainly used during the development phase since the device is fully open.
- Debug is fully open.
- Bootloader is usable.
- This state is mainly used during the development phase since the device is fully open.
- Open:
- * Provisioning:
- This state is used during the provisioning.
- It is the device state during the provisioning script execution (Provisioning.bat given as an example in STM32CubeH7RS firmware).
- So, this state is not part of the proposed state selectable at the end of the script execution.
- Debug access is only available if DA-Config is provisioned. Allowed regressions : Full-Regression or Intrusive debug
- Bootloader is usable.
- Secure Firmware install can be launched in this state (not anymore possible in the following states).
- This state is used during the provisioning.
- Closed:
- This state occurs with the fully provisioned product.
- The debug is fully closed but can be opened by launching the Debug Authentication (see Debug Authentication setting).
- This state occurs with the fully provisioned product.
- Locked:
- This state is used with the fully provisioned product without any more changes.
- Locked is a final unchangeable product state. No method can modify the embedded firmware and product configuration.
- The debug is definitively closed and cannot be reopened through debug authentication.
- No regression is possible anymore
- This state is used with the fully provisioned product without any more changes.
3.1.1.2. Define Debug Authentication method
On H7R/S User is free to select the Debug Authentication method : Password or certificate
3.1.2. Step 2 - Configuration management
3.1.2.1. OEMiRoT configuration
STM32TrustedPackageCreator tool generates OEMiRoT configuration file (.obk) based on template provided in STM32CubeH5 Software package. This configuration file generates keys used to:
- At the binary generation step:
- Encrypt the data
- Sign the user application
- In the device:
- Decrypt the data
- Check signature (authorization)
The user configures all other parameters directly in his Root of Trust firmware located in HDPL1 in User Flash.
This code must be able to perform the authenticity and integrity checks of the User application and data images.
It also configures the number of User applications and images:
- Number of data images
- Number of code images
The OEMiROT_boot applications, available for each OEMiRoT example in the folders Applications\ROT\OEMiROT_Boot\Inc\flash_layout.h, include the definition of all these parameters.
3.1.2.2. DA configuration
STM32TrustedPackageCreator also generates the Debug Authentication configuration file (.obk) based on template provided in STM32CubeH5 software package. This file configures the conditions to reopen a protected device and the debugger.
Depending on the additional configuration of the user application, the generation of files might happen.
For more details about debug authentication mechanisms, please refer to Introduction to Debug Authentication for STM32H5 MCUs.
3.1.3. Step 3 – Images generation
STM32CubeH5 FW package delivers user application projects for each OEMiRoT example in Applications\ROT folders.
The compilation of the user application projects generates a binary file. This binary file is an input file to generate the encrypted code images .hex.
Associated with an XML configuration file User can update the firmware area size and the version of the image.
STM32CubeH5 firmware package also delivers binaries data file examples in the ROT_Provisioning\OEMiROT\Binary folder.
3.1.3.1. Boot firmware image generation
During compilation, any IDE generates the binary code file of the user application.
The image creation is performed automatically by the IDE during the user application compilation by calling STM32TrustedPackageCreator in a post-build command.
STM32TrustedPackageCreator can be launched separately to generate the encrypted and signed image file using the same encryption and authenticity keys provisioned during the OEMiRoT configuration.
STM32TrustedPackageCreator uses a configuration file to generate images.
XML files examples are available for each OEMiRoT project example in the STM32Cube_FW (ROT_Provisioning\OEMiROT\Config) and are editable using STM32TrustedPackageCreator.
3.1.3.2. Code firmware Image generation
STM32TrustedPackageCreator needs to be launched separately to generate the encrypted and signed image file using the same encryption and authenticity keys provisioned during the OEMiRoT configuration. The code image generation of the user application also uses these keys.
STM32TrustedPackageCreator uses an XML configuration file for each OEMiRoT project example in the STM32Cube_FW (ROT_Provisioning\OEMiROT\Images ). These files are editable using STM32TrustedPackageCreator.
4. How to start with STM32 and OEMiRoT
You can refer to the following pages for getting started examples of OEMiRoT.