1. STM32WB-WBA - Connection Oriented Channel
A Connection Oriented Channel - COC allows the exchange of Bluetooth® Low Energy data at L2CAP layer without GATT layer. There is no notion of client/server, only central and peripheral.
To set a COC logical link, it is necessary to establish first a Bluetooth® Low Energy link.Over this Bluetooth® Low Energy link, one or several COC can be established.
The central or the peripheral may be COC initiator.
Bluetooth® LE architecture |
---|
1.1. General L2CAP Terminology
Bluetooth® LE General L2CAP Terminology | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|
|
2. L2CAP COC commands and events overview
2.1. L2CAP COC establishment
ACI_L2CAP_COC_CONNECT : This command sends a Credit Based Connection Request packet on the specified connection.
L2CAP COC connect command | ||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
ACI_L2CAP_COC_CONNECT_EVENT : This event is generated when receiving a valid Credit Based Connection Request packet.
L2CAP COC connect event | ||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
ACI_L2CAP_COC_CONNECT_CONFIRM : This command sends a Credit Based Connection Response packet. It must be used upon receipt of a connection request through an ACI_L2CAP_COC_CONNECT_EVENT event.
L2CAP COC connect confirm command | ||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|
|
ACI_L2CAP_COC_CONNECT_CONFIRM_EVENT : This event is generated when receiving a valid Credit Based Connection Response packet.
L2CAP COC connect confirm event | ||||||||||||||||
---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|---|
|
- MTU frames are fragmented into K-frames of MPS size at application level on transmitter side.
- MTU frames are reassembled at application level on receiver side.
- Initial Credits are handled at application level once they have been exchanged through both previous commands.
2.2. L2CAP COC data exchange
ACI_L2CAP_COC_TX_DATA : This command sends a K-frame packet on the specified connection-oriented channel.
L2CAP COC Tx Data command | ||||||||
---|---|---|---|---|---|---|---|---|
|
- Note: for the first K-frame of the SDU, the Information data shall contain the MTU Length coded on two octets followed by the K-frame information payload. For the next K-frames of the SDU, the Information data shall only contain the K-frame information payload.
- When the command return the error code BLE_STATUS_INSUFFICIENT_RESOURCES (0x64), the application needs to wait the ACI_L2CAP_COC_TX_POOL_AVAILABLE_EVENT event. The ACI_L2CAP_COC_TX_POOL_AVAILABLE_EVENT event is generated as soon as there is a free buffer available for sending K-frames.
- Application must handle MTU length, fragmentation in K-frame, length of current transmitted frame and credits number.
ACI_L2CAP_COC_RX_DATA_EVENT : This event is generated when receiving a valid K-frame packet on a connection-oriented channel.
L2CAP COC Rx Data event | ||||||||
---|---|---|---|---|---|---|---|---|
|
- Application must handle MTU length received in first K-frame, K-frame number, length of current received frame and credits number.
2.3. L2CAP COC flow control
ACI_L2CAP_COC_FLOW_CONTROL : This command sends a Flow Control Credit signaling packet on the specified connection-oriented channel.
L2CAP COC Flow Control command | ||||||
---|---|---|---|---|---|---|
|
ACI_L2CAP_COC_FLOW_CONTROL_EVENT : This event is generated when receiving a valid Flow Control Credit signaling packet.
L2CAP COC Flow Control command | ||||||
---|---|---|---|---|---|---|
|
2.4. L2CAP COC additional commands and events
- ACI_L2CAP_COC_RECONF : This command sends a Credit Based Reconfigure Request packet on the specified connection.
- ACI_L2CAP_COC_RECONF_CONFIRM : This command sends a Credit Based Reconfigure Response packet. It must be used upon receipt of a Credit Based Reconfigure Request through an ACI_L2CAP_COC_RECONF_EVENT event.
- ACI_L2CAP_COC_DISCONNECT : This command sends a Disconnection Request signaling packet on the specified connection-oriented channel. The ACI_L2CAP_COC_DISCONNECT_EVENT event is received when the disconnection of the channel is effective.
- ACI_L2CAP_COC_RECONF_EVENT : This event is generated when receiving a valid Credit Based Reconfigure Request packet.
- ACI_L2CAP_COC_RECONF_CONFIRM_EVENT : This event is generated when receiving a valid Credit Based Reconfigure Response packet.
- ACI_L2CAP_COC_DISCONNECT_EVENT : This event is generated when a connection-oriented channel is disconnected following an L2CAP channel termination procedure.
2.5. L2CAP COC sequence diagram
L2CAP COC example |
---|
3. L2CAP COC example
3.1. Bluetooth® LE connection and COC establishment initiated by the central
3.1.1. On central side
- Initiate a Bluetooth® Low Energy link: send aci_gap_create_connection
- Wait for HCI_LE_CONNECTION_COMPLETE_EVENT
- Initiate a CoC connection: ACI_L2CAP_COC_CONNECT
- Wait for ACI_L2CAP_COC_CONNECT_CONFIRM_EVENT (get channel_index_list)
Range of channel_index_list for the COC initiator: from 0 to 0x1F
3.1.2. On peripheral side
- Start advertising: send aci_gap_set_discoverable
- Wait for HCI_LE_CONNECTION_COMPLETE_EVENT
- Wait for ACI_L2CAP_COC_CONNECT_EVENT
- Send ACI_L2CAP_COC_CONNECT_CONFIRM
- In hci_command_complete_event, get Channel_number and Channel_Index_List values
Range of channel_index_list for the COC peripheral: from 0x20 to 0x3F
3.2. COC data exchange
3.2.1. On sender side
Used ACI_L2CAP_COC_TX_DATA (Channel_Index, length, data) to send data over L2CAP.
3.2.2. On receiver side
Recover the data through ACI_L2CAP_COC_RX_DATA_EVENT event.
3.3. Example of Bluetooth® LE connection, COC establishment and data exchange
Bluetooth® Low Energy and COC link establishment |
---|
L2CAP COC data exchange |
---|
3.4. Code Example
A STM32WB COC code example has been shared on STM32-Hotspot [1]
A STM32WBA COC code example is available with BLE_SerialCom application