How to use an RTOS with Secure Manager on STM32H5

Revision as of 18:17, 21 November 2023 by Registered User

1. Introduction

In the context of the Secure Manager, an RTOS can be used. In this article, we will explore how an RTOS can be used with the Secure Manager, with a focus on the mechanism provided to ensure secure thread-safe calls. To do this, we will take the example of a non-secure application like SMAK that uses the Secure Manager service. We will see the differences to implement for the non-secure application to use the Secure Manager in multi-thread.

The different steps and prerequisites to integrate a non-secure application with the Secure Manager can be find here Security:Secure Manager STM32H5 How to Intro - stm32mcu which details: Secure Manager installation, non-secure application development, firmware update, etc.

2. Implementation example

2.1. Thread-safe secure calls

We will have to protect the API calls. There is a mechanism in the middleware that allows interfacing with the secure-manager. This mechanism, based on functions defined as __weak, will have to be re-implemented by integrating our protection based on mutexes. The use of mutex as a mechanism to synchronize access to the PSA API.

We will need to protect the API calls. There is a mechanism in the middleware that allows interfacing with the secure handler. This mechanism, based on functions defined as '__weak, will need to be re-implemented by integrating our protection based on mutexes. The use of mutex as a mechanism to synchronize access to the PSA API is essential when using multithreading.

The functions ns_ipc_seq_begin' and ns_ipc_seq_end, which are declared by default in the secure manager library in the file tfm_ns_interface.c, will need to be re-implemented in the FreeRTOS project due to multithreaded use.

Firmware
└───ST
    └───secure_manager_api
        └───ipc
            └───nonsecure
                └───src
                    └───tfm_ns_interface.c

1. Declare a mutex and initialize it to 0:

static SemaphoreHandle_t nsIpcMutex = { 0 };

2. Create a function that creates the mutex and assigns it to the nsIpcMutex variable. If the mutex creation fails, log an error:

void tfm_ns_interface_init( void )
{
  nsIpcMutex = xSemaphoreCreateMutex();
  if(nsIpcMutex == NULL)
  {
   // Logging Error
  }
}


3. Implement the acquisition and release of the mutex in the ns_ipc_seq_begin and ns_ipc_seq_end functions, respectively. This ensuring that shared resources are not accessed simultaneously:

void ns_ipc_seq_begin(const ns_ipc_seq_info_t* info)
{
  /* Lock mutex */
  if(nsIpcMutex != NULL)
  {
    xSemaphoreTake(nsIpcMutex, portMAX_DELAY );
  }
  ….
}
void ns_ipc_seq_end(const ns_ipc_seq_info_t* info)
{
  /* Unlock mutex */
  if(nsIpcMutex != NULL)
  {
    xSemaphoreGive(nsIpcMutex);
  }
  ….
}

For more concrete examples, an actual implementations can be found in X-Cube-AWS & X-Cube-Azure using the Secure Manager with a real-time operating system.

2.2. Memory Management

SRAM 3 can be configured with heap RTOS configuration. The heap_5 implementation of FreeRTOS dynamic memory allocator is selected to use non-contiguous memory regions in SRAM1 and SRAM3. During initialization, prvInitializeHeap() needs to be set up.

No categories assignedEdit